examples: classification example with command line defined labels and class filtering
[tidl/tidl-api.git] / viewer / main.cpp
1 /******************************************************************************
2  * Copyright (c) 2017-2018, Texas Instruments Incorporated - http://www.ti.com/
3  *  All rights reserved.
4  *
5  *  Redistribution and use in source and binary forms, with or without
6  *  modification, are permitted provided that the following conditions are met:
7  *      * Redistributions of source code must retain the above copyright
8  *        notice, this list of conditions and the following disclaimer.
9  *      * Redistributions in binary form must reproduce the above copyright
10  *        notice, this list of conditions and the following disclaimer in the
11  *        documentation and/or other materials provided with the distribution.
12  *      * Neither the name of Texas Instruments Incorporated nor the
13  *        names of its contributors may be used to endorse or promote products
14  *        derived from this software without specific prior written permission.
15  *
16  *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
17  *  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
18  *  IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
19  *  ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
20  *  LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
21  *  CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
22  *  SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
23  *  INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
24  *  CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
25  *  ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
26  *  THE POSSIBILITY OF SUCH DAMAGE.
27  *****************************************************************************/
28 #include <signal.h>
29 #include <getopt.h>
30 #include <iostream>
31 #include <iomanip>
32 #include <fstream>
33 #include <cassert>
34 #include <string>
35 #include <cstdlib>
37 #include <sys/types.h>
38 #include <sys/stat.h>
39 #include <unistd.h>
42 #include "tidl_viewer.h"
44 using namespace tidl;
46 static void ProcessArgs(int argc, char *argv[], std::string& network_file,
47                         bool& do_print, std::string& dot_file);
49 static void DisplayHelp();
50 static bool fs_exists(std::string path);
52 int main(int argc, char *argv[])
53 {
54     // Catch ctrl-c to ensure a clean exit
55     signal(SIGABRT, exit);
56     signal(SIGTERM, exit);
58     // Process arguments
59     std::string network_file;
60     std::string dot_file;
61     bool do_print = false;
62     ProcessArgs(argc, argv, network_file, do_print, dot_file);
64     bool status = true;
66     // Dump network to stdout if requested
67     if (do_print)
68         status &= util::PrintNetwork(network_file);
70     // Generate a dot file
71     status &= util::GenerateDotGraphForNetwork(network_file, dot_file);
73     // If the dot utility exists, generate a SVG file
74     const std::string dot_bin("/usr/bin/dot");
75     if (fs_exists(dot_bin))
76     {
77         std::string command = dot_bin;
78         command += " -Tsvg " + dot_file + " -o " + dot_file + ".svg";
79         int x = std::system(command.c_str());
80         if (x != 0) status = false;
82     }
84     if (!status)
85         return EXIT_FAILURE;
87     return EXIT_SUCCESS;
88 }
91 void ProcessArgs(int argc, char *argv[], std::string& network_file,
92                  bool& do_print, std::string& dot_file)
93 {
94     if (argc < 4)
95     {
96         DisplayHelp();
97         exit(EXIT_SUCCESS);
98     }
100     const struct option long_options[] =
101     {
102         {"help",         no_argument,       0, 'h'},
103         {"dot",          required_argument, 0, 'd'},
104         {"print",        no_argument,       0, 'p'},
105         {0, 0, 0, 0}
106     };
108     int option_index = 0;
110     while (true)
111     {
112         int this_option_optind = optind ? optind : 1;
113         int c = getopt_long(argc, argv, "-d:ph", long_options, &option_index);
115         if (c == -1)
116             break;
118         switch (c)
119         {
120             case 1:   network_file = argv[this_option_optind];
121                       break;
123             case 'd': dot_file = optarg;
124                       break;
126             case 'p': do_print = true;
127                       break;
129             case 'h': DisplayHelp();
130                       exit(EXIT_SUCCESS);
131                       break;
133             case '?': // Error in getopt_long
134                       exit(EXIT_FAILURE);
135                       break;
137             default:
138                       std::cerr << "Unsupported option: " << c << std::endl;
139                       break;
140         }
141     }
143     if (dot_file.empty())
144     {
145         std::cerr << "ERROR: output dot file not specified." << std::endl;
146         DisplayHelp();
147         exit(EXIT_FAILURE);
148     }
151 #define STRING(S)  XSTRING(S)
152 #define XSTRING(S) #S
153 void DisplayHelp()
155     std::string version = STRING(_BUILD_VER);
156     version += ".";
157     version += STRING(_BUILD_SHA);
159     std::cout << "Usage: tidl_viewer -d <dot file name> <network binary file>\n"
160               << "Version: " << version << std::endl
161               << "Options:  \n"
162                  " -p              Print network layer info\n"
163                  " -h              Display this help message\n";
166 bool fs_exists(std::string path)
168     struct stat statbuf;
169     if (stat(path.c_str(), &statbuf) == 0) return true;
170     else                                   return false;