################################################## Why do I get an assertion failure from malloc_ddr? ################################################## Application execution fails with the following error message: .. code:: shell tidl: device_alloc.h:31: T* tidl::malloc_ddr(size_t) [with T = char; size_t = unsigned int]: Assertion `val != nullptr' failed Allocations not freed +++++++++++++++++++++ One possible reason is that previous runs of the application were aborted (e.g. using :kbd:`Ctrl-C`) and did not release their allocations. Use the ``ti-mct-heap-check`` command with "-c" option to clean up. .. code:: bash root@am57xx-evm:~# ti-mct-heap-check -c -- ddr_heap1 ------------------------------ Addr : 0xa2000000 Size : 0xa000000 Avail: 0xa000000 Align: 0x80 ----------------------------------------- .. _opencl-global-memory: Insufficient OpenCL global memory +++++++++++++++++++++++++++++++++ Another possible reason is that total memory requirement specified in the ``Configuration`` using NETWORK_HEAP_SIZE and PARAM_HEAP_SIZE exceeds default memory available for OpenCL. Follow the instructions below to increase the amount of CMEM (contiguous memory available for OpenCL) from 192MB (0xc000000) to 384MB (0x18000000): .. code:: bash $ sudo apt-get install device-tree-compiler # In case dtc is not already installed $ scp root@am57:/boot/am57xx-evm-reva3.dtb . $ dtc -I dtb -O dts am57xx-evm-reva3.dtb -o am57xx-evm-reva3.dts $ cp am57xx-evm-reva3.dts am57xx-evm-reva3.dts.orig $ # increase cmem block size $ diff -u am57xx-evm-reva3.dts.orig am57xx-evm-reva3.dts --- am57xx-evm-reva3.dts.orig 2018-01-11 14:47:51.491572739 -0600 +++ am57xx-evm-reva3.dts 2018-01-16 15:43:33.981431971 -0600 @@ -5657,7 +5657,7 @@ }; cmem_block_mem@a0000000 { - reg = <0x0 0xa0000000 0x0 0xc000000>; + reg = <0x0 0xa0000000 0x0 0x18000000>; no-map; status = "okay"; linux,phandle = <0x13c>; @@ -5823,7 +5823,7 @@ cmem_block@0 { reg = <0x0>; memory-region = <0x13c>; - cmem-buf-pools = <0x1 0x0 0xc000000>; + cmem-buf-pools = <0x1 0x0 0x18000000>; }; cmem_block@1 { $ dtc -I dts -O dtb am57xx-evm-reva3.dts -o am57xx-evm-reva3.dtb $ scp am57xx-evm-reva3.dtb root@am57:/boot/ # reboot to make memory changes effective (run "cat /proc/iomem" to check) For further details, refer the OpenCL User's Guide, section :ref:`Changing DDR3 Partition for OpenCL `