/****************************************************************************** * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ #include #include #include #include #include #include #include #include #include #include #include #include #include #include "executor.h" #include "execution_object.h" #include "configuration.h" #include "imagenet_classes.h" #include "imgutil.h" #include "opencv2/core.hpp" #include "opencv2/imgproc.hpp" #include "opencv2/highgui.hpp" #include "opencv2/videoio.hpp" bool __TI_show_debug_ = false; using namespace tidl; using namespace tidl::imgutil; using namespace cv; #define NUM_VIDEO_FRAMES 100 bool RunConfiguration(const std::string& config_file, int num_devices, DeviceType device_type, std::string& input_file); bool RunAllConfigurations(int32_t num_devices, DeviceType device_type); bool ReadFrame(ExecutionObject& eo, int frame_idx, const Configuration& configuration, int num_frames, std::string& image_file, VideoCapture &cap); bool WriteFrameOutput(const ExecutionObject &eo); static void ProcessArgs(int argc, char *argv[], std::string& config, int& num_devices, DeviceType& device_type, std::string& input_file); static void DisplayHelp(); static double ms_diff(struct timespec &t0, struct timespec &t1) { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; } int main(int argc, char *argv[]) { // Catch ctrl-c to ensure a clean exit signal(SIGABRT, exit); signal(SIGTERM, exit); // If there are no devices capable of offloading TIDL on the SoC, exit uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE); uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP); if (num_eve == 0 && num_dsp == 0) { std::cout << "TI DL not supported on this SoC." << std::endl; return EXIT_SUCCESS; } // Process arguments std::string config = "j11_v2"; std::string input_file = "../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg"; int num_devices = 1; DeviceType device_type = (num_eve > 0 ? DeviceType::EVE:DeviceType::DSP); ProcessArgs(argc, argv, config, num_devices, device_type, input_file); std::cout << "Input: " << input_file << std::endl; std::string config_file = "../test/testvecs/config/infer/tidl_config_" + config + ".txt"; bool status = RunConfiguration(config_file, num_devices, device_type, input_file); if (!status) { std::cout << "imagenet FAILED" << std::endl; return EXIT_FAILURE; } std::cout << "imagenet PASSED" << std::endl; return EXIT_SUCCESS; } bool RunConfiguration(const std::string& config_file, int num_devices, DeviceType device_type, std::string& input_file) { DeviceIds ids; for (int i = 0; i < num_devices; i++) ids.insert(static_cast(i)); // Read the TI DL configuration file Configuration configuration; bool status = configuration.ReadFromFile(config_file); if (!status) { std::cerr << "Error in configuration file: " << config_file << std::endl; return false; } // setup input int num_frames = 1; VideoCapture cap; std::string image_file; if (input_file == "camera") { cap = VideoCapture(1); // cap = VideoCapture("test.mp4"); if (! cap.isOpened()) { std::cerr << "Cannot open camera input." << std::endl; return false; } num_frames = NUM_VIDEO_FRAMES; namedWindow("ImageNet", WINDOW_AUTOSIZE | CV_GUI_NORMAL); } else { image_file = input_file; } try { // Create a executor with the approriate core type, number of cores // and configuration specified Executor executor(device_type, ids, configuration); // Query Executor for set of ExecutionObjects created const ExecutionObjects& execution_objects = executor.GetExecutionObjects(); int num_eos = execution_objects.size(); // Allocate input and output buffers for each execution object std::vector buffers; for (auto &eo : execution_objects) { size_t in_size = eo->GetInputBufferSizeInBytes(); size_t out_size = eo->GetOutputBufferSizeInBytes(); ArgInfo in = { ArgInfo(malloc(in_size), in_size)}; ArgInfo out = { ArgInfo(malloc(out_size), out_size)}; eo->SetInputOutputBuffer(in, out); buffers.push_back(in.ptr()); buffers.push_back(out.ptr()); } #define MAX_NUM_EOS 4 struct timespec t0[MAX_NUM_EOS], t1; // Process frames with available execution objects in a pipelined manner // additional num_eos iterations to flush the pipeline (epilogue) for (int frame_idx = 0; frame_idx < num_frames + num_eos; frame_idx++) { ExecutionObject* eo = execution_objects[frame_idx % num_eos].get(); // Wait for previous frame on the same eo to finish processing if (eo->ProcessFrameWait()) { clock_gettime(CLOCK_MONOTONIC, &t1); double elapsed_host = ms_diff(t0[eo->GetFrameIndex() % num_eos], t1); double elapsed_device = eo->GetProcessTimeInMilliSeconds(); double overhead = 100 - (elapsed_device/elapsed_host*100); std::cout << "frame[" << eo->GetFrameIndex() << "]: " << "Time on device: " << std::setw(6) << std::setprecision(4) << elapsed_device << "ms, " << "host: " << std::setw(6) << std::setprecision(4) << elapsed_host << "ms "; std::cout << "API overhead: " << std::setw(6) << std::setprecision(3) << overhead << " %" << std::endl; WriteFrameOutput(*eo); } // Read a frame and start processing it with current eo if (ReadFrame(*eo, frame_idx, configuration, num_frames, image_file, cap)) { clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]); eo->ProcessFrameStartAsync(); } } for (auto b : buffers) free(b); } catch (tidl::Exception &e) { std::cerr << e.what() << std::endl; status = false; } return status; } bool ReadFrame(ExecutionObject &eo, int frame_idx, const Configuration& configuration, int num_frames, std::string& image_file, VideoCapture &cap) { if (frame_idx >= num_frames) return false; eo.SetFrameIndex(frame_idx); char* frame_buffer = eo.GetInputBufferPtr(); assert (frame_buffer != nullptr); Mat image; if (! image_file.empty()) { image = cv::imread(image_file, CV_LOAD_IMAGE_COLOR); if (image.empty()) { std::cerr << "Unable to read from: " << image_file << std::endl; return false; } } else { Mat v_image; if (! cap.grab()) return false; if (! cap.retrieve(v_image)) return false; // Crop 640x480 camera input to center 256x256 input image = Mat(v_image, Rect(192, 112, 256, 256)); cv::imshow("ImageNet", image); waitKey(2); } // TI DL image preprocessing, into frame_buffer return PreProcImage(image, frame_buffer, 1, 3, configuration.inWidth, configuration.inHeight, configuration.inWidth, configuration.inWidth * configuration.inHeight, 1, configuration.preProcType); } // Display top 5 classified imagenet classes with probabilities bool WriteFrameOutput(const ExecutionObject &eo) { const int k = 5; unsigned char *out = (unsigned char *) eo.GetOutputBufferPtr(); int out_size = eo.GetOutputBufferSizeInBytes(); // sort and get k largest values and corresponding indices typedef std::pair val_index; auto constexpr cmp = [](val_index &left, val_index &right) { return left.first > right.first; }; std::priority_queue, decltype(cmp)> queue(cmp); // initialize priority queue with smallest value on top for (int i = 0; i < k; i++) queue.push(val_index(out[i], i)); // for rest output, if larger than current min, pop min, push new val for (int i = k; i < out_size; i++) { if (out[i] > queue.top().first) { queue.pop(); queue.push(val_index(out[i], i)); } } // output top k values in reverse order: largest val first std::vector sorted; while (! queue.empty()) { sorted.push_back(queue.top()); queue.pop(); } for (int i = k - 1; i >= 0; i--) { std::cout << k-i << ": " << imagenet_classes[sorted[i].second] << ", prob = " << (float) sorted[i].first / 256 << std::endl; } return true; } void ProcessArgs(int argc, char *argv[], std::string& config, int& num_devices, DeviceType& device_type, std::string& input_file) { const struct option long_options[] = { {"config", required_argument, 0, 'c'}, {"num_devices", required_argument, 0, 'n'}, {"device_type", required_argument, 0, 't'}, {"image_file", required_argument, 0, 'i'}, {"help", no_argument, 0, 'h'}, {"verbose", no_argument, 0, 'v'}, {0, 0, 0, 0} }; int option_index = 0; while (true) { int c = getopt_long(argc, argv, "c:n:t:i:hv", long_options, &option_index); if (c == -1) break; switch (c) { case 'c': config = optarg; break; case 'n': num_devices = atoi(optarg); assert (num_devices > 0 && num_devices <= 4); break; case 't': if (*optarg == 'e') device_type = DeviceType::EVE; else if (*optarg == 'd') device_type = DeviceType::DSP; else { std::cerr << "Invalid argument to -t, only e or d" " allowed" << std::endl; exit(EXIT_FAILURE); } break; case 'i': input_file = optarg; break; case 'v': __TI_show_debug_ = true; break; case 'h': DisplayHelp(); exit(EXIT_SUCCESS); break; case '?': // Error in getopt_long exit(EXIT_FAILURE); break; default: std::cerr << "Unsupported option: " << c << std::endl; break; } } } void DisplayHelp() { std::cout << "Usage: imagenet\n" " Will run imagenet network to predict top 5 object" " classes for the input.\n Use -c to run a" " different imagenet network. Default is j11_v2.\n" "Optional arguments:\n" " -c Valid configs: j11_bn, j11_prelu, j11_v2\n" " -n Number of cores to use (1 - 4)\n" " -t Type of core. d -> DSP, e -> EVE\n" " -i Path to the image file\n" " -i camera Use camera as input\n" " -v Verbose output during execution\n" " -h Help\n"; }