/****************************************************************************** * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "executor.h" #include "execution_object.h" #include "configuration.h" #include "../segmentation/object_classes.h" #include "opencv2/core.hpp" #include "opencv2/imgproc.hpp" #include "opencv2/highgui.hpp" #include "opencv2/videoio.hpp" #define NUM_VIDEO_FRAMES 100 #define DEFAULT_CONFIG "jdetnet" #define DEFAULT_INPUT "../test/testvecs/input/preproc_0_768x320.y" bool __TI_show_debug_ = false; bool is_default_input = false; bool is_preprocessed_input = false; bool is_camera_input = false; int orig_width; int orig_height; object_class_table_t *object_class_table; using namespace tidl; using namespace cv; bool RunConfiguration(const std::string& config_file, uint32_t num_devices, DeviceType device_type, std::string& input_file); bool ReadFrame(ExecutionObject& eo, int frame_idx, const Configuration& configuration, int num_frames, std::string& image_file, VideoCapture &cap); bool WriteFrameOutput(const ExecutionObject &eo_in, const ExecutionObject &eo_out, const Configuration& configuration); void ReportTime(int frame_index, std::string device_name, double elapsed_host, double elapsed_device); static void ProcessArgs(int argc, char *argv[], std::string& config, uint32_t& num_devices, DeviceType& device_type, std::string& input_file); static void DisplayHelp(); static double ms_diff(struct timespec &t0, struct timespec &t1) { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; } int main(int argc, char *argv[]) { // Catch ctrl-c to ensure a clean exit signal(SIGABRT, exit); signal(SIGTERM, exit); // If there are no devices capable of offloading TIDL on the SoC, exit uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE); uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP); if (num_eve == 0 || num_dsp == 0) { std::cout << "ssd_multibox requires both EVE and DSP for execution." << std::endl; return EXIT_SUCCESS; } // Process arguments std::string config = DEFAULT_CONFIG; std::string input_file = DEFAULT_INPUT; uint32_t num_devices = 1; DeviceType device_type = DeviceType::EVE; ProcessArgs(argc, argv, config, num_devices, device_type, input_file); // Use same number of EVEs and DSPs num_devices = std::min(num_devices, std::min(num_eve, num_dsp)); if (num_devices == 0) { std::cout << "Partitioned execution requires at least 1 EVE and 1 DSP." << std::endl; return EXIT_FAILURE; } if ((object_class_table = GetObjectClassTable(config)) == nullptr) { std::cout << "No object classes defined for this config." << std::endl; return EXIT_FAILURE; } if (input_file == DEFAULT_INPUT) is_default_input = true; if (input_file == "camera") is_camera_input = true; if (input_file.length() > 2 && input_file.compare(input_file.length() - 2, 2, ".y") == 0) is_preprocessed_input = true; std::cout << "Input: " << input_file << std::endl; std::string config_file = "../test/testvecs/config/infer/tidl_config_" + config + ".txt"; bool status = RunConfiguration(config_file, num_devices, device_type, input_file); if (!status) { std::cout << "ssd_multibox FAILED" << std::endl; return EXIT_FAILURE; } std::cout << "ssd_multibox PASSED" << std::endl; return EXIT_SUCCESS; } bool RunConfiguration(const std::string& config_file, uint32_t num_devices, DeviceType device_type, std::string& input_file) { DeviceIds ids; for (int i = 0; i < num_devices; i++) ids.insert(static_cast(i)); // Read the TI DL configuration file Configuration configuration; bool status = configuration.ReadFromFile(config_file); if (!status) { std::cerr << "Error in configuration file: " << config_file << std::endl; return false; } // setup input int num_frames = is_default_input ? 3 : 1; VideoCapture cap; std::string image_file; if (is_camera_input) { cap = VideoCapture(1); // cap = VideoCapture("test.mp4"); if (! cap.isOpened()) { std::cerr << "Cannot open camera input." << std::endl; return false; } num_frames = NUM_VIDEO_FRAMES; namedWindow("SSD_Multibox", WINDOW_AUTOSIZE | CV_GUI_NORMAL); } else { image_file = input_file; } try { // Create a executor with the approriate core type, number of cores // and configuration specified // EVE will run layersGroupId 1 in the network, while // DSP will run layersGroupId 2 in the network Executor executor_eve(DeviceType::EVE, ids, configuration, 1); Executor executor_dsp(DeviceType::DSP, ids, configuration, 2); // Query Executor for set of ExecutionObjects created const ExecutionObjects& execution_objects_eve = executor_eve.GetExecutionObjects(); const ExecutionObjects& execution_objects_dsp = executor_dsp.GetExecutionObjects(); int num_eos = execution_objects_eve.size(); // Allocate input and output buffers for each execution object // Note that "out" is both the output of eo_eve and the input of eo_dsp // This is how two layersGroupIds, 1 and 2, are tied together std::vector buffers; for (int i = 0; i < num_eos; i++) { ExecutionObject *eo_eve = execution_objects_eve[i].get(); size_t in_size = eo_eve->GetInputBufferSizeInBytes(); size_t out_size = eo_eve->GetOutputBufferSizeInBytes(); ArgInfo in = { ArgInfo(malloc(in_size), in_size) }; ArgInfo out = { ArgInfo(malloc(out_size), out_size) }; eo_eve->SetInputOutputBuffer(in, out); ExecutionObject *eo_dsp = execution_objects_dsp[i].get(); size_t out2_size = eo_dsp->GetOutputBufferSizeInBytes(); ArgInfo out2 = { ArgInfo(malloc(out2_size), out2_size) }; eo_dsp->SetInputOutputBuffer(out, out2); buffers.push_back(in.ptr()); buffers.push_back(out.ptr()); buffers.push_back(out2.ptr()); } #define MAX_NUM_EOS 4 struct timespec t0[MAX_NUM_EOS], t1, tloop0, tloop1; clock_gettime(CLOCK_MONOTONIC, &tloop0); // Process frames with available execution objects in a pipelined manner // additional num_eos iterations to flush the pipeline (epilogue) ExecutionObject *eo_eve, *eo_dsp, *eo_input; for (int frame_idx = 0; frame_idx < num_frames + num_eos; frame_idx++) { eo_eve = execution_objects_eve[frame_idx % num_eos].get(); eo_dsp = execution_objects_dsp[frame_idx % num_eos].get(); // Wait for previous frame on the same eo to finish processing if (eo_dsp->ProcessFrameWait()) { int finished_idx = eo_dsp->GetFrameIndex(); clock_gettime(CLOCK_MONOTONIC, &t1); ReportTime(finished_idx, "DSP", ms_diff(t0[finished_idx % num_eos], t1), eo_dsp->GetProcessTimeInMilliSeconds()); eo_input = execution_objects_eve[finished_idx % num_eos].get(); WriteFrameOutput(*eo_input, *eo_dsp, configuration); } // Read a frame and start processing it with current eo if (ReadFrame(*eo_eve, frame_idx, configuration, num_frames, image_file, cap)) { clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]); eo_eve->ProcessFrameStartAsync(); if (eo_eve->ProcessFrameWait()) { clock_gettime(CLOCK_MONOTONIC, &t1); ReportTime(frame_idx, "EVE", ms_diff(t0[frame_idx % num_eos], t1), eo_eve->GetProcessTimeInMilliSeconds()); clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]); eo_dsp->ProcessFrameStartAsync(); } } } clock_gettime(CLOCK_MONOTONIC, &tloop1); std::cout << "Loop total time (including read/write/print/etc): " << std::setw(6) << std::setprecision(4) << ms_diff(tloop0, tloop1) << "ms" << std::endl; for (auto b : buffers) free(b); } catch (tidl::Exception &e) { std::cerr << e.what() << std::endl; status = false; } return status; } void ReportTime(int frame_index, std::string device_name, double elapsed_host, double elapsed_device) { double overhead = 100 - (elapsed_device/elapsed_host*100); std::cout << "frame[" << frame_index << "]: " << "Time on " << device_name << ": " << std::setw(6) << std::setprecision(4) << elapsed_device << "ms, " << "host: " << std::setw(6) << std::setprecision(4) << elapsed_host << "ms "; std::cout << "API overhead: " << std::setw(6) << std::setprecision(3) << overhead << " %" << std::endl; } bool ReadFrame(ExecutionObject &eo, int frame_idx, const Configuration& configuration, int num_frames, std::string& image_file, VideoCapture &cap) { if (frame_idx >= num_frames) return false; eo.SetFrameIndex(frame_idx); char* frame_buffer = eo.GetInputBufferPtr(); assert (frame_buffer != nullptr); int channel_size = configuration.inWidth * configuration.inHeight; Mat image; if (! image_file.empty()) { if (is_preprocessed_input) { std::ifstream ifs(image_file, std::ios::binary); ifs.seekg(frame_idx * channel_size * 3); ifs.read(frame_buffer, channel_size * 3); bool ifs_status = ifs.good(); ifs.close(); orig_width = configuration.inWidth; orig_height = configuration.inHeight; return ifs_status; // already PreProc-ed } else { image = cv::imread(image_file, CV_LOAD_IMAGE_COLOR); if (image.empty()) { std::cerr << "Unable to read from: " << image_file << std::endl; return false; } } } else { // 640x480 camera input, process one in every 5 frames, // can adjust number of skipped frames to match real time processing if (! cap.grab()) return false; if (! cap.grab()) return false; if (! cap.grab()) return false; if (! cap.grab()) return false; if (! cap.grab()) return false; if (! cap.retrieve(image)) return false; } // scale to network input size Mat s_image, bgr_frames[3]; orig_width = image.cols; orig_height = image.rows; cv::resize(image, s_image, Size(configuration.inWidth, configuration.inHeight), 0, 0, cv::INTER_AREA); cv::split(s_image, bgr_frames); memcpy(frame_buffer, bgr_frames[0].ptr(), channel_size); memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size); memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size); return true; } // Create frame with boxes drawn around classified objects bool WriteFrameOutput(const ExecutionObject &eo_in, const ExecutionObject &eo_out, const Configuration& configuration) { // Asseembly original frame int width = configuration.inWidth; int height = configuration.inHeight; int channel_size = width * height; Mat frame, r_frame, bgr[3]; unsigned char *in = (unsigned char *) eo_in.GetInputBufferPtr(); bgr[0] = Mat(height, width, CV_8UC(1), in); bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size); bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2); cv::merge(bgr, 3, frame); int frame_index = eo_in.GetFrameIndex(); char outfile_name[64]; if (! is_camera_input && is_preprocessed_input) { snprintf(outfile_name, 64, "frame_%d.png", frame_index); cv::imwrite(outfile_name, frame); printf("Saving frame %d to: %s\n", frame_index, outfile_name); } // Draw boxes around classified objects float *out = (float *) eo_out.GetOutputBufferPtr(); int num_floats = eo_out.GetOutputBufferSizeInBytes() / sizeof(float); for (int i = 0; i < num_floats / 7; i++) { int index = (int) out[i * 7 + 0]; if (index < 0) break; int label = (int) out[i * 7 + 1]; float score = out[i * 7 + 2]; int xmin = (int) (out[i * 7 + 3] * width); int ymin = (int) (out[i * 7 + 4] * height); int xmax = (int) (out[i * 7 + 5] * width); int ymax = (int) (out[i * 7 + 6] * height); object_class_t *object_class = GetObjectClass(object_class_table, label); if (object_class == nullptr) continue; #if 0 printf("(%d, %d) -> (%d, %d): %s, score=%f\n", xmin, ymin, xmax, ymax, object_class->label, score); #endif cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax), Scalar(object_class->color.blue, object_class->color.green, object_class->color.red), 2); } // output cv::resize(frame, r_frame, Size(orig_width, orig_height)); if (is_camera_input) { cv::imshow("SSD_Multibox", r_frame); waitKey(1); } else { snprintf(outfile_name, 64, "multibox_%d.png", frame_index); cv::imwrite(outfile_name, r_frame); printf("Saving frame %d with SSD multiboxes to: %s\n", frame_index, outfile_name); } return true; } void ProcessArgs(int argc, char *argv[], std::string& config, uint32_t& num_devices, DeviceType& device_type, std::string& input_file) { const struct option long_options[] = { {"config", required_argument, 0, 'c'}, {"num_devices", required_argument, 0, 'n'}, {"image_file", required_argument, 0, 'i'}, {"help", no_argument, 0, 'h'}, {"verbose", no_argument, 0, 'v'}, {0, 0, 0, 0} }; int option_index = 0; while (true) { int c = getopt_long(argc, argv, "c:n:i:hv", long_options, &option_index); if (c == -1) break; switch (c) { case 'c': config = optarg; break; case 'n': num_devices = atoi(optarg); assert (num_devices > 0 && num_devices <= 4); break; case 'i': input_file = optarg; break; case 'v': __TI_show_debug_ = true; break; case 'h': DisplayHelp(); exit(EXIT_SUCCESS); break; case '?': // Error in getopt_long exit(EXIT_FAILURE); break; default: std::cerr << "Unsupported option: " << c << std::endl; break; } } } void DisplayHelp() { std::cout << "Usage: ssd_multibox\n" " Will run partitioned ssd_multibox network to perform " "multi-objects detection\n" " and classification. First part of network " "(layersGroupId 1) runs on EVE,\n" " second part (layersGroupId 2) runs on DSP.\n" " Use -c to run a different segmentation network. " "Default is jdetnet.\n" "Optional arguments:\n" " -c Valid configs: jdetnet \n" " -n Number of cores to use (1 - 4)\n" " -i Path to the image file\n" " Default is 1 frame in testvecs\n" " -i camera Use camera as input\n" " -v Verbose output during execution\n" " -h Help\n"; }