/****************************************************************************** * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "executor.h" #include "execution_object.h" #include "execution_object_pipeline.h" #include "configuration.h" #include "../segmentation/object_classes.h" #include "../common/utils.h" #include "../common/video_utils.h" using namespace std; using namespace tidl; using namespace cv; #define NUM_VIDEO_FRAMES 100 #define DEFAULT_CONFIG "jdetnet" #define DEFAULT_INPUT "../test/testvecs/input/preproc_0_768x320.y" #define DEFAULT_INPUT_FRAMES (1) object_class_table_t *object_class_table; uint32_t orig_width; uint32_t orig_height; bool RunConfiguration(const cmdline_opts_t& opts); Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c, int layers_group_id); bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx, const Configuration& c, const cmdline_opts_t& opts, VideoCapture &cap); bool WriteFrameOutput(const ExecutionObjectPipeline& eop, const Configuration& c, const cmdline_opts_t& opts); static void DisplayHelp(); int main(int argc, char *argv[]) { // Catch ctrl-c to ensure a clean exit signal(SIGABRT, exit); signal(SIGTERM, exit); // If there are no devices capable of offloading TIDL on the SoC, exit uint32_t num_eves = Executor::GetNumDevices(DeviceType::EVE); uint32_t num_dsps = Executor::GetNumDevices(DeviceType::DSP); if (num_eves == 0 || num_dsps == 0) { cout << "ssd_multibox requires both EVE and DSP for execution." << endl; return EXIT_SUCCESS; } // Process arguments cmdline_opts_t opts; opts.config = DEFAULT_CONFIG; opts.num_eves = 1; opts.num_dsps = 1; if (! ProcessArgs(argc, argv, opts)) { DisplayHelp(); exit(EXIT_SUCCESS); } assert(opts.num_dsps != 0 && opts.num_eves != 0); if (opts.num_frames == 0) opts.num_frames = (opts.is_camera_input || opts.is_video_input) ? NUM_VIDEO_FRAMES : (opts.input_file.empty() ? DEFAULT_INPUT_FRAMES : 1); if (opts.input_file.empty()) cout << "Input: " << DEFAULT_INPUT << endl; else cout << "Input: " << opts.input_file << endl; // Get object class table if ((object_class_table = GetObjectClassTable(opts.config)) == nullptr) { cout << "No object classes defined for this config." << endl; return EXIT_FAILURE; } // Run network bool status = RunConfiguration(opts); if (!status) { cout << "ssd_multibox FAILED" << endl; return EXIT_FAILURE; } cout << "ssd_multibox PASSED" << endl; return EXIT_SUCCESS; } bool RunConfiguration(const cmdline_opts_t& opts) { // Read the TI DL configuration file Configuration c; std::string config_file = "../test/testvecs/config/infer/tidl_config_" + opts.config + ".txt"; bool status = c.ReadFromFile(config_file); if (!status) { cerr << "Error in configuration file: " << config_file << endl; return false; } c.enableApiTrace = opts.verbose; // setup camera/video input VideoCapture cap; if (! SetVideoInputOutput(cap, opts, "SSD_Multibox")) return false; try { // Create Executors with the approriate core type, number of cores // and configuration specified // EVE will run layersGroupId 1 in the network, while // DSP will run layersGroupId 2 in the network Executor* e_eve = CreateExecutor(DeviceType::EVE, opts.num_eves, c, 1); Executor* e_dsp = CreateExecutor(DeviceType::DSP, opts.num_dsps, c, 2); // Construct ExecutionObjectPipeline that utilizes multiple // ExecutionObjects to process a single frame, each ExecutionObject // processes one layerGroup of the network // // Pipeline depth can enable more optimized pipeline execution: // Given one EVE and one DSP as an example, with different // pipeline_depth, we have different execution behavior: // If pipeline_depth is set to 1, // we create one EOP: eop0 (eve0, dsp0) // pipeline execution of multiple frames over time is as follows: // --------------------- time -------------------> // eop0: [eve0...][dsp0] // eop0: [eve0...][dsp0] // eop0: [eve0...][dsp0] // eop0: [eve0...][dsp0] // If pipeline_depth is set to 2, // we create two EOPs: eop0 (eve0, dsp0), eop1(eve0, dsp0) // pipeline execution of multiple frames over time is as follows: // --------------------- time -------------------> // eop0: [eve0...][dsp0] // eop1: [eve0...][dsp0] // eop0: [eve0...][dsp0] // eop1: [eve0...][dsp0] // Additional benefit of setting pipeline_depth to 2 is that // it can also overlap host ReadFrame() with device processing: // --------------------- time -------------------> // eop0: [RF][eve0...][dsp0] // eop1: [RF] [eve0...][dsp0] // eop0: [RF][eve0...][dsp0] // eop1: [RF][eve0...][dsp0] vector eops; uint32_t pipeline_depth = 2; // 2 EOs in EOP -> depth 2 for (uint32_t j = 0; j < pipeline_depth; j++) for (uint32_t i = 0; i < max(opts.num_eves, opts.num_dsps); i++) eops.push_back(new ExecutionObjectPipeline( {(*e_eve)[i%opts.num_eves], (*e_dsp)[i%opts.num_dsps]})); uint32_t num_eops = eops.size(); // Allocate input/output memory for each EOP AllocateMemory(eops); chrono::time_point tloop0, tloop1; tloop0 = chrono::steady_clock::now(); // Process frames with available eops in a pipelined manner // additional num_eops iterations to flush pipeline (epilogue) for (uint32_t frame_idx = 0; frame_idx < opts.num_frames + num_eops; frame_idx++) { ExecutionObjectPipeline* eop = eops[frame_idx % num_eops]; // Wait for previous frame on the same eop to finish processing if (eop->ProcessFrameWait()) { WriteFrameOutput(*eop, c, opts); } // Read a frame and start processing it with current eo if (ReadFrame(*eop, frame_idx, c, opts, cap)) eop->ProcessFrameStartAsync(); } tloop1 = chrono::steady_clock::now(); chrono::duration elapsed = tloop1 - tloop0; cout << "Loop total time (including read/write/opencv/print/etc): " << setw(6) << setprecision(4) << (elapsed.count() * 1000) << "ms" << endl; FreeMemory(eops); for (auto eop : eops) delete eop; delete e_eve; delete e_dsp; } catch (tidl::Exception &e) { cerr << e.what() << endl; status = false; } return status; } // Create an Executor with the specified type and number of EOs Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c, int layers_group_id) { if (num == 0) return nullptr; DeviceIds ids; for (uint32_t i = 0; i < num; i++) ids.insert(static_cast(i)); return new Executor(dt, ids, c, layers_group_id); } bool ReadFrame(ExecutionObjectPipeline& eop, uint32_t frame_idx, const Configuration& c, const cmdline_opts_t& opts, VideoCapture &cap) { if ((uint32_t)frame_idx >= opts.num_frames) return false; eop.SetFrameIndex(frame_idx); char* frame_buffer = eop.GetInputBufferPtr(); assert (frame_buffer != nullptr); int channel_size = c.inWidth * c.inHeight; Mat image; if (!opts.is_camera_input && !opts.is_video_input) { if (opts.input_file.empty()) { ifstream ifs(DEFAULT_INPUT, ios::binary); ifs.seekg((frame_idx % DEFAULT_INPUT_FRAMES) * channel_size * 3); ifs.read(frame_buffer, channel_size * 3); bool ifs_status = ifs.good(); ifs.close(); orig_width = c.inWidth; orig_height = c.inHeight; return ifs_status; // already PreProc-ed } else { image = cv::imread(opts.input_file, CV_LOAD_IMAGE_COLOR); if (image.empty()) { cerr << "Unable to read from: " << opts.input_file << endl; return false; } } } else { // 640x480 camera input, process one in every 5 frames, // can adjust number of skipped frames to match real time processing if (! cap.grab()) return false; if (! cap.grab()) return false; if (! cap.grab()) return false; if (! cap.grab()) return false; if (! cap.grab()) return false; if (! cap.retrieve(image)) return false; } // scale to network input size Mat s_image, bgr_frames[3]; orig_width = image.cols; orig_height = image.rows; cv::resize(image, s_image, Size(c.inWidth, c.inHeight), 0, 0, cv::INTER_AREA); cv::split(s_image, bgr_frames); memcpy(frame_buffer, bgr_frames[0].ptr(), channel_size); memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size); memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size); return true; } // Create frame with boxes drawn around classified objects bool WriteFrameOutput(const ExecutionObjectPipeline& eop, const Configuration& c, const cmdline_opts_t& opts) { // Asseembly original frame int width = c.inWidth; int height = c.inHeight; int channel_size = width * height; Mat frame, r_frame, bgr[3]; unsigned char *in = (unsigned char *) eop.GetInputBufferPtr(); bgr[0] = Mat(height, width, CV_8UC(1), in); bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size); bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2); cv::merge(bgr, 3, frame); int frame_index = eop.GetFrameIndex(); char outfile_name[64]; if (opts.input_file.empty()) { snprintf(outfile_name, 64, "frame_%d.png", frame_index); cv::imwrite(outfile_name, frame); printf("Saving frame %d to: %s\n", frame_index, outfile_name); } // Draw boxes around classified objects float *out = (float *) eop.GetOutputBufferPtr(); int num_floats = eop.GetOutputBufferSizeInBytes() / sizeof(float); for (int i = 0; i < num_floats / 7; i++) { int index = (int) out[i * 7 + 0]; if (index < 0) break; int label = (int) out[i * 7 + 1]; int xmin = (int) (out[i * 7 + 3] * width); int ymin = (int) (out[i * 7 + 4] * height); int xmax = (int) (out[i * 7 + 5] * width); int ymax = (int) (out[i * 7 + 6] * height); object_class_t *object_class = GetObjectClass(object_class_table, label); if (object_class == nullptr) continue; #if 0 printf("(%d, %d) -> (%d, %d): %s, score=%f\n", xmin, ymin, xmax, ymax, object_class->label, score); #endif cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax), Scalar(object_class->color.blue, object_class->color.green, object_class->color.red), 2); } // Resize to output width/height, keep aspect ratio uint32_t output_width = opts.output_width; if (output_width == 0) output_width = orig_width; uint32_t output_height = (output_width*1.0f) / orig_width * orig_height; cv::resize(frame, r_frame, Size(output_width, output_height)); if (opts.is_camera_input || opts.is_video_input) { cv::imshow("SSD_Multibox", r_frame); waitKey(1); } else { snprintf(outfile_name, 64, "multibox_%d.png", frame_index); cv::imwrite(outfile_name, r_frame); printf("Saving frame %d with SSD multiboxes to: %s\n", frame_index, outfile_name); } return true; } void DisplayHelp() { std::cout << "Usage: ssd_multibox\n" " Will run partitioned ssd_multibox network to perform " "multi-objects detection\n" " and classification. First part of network " "(layersGroupId 1) runs on EVE,\n" " second part (layersGroupId 2) runs on DSP.\n" " Use -c to run a different segmentation network. Default is jdetnet.\n" "Optional arguments:\n" " -c Valid configs: jdetnet \n" " -d Number of dsp cores to use\n" " -e Number of eve cores to use\n" " -i Path to the image file as input\n" " Default are 9 frames in testvecs\n" " -i camera Use camera as input\n" " video input port: /dev/video\n" " -i .{mp4,mov,avi} Use video file as input\n" " -f Number of frames to process\n" " -w Output image/video width\n" " -v Verbose output during execution\n" " -h Help\n"; }