/****************************************************************************** * Copyright (c) 2017, Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ #include #include #include #include #include #include #include #include #include #include #include "executor.h" #include "execution_object.h" #include "configuration.h" bool __TI_show_debug_ = false; using namespace tinn; bool RunMultipleExecutors(const std::string& config_file_1, const std::string& config_file_2, uint32_t num_devices_available); bool RunConfiguration(const std::string& config_file, int num_devices, DeviceType device_type); bool RunAllConfigurations(int32_t num_devices, DeviceType device_type); bool ReadFrame(ExecutionObject& eo, int frame_idx, const Configuration& configuration, std::istream& input_file); bool WriteFrame(const ExecutionObject &eo, std::ostream& output_file); static void ProcessArgs(int argc, char *argv[], std::string& config_file, int& num_devices, DeviceType& device_type); static void DisplayHelp(); static double ms_diff(struct timespec &t0, struct timespec &t1) { return (t1.tv_sec - t0.tv_sec) * 1e3 + (t1.tv_nsec - t0.tv_nsec) / 1e6; } int main(int argc, char *argv[]) { // Catch ctrl-c to ensure a clean exit signal(SIGABRT, exit); signal(SIGTERM, exit); // If there are no devices capable of offloading TINN on the SoC, exit uint32_t num_dla = Executor::GetNumDevices(DeviceType::DLA); uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP); if (num_dla == 0 && num_dsp == 0) { std::cout << "TI DL not supported on this SoC." << std::endl; return EXIT_SUCCESS; } std::cout << "API Version: " << Executor::GetAPIVersion() << std::endl; // Process arguments std::string config_file; int num_devices = 1; DeviceType device_type = DeviceType::DLA; ProcessArgs(argc, argv, config_file, num_devices, device_type); bool status = true; if (!config_file.empty()) status = RunConfiguration(config_file, num_devices, device_type); else { if (num_dla > 0) { //TODO: Use memory availability to determine # devices // Run on 2 devices because there is not enough CMEM available by // default if (num_dla = 4) num_dla = 2; status = RunAllConfigurations(num_dla, DeviceType::DLA); status &= RunMultipleExecutors( "testvecs/config/infer/tidl_config_j11_v2.txt", "testvecs/config/infer/tidl_config_j11_cifar.txt", num_dla); } if (num_dsp > 0) { status &= RunAllConfigurations(num_dsp, DeviceType::DSP); } } if (!status) { std::cout << "tidl FAILED" << std::endl; return EXIT_FAILURE; } std::cout << "tidl PASSED" << std::endl; return EXIT_SUCCESS; } bool RunConfiguration(const std::string& config_file, int num_devices, DeviceType device_type) { DeviceIds ids; for (int i = 0; i < num_devices; i++) ids.insert(static_cast(i)); // Read the TI DL configuration file Configuration configuration; bool status = configuration.ReadFromFile(config_file); if (!status) { std::cerr << "Error in configuration file: " << config_file << std::endl; return false; } // Open input and output files std::ifstream input_data_file(configuration.inData, std::ios::binary); std::ofstream output_data_file(configuration.outData, std::ios::binary); assert (input_data_file.good()); assert (output_data_file.good()); // Determine input frame size from configuration size_t frame_sz = configuration.inWidth * configuration.inHeight * configuration.inNumChannels; try { // Create a executor with the approriate core type, number of cores // and configuration specified Executor executor(device_type, ids, configuration); // Query Executor for set of ExecutionObjects created const ExecutionObjects& execution_objects = executor.GetExecutionObjects(); int num_eos = execution_objects.size(); // Allocate input and output buffers for each execution object std::vector buffers; for (auto &eo : execution_objects) { ArgInfo in = { ArgInfo(malloc(frame_sz), frame_sz)}; ArgInfo out = { ArgInfo(malloc(frame_sz), frame_sz)}; eo->SetInputOutputBuffer(in, out); buffers.push_back(in.ptr()); buffers.push_back(out.ptr()); } #define MAX_NUM_EOS 4 struct timespec t0[MAX_NUM_EOS], t1; // Process frames with available execution objects in a pipelined manner // additional num_eos iterations to flush the pipeline (epilogue) for (int frame_idx = 0; frame_idx < configuration.numFrames + num_eos; frame_idx++) { ExecutionObject* eo = execution_objects[frame_idx % num_eos].get(); // Wait for previous frame on the same eo to finish processing if (eo->ProcessFrameWait()) { clock_gettime(CLOCK_MONOTONIC, &t1); double elapsed_host = ms_diff(t0[eo->GetFrameIndex() % num_eos], t1); double elapsed_device = eo->GetProcessTimeInMilliSeconds(); double overhead = 100 - (elapsed_device/elapsed_host*100); std::cout << "frame[" << eo->GetFrameIndex() << "]: " << "Time on device: " << std::setw(6) << std::setprecision(4) << elapsed_device << "ms, " << "host: " << std::setw(6) << std::setprecision(4) << elapsed_host << "ms "; std::cout << "API overhead: " << std::setw(6) << std::setprecision(3) << overhead << " %" << std::endl; WriteFrame(*eo, output_data_file); } // Read a frame and start processing it with current eo if (ReadFrame(*eo, frame_idx, configuration, input_data_file)) { clock_gettime(CLOCK_MONOTONIC, &t0[frame_idx % num_eos]); eo->ProcessFrameStartAsync(); } } for (auto b : buffers) free(b); } catch (tinn::Exception &e) { std::cerr << e.what() << std::endl; status = false; } input_data_file.close(); output_data_file.close(); return status; } namespace tinn { extern bool CompareFiles (const std::string &F1, const std::string &F2); extern bool CompareFrames(const std::string &F1, const std::string &F2, int numFrames, int width, int height); } bool RunAllConfigurations(int32_t num_devices, DeviceType device_type) { std::vector configurations; if (device_type == DeviceType::DLA) configurations = {"dense_1x1", "j11_bn", "j11_cifar", "j11_controlLayers", "j11_prelu", "j11_v2", "jseg21", "jseg21_tiscapes", "smallRoi", "squeeze1_1"}; else configurations = {"j11_bn", "j11_controlLayers", "j11_v2", "jseg21", "jseg21_tiscapes", "smallRoi", "squeeze1_1"}; int errors = 0; for (auto config : configurations) { std::string config_file = "testvecs/config/infer/tidl_config_" + config + ".txt"; std::cout << "Running " << config << " on " << num_devices << " devices, type " << ((device_type == DeviceType::DLA) ? "EVE" : "DSP") << std::endl; Configuration configuration; bool status = configuration.ReadFromFile(config_file); if (!status) { errors++; continue; } status = RunConfiguration(config_file, num_devices, device_type); if (!status) { errors++; continue; } // Check output against reference output std::string reference_output = "testvecs/reference/" + config + "_ref.bin"; // Reference for jseg21_tiscapes only has one frame if (config.compare("jseg21_tiscapes") == 0) status = CompareFrames(configuration.outData, reference_output, 1, 1024, 512); else status = CompareFiles(configuration.outData, reference_output); if (status) std::cout << config << " : PASSED" << std::endl; else std::cout << config << " : FAILED" << std::endl; if (!status) errors++; } if (errors > 0) return false; return true; } bool ReadFrame(ExecutionObject &eo, int frame_idx, const Configuration& configuration, std::istream& input_file) { if (frame_idx >= configuration.numFrames) return false; char* frame_buffer = eo.GetInputBufferPtr(); assert (frame_buffer != nullptr); input_file.read(eo.GetInputBufferPtr(), eo.GetInputBufferSizeInBytes()); if (input_file.eof()) return false; assert (input_file.good()); // Set the frame index being processed by the EO. This is used to // sort the frames before they are output eo.SetFrameIndex(frame_idx); if (input_file.good()) return true; return false; } bool WriteFrame(const ExecutionObject &eo, std::ostream& output_file) { output_file.write( eo.GetOutputBufferPtr(), eo.GetOutputBufferSizeInBytes()); assert(output_file.good() == true); if (output_file.good()) return true; return false; } void ProcessArgs(int argc, char *argv[], std::string& config_file, int& num_devices, DeviceType& device_type) { const struct option long_options[] = { {"config_file", required_argument, 0, 'c'}, {"num_devices", required_argument, 0, 'n'}, {"device_type", required_argument, 0, 't'}, {"help", no_argument, 0, 'h'}, {"verbose", no_argument, 0, 'v'}, {0, 0, 0, 0} }; int option_index = 0; while (true) { int c = getopt_long(argc, argv, "c:n:t:hv", long_options, &option_index); if (c == -1) break; switch (c) { case 'c': config_file = optarg; break; case 'n': num_devices = atoi(optarg); assert (num_devices > 0 && num_devices <= 4); break; case 't': if (*optarg == 'e') device_type = DeviceType::DLA; else if (*optarg == 'd') device_type = DeviceType::DSP; else { std::cerr << "Invalid argument to -t, only e or d" " allowed" << std::endl; exit(EXIT_FAILURE); } break; case 'v': __TI_show_debug_ = true; break; case 'h': DisplayHelp(); exit(EXIT_SUCCESS); break; case '?': // Error in getopt_long exit(EXIT_FAILURE); break; default: std::cerr << "Unsupported option: " << c << std::endl; break; } } } void DisplayHelp() { std::cout << "Usage: test_tinn\n" " Will run all available networks if invoked without" " any arguments.\n Use -c to run a single network.\n" "Optional arguments:\n" " -c Path to the configuration file\n" " -n Number of cores to use (1 - 4)\n" " -t Type of core. d -> DSP, e -> DLA\n" " -v Verbose output during execution\n" " -h Help\n"; }