/****************************************************************************** * Copyright (c) 2018, Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ //! @file multiple_executors.cpp //! Illustrates how to setup multiple Executor instances using //! non-overlapping sets of device ids and running the Executor instances //! in parallel - each in its own thread #include #include #include #include #include #include #include #include #include #include "executor.h" #include "execution_object.h" #include "configuration.h" using namespace tinn; extern bool ReadFrame(ExecutionObject& eo, int frame_idx, const Configuration& configuration, std::istream& input_file); extern bool WriteFrame(const ExecutionObject &eo, std::ostream& output_file); void* run_network(void *data); struct ThreadArg { std::string config_file; DeviceIds ids; ThreadArg(const DeviceIds& ids, const std::string& s): ids(ids), config_file(s) {} }; bool thread_status[2]; bool RunMultipleExecutors(const std::string& config_file_1, const std::string& config_file_2, uint32_t num_devices_available) { // If there is only 1 device available, skip if (num_devices_available == 1) return true; DeviceIds ids1, ids2; if (num_devices_available == 4) { ids1 = {DeviceId::ID2, DeviceId::ID3}; ids2 = {DeviceId::ID0, DeviceId::ID1}; } else { ids1 = {DeviceId::ID0}; ids2 = {DeviceId::ID1}; } // Set up devices and config files for each thread ThreadArg arg1(ids2, config_file_1); ThreadArg arg2(ids1, config_file_2); // Run network 1 in a thread std::cout << std::endl << "Multiple Executor..." << std::endl; std::cout << "Running network " << arg1.config_file.substr(arg1.config_file.find("tidl")) << " on EVEs: "; for (DeviceId id : arg1.ids) std::cout << static_cast(id) << " "; std::cout << " in thread 0" << std::endl; pthread_t network_thread_1; pthread_create(&network_thread_1, 0, &run_network, &arg1); // Run network 2 in a thread std::cout << "Running network " << arg2.config_file.substr(arg2.config_file.find("tidl")) << " on EVEs: "; for (DeviceId id : arg2.ids) std::cout << static_cast(id) << " "; std::cout << " in thread 1" << std::endl; pthread_t network_thread_2; pthread_create(&network_thread_2, 0, &run_network, &arg2); // Wait for both networks to complete void *thread_return_val1; void *thread_return_val2; pthread_join(network_thread_1, &thread_return_val1); pthread_join(network_thread_2, &thread_return_val2); if (thread_return_val1 == 0 || thread_return_val2 == 0) { std::cout << "Multiple executors: FAILED" << std::endl; return false; } std::cout << "Multiple executors: PASSED" << std::endl; return true; } void* run_network(void *data) { const ThreadArg* arg = static_cast(data); const DeviceIds& ids = arg->ids; const std::string& config_file = arg->config_file; // Read the TI DL configuration file Configuration configuration; bool status = configuration.ReadFromFile(config_file); assert (status != false); configuration.outData += std::to_string(pthread_self()); // Open input and output files std::ifstream input_data_file(configuration.inData, std::ios::binary); std::ofstream output_data_file(configuration.outData, std::ios::binary); assert (input_data_file.good()); assert (output_data_file.good()); // Determine input frame size from configuration size_t frame_sz = configuration.inWidth * configuration.inHeight * configuration.inNumChannels; try { // Create a executor with the approriate core type, number of cores // and configuration specified Executor executor(DeviceType::DLA, ids, configuration); const ExecutionObjects& execution_objects = executor.GetExecutionObjects(); int num_eos = execution_objects.size(); // Allocate input and output buffers for each execution object std::vector buffers; for (auto &eo : execution_objects) { ArgInfo in = { ArgInfo(malloc_ddr(frame_sz), frame_sz)}; ArgInfo out = { ArgInfo(malloc_ddr(frame_sz), frame_sz)}; eo->SetInputOutputBuffer(in, out); buffers.push_back(in.ptr()); buffers.push_back(out.ptr()); } // Process frames with available execution objects in a pipelined manner // additional num_eos iterations to flush the pipeline (epilogue) for (int frame_idx = 0; frame_idx < configuration.numFrames + num_eos; frame_idx++) { ExecutionObject* eo = execution_objects[frame_idx % num_eos].get(); // Wait for previous frame on the same eo to finish processing if (eo->ProcessFrameWait()) WriteFrame(*eo, output_data_file); // Read a frame and start processing it with current eo if (ReadFrame(*eo, frame_idx, configuration, input_data_file)) eo->ProcessFrameStartAsync(); } for (auto b : buffers) __free_ddr(b); } catch (tinn::Exception &e) { std::cerr << e.what() << std::endl; status = false; } input_data_file.close(); output_data_file.close(); // Return 1 for true, 0 for false. void * pattern follows example from: // "Advanced programming in the Unix Environment" if (!status) return ((void *)0); return ((void *)1); }