/****************************************************************************** * Copyright (c) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ // // This example illustrates using multiple EOs to process a single frame // For details, refer http://downloads.ti.com/mctools/esd/docs/tidl-api/ // #include #include #include #include #include #include "executor.h" #include "execution_object.h" #include "execution_object_pipeline.h" #include "configuration.h" #include "utils.h" using namespace tidl; using std::string; using std::unique_ptr; using std::vector; using EOP = tidl::ExecutionObjectPipeline; bool Run(int num_eve,int num_dsp, const char* ref_output); Executor* CreateExecutor(DeviceType dt, int num, const Configuration& c, int layer_group_id); void AllocateMemory(const vector& EOPs); void FreeMemory (const vector& EOPs); int main(int argc, char *argv[]) { // Catch ctrl-c to ensure a clean exit signal(SIGABRT, exit); signal(SIGTERM, exit); // This example requires both EVE and C66x uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE); uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP); if (num_eve == 0 || num_dsp == 0) { std::cout << "TI DL not supported on this SoC." << std::endl; return EXIT_SUCCESS; } string ref_file ="../test/testvecs/reference/j11_v2_ref.bin"; unique_ptr reference_output(ReadReferenceOutput(ref_file)); bool status = Run(num_eve, num_dsp, reference_output.get()); if (!status) { std::cout << "FAILED" << std::endl; return EXIT_FAILURE; } std::cout << "PASSED" << std::endl; return EXIT_SUCCESS; } bool Run(int num_eve, int num_dsp, const char* ref_output) { string config_file ="../test/testvecs/config/infer/tidl_config_j11_v2.txt"; Configuration c; if (!c.ReadFromFile(config_file)) return false; // Heap sizes for this network determined using Configuration::showHeapStats c.PARAM_HEAP_SIZE = (3 << 20); // 3MB c.NETWORK_HEAP_SIZE = (20 << 20); // 20MB c.numFrames = 16; // Assign layers 12, 13 and 14 to layer group 2 c.layerIndex2LayerGroupId = { {12, 2}, {13, 2}, {14, 2} }; // Open input file for reading std::ifstream input(c.inData, std::ios::binary); bool status = true; try { // Create Executors - use all the DSP and EVE cores available // Layer group 1 will be executed on EVE, 2 on DSP unique_ptr eve(CreateExecutor(DeviceType::EVE,num_eve,c,1)); unique_ptr dsp(CreateExecutor(DeviceType::DSP,num_dsp,c,2)); // Create pipelines. Each pipeline has 1 EVE and 1 DSP. If there are // more EVEs than DSPs, the DSPs are shared across multiple // pipelines. E.g. // 2 EVE, 2 DSP: EVE1 -> DSP1, EVE2 -> DSP2 // 4 EVE, 2 DSP: EVE1 -> DSP1, EVE2 -> DSP2, EVE3 -> DSP1, EVE4 ->DSP2 std::vector EOPs; uint32_t num_pipe = std::max(num_eve, num_dsp); for (uint32_t i = 0; i < num_pipe; i++) EOPs.push_back(new EOP( { (*eve)[i % num_eve], (*dsp)[i % num_dsp] } )); AllocateMemory(EOPs); // Process frames with EOs in a pipelined manner // additional num_eos iterations to flush the pipeline (epilogue) int num_eops = EOPs.size(); for (int frame_idx = 0; frame_idx < c.numFrames + num_eops; frame_idx++) { EOP* eop = EOPs[frame_idx % num_eops]; // Wait for previous frame on the same eo to finish processing if (eop->ProcessFrameWait()) { ReportTime(eop); // The reference output is valid only for the first frame // processed on each EOP if (frame_idx < num_eops && !CheckFrame(eop, ref_output)) status = false; } // Read a frame and start processing it with current eo if (ReadFrame(eop, frame_idx, c, input)) eop->ProcessFrameStartAsync(); } FreeMemory(EOPs); } catch (tidl::Exception &e) { std::cerr << e.what() << std::endl; status = false; } input.close(); return status; } // Create an Executor with the specified type and number of EOs Executor* CreateExecutor(DeviceType dt, int num, const Configuration& c, int layer_group_id) { if (num == 0) return nullptr; DeviceIds ids; for (int i = 0; i < num; i++) ids.insert(static_cast(i)); return new Executor(dt, ids, c, layer_group_id); } // Allocate input and output memory for each EO void AllocateMemory(const vector& EOPs) { // Allocate input and output buffers for each execution object for (auto eop : EOPs) { size_t in_size = eop->GetInputBufferSizeInBytes(); size_t out_size = eop->GetOutputBufferSizeInBytes(); ArgInfo in = { ArgInfo(malloc(in_size), in_size)}; ArgInfo out = { ArgInfo(malloc(out_size), out_size)}; eop->SetInputOutputBuffer(in, out); } } // Free the input and output memory associated with each EO void FreeMemory(const vector& EOPs) { for (auto eop : EOPs) { free(eop->GetInputBufferPtr()); free(eop->GetOutputBufferPtr()); } }