/****************************************************************************** * Copyright (c) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ // // This example illustrates using multiple EOs to process a single frame // For details, refer http://downloads.ti.com/mctools/esd/docs/tidl-api/ // #include #include #include #include #include #include "executor.h" #include "execution_object.h" #include "execution_object_pipeline.h" #include "configuration.h" #include "utils.h" using namespace tidl; using std::string; using std::unique_ptr; using std::vector; using EOP = tidl::ExecutionObjectPipeline; bool Run(int num_eve,int num_dsp, const char* ref_output); int main(int argc, char *argv[]) { // Catch ctrl-c to ensure a clean exit signal(SIGABRT, exit); signal(SIGTERM, exit); // This example requires both EVE and C66x uint32_t num_eve = Executor::GetNumDevices(DeviceType::EVE); uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP); if (num_eve == 0 || num_dsp == 0) { std::cout << "TI DL not supported on this SoC." << std::endl; return EXIT_SUCCESS; } string ref_file ="../test/testvecs/reference/j11_v2_ref.bin"; unique_ptr reference_output(ReadReferenceOutput(ref_file)); // Enable time stamp generation. The timestamp file is post processed // by execution_graph.py to generate graphical view of frame execution. // Refer to the User's Guide for details. EnableTimeStamps("2eo_opt.log"); bool status = Run(num_eve, num_dsp, reference_output.get()); if (!status) { std::cout << "FAILED" << std::endl; return EXIT_FAILURE; } std::cout << "PASSED" << std::endl; return EXIT_SUCCESS; } bool Run(int num_eve, int num_dsp, const char* ref_output) { string config_file ="../test/testvecs/config/infer/tidl_config_j11_v2.txt"; Configuration c; if (!c.ReadFromFile(config_file)) return false; // Heap sizes for this network determined using Configuration::showHeapStats c.PARAM_HEAP_SIZE = (3 << 20); // 3MB c.NETWORK_HEAP_SIZE = (34 << 20); // 34MB // Run this example for 16 input frames c.numFrames = 16; // Assign layers 12, 13 and 14 to the DSP layer group const int EVE_LG = 1; const int DSP_LG = 2; c.layerIndex2LayerGroupId = { {12, DSP_LG}, {13, DSP_LG}, {14, DSP_LG} }; // Open input file for reading std::ifstream input(c.inData, std::ios::binary); bool status = true; try { // Create Executors - use all the DSP and EVE cores available // Specify layer group id for each Executor unique_ptr eve(CreateExecutor(DeviceType::EVE, num_eve, c, EVE_LG)); unique_ptr dsp(CreateExecutor(DeviceType::DSP, num_dsp, c, DSP_LG)); // On AM5749, create a total of 4 pipelines (EOPs): // EOPs[0] : { EVE1, DSP1 } // EOPs[1] : { EVE1, DSP1 } for double buffering // EOPs[2] : { EVE2, DSP2 } // EOPs[3] : { EVE2, DSP2 } for double buffering const uint32_t pipeline_depth = 2; // 2 EOs in EOP => depth 2 std::vector EOPs; uint32_t num_pipe = std::max(num_eve, num_dsp); for (uint32_t i = 0; i < num_pipe; i++) for (uint32_t j = 0; j < pipeline_depth; j++) EOPs.push_back(new EOP( { (*eve)[i % num_eve], (*dsp)[i % num_dsp] } )); AllocateMemory(EOPs); // Process frames with EOs in a pipelined manner // additional num_eos iterations to flush the pipeline (epilogue) int num_eops = EOPs.size(); for (int frame_idx = 0; frame_idx < c.numFrames + num_eops; frame_idx++) { EOP* eop = EOPs[frame_idx % num_eops]; // Wait for previous frame on the same EOP to finish processing if (eop->ProcessFrameWait()) { // The reference output is valid only for the first frame // processed on each EOP if (frame_idx < num_eops && !CheckFrame(eop, ref_output)) status = false; } // Read a frame and start processing it with current eo if (ReadFrame(eop, frame_idx, c, input)) eop->ProcessFrameStartAsync(); } FreeMemory(EOPs); } catch (tidl::Exception &e) { std::cerr << e.what() << std::endl; status = false; } input.close(); return status; }