/****************************************************************************** * Copyright (c) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ #pragma once //! @file configuration.h #include #include namespace tidl { /*! @class Configuration @brief Specifies the configuration required for a network */ class Configuration { public: //! Number of frames of input data (can be 0 if data is not read from file) int numFrames; //! Height of the input frame int inHeight; //! Width of the input frame int inWidth; //! Number of channels in the input frame (e.g. 3 for BGR) int inNumChannels; int noZeroCoeffsPercentage; //! Pre-processing type applied to the input frame //! Specific to each network, can take values from 0 to 4, default is 0 int preProcType; //! Force to run all layers, regardless of layersGroupId partitioning bool runFullNet; //! When set, inputs are taken from TIDL internal buffers that contain //! outputs of previous layersGroupId, instead of from user application bool enableInternalInput; //! Size of the TI DL per Execution Object heap size_t EXTMEM_HEAP_SIZE; //! Size of the heap used for paramter data size_t PARAM_HEAP_SIZE; //! @brief Location of the input file //! Can be empty if input data is provided by frameworks such as OpenCV. std::string inData; //! Location of the output file //! Can be empty if output data is consumed by frameworks such as OpenCV. std::string outData; //! Path to the TIDL network binary file std::string netBinFile; //! Path to the TIDL parameter binary file std::string paramsBinFile; //! Enable tracing of output buffers associated with each layer bool enableOutputTrace; //! Default constructor. Configuration(); //! Validate the fields in the configuration object bool Validate() const; //! Print the configuration void Print(std::ostream& os = std::cout) const; //! Read a configuration from the specified file and validate bool ReadFromFile(const std::string& file_name); }; }