/****************************************************************************** * Copyright (c) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ /*! @file execution_object.h */ #pragma once #include #include "configuration.h" #include "execution_object_internal.h" namespace tidl { class Kernel; class Device; class LayerOutput; class IODeviceArgInfo; /*! @class ExecutionObject @brief Runs the TIDL network on an OpenCL device */ class ExecutionObject : public ExecutionObjectInternalInterface { public: //! @private // Used by the Executor to construct an ExecutionObject ExecutionObject(Device* d, uint8_t device_index, const ArgInfo& create_arg, const ArgInfo& param_heap_arg, const Configuration& configuration, int layersGroupId); //! @private ~ExecutionObject(); //! Specify the input and output buffers used by the EO //! @param in buffer used for input. //! @param out buffer used for output. void SetInputOutputBuffer(const ArgInfo& in, const ArgInfo& out) override; //! Returns a pointer to the input buffer set via SetInputOutputBuffer char* GetInputBufferPtr() const override; //! Returns size of the input buffer size_t GetInputBufferSizeInBytes() const override; //! Returns a pointer to the output buffer char* GetOutputBufferPtr() const override; //! Returns size of the output buffer size_t GetOutputBufferSizeInBytes() const override; //! @brief Set the frame index of the frame currently processed by the //! ExecutionObject. Used for trace/debug messages //! @param idx index of the frame void SetFrameIndex(int idx) override; //! Returns the index of a frame being processed (set by SetFrameIndex) int GetFrameIndex() const override; //! @brief Start processing a frame. The call is asynchronous and //! returns immediately. Use ExecutionObject::ProcessFrameWait to wait bool ProcessFrameStartAsync() override; //! Wait for the execution object to complete processing a frame //! @return false if ExecutionObject::ProcessFrameWait was called //! without a corresponding call to //! ExecutionObject::ProcessFrameStartAsync. bool ProcessFrameWait() override; //! @brief return the number of milliseconds taken *on the device* to //! execute the process call //! @return Number of milliseconds to process a frame on the device. float GetProcessTimeInMilliSeconds() const override; //! @brief return the number of milliseconds taken *on the host* to //! execute the process call //! @return Number of milliseconds to process a frame on the host. float GetHostProcessTimeInMilliSeconds() const override; //! Returns the device name that the ExecutionObject runs on const std::string& GetDeviceName() const override; //! Write the output buffer for each layer to a file //! \__HxW.bin void WriteLayerOutputsToFile(const std::string& filename_prefix= "trace_dump_") const override; //! Returns a LayerOutput object corresponding to a layer. //! Caller is responsible for deleting the LayerOutput object. //! @see LayerOutput //! @param layer_index The layer index of the layer //! @param output_index The output index of the buffer for a given //! layer. Defaults to 0. const LayerOutput* GetOutputFromLayer(uint32_t layer_index, uint32_t output_index=0) const override; //! Get output buffers from all layers const LayerOutputs* GetOutputsFromAllLayers() const override; //! Returns the layersGrupId that the ExecutionObject is processing int GetLayersGroupId() const; //! @private // Used by the Executor enum class CallType { INIT, PROCESS, CLEANUP }; bool RunAsync(CallType ct); bool Wait (CallType ct); //! @private // Used by the ExecutionObjectPipeline bool AddCallback(CallType ct, void *user_data); void AcquireLock(); void ReleaseLock(); ExecutionObject() = delete; ExecutionObject(const ExecutionObject&) = delete; ExecutionObject& operator=(const ExecutionObject&) = delete; //! @private void SetInputOutputBuffer(const IODeviceArgInfo* in, const IODeviceArgInfo* out); private: class Impl; std::unique_ptr pimpl_m; }; /*! @class LayerOutput @brief Describes the output of a layer in terms of its shape. Also includes a pointer to the data. */ class LayerOutput { public: //! @private //! Constructor called within API, not by the user LayerOutput(int layer_index, int output_index, int buffer_id, int num_roi_m, int num_channels, size_t height, size_t width, const char* data); //! Must be called to delete the data pointer. ~LayerOutput(); //! @return The index of a layer int LayerIndex() const { return layer_index_m; } //! @return The number of channels associated with an output int NumberOfChannels() const { return num_channels_m; } //! @return The height of the output. Can be 1 for 1D outputs size_t Height() const { return height_m; } //! @return The width of the output size_t Width() const { return width_m; } //! @return Size of the output in bytes size_t Size() const { return height_m * width_m * num_channels_m; } //! @return Pointer to output. Must call destructor to free the //! memory used to hold the output. const char* Data() const { return data_m; } //! @private Disable copy construction and assignment since //! class holds a pointer to allocated data LayerOutput(const LayerOutput&) = delete; LayerOutput& operator= (const LayerOutput&) = delete; private: int layer_index_m; int output_index_m; int buffer_id_m; int num_roi_m; int num_channels_m; size_t height_m; size_t width_m; const char* data_m; }; } // namespace tidl