/****************************************************************************** * Copyright (c) 2018 Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ //! @file execution_object_pipeline.h #pragma once #include #include #include #include #include "executor.h" #include "execution_object_internal.h" #include "execution_object.h" namespace tidl { /*! @class ExecutionObjectPipeline @brief Manages the pipelined execution using multiple ExecutionObjects. Each executor runs one layersGroup of the network. ExecutionObjects must run consecutive layersGroups to form a pipelined execution. */ class ExecutionObjectPipeline : public ExecutionObjectInternalInterface { public: //! @brief Create an ExecutionObjectPipeline object. //! //! The ExecutionObjectPipeline will take the provided ExecutionObjects //! to create an execution pipeline. E.g. //! @code //! Configuration config("path to configuration file"); //! DeviceIds ids = {DeviceId::ID0, DeviceId::ID1}; //! Executor exe_eve(DeviceType::EVE, ids, config, 1); //! Executor exe_dsp(DeviceType::DSP, ids, config, 2); //! ExecutionObjectPipeline ep0({exe_eve[0], exe_dsp[0]}); //! ExecutionObjectPipeline ep1({exe_eve[1], exe_dsp[1]}); //! @endcode //! //! @param eos DSP or EVE ExecutionObjects forming a pipeline ExecutionObjectPipeline(std::vector eos); //! @brief Tear down an ExecutionObjectPipeline and free used resources ~ExecutionObjectPipeline(); //! Returns the number of ExecutionObjects associated with the //! ExecutionObjectPipeline uint32_t GetNumExecutionObjects() const; //! Specify the input and output buffers used by the EOP //! @param in buffer used for input. //! @param out buffer used for output. void SetInputOutputBuffer (const ArgInfo& in, const ArgInfo& out) override; //! Returns a pointer to the input buffer char* GetInputBufferPtr() const override; //! Returns size of the input buffer size_t GetInputBufferSizeInBytes() const override; //! Returns a pointer to the output buffer char* GetOutputBufferPtr() const override; //! Returns the number of bytes written to the output buffer size_t GetOutputBufferSizeInBytes() const override; //! @brief Set the frame index of the frame currently processed by the //! ExecutionObjectPipeline. Used for trace/debug messages //! @param idx index of the frame void SetFrameIndex(int idx) override; //! Returns the index of a frame being processed (set by SetFrameIndex) int GetFrameIndex() const override; //! @brief Start processing a frame. The call is asynchronous and //! returns immediately. Use ProcessFrameWait() to wait bool ProcessFrameStartAsync() override; //! Wait for the executor pipeline to complete processing a frame //! @return false if ProcessFrameWait() was called //! without a corresponding call to //! ExecutionObjectPipeline::ProcessFrameStartAsync(). bool ProcessFrameWait() override; //! @brief return the number of milliseconds taken *on the device* to //! execute the process call //! @return Number of milliseconds to process a frame on the device. float GetProcessTimeInMilliSeconds() const override; //! @brief return the number of milliseconds taken *on the device* //! to process a layersGroup by a componenet ExecutionObject //! @return Number of milliseconds to process a layersGroup on the //! device by a component ExecutionObject. float GetProcessTimeInMilliSeconds(uint32_t eo_index) const; //! @brief return the number of milliseconds taken *on the host* to //! execute the process call //! @return Number of milliseconds to process a frame on the host. float GetHostProcessTimeInMilliSeconds() const override; //! @brief return the number of milliseconds taken *on the host* //! to process a layersGroup by a componenet ExecutionObject //! @return Number of milliseconds to process a layersGroup on the //! host by a component ExecutionObject. float GetHostProcessTimeInMilliSeconds(uint32_t eo_index) const; //! Return the combined device names that this pipeline runs on const std::string& GetDeviceName() const override; //! Write the output buffer for each layer to a file //! \__HxW.bin void WriteLayerOutputsToFile(const std::string& filename_prefix= "trace_dump_") const override; //! Returns a LayerOutput object corresponding to a layer. //! Caller is responsible for deleting the LayerOutput object. //! @see LayerOutput //! @param layer_index The layer index of the layer //! @param output_index The output index of the buffer for a given //! layer. Defaults to 0. const LayerOutput* GetOutputFromLayer(uint32_t layer_index, uint32_t output_index=0) const override; //! Get output buffers from all layers const LayerOutputs* GetOutputsFromAllLayers() const override; //! @private Used by runtime //! @brief callback function at the completion of each ExecutionObject, //! to chain the next ExectionObject for execution void RunAsyncNext(); ExecutionObjectPipeline() = delete; ExecutionObjectPipeline(const ExecutionObjectPipeline&) = delete; ExecutionObjectPipeline& operator=(const ExecutionObjectPipeline&) = delete; private: class Impl; std::unique_ptr pimpl_m; }; } // namespace tidl