/****************************************************************************** * Copyright (c) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ //! @file executor.h #pragma once #include #include #include #include #include #include #include #include "configuration.h" #include "custom.h" namespace tidl { //! Enumerates types of devices available to offload the network. enum class DeviceType { DSP, /**< Offload to C66x DSP */ EVE /**< Offload to TI EVE */ }; //! Enumerates IDs for devices of a given type. enum class DeviceId : int { ID0=0, /**< DSP1 or EVE1 */ ID1, /**< DSP2 or EVE2 */ ID2, /**< EVE3 */ ID3 /**< EVE4 */ }; //! Used to specify the set of devices available to an Executor typedef std::set DeviceIds; class ExecutorImpl; class ExecutionObject; //! Defines the return type for Executor::GetExecutionObjects typedef std::vector> ExecutionObjects; /*! @class Executor @brief Manages the overall execution of a network using the specified configuration and the set of devices available to the executor. */ class Executor { public: //! @brief Create an Executor object. //! //! The Executor will create the required ExecutionObject's and //! initialize them with the specified TI DL network. E.g. //! @code //! Configuration configuration; //! configuration.ReadFromFile("path to configuration file"); //! DeviceIds ids1 = {DeviceId::ID2, DeviceId::ID3}; //! Executor executor(DeviceType::EVE, ids, configuration); //! @endcode //! //! @param device_type DSP or EVE device //! @param ids Set of devices uses by this instance of the Executor //! @param configuration Configuration used to initialize the Executor //! @param layers_group_id Layers group that this Executor should run Executor(DeviceType device_type, const DeviceIds& ids, const Configuration& configuration, int layers_group_id = OCL_TIDL_DEFAULT_LAYERS_GROUP_ID); //! @brief Tear down an Executor and free resources used by the //! Executor object ~Executor(); //! Returns a vector of unique_ptr's to execution objects //! available on this instance of the Executor const ExecutionObjects& GetExecutionObjects() const; //! @brief Returns the number of devices of the specified type //! available for TI DL. //! @param device_type DSP or EVE/EVE device //! @return number of devices available static uint32_t GetNumDevices(DeviceType device_type); //! @brief Returns a string corresponding to the API version //! //! @return ... static std::string GetAPIVersion(); Executor(const Executor&) = delete; Executor& operator= (const Executor&) = delete; private: std::unique_ptr pimpl_m; }; /*! @class ArgInfo * @brief Describe input and output buffers required by ExecutionObjects */ class ArgInfo { public: enum class DeviceAccess { R_ONLY=0, W_ONLY, RW }; //! Construct an ArgInfo object from a pointer to a chunk of memory //! and its size. ArgInfo(void *p, size_t size) : ptr_m(p), size_m(size), access_m(DeviceAccess::RW) {} ArgInfo(const ArgInfo& arg) = default; ArgInfo& operator=(const ArgInfo& arg) = default; //! @return Pointer to the buffer or scalar represented by ArgInfo void *ptr() const { return ptr_m; } //! @return The size of the buffer or scalar represented by ArgInfo size_t size() const { return size_m; } protected: void* ptr_m; size_t size_m; DeviceAccess access_m; }; extern "C" void __free_ddr(void *ptr); extern "C" void* __malloc_ddr(size_t s); //! template typedef for unique_ptr with __free_ddr deleter template using up_malloc_ddr = std::unique_ptr; //! __malloc_ddr wrapper - Bytes allocated determined by sizeof(T) template inline T* malloc_ddr() { assert (std::is_pointer::value == false); T* val = reinterpret_cast(__malloc_ddr(sizeof(T))); assert (val != nullptr); return val; } //! __malloc_ddr wrapper - Bytes allocated passed as argument template inline T* malloc_ddr(size_t size) { assert (std::is_pointer::value == false); T* val = reinterpret_cast(__malloc_ddr(size)); assert (val != nullptr); return val; } /*! @class Exception * @brief Used to error reporting */ class Exception : public std::exception { public: Exception() {} Exception(const std::string& error, const std::string& file, const std::string& func, uint32_t line_no); Exception(int32_t errorCode, const std::string& file, const std::string& func, uint32_t line_no); virtual ~Exception() {} //! @return String describing the error message and its location virtual const char* what() const noexcept; private: std::string message_m; }; } // namespace tidl