/* pybind11/iostream.h -- Tools to assist with redirecting cout and cerr to Python Copyright (c) 2017 Henry F. Schreiner All rights reserved. Use of this source code is governed by a BSD-style license that can be found in the LICENSE file. */ #pragma once #include "pybind11.h" #include #include #include #include #include NAMESPACE_BEGIN(PYBIND11_NAMESPACE) NAMESPACE_BEGIN(detail) // Buffer that writes to Python instead of C++ class pythonbuf : public std::streambuf { private: using traits_type = std::streambuf::traits_type; char d_buffer[1024]; object pywrite; object pyflush; int overflow(int c) { if (!traits_type::eq_int_type(c, traits_type::eof())) { *pptr() = traits_type::to_char_type(c); pbump(1); } return sync() == 0 ? traits_type::not_eof(c) : traits_type::eof(); } int sync() { if (pbase() != pptr()) { // This subtraction cannot be negative, so dropping the sign str line(pbase(), static_cast(pptr() - pbase())); pywrite(line); pyflush(); setp(pbase(), epptr()); } return 0; } public: pythonbuf(object pyostream) : pywrite(pyostream.attr("write")), pyflush(pyostream.attr("flush")) { setp(d_buffer, d_buffer + sizeof(d_buffer) - 1); } /// Sync before destroy ~pythonbuf() { sync(); } }; NAMESPACE_END(detail) /** \rst This a move-only guard that redirects output. .. code-block:: cpp #include ... { py::scoped_ostream_redirect output; std::cout << "Hello, World!"; // Python stdout } // <-- return std::cout to normal You can explicitly pass the c++ stream and the python object, for example to guard stderr instead. .. code-block:: cpp { py::scoped_ostream_redirect output{std::cerr, py::module::import("sys").attr("stderr")}; std::cerr << "Hello, World!"; } \endrst */ class scoped_ostream_redirect { protected: std::streambuf *old; std::ostream &costream; detail::pythonbuf buffer; public: scoped_ostream_redirect( std::ostream &costream = std::cout, object pyostream = module::import("sys").attr("stdout")) : costream(costream), buffer(pyostream) { old = costream.rdbuf(&buffer); } ~scoped_ostream_redirect() { costream.rdbuf(old); } scoped_ostream_redirect(const scoped_ostream_redirect &) = delete; scoped_ostream_redirect(scoped_ostream_redirect &&other) = default; scoped_ostream_redirect &operator=(const scoped_ostream_redirect &) = delete; scoped_ostream_redirect &operator=(scoped_ostream_redirect &&) = delete; }; /** \rst Like `scoped_ostream_redirect`, but redirects cerr by default. This class is provided primary to make ``py::call_guard`` easier to make. .. code-block:: cpp m.def("noisy_func", &noisy_func, py::call_guard()); \endrst */ class scoped_estream_redirect : public scoped_ostream_redirect { public: scoped_estream_redirect( std::ostream &costream = std::cerr, object pyostream = module::import("sys").attr("stderr")) : scoped_ostream_redirect(costream,pyostream) {} }; NAMESPACE_BEGIN(detail) // Class to redirect output as a context manager. C++ backend. class OstreamRedirect { bool do_stdout_; bool do_stderr_; std::unique_ptr redirect_stdout; std::unique_ptr redirect_stderr; public: OstreamRedirect(bool do_stdout = true, bool do_stderr = true) : do_stdout_(do_stdout), do_stderr_(do_stderr) {} void enter() { if (do_stdout_) redirect_stdout.reset(new scoped_ostream_redirect()); if (do_stderr_) redirect_stderr.reset(new scoped_estream_redirect()); } void exit() { redirect_stdout.reset(); redirect_stderr.reset(); } }; NAMESPACE_END(detail) /** \rst This is a helper function to add a C++ redirect context manager to Python instead of using a C++ guard. To use it, add the following to your binding code: .. code-block:: cpp #include ... py::add_ostream_redirect(m, "ostream_redirect"); You now have a Python context manager that redirects your output: .. code-block:: python with m.ostream_redirect(): m.print_to_cout_function() This manager can optionally be told which streams to operate on: .. code-block:: python with m.ostream_redirect(stdout=true, stderr=true): m.noisy_function_with_error_printing() \endrst */ inline class_ add_ostream_redirect(module m, std::string name = "ostream_redirect") { return class_(m, name.c_str(), module_local()) .def(init(), arg("stdout")=true, arg("stderr")=true) .def("__enter__", &detail::OstreamRedirect::enter) .def("__exit__", [](detail::OstreamRedirect &self, args) { self.exit(); }); } NAMESPACE_END(PYBIND11_NAMESPACE)