/****************************************************************************** * Copyright (c) 2017 Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * Neither the name of Texas Instruments Incorporated nor the * names of its contributors may be used to endorse or promote products * derived from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF * THE POSSIBILITY OF SUCH DAMAGE. *****************************************************************************/ /*! \file execution_object.cpp */ #include "executor.h" #include "execution_object.h" #include "trace.h" #include "ocl_device.h" #include "parameters.h" #include "configuration.h" #include "common_defines.h" #include using namespace tinn; class ExecutionObject::Impl { public: Impl(Device* d, uint8_t device_index, const ArgInfo& create_arg, const ArgInfo& param_heap_arg, size_t extmem_heap_size, uint32_t internal_input); ~Impl() {} bool RunAsync(CallType ct); bool Wait (CallType ct); bool SetupProcessKernel(const ArgInfo& in, const ArgInfo& out); void HostWriteNetInput(); void HostReadNetOutput(); void ComputeInputOutputSizes(); Device* device_m; std::unique_ptr k_initialize_m; std::unique_ptr k_process_m; std::unique_ptr k_cleanup_m; up_malloc_ddr tidl_extmem_heap_m; up_malloc_ddr shared_initialize_params_m; up_malloc_ddr shared_process_params_m; size_t in_size_m; size_t out_size_m; ArgInfo in_m; ArgInfo out_m; // Index of the OpenCL device/queue used by this EO uint8_t device_index_m; // Frame being processed by the EO int current_frame_idx_m; }; ExecutionObject::ExecutionObject(Device* d, uint8_t device_index, const ArgInfo& create_arg, const ArgInfo& param_heap_arg, size_t extmem_heap_size, uint32_t internal_input) { pimpl_m = std::unique_ptr { new ExecutionObject::Impl(d, device_index, create_arg, param_heap_arg, extmem_heap_size, internal_input) }; } ExecutionObject::Impl::Impl(Device* d, uint8_t device_index, const ArgInfo& create_arg, const ArgInfo& param_heap_arg, size_t extmem_heap_size, uint32_t internal_input): device_m(d), k_initialize_m(nullptr), k_process_m(nullptr), k_cleanup_m(nullptr), tidl_extmem_heap_m (nullptr, &__free_ddr), shared_initialize_params_m(nullptr, &__free_ddr), shared_process_params_m(nullptr, &__free_ddr), in_size_m(0), out_size_m(0), in_m(nullptr, 0), out_m(nullptr, 0), device_index_m(device_index), current_frame_idx_m(0) { // Allocate a heap for TI DL to use on the device tidl_extmem_heap_m.reset(malloc_ddr(extmem_heap_size)); // Create a kernel for cleanup KernelArgs cleanup_args; k_cleanup_m.reset(new Kernel(device_m, STRING(CLEANUP_KERNEL), cleanup_args, device_index_m)); // Set up parameter struct for the initialize kernel shared_initialize_params_m.reset(malloc_ddr()); memset(shared_initialize_params_m.get(), 0, sizeof(OCL_TIDL_InitializeParams)); shared_initialize_params_m->tidlHeapSize = extmem_heap_size; shared_initialize_params_m->l2HeapSize = tinn::internal::DMEM1_SIZE; shared_initialize_params_m->l1HeapSize = tinn::internal::DMEM0_SIZE; shared_initialize_params_m->enableTrace = OCL_TIDL_TRACE_OFF; shared_initialize_params_m->enableInternalInput = internal_input; // Setup kernel arguments for initialize KernelArgs args = { create_arg, param_heap_arg, ArgInfo(tidl_extmem_heap_m.get(), extmem_heap_size), ArgInfo(shared_initialize_params_m.get(), sizeof(OCL_TIDL_InitializeParams)), device_m->type() == CL_DEVICE_TYPE_ACCELERATOR ? ArgInfo(nullptr, tinn::internal::DMEM1_SIZE): ArgInfo(nullptr, 4) }; k_initialize_m.reset(new Kernel(device_m, STRING(INIT_KERNEL), args, device_index_m)); } // Pointer to implementation idiom: https://herbsutter.com/gotw/_100/: // Both unique_ptr and shared_ptr can be instantiated with an incomplete type // unique_ptr's destructor requires a complete type in order to invoke delete ExecutionObject::~ExecutionObject() = default; char* ExecutionObject::GetInputBufferPtr() const { return static_cast(pimpl_m->in_m.ptr()); } size_t ExecutionObject::GetInputBufferSizeInBytes() const { if (pimpl_m->in_m.ptr() == nullptr) return pimpl_m->in_size_m; else return pimpl_m->in_m.size(); } char* ExecutionObject::GetOutputBufferPtr() const { return static_cast(pimpl_m->out_m.ptr()); } size_t ExecutionObject::GetOutputBufferSizeInBytes() const { if (pimpl_m->out_m.ptr() == nullptr) return pimpl_m->out_size_m; else return pimpl_m->shared_process_params_m.get()->bytesWritten; } void ExecutionObject::SetFrameIndex(int idx) { pimpl_m->current_frame_idx_m = idx; } int ExecutionObject::GetFrameIndex() const { return pimpl_m->current_frame_idx_m; } void ExecutionObject::SetInputOutputBuffer(const ArgInfo& in, const ArgInfo& out) { pimpl_m->SetupProcessKernel(in, out); } bool ExecutionObject::ProcessFrameStartAsync() { return pimpl_m->RunAsync(ExecutionObject::CallType::PROCESS); } bool ExecutionObject::ProcessFrameWait() { return pimpl_m->Wait(ExecutionObject::CallType::PROCESS); } bool ExecutionObject::RunAsync (CallType ct) { return pimpl_m->RunAsync(ct); } bool ExecutionObject::Wait (CallType ct) { return pimpl_m->Wait(ct); } uint64_t ExecutionObject::GetProcessCycles() const { uint8_t factor = 1; // ARP32 running at half frequency of VCOP, multiply by 2 for VCOP cycles if (pimpl_m->device_m->type() == CL_DEVICE_TYPE_CUSTOM) factor = 2; return pimpl_m->shared_process_params_m.get()->cycles * factor; } float ExecutionObject::GetProcessTimeInMilliSeconds() const { float frequency = pimpl_m->device_m->GetFrequencyInMhz() * 1000000; return ((float)GetProcessCycles())/frequency * 1000; } // // Create a kernel to call the "process" function // bool ExecutionObject::Impl::SetupProcessKernel(const ArgInfo& in, const ArgInfo& out) { in_m = in; out_m = out; shared_process_params_m.reset(malloc_ddr()); shared_process_params_m->enableTrace = OCL_TIDL_TRACE_OFF; shared_process_params_m->enableInternalInput = shared_initialize_params_m->enableInternalInput; shared_process_params_m->cycles = 0; if (shared_process_params_m->enableInternalInput == 0) assert(in.ptr() != nullptr && in.size() > 0); KernelArgs args = { ArgInfo(shared_process_params_m.get(), sizeof(OCL_TIDL_ProcessParams)), in, out, ArgInfo(tidl_extmem_heap_m.get(), shared_initialize_params_m->tidlHeapSize) }; k_process_m.reset(new Kernel(device_m, STRING(PROCESS_KERNEL), args, device_index_m)); return true; } static size_t readDataS8(const char *readPtr, char *ptr, int roi, int n, int width, int height, int pitch, int chOffset) { if (!readPtr) return 0; for(int i2 = 0; i2 < roi; i2++) for(int i0 = 0; i0 < n; i0++) for(int i1 = 0; i1 < height; i1++) memcpy(&ptr[i2*n*chOffset + i0*chOffset + i1*pitch], &readPtr[i2*n*width*height + i0*width*height+ i1*width], width); return width*height*n*roi; } static size_t writeDataS8(char *writePtr, const char *ptr, int n, int width, int height, int pitch, int chOffset) { if (!writePtr) return 0; for(int i0 = 0; i0 < n; i0++) for(int i1 = 0; i1 < height; i1++) memcpy(&writePtr[i0*width*height + i1*width], &ptr[i0*chOffset + i1*pitch], width); return width*height*n; } void ExecutionObject::Impl::HostWriteNetInput() { char* readPtr = (char *) in_m.ptr(); PipeInfo *pipe = in_m.GetPipe(); for (unsigned int i = 0; i < shared_initialize_params_m->numInBufs; i++) { OCL_TIDL_BufParams *inBuf = &shared_initialize_params_m->inBufs[i]; if (shared_process_params_m->enableInternalInput == 0) { readPtr += readDataS8( readPtr, (char *) tidl_extmem_heap_m.get() + inBuf->bufPlaneBufOffset + inBuf->bufPlaneWidth * OCL_TIDL_MAX_PAD_SIZE + OCL_TIDL_MAX_PAD_SIZE, inBuf->numROIs, inBuf->numChannels, inBuf->ROIWidth, inBuf->ROIHeight, inBuf->bufPlaneWidth, ((inBuf->bufPlaneWidth * inBuf->bufPlaneHeight) / inBuf->numChannels)); } else { shared_process_params_m->inBufAddr[i] = pipe->bufAddr_m[i]; } shared_process_params_m->inDataQ[i] = pipe->dataQ_m[i]; } } void ExecutionObject::Impl::HostReadNetOutput() { char* writePtr = (char *) out_m.ptr(); PipeInfo *pipe = out_m.GetPipe(); for (unsigned int i = 0; i < shared_initialize_params_m->numOutBufs; i++) { OCL_TIDL_BufParams *outBuf = &shared_initialize_params_m->outBufs[i]; if (writePtr != nullptr) { writePtr += writeDataS8( writePtr, (char *) tidl_extmem_heap_m.get() + outBuf->bufPlaneBufOffset + outBuf->bufPlaneWidth * OCL_TIDL_MAX_PAD_SIZE + OCL_TIDL_MAX_PAD_SIZE, outBuf->numChannels, outBuf->ROIWidth, outBuf->ROIHeight, outBuf->bufPlaneWidth, ((outBuf->bufPlaneWidth * outBuf->bufPlaneHeight)/ outBuf->numChannels)); } pipe->dataQ_m[i] = shared_process_params_m->outDataQ[i]; pipe->bufAddr_m[i] = shared_initialize_params_m->bufAddrBase + outBuf->bufPlaneBufOffset; } shared_process_params_m->bytesWritten = writePtr - (char *) out_m.ptr(); } void ExecutionObject::Impl::ComputeInputOutputSizes() { if (shared_initialize_params_m->errorCode != OCL_TIDL_SUCCESS) return; if (shared_initialize_params_m->numInBufs > OCL_TIDL_MAX_IN_BUFS || shared_initialize_params_m->numOutBufs > OCL_TIDL_MAX_OUT_BUFS) { std::cout << "Num input/output bufs (" << shared_initialize_params_m->numInBufs << ", " << shared_initialize_params_m->numOutBufs << ") exceeded limit!" << std::endl; shared_initialize_params_m->errorCode = OCL_TIDL_INIT_FAIL; return; } in_size_m = 0; out_size_m = 0; for (unsigned int i = 0; i < shared_initialize_params_m->numInBufs; i++) { OCL_TIDL_BufParams *inBuf = &shared_initialize_params_m->inBufs[i]; in_size_m += inBuf->numROIs * inBuf->numChannels * inBuf->ROIWidth * inBuf->ROIHeight; } for (unsigned int i = 0; i < shared_initialize_params_m->numOutBufs; i++) { OCL_TIDL_BufParams *outBuf = &shared_initialize_params_m->outBufs[i]; out_size_m += outBuf->numChannels * outBuf->ROIWidth *outBuf->ROIHeight; } } bool ExecutionObject::Impl::RunAsync(CallType ct) { switch (ct) { case CallType::INIT: { k_initialize_m->RunAsync(); break; } case CallType::PROCESS: { shared_process_params_m->frameIdx = current_frame_idx_m; shared_process_params_m->bytesWritten = 0; HostWriteNetInput(); k_process_m->RunAsync(); break; } case CallType::CLEANUP: { k_cleanup_m->RunAsync(); break; } default: return false; } return true; } bool ExecutionObject::Impl::Wait(CallType ct) { switch (ct) { case CallType::INIT: { bool has_work = k_initialize_m->Wait(); if (has_work) { ComputeInputOutputSizes(); if (shared_initialize_params_m->errorCode != OCL_TIDL_SUCCESS) throw Exception(shared_initialize_params_m->errorCode, __FILE__, __FUNCTION__, __LINE__); } return has_work; } case CallType::PROCESS: { bool has_work = k_process_m->Wait(); if (has_work) { if (shared_process_params_m->errorCode != OCL_TIDL_SUCCESS) throw Exception(shared_process_params_m->errorCode, __FILE__, __FUNCTION__, __LINE__); HostReadNetOutput(); } return has_work; } case CallType::CLEANUP: { return k_cleanup_m->Wait(); break; } default: return false; } return false; }