diff --git a/docs/source/api.rst b/docs/source/api.rst
index 6fd383ca164aa275ea68d734b8ed294687b7e968..3a3d221fd1cdb5d370a76a163e10f4ba5bd3799b 100644 (file)
--- a/docs/source/api.rst
+++ b/docs/source/api.rst
This field is used to specify the size of the device heap used for network parameters. The size depends on the size of the parameter binary file. For example, ``jsegnet21v2``'s parameter file, ``tidl_param_jsegnet21v2.bin`` is 2.6MB. Due to alignment reasons, the parameter heap must be 10% larger than the binary file size - in this case, 2.9MB. The constructor for ``Configuration`` sets PARAM_HEAP_SIZE to 9MB. There is one parameter heap for each instance of ``Executor`` .
-.. data:: std::size_t Configuration.EXTMEM_HEAP_SIZE
+.. data:: std::size_t Configuration.NETWORK_HEAP_SIZE
- This field is used to specify the size of the device heap used for all allocations other than network parameters. The constructor for ``Configuration`` sets EXTMEM_HEAP_SIZE to 64MB. There is one external memory heap for each instance of ``ExecutionObject``
+ This field is used to specify the size of the device heap used for all allocations other than network parameters. The constructor for ``Configuration`` sets NETWORK_HEAP_SIZE to 64MB. There is one external memory heap for each instance of ``ExecutionObject``
Debug
+++++