diff --git a/docs/source/api.rst b/docs/source/api.rst
index d27202780ddb91a5c5889cc5f2b84597fa4b1bdc..7aa7849a9f542b8d1152cfc2184c7500d34cc0c0 100644 (file)
--- a/docs/source/api.rst
+++ b/docs/source/api.rst
+.. _api-documentation:
+
******************
TIDL API Reference
******************
-.. doxygennamespace:: tinn
+Configuration
+-------------
+The ``Configuration`` object is used to specify various parameters required for network execution. Applications can directly initialize fields in an instance of ``Configuration`` or use the ``ReadFromFile`` method to read the configuration from a file. The following sections describe the commonly used fields available in the ``Configuration`` class:
+
+Input image description
++++++++++++++++++++++++
+.. data:: std::string Configuration.inData
+
+ Path to the input image file. This field is not used by the TIDL API itself. It can be used by applications to load an input image into a buffer. Can be empty if the application uses frameworks such as OpenCV to read images. See ``test/main.cpp`` for example usage.
+
+.. data:: std::size_t Configuration.inHeight
+
+ Height of the input image. Used by the API, must be specified.
+
+.. data:: std::size_t Configuration.inWidth
+
+ Width of the input image. Used by the API, must be specified.
+
+.. data:: std::size_t Configuration.inNumChannels
+
+ Number of channels in the input image. Used by the API, must be specified.
+
+Output description
+++++++++++++++++++
+
+.. data:: std::string Configuration.outData
+
+ Path to the output image file. This field is not used by the TIDL API itself. It can be used by applications to write a buffer to file. Can be empty if the application uses frameworks such as OpenCV to read images. See ``test/main.cpp`` for example usage.
+
+Network
++++++++
+
+.. data:: std::string Configuration.netBinFile
+
+ Path to the TIDL network binary file. Used by the API, must be specified.
+
+.. data:: std::string Configuration.paramBinFile
+
+ Path to the TIDL parameter file. Used by the API, must be specified.
+
+Memory Management
++++++++++++++++++
+The ``Configuration`` object specifies the sizes of 2 heaps. These heaps are allocated from OpenCL global memory that is shared across the host and device. Refer section :ref:`opencl-global-memory` for steps to increase the size of the OpenCL global memory heap.
+
+.. data:: std::size_t Configuration.PARAM_HEAP_SIZE
+
+ This field is used to specify the size of the device heap used for network parameters. The size depends on the size of the parameter binary file. For example, ``jsegnet21v2``'s parameter file, ``tidl_param_jsegnet21v2.bin`` is 2.6MB. Due to alignment reasons, the parameter heap must be 10% larger than the binary file size - in this case, 2.9MB. The constructor for ``Configuration`` sets PARAM_HEAP_SIZE to 9MB. There is one parameter heap for each instance of ``Executor`` .
+
+.. data:: std::size_t Configuration.EXTMEM_HEAP_SIZE
+
+ This field is used to specify the size of the device heap used for all allocations other than network parameters. The constructor for ``Configuration`` sets EXTMEM_HEAP_SIZE to 64MB. There is one external memory heap for each instance of ``ExecutionObject``
+
+API Reference
+-------------
+
+.. doxygennamespace:: tidl
:project: TIDL
:members: