index 669020fe8345a5a00e8553344617257f5050fb9c..9c696ad8b6cc0f3bf301cc754c7f0747ec640db9 100644 (file)
--- a/docs/source/example.rst
+++ b/docs/source/example.rst
When there is a requirement to run the SSD networks non-partitioned,
for example, the SoC only has C66x cores but not EVE cores,
use ``-e 0`` to run the full network only on C66x cores, without partitioning.
-When running full network with C66x DSP cores, jdetnet works fine with default
-heap sizes. jdetnet_voc requires slightly larger heap size and can be run
-with environment variable, e.g.
-``TIDL_NETWORK_HEAP_SIZE_DSP=75000000 ./ssd_multibox -d 1 -e 0``.
.. _mnist-example: