index 28486ccb4d4d33690cdfcc744313504d2f7408e6..608c728d4ea94f78623ca9a6e9460b397f21414e 100644 (file)
--- a/docs/source/example.rst
+++ b/docs/source/example.rst
- OpenCV used to read input image from file or capture from camera.
* - classification
- Classification example, called from the Matrix GUI.
- -
+ - EVE or C66x
- OpenCV used to read input image from file or capture from camera.
+ * - mcbench
+ - Used to benchmark supported networks. Refer ``mcbench/scripts`` for command line options.
+ - EVE or C66x
+ - Pre-processed image read from file.
* - layer_output
- Illustrates using TIDL APIs to access output buffers of intermediate :term:`layers<Layer>` in the network.
- EVE or C66x