Add documentation for examples
[tidl/tidl-api.git] / docs / source / example.rst
index 09711a74c9b24e44f15a247a07b96a5e031df6a9..961e830b4968b9171b9132f68851af1c253cef85 100644 (file)
-******************
-Using the TINN API
-******************
+********
+Examples
+********
 
-This example illustrates using the TI Neural Network (TINN) API to offload deep learning network processing from a Linux application to the C66x DSPs or DLAs on AM57x devices.
+We ship three end-to-end examples within the tidl-api packge
+to demonstrate three categories of deep learning networks.  The first
+two examples can run on AM57x SoCs with either DLA or DSP.  The last
+example requires AM57x SoCs with both DLA and DSP.  The performance
+numbers that we present here were obtained on an AM5729 EVM, which
+includes 2 ARM A15 cores running at 1.5GHz, 4 DLA cores at 535MHz, and
+2 DSP cores at 750MHz.
 
-Step 1
-======
+Imagenet
+--------
 
-Determine if there are any TINN capable devices on the AM57x SoC:
+The imagenet example takes an image as input and outputs 1000 probabilities.
+Each probability corresponds to one object in the 1000 objects that the
+network is pre-trained with.  Our example outputs top 5 probabilities
+as the most likely objects that the input image can be.
 
-.. code-block:: c++
+The following figure and tables shows an input image, top 5 predicted
+objects as output, and the processing time on either DLA or DSP.
 
-    uint32_t num_dla = Executor::GetNumDevices(DeviceType::DLA);
-    uint32_t num_dsp = Executor::GetNumDevices(DeviceType::DSP);
+.. image:: ../../examples/test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
+   :width: 600
 
-Step 2
-======
-Create a Configuration object by reading it from a file or by initializing it directly. The example below parses a configuration file and initializes the Configuration object. See ``tidl/testvecs/config/infer`` for examples of configuration files.
+.. table::
 
-.. code::
+    ==== ============== ============
+    Rank Object Classes Probability
+    ==== ============== ============
+    1    tabby          0.996
+    2    Egyptian_cat   0.977
+    3    tiger_cat      0.973
+    4    lynx           0.941
+    5    Persian_cat    0.922
+    ==== ============== ============
 
-    Configuration configuration;
-    bool status = configuration.ReadFromFile(config_file);
+.. table::
 
-.. note::
-    Refer TINN Translation Tool documentation for creating TINN network and parameter binary files from TensorFlow and Caffe.
+   ====================== ==================== ============
+   Device Processing Time Host Processing Time API Overhead
+   ====================== ==================== ============
+   DLA: 123.1 ms          124.7 ms             1.34 %
+   **OR**
+   DSP: 117.9 ms          119.3 ms             1.14 %
+   ====================== ==================== ============
 
-Step 3
-======
-Create an Executor with the approriate device type, set of devices and a configuration. In the snippet below, an Executor is created on 2 DLAs.
+The particular network that we ran in this category, jacintonet11v2,
+has 14 layers.  User can specify whether to run the network on DLA or DSP
+for acceleration.  We can see that DLA time is slightly higher than DSP time.
+Host time includes the OpenCL runtime overhead and the time to copy user
+input data into padded TIDL buffers.  We can see that the overall overhead
+is less than 1.5%.
 
-.. code-block:: c++
+Segmentation
+------------
 
-        DeviceIds ids = {DeviceId::ID0, DeviceId::ID1};
-        Executor executor(DeviceType::DLA, ids, configuration);
+The segmentation example takes an image as input and performs pixel-level
+classification according to pre-trained categories.  The following figures
+show a street scene as input and the scene overlaid with pixel-level
+classifications as output: road in green, pedestrians in red, vehicles
+in blue and background in gray.
 
-Step 4
-======
-Get the set of available ExecutionObjects and allocate input and output buffers for each ExecutionObject.
+.. image:: ../../examples/test/testvecs/input/roads/pexels-photo-972355.jpeg
+   :width: 600
 
-.. code-block:: c++
+.. image:: images/pexels-photo-972355-seg.jpg
+   :width: 600
 
-        const ExecutionObjects& execution_objects = executor.GetExecutionObjects();
-        int num_eos = execution_objects.size();
+The network we ran in this category is jsegnet21v2, which has 26 layers.
+From the reported time in the following table, we can see that this network
+runs significantly faster on DLA than on DSP.
 
-        // Allocate input and output buffers for each execution object
-        std::vector<void *> buffers;
-        for (auto &eo : execution_objects)
-        {
-            ArgInfo in  = { ArgInfo(malloc(frame_sz), frame_sz)};
-            ArgInfo out = { ArgInfo(malloc(frame_sz), frame_sz)};
-            eo->SetInputOutputBuffer(in, out);
+.. table::
 
-            buffers.push_back(in.ptr());
-            buffers.push_back(out.ptr());
-        }
+   ====================== ==================== ============
+   Device Processing Time Host Processing Time API Overhead
+   ====================== ==================== ============
+   DLA: 296.5 ms          303.3 ms             2.26 %
+   **OR**
+   DSP: 812.0 ms          818.4 ms             0.79 %
+   ====================== ==================== ============
 
+SSD
+---
 
+SSD is the abbreviation for Single Shot multi-box Detector.
+The ssd_multibox example takes an image as input and detects multiple
+objects with bounding boxes according to pre-trained categories.
+The following figures show another street scene as input and the scene
+with recognized objects boxed as output: pedestrians in red,
+vehicles in blue and road signs in yellow.
 
-Step 5
-======
-Run the network on each input frame.  The frames are processed with available execution objects in a pipelined manner with additional num_eos iterations to flush the pipeline (epilogue).
+.. image:: ../../examples/test/testvecs/input/roads/pexels-photo-378570.jpeg
+   :width: 600
 
-.. code-block:: c++
+.. image:: images/pexels-photo-378570-ssd.jpg
+   :width: 600
 
-        for (int frame_idx = 0; frame_idx < configuration.numFrames + num_eos; frame_idx++)
-        {
-            ExecutionObject* eo = execution_objects[frame_idx % num_eos].get();
+The network can be run entirely on either DLA or DSP.  But the best
+performance comes with running the first 30 layers on DLA and the
+next 13 layers on DSP, for this particular jdetnet_ssd network.
+Note the **AND** in the following table for the reported time.
+Our end-to-end example shows how easy it is to assign a layers group id
+to an *Executor* and how easy it is to connect the output from one
+*ExecutionObject* to the input to another *ExecutionObject*.
 
-            // Wait for previous frame on the same eo to finish processing
-            if (eo->ProcessFrameWait())
-                WriteFrame(*eo, output_data_file);
+.. table::
 
-            // Read a frame and start processing it with current eo
-            if (ReadFrame(*eo, frame_idx, configuration, input_data_file))
-                eo->ProcessFrameStartAsync();
-        }
+   ====================== ==================== ============
+   Device Processing Time Host Processing Time API Overhead
+   ====================== ==================== ============
+   DLA: 175.2 ms          179.1 ms             2.14 %
+   **AND**
+   DSP:  21.1 ms           22.3 ms             5.62 %
+   ====================== ==================== ============
 
+Running Examples
+----------------
 
+The examples are located in ``/usr/share/ti/tidl-api/examples`` on
+the EVM filesystem.  Each example needs to be run its own directory.
+Running an example with ``-h`` will show help message with option set.
+The following code section shows how to run the examples, and
+the test program that tests all supported TIDL network configs.
 
-Putting it together
-===================
-The code snippet :ref:`tidl_main` illustrates using the API to offload a network.
+.. code:: shell
 
-.. literalinclude:: ../../examples/test/main.cpp
-    :name: tidl_main
-    :caption: examples/test/main.cpp
-    :lines: 161-195,213-218,220-225
-    :linenos:
+   root@am57xx-evm:~# cd /usr/share/ti/tidl-api/examples/imagenet/
+   root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# make -j4
+   root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# ./imagenet -t d
+   Input: ../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
+   frame[0]: Time on device:  117.9ms, host:  119.3ms API overhead:   1.17 %
+   1: tabby, prob = 0.996
+   2: Egyptian_cat, prob = 0.977
+   3: tiger_cat, prob = 0.973
+   4: lynx, prob = 0.941
+   5: Persian_cat, prob = 0.922
+   imagenet PASSED
 
-For a complete example of using the API, refer ``tinn/examples/opencl/tidl/main.cpp`` on the EVM filesystem.
+   root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# cd ../segmentation/; make -j4
+   root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# ./segmentation -i ../test/testvecs/input/roads/pexels-photo-972355.jpeg
+   Input: ../test/testvecs/input/roads/pexels-photo-972355.jpeg
+   frame[0]: Time on device:  296.5ms, host:  303.2ms API overhead:   2.21 %
+   Saving frame 0 overlayed with segmentation to: overlay_0.png
+   segmentation PASSED
+
+   root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# cd ../ssd_multibox/; make -j4
+   root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# ./ssd_multibox -i ../test/testvecs/input/roads/pexels-photo-378570.jpeg
+   Input: ../test/testvecs/input/roads/pexels-photo-378570.jpeg
+   frame[0]: Time on DLA:  175.2ms, host:    179ms API overhead:    2.1 %
+   frame[0]: Time on DSP:  21.06ms, host:  22.43ms API overhead:   6.08 %
+   Saving frame 0 with SSD multiboxes to: multibox_0.png
+   Loop total time (including read/write/print/etc):  423.8ms
+   ssd_multibox PASSED
+
+   root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# cd ../test; make -j4
+   root@am57xx-evm:/usr/share/ti/tidl-api/examples/test# ./test_tidl
+   API Version: 01.00.00.d91e442
+   Running dense_1x1 on 2 devices, type EVE
+   frame[0]: Time on device:  134.3ms, host:  135.6ms API overhead:  0.994 %
+   dense_1x1 : PASSED
+   Running j11_bn on 2 devices, type EVE
+   frame[0]: Time on device:  176.2ms, host:  177.7ms API overhead:  0.835 %
+   j11_bn : PASSED
+   Running j11_cifar on 2 devices, type EVE
+   frame[0]: Time on device:  53.86ms, host:  54.88ms API overhead:   1.85 %
+   j11_cifar : PASSED
+   Running j11_controlLayers on 2 devices, type EVE
+   frame[0]: Time on device:  122.9ms, host:  123.9ms API overhead:  0.821 %
+   j11_controlLayers : PASSED
+   Running j11_prelu on 2 devices, type EVE
+   frame[0]: Time on device:  300.8ms, host:  302.1ms API overhead:  0.437 %
+   j11_prelu : PASSED
+   Running j11_v2 on 2 devices, type EVE
+   frame[0]: Time on device:  124.1ms, host:  125.6ms API overhead:   1.18 %
+   j11_v2 : PASSED
+   Running jseg21 on 2 devices, type EVE
+   frame[0]: Time on device:    367ms, host:    374ms API overhead:   1.88 %
+   jseg21 : PASSED
+   Running jseg21_tiscapes on 2 devices, type EVE
+   frame[0]: Time on device:  302.2ms, host:  308.5ms API overhead:   2.02 %
+   frame[1]: Time on device:  301.9ms, host:  312.5ms API overhead:   3.38 %
+   frame[2]: Time on device:  302.7ms, host:  305.9ms API overhead:   1.04 %
+   frame[3]: Time on device:  301.9ms, host:    305ms API overhead:   1.01 %
+   frame[4]: Time on device:  302.7ms, host:  305.9ms API overhead:   1.05 %
+   frame[5]: Time on device:  301.9ms, host:  305.5ms API overhead:   1.17 %
+   frame[6]: Time on device:  302.7ms, host:  305.9ms API overhead:   1.06 %
+   frame[7]: Time on device:  301.9ms, host:    305ms API overhead:   1.02 %
+   frame[8]: Time on device:    297ms, host:  300.3ms API overhead:   1.09 %
+   Comparing frame: 0
+   jseg21_tiscapes : PASSED
+   Running smallRoi on 2 devices, type EVE
+   frame[0]: Time on device:  2.548ms, host:  3.637ms API overhead:   29.9 %
+   smallRoi : PASSED
+   Running squeeze1_1 on 2 devices, type EVE
+   frame[0]: Time on device:  292.9ms, host:  294.6ms API overhead:  0.552 %
+   squeeze1_1 : PASSED
+
+   Multiple Executor...
+   Running network tidl_config_j11_v2.txt on EVEs: 1  in thread 0
+   Running network tidl_config_j11_cifar.txt on EVEs: 0  in thread 1
+   Multiple executors: PASSED
+   Running j11_bn on 2 devices, type DSP
+   frame[0]: Time on device:  170.5ms, host:  171.5ms API overhead:  0.568 %
+   j11_bn : PASSED
+   Running j11_controlLayers on 2 devices, type DSP
+   frame[0]: Time on device:  416.4ms, host:  417.1ms API overhead:  0.176 %
+   j11_controlLayers : PASSED
+   Running j11_v2 on 2 devices, type DSP
+   frame[0]: Time on device:    118ms, host:  119.2ms API overhead:   1.01 %
+   j11_v2 : PASSED
+   Running jseg21 on 2 devices, type DSP
+   frame[0]: Time on device:   1123ms, host:   1128ms API overhead:  0.443 %
+   jseg21 : PASSED
+   Running jseg21_tiscapes on 2 devices, type DSP
+   frame[0]: Time on device:  812.3ms, host:  817.3ms API overhead:  0.614 %
+   frame[1]: Time on device:  812.6ms, host:  818.6ms API overhead:  0.738 %
+   frame[2]: Time on device:  812.3ms, host:  815.1ms API overhead:  0.343 %
+   frame[3]: Time on device:  812.7ms, host:  815.2ms API overhead:  0.312 %
+   frame[4]: Time on device:  812.3ms, host:  815.1ms API overhead:  0.353 %
+   frame[5]: Time on device:  812.6ms, host:  815.1ms API overhead:  0.302 %
+   frame[6]: Time on device:  812.2ms, host:  815.1ms API overhead:  0.357 %
+   frame[7]: Time on device:  812.6ms, host:  815.2ms API overhead:  0.315 %
+   frame[8]: Time on device:    812ms, host:    815ms API overhead:  0.367 %
+   Comparing frame: 0
+   jseg21_tiscapes : PASSED
+   Running smallRoi on 2 devices, type DSP
+   frame[0]: Time on device:  14.21ms, host:  14.94ms API overhead:   4.89 %
+   smallRoi : PASSED
+   Running squeeze1_1 on 2 devices, type DSP
+   frame[0]: Time on device:    960ms, host:  961.1ms API overhead:  0.116 %
+   squeeze1_1 : PASSED
+   tidl PASSED
+
+Possible runtime errors: out of memory
+""""""""""""""""""""""""""""""""""""""
+
+.. code:: shell
+
+   tidl: device_alloc.h:31: T* tidl::malloc_ddr(size_t) [with T = char; size_t = unsigned int]: Assertion `val != nullptr' failed
+
+One possible reason is that previous aborted runs didn't properly release
+allocation.  Use ti-mct-heap-check with "-c" option to clean up.
+
+.. code:: shell
+
+   root@am57xx-evm:~# ti-mct-heap-check -c
+   -- ddr_heap1 ------------------------------
+      Addr : 0xa2000000
+      Size : 0xa000000
+      Avail: 0xa000000
+      Align: 0x80
+   -----------------------------------------
+
+Another possible reason is that total memory requirement exceeds default
+memory allocated for OpenCL.  See below how to patch device tree to
+increase OpenCL memory.
+
+.. code:: shell
+
+   $ sudo apt-get install device-tree-compiler # In case dtc is not already installed
+   $ scp root@am57:/boot/am57xx-evm-reva3.dtb .
+   $ dtc -I dtb -O dts am57xx-evm-reva3.dtb -o am57xx-evm-reva3.dts
+   $ cp am57xx-evm-reva3.dts am57xx-evm-reva3.dts.orig
+   $ # increase cmem block size
+   $ diff -u am57xx-evm-reva3.dts.orig am57xx-evm-reva3.dts
+   --- am57xx-evm-reva3.dts.orig    2018-01-11 14:47:51.491572739 -0600
+   +++ am57xx-evm-reva3.dts    2018-01-16 15:43:33.981431971 -0600
+   @@ -5657,7 +5657,7 @@
+            };
+
+            cmem_block_mem@a0000000 {
+   -            reg = <0x0 0xa0000000 0x0 0xc000000>;
+   +            reg = <0x0 0xa0000000 0x0 0x18000000>;
+                no-map;
+                status = "okay";
+                linux,phandle = <0x13c>;
+   @@ -5823,7 +5823,7 @@
+            cmem_block@0 {
+                reg = <0x0>;
+                memory-region = <0x13c>;
+   -            cmem-buf-pools = <0x1 0x0 0xc000000>;
+   +            cmem-buf-pools = <0x1 0x0 0x18000000>;
+            };
+
+            cmem_block@1 {
+   $ dtc -I dts -O dtb am57xx-evm-reva3.dts -o am57xx-evm-reva3.dtb
+   $ scp am57xx-evm-reva3.dtb root@am57:/boot/
+   # reboot to make memory changes effective (run "cat /proc/iomem" to check)