index 8ed6be2f5d6616b23b04da7919f5e303e013e74a..531bb6dc2bb9798156a4717d7305f338aeb72e68 100644 (file)
/*! @class Configuration
@brief Specifies the configuration required for a network
/*! @class Configuration
@brief Specifies the configuration required for a network
+
+ The Configuration object is used to specify various parameters required
+ for network execution. Applications can directly initialize fields in an
+ instance of Configuration or use the ReadFromFile method to read the
+ configuration from a file.
*/
*/
+
class Configuration
{
public:
class Configuration
{
public:
//! Number of frames of input data (can be 0 if data is not read from file)
int numFrames;
//! Number of frames of input data (can be 0 if data is not read from file)
int numFrames;
- //! Height of the input frame
+ //! Height of the input image. Used by the API, must be specified.
int inHeight;
int inHeight;
- //! Width of the input frame
+ //! Width of the input image. Used by the API, must be specified.
int inWidth;
//! Number of channels in the input frame (e.g. 3 for BGR)
int inWidth;
//! Number of channels in the input frame (e.g. 3 for BGR)
+ //! Used by the API, must be specified.
int inNumChannels;
//! @private
int inNumChannels;
//! @private
//! outputs of previous layersGroupId, instead of from user application
bool enableInternalInput;
//! outputs of previous layersGroupId, instead of from user application
bool enableInternalInput;
- //! Size of the device side heap, used for allocating memory required to
+ //! @brief Size of the device side network heap
+ //! This heap is used for allocating memory required to
//! run the network on the device. One per Execution Object.
size_t NETWORK_HEAP_SIZE;
//! run the network on the device. One per Execution Object.
size_t NETWORK_HEAP_SIZE;
- //! Size of the heap used for parameter data. One per Executor.
+ //! @brief Size of the device side heap used for parameter data.
+ //! The size depends on the size of the parameter binary file. The
+ //! constructor for ``Configuration`` sets PARAM_HEAP_SIZE to 9MB.
+ //! There is one parameter heap for each instance of ``Executor`` .
size_t PARAM_HEAP_SIZE;
size_t PARAM_HEAP_SIZE;
- //! @brief Location of the input file
- //! Can be empty if input data is provided by frameworks such as OpenCV.
+ //! @brief Path to the input image file.
+ //! This field is not used by the TIDL API itself. It can be used by
+ //! applications to load an input image into a buffer. Can be empty if
+ //! the application uses frameworks such as OpenCV to read images. Refer
+ //! examples/test/main.cpp for usage.
std::string inData;
std::string inData;
- //! Location of the output file
- //! Can be empty if output data is consumed by frameworks such as OpenCV.
+ //! @brief Path to the output image file.
+ //! This field is not used by the TIDL API itself. It can be used by
+ //! applications to specify a name for the output file. Can be empty
+ //! if the application uses frameworks such as OpenCV to read images.
+ //! Refer examples/test/main.cpp for usage.
std::string outData;
std::string outData;
- //! Path to the TIDL network binary file
+ //! Path to the TIDL network binary file.
+ //! Used by the API, must be specified.
std::string netBinFile;
//! Path to the TIDL parameter binary file
std::string netBinFile;
//! Path to the TIDL parameter binary file
+ //! Used by the API, must be specified.
std::string paramsBinFile;
std::string paramsBinFile;
+ //! Map of layer index to layer group id. Used to override layer group
+ //! assigment for layers. Any layer not specified in this map will
+ //! retain its existing mapping.
+ std::map<int, int> layerIndex2LayerGroupId;
+
//! Enable tracing of output buffers associated with each layer
bool enableOutputTrace;
//! Enable tracing of output buffers associated with each layer
bool enableOutputTrace;
//! Debug - Shows total size of PARAM and NETWORK heaps. Also shows bytes
//! available after all allocations. Can be used to adjust the heap
//! Debug - Shows total size of PARAM and NETWORK heaps. Also shows bytes
//! available after all allocations. Can be used to adjust the heap
- //! size
+ //! size.
bool showHeapStats;
bool showHeapStats;
- //! Map of layer index to layer group id. Used to override layer group
- //! assigment for layers. Any layer not specified in this map will
- //! retain its existing mapping.
- std::map<int, int> layerIndex2LayerGroupId;
-
//! Default constructor.
Configuration();
//! Validate the fields in the configuration object
bool Validate() const;
//! Default constructor.
Configuration();
//! Validate the fields in the configuration object
bool Validate() const;
- //! Print the configuration
+ //! Debug - Print the configuration.
void Print(std::ostream& os = std::cout) const;
//! Read a configuration from the specified file and validate
void Print(std::ostream& os = std::cout) const;
//! Read a configuration from the specified file and validate