index 531bb6dc2bb9798156a4717d7305f338aeb72e68..913272a7f2bc1954e156507f448befdfb0eb01d8 100644 (file)
//! Force to run all layers, regardless of layersGroupId partitioning
bool runFullNet;
- //! When set, inputs are taken from TIDL internal buffers that contain
- //! outputs of previous layersGroupId, instead of from user application
- bool enableInternalInput;
-
//! @brief Size of the device side network heap
//! This heap is used for allocating memory required to
//! run the network on the device. One per Execution Object.
//! size.
bool showHeapStats;
+ int quantHistoryParam1;
+ int quantHistoryParam2;
+ int quantMargin;
+
//! Default constructor.
Configuration();