ExecutionObjectPipeline for executing layersGroups
[tidl/tidl-api.git] / tidl_api / inc / execution_object.h
index e78ad2e98f0ec8ffd4305536bca46c368dbb4f3b..c1d86fc126bb8e243a67df04d30bfb5c3aca63d8 100644 (file)
@@ -31,6 +31,7 @@
 #pragma once
 
 #include <memory>
+#include "execution_object_internal.h"
 
 namespace tidl {
 
@@ -39,13 +40,12 @@ class Device;
 class LayerOutput;
 class IODeviceArgInfo;
 
-typedef std::vector<std::unique_ptr<const LayerOutput>> LayerOutputs;
 
 /*! @class ExecutionObject
     @brief Runs the TIDL network on an OpenCL device
 */
 
-class ExecutionObject
+class ExecutionObject : public ExecutionObjectInternalInterface
 {
     public:
 
@@ -55,6 +55,8 @@ class ExecutionObject
                         const  ArgInfo& create_arg,
                         const  ArgInfo& param_heap_arg,
                         size_t extmem_heap_size,
+                        int    layersGroupId,
+                        bool   output_trace,
                         bool   internal_input);
         //! @private
         ~ExecutionObject();
@@ -62,52 +64,56 @@ class ExecutionObject
         //! Specify the input and output buffers used by the EO
         //! @param in buffer used for input.
         //! @param out buffer used for output.
-        void SetInputOutputBuffer (const ArgInfo& in, const ArgInfo& out);
+        void SetInputOutputBuffer(const ArgInfo& in,
+                                  const ArgInfo& out) override;
 
         //! Returns a pointer to the input buffer set via SetInputOutputBuffer
-        char* GetInputBufferPtr() const;
+        char* GetInputBufferPtr() const override;
 
         //! Returns size of the input buffer
-        size_t GetInputBufferSizeInBytes() const;
+        size_t GetInputBufferSizeInBytes() const override;
+
+        //! Returns a pointer to the output buffer
+        char* GetOutputBufferPtr() const override;
+
+        //! Returns size of the output buffer
+        size_t GetOutputBufferSizeInBytes() const override;
 
         //! @brief Set the frame index of the frame currently processed by the
         //! ExecutionObject. Used for trace/debug messages
         //! @param idx index of the frame
-        void  SetFrameIndex(int idx);
+        void  SetFrameIndex(int idx) override;
 
         //! Returns the index of a frame being processed (set by SetFrameIndex)
-        int   GetFrameIndex() const;
-
-        //! Returns a pointer to the output buffer
-        char* GetOutputBufferPtr() const;
-
-        //! Returns the number of bytes written to the output buffer
-        size_t GetOutputBufferSizeInBytes() const;
+        int   GetFrameIndex() const override;
 
-        //! @brief Start processing a frame. The call is asynchronous and returns
-        //! immediately. Use ExecutionObject::ProcessFrameWait to wait
-        bool ProcessFrameStartAsync();
+        //! @brief Start processing a frame. The call is asynchronous and
+        //! returns immediately. Use ExecutionObject::ProcessFrameWait to wait
+        bool ProcessFrameStartAsync() override;
 
         //! Wait for the execution object to complete processing a frame
         //! @return false if ExecutionObject::ProcessFrameWait was called
         //! without a corresponding call to
         //! ExecutionObject::ProcessFrameStartAsync.
-        bool ProcessFrameWait();
-
-        //! @brief return the number of cycles taken *on the device* to
-        //! execute the process call
-        //! @return Number of cycles to process a frame on the device.
-        uint64_t GetProcessCycles() const;
+        bool ProcessFrameWait() override;
 
         //! @brief return the number of milliseconds taken *on the device* to
         //! execute the process call
         //! @return Number of milliseconds to process a frame on the device.
-        float    GetProcessTimeInMilliSeconds() const;
+        float GetProcessTimeInMilliSeconds() const override;
+
+        //! @brief return the number of milliseconds taken *on the host* to
+        //! execute the process call
+        //! @return Number of milliseconds to process a frame on the host.
+        float GetHostProcessTimeInMilliSeconds() const override;
+
+        //! Returns the device name that the ExecutionObject runs on
+        const std::string& GetDeviceName() const override;
 
         //! Write the output buffer for each layer to a file
-        //! <filename_prefix>_<ID>_HxW.bin
+        //! \<filename_prefix>_<ID>_HxW.bin
         void WriteLayerOutputsToFile(const std::string& filename_prefix=
-                                     "trace_dump_") const;
+                                     "trace_dump_") const override;
 
         //! Returns a LayerOutput object corresponding to a layer.
         //! Caller is responsible for deleting the LayerOutput object.
@@ -116,10 +122,13 @@ class ExecutionObject
         //! @param output_index The output index of the buffer for a given
         //!                     layer. Defaults to 0.
         const LayerOutput* GetOutputFromLayer(uint32_t layer_index,
-                                              uint32_t output_index=0) const;
+                                       uint32_t output_index=0) const override;
 
         //! Get output buffers from all layers
-        const LayerOutputs* GetOutputsFromAllLayers() const;
+        const LayerOutputs* GetOutputsFromAllLayers() const override;
+
+        //! Returns the layersGrupId that the ExecutionObject is processing
+        int   GetLayersGroupId() const;
 
         //! @private
         // Used by the Executor
@@ -127,12 +136,16 @@ class ExecutionObject
         bool RunAsync(CallType ct);
         bool Wait    (CallType ct);
 
+        //! @private
+        // Used by the ExecutionObjectPipeline
+        bool AddCallback(CallType ct, void *user_data);
+        void AcquireLock();
+        void ReleaseLock();
+
         ExecutionObject()                                  = delete;
         ExecutionObject(const ExecutionObject&)            = delete;
         ExecutionObject& operator=(const ExecutionObject&) = delete;
 
-        void EnableOutputBufferTrace();
-
         //! @private
         void SetInputOutputBuffer(const IODeviceArgInfo* in,
                                   const IODeviceArgInfo* out);