index 98b542a0618055dcf283c1360ac32768431e7004..ccc088180dd975e92e79e2e01ee0ce3f55873996 100644 (file)
/******************************************************************************
- * Copyright (c) 2017 Texas Instruments Incorporated - http://www.ti.com/
+ * Copyright (c) 2017-2018 Texas Instruments Incorporated - http://www.ti.com/
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
class Kernel;
class Device;
+class LayerOutput;
+
+typedef std::vector<std::unique_ptr<const LayerOutput>> LayerOutputs;
/*! @class ExecutionObject
@brief Runs the TIDL network on an OpenCL device
//! @return Number of milliseconds to process a frame on the device.
float GetProcessTimeInMilliSeconds() const;
+ //! Write the output buffer for each layer to a file
+ //! <filename_prefix>_<ID>_HxW.bin
+ void WriteLayerOutputsToFile(const std::string& filename_prefix=
+ "trace_dump_") const;
+
+ //! Returns a LayerOutput object corresponding to a layer.
+ //! Caller is responsible for deleting the LayerOutput object.
+ //! @see LayerOutput
+ //! @param layer_index The layer index of the layer
+ //! @param output_index The output index of the buffer for a given
+ //! layer. Defaults to 0.
+ const LayerOutput* GetOutputFromLayer(uint32_t layer_index,
+ uint32_t output_index=0) const;
+
+ //! Get output buffers from all layers
+ const LayerOutputs* GetOutputsFromAllLayers() const;
+
//! @private
// Used by the Executor
enum class CallType { INIT, PROCESS, CLEANUP };
ExecutionObject(const ExecutionObject&) = delete;
ExecutionObject& operator=(const ExecutionObject&) = delete;
+ void EnableOutputBufferTrace();
+
private:
class Impl;
std::unique_ptr<Impl> pimpl_m;
};
+
+/*! @class LayerOutput
+ @brief Describes the output of a layer in terms of its shape. Also
+ includes a pointer to the data.
+*/
+class LayerOutput
+{
+ public:
+ //! @private
+ //! Constructor called within API, not by the user
+ LayerOutput(int layer_index, int output_index, int buffer_id,
+ int num_roi_m, int num_channels, size_t height,
+ size_t width, const char* data);
+
+ //! Must be called to delete the data pointer.
+ ~LayerOutput();
+
+ //! @return The index of a layer
+ int LayerIndex() const { return layer_index_m; }
+
+ //! @return The number of channels associated with an output
+ int NumberOfChannels() const { return num_channels_m; }
+
+ //! @return The height of the output. Can be 1 for 1D outputs
+ size_t Height() const { return height_m; }
+
+ //! @return The width of the output
+ size_t Width() const { return width_m; }
+
+ //! @return Size of the output in bytes
+ size_t Size() const { return height_m * width_m *
+ num_channels_m; }
+ //! @return Pointer to output. Must call destructor to free the
+ //! memory used to hold the output.
+ const char* Data() const { return data_m; }
+
+ //! @private Disable copy construction and assignment since
+ //! class holds a pointer to allocated data
+ LayerOutput(const LayerOutput&) = delete;
+ LayerOutput& operator= (const LayerOutput&) = delete;
+
+ private:
+ int layer_index_m;
+ int output_index_m;
+ int buffer_id_m;
+ int num_roi_m;
+ int num_channels_m;
+ size_t height_m;
+ size_t width_m;
+ const char* data_m;
+};
+
+
} // namespace tidl