index 816da94adeffa9b45810646a8a683af75708a500..e9da88b7249c0c4ce3ad31f5b6754ada73370aee 100644 (file)
//! ExecutionObject::ProcessFrameStartAsync.
virtual bool ProcessFrameWait() =0;
- //! @brief return the number of milliseconds taken *on the device* to
- //! execute the process call
- //! @return Number of milliseconds to process a frame on the device.
- virtual float GetProcessTimeInMilliSeconds() const =0;
-
- //! @brief return the number of milliseconds taken *on the host* to
- //! execute the process call
- //! @return Number of milliseconds to process a frame on the host.
- virtual float GetHostProcessTimeInMilliSeconds() const =0;
-
//! Returns the device name that the ExecutionObject runs on
virtual const std::string& GetDeviceName() const =0;