Reduce complexity of ssd_multibox example
[tidl/tidl-api.git] / tinn_api / inc / configuration.h
index a707a8553704686e84322bf553d72862692ee386..088a6291a413af379087acc12d7005826b293128 100644 (file)
@@ -59,12 +59,13 @@ class Configuration
     //! Specific to each network, can take values from 0 to 4, default is 0
     int     preProcType;
 
-    //! layersGroupId in the network that the executor should work on
-    int     layersGroupId;
-
     //! Force to run all layers, regardless of layersGroupId partitioning
     int     runFullNet;
 
+    //! When set, inputs are taken from TIDL internal buffers that contain
+    //! outputs of previous layersGroupId, instead of from user application
+    int     enableInternalInput;
+
     //! Size of the TI DL per Execution Object heap
     size_t EXTMEM_HEAP_SIZE;