X-Git-Url: https://git.ti.com/gitweb?p=tidl%2Ftidl-api.git;a=blobdiff_plain;f=docs%2Fsource%2Fapi.rst;h=7aa7849a9f542b8d1152cfc2184c7500d34cc0c0;hp=c692b05a12284d8d67392a9ffcd9ad9f3a5e7ac2;hb=7b65cbba3878d793ff0c2480bc31ae28a9fa6e67;hpb=fca106efb6d808d832f26caefa5018076a2319da;ds=sidebyside diff --git a/docs/source/api.rst b/docs/source/api.rst index c692b05..7aa7849 100644 --- a/docs/source/api.rst +++ b/docs/source/api.rst @@ -1,7 +1,64 @@ +.. _api-documentation: + ****************** TIDL API Reference ****************** +Configuration +------------- +The ``Configuration`` object is used to specify various parameters required for network execution. Applications can directly initialize fields in an instance of ``Configuration`` or use the ``ReadFromFile`` method to read the configuration from a file. The following sections describe the commonly used fields available in the ``Configuration`` class: + +Input image description ++++++++++++++++++++++++ +.. data:: std::string Configuration.inData + + Path to the input image file. This field is not used by the TIDL API itself. It can be used by applications to load an input image into a buffer. Can be empty if the application uses frameworks such as OpenCV to read images. See ``test/main.cpp`` for example usage. + +.. data:: std::size_t Configuration.inHeight + + Height of the input image. Used by the API, must be specified. + +.. data:: std::size_t Configuration.inWidth + + Width of the input image. Used by the API, must be specified. + +.. data:: std::size_t Configuration.inNumChannels + + Number of channels in the input image. Used by the API, must be specified. + +Output description +++++++++++++++++++ + +.. data:: std::string Configuration.outData + + Path to the output image file. This field is not used by the TIDL API itself. It can be used by applications to write a buffer to file. Can be empty if the application uses frameworks such as OpenCV to read images. See ``test/main.cpp`` for example usage. + +Network ++++++++ + +.. data:: std::string Configuration.netBinFile + + Path to the TIDL network binary file. Used by the API, must be specified. + +.. data:: std::string Configuration.paramBinFile + + Path to the TIDL parameter file. Used by the API, must be specified. + +Memory Management ++++++++++++++++++ +The ``Configuration`` object specifies the sizes of 2 heaps. These heaps are allocated from OpenCL global memory that is shared across the host and device. Refer section :ref:`opencl-global-memory` for steps to increase the size of the OpenCL global memory heap. + +.. data:: std::size_t Configuration.PARAM_HEAP_SIZE + + This field is used to specify the size of the device heap used for network parameters. The size depends on the size of the parameter binary file. For example, ``jsegnet21v2``'s parameter file, ``tidl_param_jsegnet21v2.bin`` is 2.6MB. Due to alignment reasons, the parameter heap must be 10% larger than the binary file size - in this case, 2.9MB. The constructor for ``Configuration`` sets PARAM_HEAP_SIZE to 9MB. There is one parameter heap for each instance of ``Executor`` . + +.. data:: std::size_t Configuration.EXTMEM_HEAP_SIZE + + This field is used to specify the size of the device heap used for all allocations other than network parameters. The constructor for ``Configuration`` sets EXTMEM_HEAP_SIZE to 64MB. There is one external memory heap for each instance of ``ExecutionObject`` + +API Reference +------------- + .. doxygennamespace:: tidl :project: TIDL :members: