summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 2f0aa48)
raw | patch | inline | side by side (parent: 2f0aa48)
author | Yuan Zhao <yuanzhao@ti.com> | |
Wed, 19 Dec 2018 16:53:18 +0000 (10:53 -0600) | ||
committer | Yuan Zhao <yuanzhao@ti.com> | |
Wed, 19 Dec 2018 16:58:03 +0000 (10:58 -0600) |
- It turns out DSP implementation of InnerProduct layer in TIDL library
requires input size to be multiple of 8, because it is doing
aligned 8-byte loads.
- Original LeNet network used in the MNIST example has a second InnerProduct
layer of size 500, which is not a multiple of 8. Change the size to 504,
re-train the network, re-import into TIDL format. Now the MNIST example
works correctly on DSP as well.
- MCT-1105
requires input size to be multiple of 8, because it is doing
aligned 8-byte loads.
- Original LeNet network used in the MNIST example has a second InnerProduct
layer of size 500, which is not a multiple of 8. Change the size to 504,
re-train the network, re-import into TIDL format. Now the MNIST example
works correctly on DSP as well.
- MCT-1105
index d933cccf9b26edca6f9d3724216792f2f918a2dc..75e128312ae93f5e4312b39789afadc074d81464 100644 (file)
--- a/examples/mnist/main.cpp
+++ b/examples/mnist/main.cpp
exit(EXIT_SUCCESS);
}
assert(opts.num_dsps != 0 || opts.num_eves != 0);
- if (opts.num_dsps != 0)
- {
- cout << "MNIST network not supported on DSP yet." << endl;
- exit(EXIT_SUCCESS);
- }
if (opts.input_file.empty())
{
" different MNIST network. Default is mnist_lenet.\n"
"Optional arguments:\n"
" -c <config> Valid configs: mnist_lenet\n"
+ " -d <number> Number of dsp cores to use\n"
" -e <number> Number of eve cores to use\n"
" -i <images> Path to the MNIST white-on-black images file\n"
" -l <labels> Path to the MNIST labels file\n"
diff --git a/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin b/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin
index ea9ac6caf61b4522dbf831088f246d62b38bd149..96a75833dbca641e333d4c247b484644334f2ed9 100644 (file)
Binary files a/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin and b/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin differ
Binary files a/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin and b/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin differ
diff --git a/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin b/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin
index 66cc8a6b6f26de71da0947d802b3397d4b5c698c..54405aa9bb22a966398c915a27e78004672c4e62 100644 (file)
Binary files a/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin and b/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin differ
Binary files a/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin and b/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin differ