summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (from parent 1: 923d5b5)
raw | patch | inline | side by side (from parent 1: 923d5b5)
author | Yuan Zhao <yuanzhao@ti.com> | |
Mon, 10 Jun 2019 20:12:03 +0000 (15:12 -0500) | ||
committer | Yuan Zhao <yuanzhao@ti.com> | |
Mon, 10 Jun 2019 20:12:03 +0000 (15:12 -0500) |
- Customer reported this problem. unique_ptr that holds an allocated
array was created as "unique_ptr<char>", which will call "delete"
at destruction. However, the array was created with "new char[]".
The proper way should be "unique_ptr<char[]>", so that "delete []"
will be called at destrution.
- One minor trace message update so that we know which type of device
is being dispatched to.
- MCT-1196
array was created as "unique_ptr<char>", which will call "delete"
at destruction. However, the array was created with "new char[]".
The proper way should be "unique_ptr<char[]>", so that "delete []"
will be called at destrution.
- One minor trace message update so that we know which type of device
is being dispatched to.
- MCT-1196
tidl_api/src/ocl_device.cpp | patch | blob | history |
index 864551d3dd7d230e70473a0e1eafb3f0331a09f3..867d7422e553e2a66f24c5a5925422c1e39c1cf9 100644 (file)
Kernel& Kernel::RunAsync(uint32_t context_idx)
{
// Execute kernel
- TRACE::print("\tKernel: device %d executing %s, context %d\n",
+ TRACE::print("\tKernel: %s device %d executing %s, context %d\n",
+ device_m->GetDeviceName().c_str(),
device_index_m, name_m.c_str(), context_idx);
cl_int ret = clEnqueueTask(device_m->queue_m[device_index_m],
kernel_m, 0, 0, &event_m[context_idx]);
err = clGetPlatformInfo(id, CL_PLATFORM_VERSION, 0, nullptr, &length);
if (err != CL_SUCCESS) return false;
- std::unique_ptr<char> version(new char[length]);
+ std::unique_ptr<char[]> version(new char[length]);
err = clGetPlatformInfo(id, CL_PLATFORM_VERSION, length, version.get(),
nullptr);
if (err != CL_SUCCESS) return false;
err = clGetPlatformInfo(id, CL_PLATFORM_NAME, 0, nullptr, &length);
if (err != CL_SUCCESS) return false;
- std::unique_ptr<char> name(new char[length]);
+ std::unique_ptr<char[]> name(new char[length]);
err = clGetPlatformInfo(id, CL_PLATFORM_NAME, length, name.get(), nullptr);
if (err != CL_SUCCESS) return false;