summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 2a68a9f)
raw | patch | inline | side by side (parent: 2a68a9f)
author | Yuan Zhao <yuanzhao@ti.com> | |
Thu, 28 Jun 2018 20:09:32 +0000 (15:09 -0500) | ||
committer | Yuan Zhao <yuanzhao@ti.com> | |
Thu, 28 Jun 2018 20:09:32 +0000 (15:09 -0500) |
- Elaborate device and host processing time in examples
- Clarify reported probability in imagenet example
- MCT-1008
- Clarify reported probability in imagenet example
- MCT-1008
docs/source/example.rst | patch | blob | history |
index 7036d8dff87c1169aaf00b37be9cab339e1bc433..73f88f6067fb6e0a8e396bedf1b968c7a6a2ce5d 100644 (file)
--- a/docs/source/example.rst
+++ b/docs/source/example.rst
includes 2 ARM A15 cores running at 1.5GHz, 4 EVE cores at 535MHz, and
2 DSP cores at 750MHz.
+For each example, we report device processing time, host processing time,
+and TIDL API overhead. Device processing time is measured on the device,
+from the moment processing starts till the moment processing finishes.
+Host processing time is measured on the host, from the moment
+``ProcessFrameStartAsync()`` is called till ``ProcessFrameWait()`` returns
+in user application. It includes the TIDL API overhead, the OpenCL runtime
+overhead, and the time to copy user input data into padded TIDL internal
+buffers.
+
Imagenet
--------
.. table::
- ==== ============== ============
- Rank Object Classes Probability
- ==== ============== ============
+ ==== ============== =====================
+ Rank Object Classes Probability (softmax)
+ ==== ============== =====================
1 tabby 0.996
2 Egyptian_cat 0.977
3 tiger_cat 0.973
4 lynx 0.941
5 Persian_cat 0.922
- ==== ============== ============
+ ==== ============== =====================
.. table::
The particular network that we ran in this category, jacintonet11v2,
has 14 layers. User can specify whether to run the network on EVE or DSP
for acceleration. We can see that EVE time is slightly higher than DSP time.
-Host time includes the OpenCL runtime overhead and the time to copy user
-input data into padded TIDL buffers. We can see that the overall overhead
-is less than 1.5%.
+We can also see that the overall overhead is less than 1.5%.
+
+.. note::
+ The probabilities reported here are the output of the softmax layer
+ in the network, and are not normalized to the real probabilities.
Segmentation
------------