summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: cc121e4)
raw | patch | inline | side by side (parent: cc121e4)
author | Yuan Zhao <yuanzhao@ti.com> | |
Wed, 23 May 2018 17:17:58 +0000 (12:17 -0500) | ||
committer | Yuan Zhao <yuanzhao@ti.com> | |
Wed, 23 May 2018 19:26:44 +0000 (14:26 -0500) |
- MCT-982
docs/source/example.rst | patch | blob | history | |
docs/source/images/pexels-photo-378570-ssd.jpg | [new file with mode: 0644] | patch | blob |
docs/source/images/pexels-photo-972355-seg.jpg | [new file with mode: 0644] | patch | blob |
index 316a6ae316f3cf6e5c1f7d8ac5e6b28aa73b364c..961e830b4968b9171b9132f68851af1c253cef85 100644 (file)
--- a/docs/source/example.rst
+++ b/docs/source/example.rst
Examples
********
+We ship three end-to-end examples within the tidl-api packge
+to demonstrate three categories of deep learning networks. The first
+two examples can run on AM57x SoCs with either DLA or DSP. The last
+example requires AM57x SoCs with both DLA and DSP. The performance
+numbers that we present here were obtained on an AM5729 EVM, which
+includes 2 ARM A15 cores running at 1.5GHz, 4 DLA cores at 535MHz, and
+2 DSP cores at 750MHz.
+
Imagenet
--------
+The imagenet example takes an image as input and outputs 1000 probabilities.
+Each probability corresponds to one object in the 1000 objects that the
+network is pre-trained with. Our example outputs top 5 probabilities
+as the most likely objects that the input image can be.
+
+The following figure and tables shows an input image, top 5 predicted
+objects as output, and the processing time on either DLA or DSP.
+
+.. image:: ../../examples/test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
+ :width: 600
+
+.. table::
+
+ ==== ============== ============
+ Rank Object Classes Probability
+ ==== ============== ============
+ 1 tabby 0.996
+ 2 Egyptian_cat 0.977
+ 3 tiger_cat 0.973
+ 4 lynx 0.941
+ 5 Persian_cat 0.922
+ ==== ============== ============
+
+.. table::
+
+ ====================== ==================== ============
+ Device Processing Time Host Processing Time API Overhead
+ ====================== ==================== ============
+ DLA: 123.1 ms 124.7 ms 1.34 %
+ **OR**
+ DSP: 117.9 ms 119.3 ms 1.14 %
+ ====================== ==================== ============
+
+The particular network that we ran in this category, jacintonet11v2,
+has 14 layers. User can specify whether to run the network on DLA or DSP
+for acceleration. We can see that DLA time is slightly higher than DSP time.
+Host time includes the OpenCL runtime overhead and the time to copy user
+input data into padded TIDL buffers. We can see that the overall overhead
+is less than 1.5%.
+
Segmentation
------------
+The segmentation example takes an image as input and performs pixel-level
+classification according to pre-trained categories. The following figures
+show a street scene as input and the scene overlaid with pixel-level
+classifications as output: road in green, pedestrians in red, vehicles
+in blue and background in gray.
+
+.. image:: ../../examples/test/testvecs/input/roads/pexels-photo-972355.jpeg
+ :width: 600
+
+.. image:: images/pexels-photo-972355-seg.jpg
+ :width: 600
+
+The network we ran in this category is jsegnet21v2, which has 26 layers.
+From the reported time in the following table, we can see that this network
+runs significantly faster on DLA than on DSP.
+
+.. table::
+
+ ====================== ==================== ============
+ Device Processing Time Host Processing Time API Overhead
+ ====================== ==================== ============
+ DLA: 296.5 ms 303.3 ms 2.26 %
+ **OR**
+ DSP: 812.0 ms 818.4 ms 0.79 %
+ ====================== ==================== ============
+
SSD
---
+
+SSD is the abbreviation for Single Shot multi-box Detector.
+The ssd_multibox example takes an image as input and detects multiple
+objects with bounding boxes according to pre-trained categories.
+The following figures show another street scene as input and the scene
+with recognized objects boxed as output: pedestrians in red,
+vehicles in blue and road signs in yellow.
+
+.. image:: ../../examples/test/testvecs/input/roads/pexels-photo-378570.jpeg
+ :width: 600
+
+.. image:: images/pexels-photo-378570-ssd.jpg
+ :width: 600
+
+The network can be run entirely on either DLA or DSP. But the best
+performance comes with running the first 30 layers on DLA and the
+next 13 layers on DSP, for this particular jdetnet_ssd network.
+Note the **AND** in the following table for the reported time.
+Our end-to-end example shows how easy it is to assign a layers group id
+to an *Executor* and how easy it is to connect the output from one
+*ExecutionObject* to the input to another *ExecutionObject*.
+
+.. table::
+
+ ====================== ==================== ============
+ Device Processing Time Host Processing Time API Overhead
+ ====================== ==================== ============
+ DLA: 175.2 ms 179.1 ms 2.14 %
+ **AND**
+ DSP: 21.1 ms 22.3 ms 5.62 %
+ ====================== ==================== ============
+
+Running Examples
+----------------
+
+The examples are located in ``/usr/share/ti/tidl-api/examples`` on
+the EVM filesystem. Each example needs to be run its own directory.
+Running an example with ``-h`` will show help message with option set.
+The following code section shows how to run the examples, and
+the test program that tests all supported TIDL network configs.
+
+.. code:: shell
+
+ root@am57xx-evm:~# cd /usr/share/ti/tidl-api/examples/imagenet/
+ root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# make -j4
+ root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# ./imagenet -t d
+ Input: ../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
+ frame[0]: Time on device: 117.9ms, host: 119.3ms API overhead: 1.17 %
+ 1: tabby, prob = 0.996
+ 2: Egyptian_cat, prob = 0.977
+ 3: tiger_cat, prob = 0.973
+ 4: lynx, prob = 0.941
+ 5: Persian_cat, prob = 0.922
+ imagenet PASSED
+
+ root@am57xx-evm:/usr/share/ti/tidl-api/examples/imagenet# cd ../segmentation/; make -j4
+ root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# ./segmentation -i ../test/testvecs/input/roads/pexels-photo-972355.jpeg
+ Input: ../test/testvecs/input/roads/pexels-photo-972355.jpeg
+ frame[0]: Time on device: 296.5ms, host: 303.2ms API overhead: 2.21 %
+ Saving frame 0 overlayed with segmentation to: overlay_0.png
+ segmentation PASSED
+
+ root@am57xx-evm:/usr/share/ti/tidl-api/examples/segmentation# cd ../ssd_multibox/; make -j4
+ root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# ./ssd_multibox -i ../test/testvecs/input/roads/pexels-photo-378570.jpeg
+ Input: ../test/testvecs/input/roads/pexels-photo-378570.jpeg
+ frame[0]: Time on DLA: 175.2ms, host: 179ms API overhead: 2.1 %
+ frame[0]: Time on DSP: 21.06ms, host: 22.43ms API overhead: 6.08 %
+ Saving frame 0 with SSD multiboxes to: multibox_0.png
+ Loop total time (including read/write/print/etc): 423.8ms
+ ssd_multibox PASSED
+
+ root@am57xx-evm:/usr/share/ti/tidl-api/examples/ssd_multibox# cd ../test; make -j4
+ root@am57xx-evm:/usr/share/ti/tidl-api/examples/test# ./test_tidl
+ API Version: 01.00.00.d91e442
+ Running dense_1x1 on 2 devices, type EVE
+ frame[0]: Time on device: 134.3ms, host: 135.6ms API overhead: 0.994 %
+ dense_1x1 : PASSED
+ Running j11_bn on 2 devices, type EVE
+ frame[0]: Time on device: 176.2ms, host: 177.7ms API overhead: 0.835 %
+ j11_bn : PASSED
+ Running j11_cifar on 2 devices, type EVE
+ frame[0]: Time on device: 53.86ms, host: 54.88ms API overhead: 1.85 %
+ j11_cifar : PASSED
+ Running j11_controlLayers on 2 devices, type EVE
+ frame[0]: Time on device: 122.9ms, host: 123.9ms API overhead: 0.821 %
+ j11_controlLayers : PASSED
+ Running j11_prelu on 2 devices, type EVE
+ frame[0]: Time on device: 300.8ms, host: 302.1ms API overhead: 0.437 %
+ j11_prelu : PASSED
+ Running j11_v2 on 2 devices, type EVE
+ frame[0]: Time on device: 124.1ms, host: 125.6ms API overhead: 1.18 %
+ j11_v2 : PASSED
+ Running jseg21 on 2 devices, type EVE
+ frame[0]: Time on device: 367ms, host: 374ms API overhead: 1.88 %
+ jseg21 : PASSED
+ Running jseg21_tiscapes on 2 devices, type EVE
+ frame[0]: Time on device: 302.2ms, host: 308.5ms API overhead: 2.02 %
+ frame[1]: Time on device: 301.9ms, host: 312.5ms API overhead: 3.38 %
+ frame[2]: Time on device: 302.7ms, host: 305.9ms API overhead: 1.04 %
+ frame[3]: Time on device: 301.9ms, host: 305ms API overhead: 1.01 %
+ frame[4]: Time on device: 302.7ms, host: 305.9ms API overhead: 1.05 %
+ frame[5]: Time on device: 301.9ms, host: 305.5ms API overhead: 1.17 %
+ frame[6]: Time on device: 302.7ms, host: 305.9ms API overhead: 1.06 %
+ frame[7]: Time on device: 301.9ms, host: 305ms API overhead: 1.02 %
+ frame[8]: Time on device: 297ms, host: 300.3ms API overhead: 1.09 %
+ Comparing frame: 0
+ jseg21_tiscapes : PASSED
+ Running smallRoi on 2 devices, type EVE
+ frame[0]: Time on device: 2.548ms, host: 3.637ms API overhead: 29.9 %
+ smallRoi : PASSED
+ Running squeeze1_1 on 2 devices, type EVE
+ frame[0]: Time on device: 292.9ms, host: 294.6ms API overhead: 0.552 %
+ squeeze1_1 : PASSED
+
+ Multiple Executor...
+ Running network tidl_config_j11_v2.txt on EVEs: 1 in thread 0
+ Running network tidl_config_j11_cifar.txt on EVEs: 0 in thread 1
+ Multiple executors: PASSED
+ Running j11_bn on 2 devices, type DSP
+ frame[0]: Time on device: 170.5ms, host: 171.5ms API overhead: 0.568 %
+ j11_bn : PASSED
+ Running j11_controlLayers on 2 devices, type DSP
+ frame[0]: Time on device: 416.4ms, host: 417.1ms API overhead: 0.176 %
+ j11_controlLayers : PASSED
+ Running j11_v2 on 2 devices, type DSP
+ frame[0]: Time on device: 118ms, host: 119.2ms API overhead: 1.01 %
+ j11_v2 : PASSED
+ Running jseg21 on 2 devices, type DSP
+ frame[0]: Time on device: 1123ms, host: 1128ms API overhead: 0.443 %
+ jseg21 : PASSED
+ Running jseg21_tiscapes on 2 devices, type DSP
+ frame[0]: Time on device: 812.3ms, host: 817.3ms API overhead: 0.614 %
+ frame[1]: Time on device: 812.6ms, host: 818.6ms API overhead: 0.738 %
+ frame[2]: Time on device: 812.3ms, host: 815.1ms API overhead: 0.343 %
+ frame[3]: Time on device: 812.7ms, host: 815.2ms API overhead: 0.312 %
+ frame[4]: Time on device: 812.3ms, host: 815.1ms API overhead: 0.353 %
+ frame[5]: Time on device: 812.6ms, host: 815.1ms API overhead: 0.302 %
+ frame[6]: Time on device: 812.2ms, host: 815.1ms API overhead: 0.357 %
+ frame[7]: Time on device: 812.6ms, host: 815.2ms API overhead: 0.315 %
+ frame[8]: Time on device: 812ms, host: 815ms API overhead: 0.367 %
+ Comparing frame: 0
+ jseg21_tiscapes : PASSED
+ Running smallRoi on 2 devices, type DSP
+ frame[0]: Time on device: 14.21ms, host: 14.94ms API overhead: 4.89 %
+ smallRoi : PASSED
+ Running squeeze1_1 on 2 devices, type DSP
+ frame[0]: Time on device: 960ms, host: 961.1ms API overhead: 0.116 %
+ squeeze1_1 : PASSED
+ tidl PASSED
+
+Possible runtime errors: out of memory
+""""""""""""""""""""""""""""""""""""""
+
+.. code:: shell
+
+ tidl: device_alloc.h:31: T* tidl::malloc_ddr(size_t) [with T = char; size_t = unsigned int]: Assertion `val != nullptr' failed
+
+One possible reason is that previous aborted runs didn't properly release
+allocation. Use ti-mct-heap-check with "-c" option to clean up.
+
+.. code:: shell
+
+ root@am57xx-evm:~# ti-mct-heap-check -c
+ -- ddr_heap1 ------------------------------
+ Addr : 0xa2000000
+ Size : 0xa000000
+ Avail: 0xa000000
+ Align: 0x80
+ -----------------------------------------
+
+Another possible reason is that total memory requirement exceeds default
+memory allocated for OpenCL. See below how to patch device tree to
+increase OpenCL memory.
+
+.. code:: shell
+
+ $ sudo apt-get install device-tree-compiler # In case dtc is not already installed
+ $ scp root@am57:/boot/am57xx-evm-reva3.dtb .
+ $ dtc -I dtb -O dts am57xx-evm-reva3.dtb -o am57xx-evm-reva3.dts
+ $ cp am57xx-evm-reva3.dts am57xx-evm-reva3.dts.orig
+ $ # increase cmem block size
+ $ diff -u am57xx-evm-reva3.dts.orig am57xx-evm-reva3.dts
+ --- am57xx-evm-reva3.dts.orig 2018-01-11 14:47:51.491572739 -0600
+ +++ am57xx-evm-reva3.dts 2018-01-16 15:43:33.981431971 -0600
+ @@ -5657,7 +5657,7 @@
+ };
+
+ cmem_block_mem@a0000000 {
+ - reg = <0x0 0xa0000000 0x0 0xc000000>;
+ + reg = <0x0 0xa0000000 0x0 0x18000000>;
+ no-map;
+ status = "okay";
+ linux,phandle = <0x13c>;
+ @@ -5823,7 +5823,7 @@
+ cmem_block@0 {
+ reg = <0x0>;
+ memory-region = <0x13c>;
+ - cmem-buf-pools = <0x1 0x0 0xc000000>;
+ + cmem-buf-pools = <0x1 0x0 0x18000000>;
+ };
+
+ cmem_block@1 {
+ $ dtc -I dts -O dtb am57xx-evm-reva3.dts -o am57xx-evm-reva3.dtb
+ $ scp am57xx-evm-reva3.dtb root@am57:/boot/
+ # reboot to make memory changes effective (run "cat /proc/iomem" to check)
diff --git a/docs/source/images/pexels-photo-378570-ssd.jpg b/docs/source/images/pexels-photo-378570-ssd.jpg
new file mode 100644 (file)
index 0000000..9977132
Binary files /dev/null and b/docs/source/images/pexels-photo-378570-ssd.jpg differ
index 0000000..9977132
Binary files /dev/null and b/docs/source/images/pexels-photo-378570-ssd.jpg differ
diff --git a/docs/source/images/pexels-photo-972355-seg.jpg b/docs/source/images/pexels-photo-972355-seg.jpg
new file mode 100644 (file)
index 0000000..9d7c728
Binary files /dev/null and b/docs/source/images/pexels-photo-972355-seg.jpg differ
index 0000000..9d7c728
Binary files /dev/null and b/docs/source/images/pexels-photo-972355-seg.jpg differ