summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b039c5c)
raw | patch | inline | side by side (parent: b039c5c)
author | Yuan Zhao <yuanzhao@ti.com> | |
Tue, 27 Nov 2018 15:58:46 +0000 (09:58 -0600) | ||
committer | Yuan Zhao <yuanzhao@ti.com> | |
Tue, 27 Nov 2018 19:16:32 +0000 (13:16 -0600) |
- Constrained to EVE only for now.
- Add documentation for mnist example.
- MCT-1083
- Add documentation for mnist example.
- MCT-1083
docs/source/example.rst | patch | blob | history | |
examples/mnist/main.cpp | patch | blob | history | |
examples/test/testvecs/config/infer/tidl_config_mnist_lenet.txt | [moved from examples/test/testvecs/config/infer/tidl_config_mnist.txt with 71% similarity] | patch | blob | history |
examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin | [new file with mode: 0644] | patch | blob |
examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin | [new file with mode: 0644] | patch | blob |
examples/test/testvecs/input/digits10_images_28x28.y | [new file with mode: 0644] | patch | blob |
examples/test/testvecs/input/digits10_labels_10x1.y | [new file with mode: 0644] | patch | blob |
index 608c728d4ea94f78623ca9a6e9460b397f21414e..6c7a3ac23bf598c0b2ed9485282793d833f2ac3a 100644 (file)
--- a/docs/source/example.rst
+++ b/docs/source/example.rst
- Object detection
- EVE and C66x (network is split across both EVE and C66x)
- OpenCV used to read input image from file or capture from camera.
+ * - mnist
+ - handwritten digits recognition (MNIST). This example illustrates
+ low TIDL API overhead (~1.8%) for small networks with low compute
+ requirements (<5ms).
+ - EVE
+ - Pre-processed white-on-black images read from file, with or without
+ MNIST database file headers.
* - classification
- Classification example, called from the Matrix GUI.
- EVE or C66x
- 1630 ms
- 1408 ms
+MNIST
+-----
+
+The MNIST example takes a pre-processed 28x28 white-on-black frame from
+a file as input and predicts the hand-written digit in the frame.
+For example, the example will predict 0 for the following frame.
+
+.. code-block:: none
+
+ root@am57xx-evm:~/tidl/examples/mnist# hexdump -v -e '28/1 "%2x" "\n"' -n 784 ../test/testvecs/input/digits10_images_28x28.y
+ 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 0 0 0 0 0 3 314 8 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 0 0 0319bdfeec1671b 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 0 01ed5ffd2a4e4ec89 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 0 1bcffee2a 031e6e225 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 05ff7ffbf 2 0 078ffa1 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 0b2f2f34e 0 0 015e0d8 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0148deab2 0 0 0 0 0bdec 2 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 084f845 0 0 0 0 0a4f222 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 0c4d3 5 0 0 0 0 096f21c 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 052f695 0 0 0 0 0 0a7ed 8 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 09af329 0 0 0 0 0 0d1cf 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 2d4c8 0 0 0 0 0 01ae9a2 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 038fa9a 0 0 0 0 0 062ff76 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 07afe5d 0 0 0 0 0 0a9e215 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0bdec1d 0 0 0 0 017e7aa 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 1e7d6 0 0 0 0 0 096f85a 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 01df2bf 0 0 0 0 015e1ca 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 061fc95 0 0 0 0 084f767 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 06eff8b 0 0 0 033e8ca 4 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 060fc9e 0 0 0 092d63e 0 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 01bf1da 6 0 019b656 0 0 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0c3fb8e a613e7b 5 0 0 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 049f1fcf5f696 9 0 0 0 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 04ca0b872 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
+ 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
+
+The file can contain multiple frames. If an optional label file is also
+given, the example will compare predicted result against pre-determined
+label for accuracy. The input files may or may not have `MNIST dataset
+file headers <http://yann.lecun.com/exdb/mnist/>`_. If using headers,
+input filenames must end with idx3-ubyte or idx1-ubyte.
+
+The MNIST example also illustrates low overhead of TIDL API for small
+networks with low compute requirements (<5ms). The network runs about 3ms
+on EVE for a single frame. As shown in the following table, when running
+over 1000 frames, the overhead is about 1.8%.
+
+.. list-table:: Loop overall time over 1000 frames
+ :header-rows: 1
+
+ * - Device(s)
+ - Device Processing Time
+ - Host Processing Time
+ - API Overhead
+ * - 1 EVE
+ - 3091 ms
+ - 3146 ms
+ - 1.78%
+
Running Examples
----------------
Loop total time (including read/write/opencv/print/etc): 320.2ms
ssd_multibox PASSED
+ root@am57xx-evm:~/tidl/examples/mnist# ./mnist
+ Input images: ../test/testvecs/input/digits10_images_28x28.y
+ Input labels: ../test/testvecs/input/digits10_labels_10x1.y
+ 0
+ 1
+ 2
+ 3
+ 4
+ 5
+ 6
+ 7
+ 8
+ 9
+ Device total time: 31.02ms
+ Loop total time (including read/write/print/etc): 32.49ms
+ Accuracy: 100%
+ mnist PASSED
+
Image input
^^^^^^^^^^^
index 7794c5177b1d40553340c4b3b9d43e0a923f89f8..d933cccf9b26edca6f9d3724216792f2f918a2dc 100644 (file)
--- a/examples/mnist/main.cpp
+++ b/examples/mnist/main.cpp
#include "imgutil.h"
#include "../common/video_utils.h"
-#include "opencv2/core.hpp"
-#include "opencv2/imgproc.hpp"
-#include "opencv2/highgui.hpp"
-#include "opencv2/videoio.hpp"
-
using namespace std;
using namespace tidl;
-using namespace cv;
-#define NUM_VIDEO_FRAMES 300
-#define DEFAULT_CONFIG "mnist"
-#define NUM_DEFAULT_INPUTS 1
-#define DEFAULT_INPUT_FRAMES 1
-const char *default_inputs[NUM_DEFAULT_INPUTS] =
-{
- "../test/testvecs/input/digit_28x28.y"
-};
+#define DEFAULT_CONFIG "mnist_lenet"
+#define DEFAULT_INPUT_IMAGES "../test/testvecs/input/digits10_images_28x28.y"
+#define DEFAULT_INPUT_LABELS "../test/testvecs/input/digits10_labels_10x1.y"
+
+uint32_t images_file_offset = 0;
+uint32_t labels_file_offset = 0;
+uint32_t num_frames_file = 0;
+uint32_t num_wrong_results = 0;
Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c);
bool RunConfiguration(cmdline_opts_t& opts);
bool ReadFrame(ExecutionObjectPipeline& eop,
uint32_t frame_idx, const Configuration& c,
- const cmdline_opts_t& opts, VideoCapture &cap);
-bool WriteFrameOutput(const ExecutionObjectPipeline &eop);
+ const cmdline_opts_t& opts, ifstream &ifs);
+bool WriteFrameOutput(const ExecutionObjectPipeline &eop, ifstream &ifs_labels);
void DisplayHelp();
exit(EXIT_SUCCESS);
}
assert(opts.num_dsps != 0 || opts.num_eves != 0);
- if (opts.num_frames == 0)
- opts.num_frames = (opts.is_camera_input || opts.is_video_input) ?
- NUM_VIDEO_FRAMES : 1;
+ if (opts.num_dsps != 0)
+ {
+ cout << "MNIST network not supported on DSP yet." << endl;
+ exit(EXIT_SUCCESS);
+ }
+
if (opts.input_file.empty())
- cout << "Input: " << default_inputs[0] << endl;
- else
- cout << "Input: " << opts.input_file << endl;
+ {
+ opts.input_file = DEFAULT_INPUT_IMAGES;
+ opts.object_classes_list_file = DEFAULT_INPUT_LABELS;
+ }
+
+ // if inputs are MNIST data set: skip MNIST header
+ string& s_images = opts.input_file;
+ if (s_images.size() > 10 &&
+ s_images.compare(s_images.size() - 10, 10, "idx3-ubyte") == 0)
+ images_file_offset = 16;
+ string& s_labels = opts.object_classes_list_file;
+ if (s_labels.size() > 10 &&
+ s_labels.compare(s_labels.size() - 10, 10, "idx1-ubyte") == 0)
+ labels_file_offset = 8;
+
+ cout << "Input images: " << opts.input_file << endl;
+ if (! opts.object_classes_list_file.empty())
+ cout << "Input labels: " << opts.object_classes_list_file << endl;
// Run network
bool status = RunConfiguration(opts);
// Read the TI DL configuration file
Configuration c;
string config_file = "../test/testvecs/config/infer/tidl_config_"
- + opts.config + ".txt";
+ + opts.config + ".txt";
bool status = c.ReadFromFile(config_file);
if (!status)
{
}
c.enableApiTrace = opts.verbose;
- // setup camera/video input/output
- VideoCapture cap;
- if (! SetVideoInputOutput(cap, opts, "MNIST")) return false;
+ // setup images/labels input/output
+ ifstream ifs, ifs_labels;
+ ifs.open(opts.input_file, ios::binary | ios::ate);
+ if (! ifs.good())
+ {
+ cerr << "Cannot open " << opts.input_file << endl;
+ return false;
+ }
+ num_frames_file = (((int) ifs.tellg()) - images_file_offset) /
+ (c.inWidth * c.inHeight);
+ if (opts.num_frames == 0)
+ opts.num_frames = num_frames_file;
+ if (! opts.object_classes_list_file.empty())
+ {
+ ifs_labels.open(opts.object_classes_list_file, ios::binary);
+ if (! ifs_labels.good())
+ {
+ cerr << "Cannot open " << opts.object_classes_list_file << endl;
+ return false;
+ }
+ }
try
{
{
device_time +=
eos[frame_idx % num_eos]->GetProcessTimeInMilliSeconds();
- WriteFrameOutput(*eop);
+ WriteFrameOutput(*eop, ifs_labels);
}
// Read a frame and start processing it with current eop
- if (ReadFrame(*eop, frame_idx, c, opts, cap))
+ if (ReadFrame(*eop, frame_idx, c, opts, ifs))
eop->ProcessFrameStartAsync();
}
chrono::duration<float> elapsed = tloop1 - tloop0;
cout << "Device total time: " << setw(6) << setprecision(4)
<< device_time << "ms" << endl;
- cout << "Loop total time (including read/write/opencv/print/etc): "
+ cout << "Loop total time (including read/write/print/etc): "
<< setw(6) << setprecision(4)
<< (elapsed.count() * 1000) << "ms" << endl;
+ if (opts.num_frames > 0 && ifs_labels.is_open())
+ {
+ cout << "Accuracy: " << setw(6) << setprecision(4)
+ << (opts.num_frames-num_wrong_results)*100.f / opts.num_frames
+ << "%" << endl;
+ if (opts.input_file == DEFAULT_INPUT_IMAGES && num_wrong_results >0)
+ status = false;
+ }
FreeMemory(eops);
for (auto eop : eops) delete eop;
bool ReadFrame(ExecutionObjectPipeline &eop,
uint32_t frame_idx, const Configuration& c,
- const cmdline_opts_t& opts, VideoCapture &cap)
+ const cmdline_opts_t& opts, ifstream &ifs)
{
if (frame_idx >= opts.num_frames)
return false;
assert (frame_buffer != nullptr);
int channel_size = c.inWidth * c.inHeight;
- Mat image;
- if (! opts.is_camera_input && ! opts.is_video_input)
- {
- if (opts.input_file.empty())
- {
- ifstream ifs(default_inputs[frame_idx % NUM_DEFAULT_INPUTS],
- ios::binary);
- ifs.seekg((frame_idx % DEFAULT_INPUT_FRAMES) * channel_size);
- ifs.read(frame_buffer, channel_size);
- memcpy(frame_buffer+channel_size, frame_buffer, channel_size);
- bool ifs_status = ifs.good();
- ifs.close();
- return ifs_status; // already PreProc-ed
- }
- else
- {
- image = cv::imread(opts.input_file, CV_LOAD_IMAGE_COLOR);
- if (image.empty())
- {
- cerr << "Unable to read input image" << endl;
- return false;
- }
- }
- }
- else
- {
- Mat v_image;
- if (! cap.grab()) return false;
- if (! cap.retrieve(v_image)) return false;
- #define DISPLAY_SIZE 112
- int orig_width = v_image.cols;
- int orig_height = v_image.rows;
- // Crop camera/video input to center DISPLAY_SIZE x DISPLAY_SIZE input
- if (orig_width > DISPLAY_SIZE && orig_height > DISPLAY_SIZE)
- {
- image = Mat(v_image, Rect((orig_width-DISPLAY_SIZE)/2,
- (orig_height-DISPLAY_SIZE)/2,
- DISPLAY_SIZE, DISPLAY_SIZE));
- }
- else
- image = v_image;
- cv::imshow("MNIST", image);
- waitKey(2);
- }
-
- // Convert to Gray image, resize to 28x28, copy into frame_buffer
- Mat s_image, bgr_frames[3];
- cv::resize(image, s_image, Size(c.inWidth, c.inHeight),
- 0, 0, cv::INTER_AREA);
- cv::split(s_image, bgr_frames);
- memcpy(frame_buffer, bgr_frames[0].ptr(), channel_size);
- memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
- return true;
+ // already PreProc-ed white-on-black 28x28 frames
+ ifs.seekg(images_file_offset + (frame_idx%num_frames_file) * channel_size);
+ ifs.read(frame_buffer, channel_size);
+ return ifs.good();
}
// Display top 5 classified imagenet classes with probabilities
-bool WriteFrameOutput(const ExecutionObjectPipeline &eop)
+bool WriteFrameOutput(const ExecutionObjectPipeline &eop, ifstream &ifs_labels)
{
unsigned char *out = (unsigned char *) eop.GetOutputBufferPtr();
int out_size = eop.GetOutputBufferSizeInBytes();
int maxloc = -1;
for (int i = 0; i < out_size; i++)
{
- // cout << (int) out[i] << " ";
+ // cout << (int) out[i] << " "; // 10 probability outputs
if (out[i] > maxval)
{
maxval = out[i];
}
cout << maxloc << endl;
+ // check inference result against pre-determined label
+ if (ifs_labels.is_open())
+ {
+ int frame_index = eop.GetFrameIndex();
+ char label = -1;
+ ifs_labels.seekg(labels_file_offset + (frame_index % num_frames_file));
+ ifs_labels.read(&label, 1);
+ if (maxloc != (int) label)
+ num_wrong_results += 1;
+ }
+
return true;
}
void DisplayHelp()
{
cout <<
- "Usage: imagenet\n"
- " Will run imagenet network to predict top 5 object"
- " classes for the input.\n Use -c to run a"
- " different imagenet network. Default is j11_v2.\n"
+ "Usage: mnist\n"
+ " Will run MNIST LeNet to predict the digit in a 28x28"
+ " white-on-black image.\n Use -c to run a"
+ " different MNIST network. Default is mnist_lenet.\n"
"Optional arguments:\n"
- " -c <config> Valid configs: j11_bn, j11_prelu, j11_v2\n"
- " -d <number> Number of dsp cores to use\n"
+ " -c <config> Valid configs: mnist_lenet\n"
" -e <number> Number of eve cores to use\n"
- " -i <image> Path to the image file as input\n"
- " -i camera<number> Use camera as input\n"
- " video input port: /dev/video<number>\n"
- " -i <name>.{mp4,mov,avi} Use video file as input\n"
- " -l <objects_list> Path to the object classes list file\n"
+ " -i <images> Path to the MNIST white-on-black images file\n"
+ " -l <labels> Path to the MNIST labels file\n"
" -f <number> Number of frames to process\n"
" -v Verbose output during execution\n"
" -h Help\n";
diff --git a/examples/test/testvecs/config/infer/tidl_config_mnist.txt b/examples/test/testvecs/config/infer/tidl_config_mnist_lenet.txt
similarity index 71%
rename from examples/test/testvecs/config/infer/tidl_config_mnist.txt
rename to examples/test/testvecs/config/infer/tidl_config_mnist_lenet.txt
index b62b859234ae6d028c741ce30140c539823dbea3..f4b0b7fc8e94987dff59cf8a182e6ac1457c5dd7 100755 (executable)
rename from examples/test/testvecs/config/infer/tidl_config_mnist.txt
rename to examples/test/testvecs/config/infer/tidl_config_mnist_lenet.txt
index b62b859234ae6d028c741ce30140c539823dbea3..f4b0b7fc8e94987dff59cf8a182e6ac1457c5dd7 100755 (executable)
numFrames = 1
preProcType = 0
-inData = ../test/testvecs/input/digit_28x28.y
+inData = ../test/testvecs/input/digits10_images_28x28.y
outData = "stats_tool_out.bin"
-netBinFile = "../test/testvecs/config/tidl_models/tidl_net_mnist_cnn.bin"
-paramsBinFile = "../test/testvecs/config/tidl_models/tidl_param_mnist_cnn.bin"
+netBinFile = "../test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin"
+paramsBinFile = "../test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin"
inWidth = 28
inHeight = 28
inNumChannels = 2
diff --git a/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin b/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin
new file mode 100644 (file)
index 0000000..ea9ac6c
Binary files /dev/null and b/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin differ
index 0000000..ea9ac6c
Binary files /dev/null and b/examples/test/testvecs/config/tidl_models/tidl_net_mnist_lenet.bin differ
diff --git a/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin b/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin
new file mode 100644 (file)
index 0000000..66cc8a6
Binary files /dev/null and b/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin differ
index 0000000..66cc8a6
Binary files /dev/null and b/examples/test/testvecs/config/tidl_models/tidl_param_mnist_lenet.bin differ
diff --git a/examples/test/testvecs/input/digits10_images_28x28.y b/examples/test/testvecs/input/digits10_images_28x28.y
new file mode 100644 (file)
index 0000000..8799ea3
Binary files /dev/null and b/examples/test/testvecs/input/digits10_images_28x28.y differ
index 0000000..8799ea3
Binary files /dev/null and b/examples/test/testvecs/input/digits10_images_28x28.y differ
diff --git a/examples/test/testvecs/input/digits10_labels_10x1.y b/examples/test/testvecs/input/digits10_labels_10x1.y
new file mode 100644 (file)
index 0000000..df93f5f
Binary files /dev/null and b/examples/test/testvecs/input/digits10_labels_10x1.y differ
index 0000000..df93f5f
Binary files /dev/null and b/examples/test/testvecs/input/digits10_labels_10x1.y differ