summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 790be35)
raw | patch | inline | side by side (parent: 790be35)
author | Yuan Zhao <yuanzhao@ti.com> | |
Tue, 27 Nov 2018 23:36:44 +0000 (17:36 -0600) | ||
committer | Yuan Zhao <yuanzhao@ti.com> | |
Tue, 27 Nov 2018 23:38:04 +0000 (17:38 -0600) |
- MCT-1089
docs/source/example.rst | patch | blob | history | |
examples/imagenet/main.cpp | patch | blob | history |
index 03a100293f455fe8fdf27a1c7c5e808f151c1969..5abdb24815267242af439ad4cd8cd94e71aebff4 100644 (file)
--- a/docs/source/example.rst
+++ b/docs/source/example.rst
The imagenet example takes an image as input and outputs 1000 probabilities.
Each probability corresponds to one object in the 1000 objects that the
-network is pre-trained with. The example outputs top 5 predictions for a given input image.
+network is pre-trained with. The example outputs top 5 (up to) predictions
+with probabilities of 5% or higher for a given input image.
The following figure and tables shows an input image, top 5 predicted
objects as output, and the processing time on either EVE or C66x.
:width: 600
-==== ==============
-Rank Object Classes
-==== ==============
-1 tabby
-2 Egyptian_cat
-3 tiger_cat
-4 lynx
-5 Persian_cat
-==== ==============
+==== ============== ===========
+Rank Object Classes Probability
+==== ============== ===========
+1 tabby 52.55%
+2 Egyptian_cat 21.18%
+3 tiger_cat 17.65%
+==== ============== ===========
======= ====================== ==================== ============
Device Device Processing Time Host Processing Time API Overhead
- 1021 ms
- 814 ms
-.. note::
- The predicitions reported here are based on the output of the softmax
- layer in the network, which are not normalized to the real probabilities.
-
Segmentation
------------
.. code-block:: shell
- root@am57xx-evm:~/tidl-api/examples/imagenet# ./imagenet
+ root@am57xx-evm:~/tidl/examples/imagenet# ./imagenet
Input: ../test/testvecs/input/objects/cat-pet-animal-domestic-104827.jpeg
- frame[ 0]: Time on EVE0: 106.50 ms, host: 107.96 ms API overhead: 1.35 %
- 1: tabby
- 2: Egyptian_cat
- 3: tiger_cat
- 4: lynx
- 5: Persian_cat
- Loop total time (including read/write/opencv/print/etc): 202.6ms
+ 1: tabby, prob = 52.55%
+ 2: Egyptian_cat, prob = 21.18%
+ 3: tiger_cat, prob = 17.65%
+ Loop total time (including read/write/opencv/print/etc): 183.3ms
imagenet PASSED
root@am57xx-evm:~/tidl-api/examples/segmentation# ./segmentation
index 89c203ee93f37f2588cd492c4a7f3c6fa4a720cc..dbb8de4c89b218055c774311b32f9e7858686623 100644 (file)
return imgutil::PreprocessImage(image, frame_buffer, c);
}
-// Display top 5 classified imagenet classes with probabilities
+// Display top 5 classified imagenet classes with probabilities 5% or higher
+#define REPORT_THRESHOLD 13 // 13/255 = 5.098%
bool WriteFrameOutput(const ExecutionObjectPipeline &eop)
{
const int k = 5;
}
for (int i = k - 1; i >= 0; i--)
+ {
+ if (sorted[i].first <= REPORT_THRESHOLD) break;
cout << k-i << ": "
- << object_classes->At(sorted[i].second).label << endl;
+ << object_classes->At(sorted[i].second).label
+ << ", prob = " << setprecision(4)
+ << ((sorted[i].first * 100) / 255.0f) << "%" << endl;
+ }
return true;
}