Merge branch 'release/v01.02.00'
Add jdetnet_voc network and make it the default
- jdetnet_voc is trained with more object categories than original
jdetnet. Make jdetnet_voc the default in the ssd example. User can
still use command line options to run the original jdetnet network.
- MCT-1091
- jdetnet_voc is trained with more object categories than original
jdetnet. Make jdetnet_voc the default in the ssd example. User can
still use command line options to run the original jdetnet network.
- MCT-1091
Update imagenet example with new softmax output
- MCT-1089
- MCT-1089
Added Python variant of mnist example
Also fix one_eo_per_frame.py to avoid creating an EVE executor if there are
no EVEs available.
(MCT-1088)
Also fix one_eo_per_frame.py to avoid creating an EVE executor if there are
no EVEs available.
(MCT-1088)
Add link in changelog for mnist example
- MCT-1083
- MCT-1083
Add MNIST LeNet network model and test input
- Constrained to EVE only for now.
- Add documentation for mnist example.
- MCT-1083
- Constrained to EVE only for now.
- Add documentation for mnist example.
- MCT-1083
Add mnist example with low compute
- Show that TIDL API with multiple contexts and pipelined computation
offers low overhead for small networks as well.
- MCT-1083
- Show that TIDL API with multiple contexts and pipelined computation
offers low overhead for small networks as well.
- MCT-1083
Update reference output for unit tests
A defect fix in the softmax layer necessitated updates to the reference
output of networks using the softmax layer.
(MCT-1087)
A defect fix in the softmax layer necessitated updates to the reference
output of networks using the softmax layer.
(MCT-1087)
Documentation - update 'Using the API' chapter
(MCT-1086)
(MCT-1086)
Initialize EO::current_frame_idx_m in constructor
Initialize ExecutionObject::current_frame_idx_m array to 0 in the
ExecutionObject constructor to prevent out of range entries when
recording trace data.
In a pipelined processing loop, the application executes
ExecutionObject::ProcessFrameWait() on the first frame before it calls
ExecutionObject::ProcessFrameStartAsync. The side effect is that the
current_frame_idx_m is not initialized. This can result in negative
frame indices when writing trace data using ReportTrace or UpdateTrace
leading to memory errors.
Setting ExecutionObject::current_frame_idx_m to 0 in the constructor
avoids this scenario.
(MCT-1085)
Initialize ExecutionObject::current_frame_idx_m array to 0 in the
ExecutionObject constructor to prevent out of range entries when
recording trace data.
In a pipelined processing loop, the application executes
ExecutionObject::ProcessFrameWait() on the first frame before it calls
ExecutionObject::ProcessFrameStartAsync. The side effect is that the
current_frame_idx_m is not initialized. This can result in negative
frame indices when writing trace data using ReportTrace or UpdateTrace
leading to memory errors.
Setting ExecutionObject::current_frame_idx_m to 0 in the constructor
avoids this scenario.
(MCT-1085)
Updated parameter description in doxygen comments
(MCT-1084)
(MCT-1084)
Build Python bindings library by default
(MCT-1069)
(MCT-1069)
Updated manifest for v1.2.0
(MCT-1060)
(MCT-1060)
Add option to specify object classes list file
- so that user can specify a different object classes list file
without re-compiling the application.
- MCT-1081
- so that user can specify a different object classes list file
without re-compiling the application.
- MCT-1081
mcbench: image preprocessing, handle layergroups=1
- Add image preprocessing for types 1 and 2.
- if layer groups is 1, force all layers to be in the same group
(MCT-1075)
- Add image preprocessing for types 1 and 2.
- if layer groups is 1, force all layers to be in the same group
(MCT-1075)
classification: Support different network models
jacinto11, mobilenet and inceptionet models can be used with this example.
jacinto11, mobilenet and inceptionet models can be used with this example.
infer: Add configuration files for inceptionnet and mobilenet that can run as two layer groups
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Signed-off-by: Djordje Senicic <x0157990@ti.com>
tidl_models: Add mobilenet and inceptionnet models, trained on ImageNet
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Signed-off-by: Djordje Senicic <x0157990@ti.com>
mcbench: Multicore benchmark with minimal overhead
- Add required models, input test vectors and platform specific scripts
- Add inference configuration files for multicore benchmarking
- Rename input files to indicate multiple frames and add more inference
configurations, covered in regression scripts
(MCT-1075)
- Add required models, input test vectors and platform specific scripts
- Add inference configuration files for multicore benchmarking
- Rename input files to indicate multiple frames and add more inference
configurations, covered in regression scripts
(MCT-1075)
examples: Add layers group command line parameter
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Updated Python bindings to reflect API changes
(MCT-1080)
(MCT-1080)
Add contextSize: hide OCL_TIDL_CACHE_ALIGN on host
- MCT-1059
- MCT-1059
Added graph viewer for TIDL API timestamp data
1. Created a python matplotlib based utility for viewing timestamp data
generated from the TIDL API (viewer/execution_graph.py)
2. Minor updates to API internals to add ExecutionObject type, index to
timestamp output
(MCT-1073)
1. Created a python matplotlib based utility for viewing timestamp data
generated from the TIDL API (viewer/execution_graph.py)
2. Minor updates to API internals to add ExecutionObject type, index to
timestamp output
(MCT-1073)
Simplify API for multiple contexts
1. Simplify context API in ExecutionObject. Replace context_id variants to
multiple existing APIs with these two APIs:
bool AcquireAndRunContext(uint32_t& context_idx,
int frame_idx,
const IODeviceArgInfo& in,
const IODeviceArgInfo& out);
bool WaitAndReleaseContext(uint32_t context_idx);
2. The timing methods for host execution in EOPs and EOs:
* GetProcessTimeInMilliSeconds()
* GetHostProcessTimeInMilliSeconds()
are no longer accurate with multiple contexts and pipelining.
Replace these methods and replace with a generic timestamp
based approach. There is a single API call to enable time stamps in an
application:
//! Enable time stamp generation for TIDL API events
bool EnableTimeStamps(const std::string& file = "timestamp.log", size_t
num_frames=32);
If this method is called before TIDL API frame processing, the API will
generate timestamps for events corresponding to each frame (e.g.
EOP::ProcessFrameStartAsync, EOP::ProcessFrameWait, etc.). These
timestamps are then written to file when the user's application
completes.
A separate script is used for post-processing the time stamps and
generating data for the user.
(MCT-1073, MCT-1074)
1. Simplify context API in ExecutionObject. Replace context_id variants to
multiple existing APIs with these two APIs:
bool AcquireAndRunContext(uint32_t& context_idx,
int frame_idx,
const IODeviceArgInfo& in,
const IODeviceArgInfo& out);
bool WaitAndReleaseContext(uint32_t context_idx);
2. The timing methods for host execution in EOPs and EOs:
* GetProcessTimeInMilliSeconds()
* GetHostProcessTimeInMilliSeconds()
are no longer accurate with multiple contexts and pipelining.
Replace these methods and replace with a generic timestamp
based approach. There is a single API call to enable time stamps in an
application:
//! Enable time stamp generation for TIDL API events
bool EnableTimeStamps(const std::string& file = "timestamp.log", size_t
num_frames=32);
If this method is called before TIDL API frame processing, the API will
generate timestamps for events corresponding to each frame (e.g.
EOP::ProcessFrameStartAsync, EOP::ProcessFrameWait, etc.). These
timestamps are then written to file when the user's application
completes.
A separate script is used for post-processing the time stamps and
generating data for the user.
(MCT-1073, MCT-1074)
Enqueue multiple frames at device side
- Previous implementation won't send/enqueue next frame to device
until the host has received completion message for current frame.
The improvement is to create multiple sets/contexts of internal
TIDL input/output buffers at device side, and to send/enqueue next
frame using a different set/context of internal TIDL input/output
buffers to device while device is still processing the current frame.
When device finishes current frame, it can immediately read
its messageQ and start processing the next frame, without waiting
for the completion message reaching the host and the hosting sending
the next frame.
- In pipelined processing of multiple frames, this optimization can
effectively hide the round-trip communication between host and device.
- Removed deprecated enableInternalInput feature
- MCT-1059
- Previous implementation won't send/enqueue next frame to device
until the host has received completion message for current frame.
The improvement is to create multiple sets/contexts of internal
TIDL input/output buffers at device side, and to send/enqueue next
frame using a different set/context of internal TIDL input/output
buffers to device while device is still processing the current frame.
When device finishes current frame, it can immediately read
its messageQ and start processing the next frame, without waiting
for the completion message reaching the host and the hosting sending
the next frame.
- In pipelined processing of multiple frames, this optimization can
effectively hide the round-trip communication between host and device.
- Removed deprecated enableInternalInput feature
- MCT-1059
Quantization history configuration parameters
Added the following parameters to Configuration:
* quantHistoryParam1
* quantHistoryParam2
* quantMargin
These parameters can be specified in the configuration file or set
directly in the code.
(MCT-1062)
Added the following parameters to Configuration:
* quantHistoryParam1
* quantHistoryParam2
* quantMargin
These parameters can be specified in the configuration file or set
directly in the code.
(MCT-1062)
Removed unused API functionality, added changelog
(MCT-1062)
(MCT-1062)
Refactor imgutils::PreProcImage function
- Renamed to imgutils::PreprocessImage
- Remove alloc/memcpy of data buffer, work off split OpenCV::Mat(s)
- Use Configuration to extract width, height, #channels etc.
- Number of ROIs is always 1 for TIDL API, remove from parameter list
(MCT-1063)
- Renamed to imgutils::PreprocessImage
- Remove alloc/memcpy of data buffer, work off split OpenCV::Mat(s)
- Use Configuration to extract width, height, #channels etc.
- Number of ROIs is always 1 for TIDL API, remove from parameter list
(MCT-1063)
Adding pybind11 v2.2.4 to repo
- https://github.com/pybind/pybind11.git, branch v2.2
- commit sha: 9a19306fbf30642ca331d0ec88e7da54a96860f9
(MCT-1009)
- https://github.com/pybind/pybind11.git, branch v2.2
- commit sha: 9a19306fbf30642ca331d0ec88e7da54a96860f9
(MCT-1009)
Added Python 3 bindings for TIDL API
* Using pybind11 v2.2 to add Python 3 bindings to TIDL API classes/methods
https://pybind11.readthedocs.io/en/stable/index.html
https://github.com/pybind/pybind11/tree/v2.2
* Leveraging the Python buffer protocol to expose input/output buffers
from ExecutionObject/ExecutionObjectPipeline to Python application
code. This eliminates copies between the Python application and the TIDL
API library. (see examples/pybind/one_eo_per_frame.py).
* Methods renamed to follow Python style guide (PEP8)
* Bindings split across multiple pybind_* source files to reduce compile
time
* tidl_api/Makefile builds a shared object - tidl.so. Add this so to
PYTHONPATH to make the tidl module available to the Python interpreter.
>>> import tidl
>>> help (tidl)
* See examples/pybind for examples of using the Python bindings
(MCT-1009)
* Using pybind11 v2.2 to add Python 3 bindings to TIDL API classes/methods
https://pybind11.readthedocs.io/en/stable/index.html
https://github.com/pybind/pybind11/tree/v2.2
* Leveraging the Python buffer protocol to expose input/output buffers
from ExecutionObject/ExecutionObjectPipeline to Python application
code. This eliminates copies between the Python application and the TIDL
API library. (see examples/pybind/one_eo_per_frame.py).
* Methods renamed to follow Python style guide (PEP8)
* Bindings split across multiple pybind_* source files to reduce compile
time
* tidl_api/Makefile builds a shared object - tidl.so. Add this so to
PYTHONPATH to make the tidl module available to the Python interpreter.
>>> import tidl
>>> help (tidl)
* See examples/pybind for examples of using the Python bindings
(MCT-1009)
Restore version to 1.2.0.0
Merge tag 'v01.01.00.01' into develop
For PSDK 5.1 release
For PSDK 5.1 release
Merge branch 'hotfix/v01.01.00.01'
Optimize classification perf, report loop avg_fps
- Double buffer EOPs to overlap host pre/post-processing
and device processing. When EOP contains more than one EO,
pipeline at EO level rather than at EOP level.
- Compute average FPS across a sliding window of frames
using host loop iteration/frame time.
- MCT-1049
- Double buffer EOPs to overlap host pre/post-processing
and device processing. When EOP contains more than one EO,
pipeline at EO level rather than at EOP level.
- Compute average FPS across a sliding window of frames
using host loop iteration/frame time.
- MCT-1049
Start hotfix v01.01.00.01
Merge tag 'v01.01.00.00' into develop
Merge branch 'release/v01.01.00.00'
Updated TIDL API manifest for v1.1
(MCT-1050)
(MCT-1050)
examples:classification: Use configuration.numFrames instead of hard coded big value
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Signed-off-by: Djordje Senicic <x0157990@ti.com>
examples:classification: Increase main window and update picture of TIDL SW stack
- MCT-1049
Signed-off-by: Djordje Senicic <x0157990@ti.com>
- MCT-1049
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Updated version to 1.2.0
Classification example code refactor and clean up
- MCT-1049
- MCT-1049
Optimize examples with EOP double buffering
- Improve overall loop performance for imagenet and segmentation
- Update documentation on performance
- MCT-1039
- Improve overall loop performance for imagenet and segmentation
- Update documentation on performance
- MCT-1039
Updates to User's Guide and related examples
Changes:
* Overview chapter, includes a Terminology section.
* Section on different use cases in the "Using the API" chapter.
* Updated the Examples chapter to reflect new examples and AM5749
benchmarking.
* Added the two_eo_per_frame_opt example to illustrate double buffering.
(MCT-1043)
Changes:
* Overview chapter, includes a Terminology section.
* Section on different use cases in the "Using the API" chapter.
* Updated the Examples chapter to reflect new examples and AM5749
benchmarking.
* Added the two_eo_per_frame_opt example to illustrate double buffering.
(MCT-1043)
Wall cleanup, optimize ssd_multibox
- Fix -Wall errors
- Optimize pipeline execution for ssd_multibox
- MCT-1015
- Fix -Wall errors
- Optimize pipeline execution for ssd_multibox
- MCT-1015
Video input option and document update
- mp4/avi/mov as pre-recorded video input
- camera as live video input, let user choose video input port #
- refactor examples code
- bookkeep each EO's device/host time inside EOP since EO could be shared
- documentation update on 650MHz EVE
- documentation on video inputs and output
- MCT-1015
- mp4/avi/mov as pre-recorded video input
- camera as live video input, let user choose video input port #
- refactor examples code
- bookkeep each EO's device/host time inside EOP since EO could be shared
- documentation update on 650MHz EVE
- documentation on video inputs and output
- MCT-1015
Added example to illustrate pipelining across EOs
two_eo_per_frame is a simple example to illustrate using
ExecutionObjectPipeline to split processing a single frame across EVE
and DSP.
(MCT-1048)
two_eo_per_frame is a simple example to illustrate using
ExecutionObjectPipeline to split processing a single frame across EVE
and DSP.
(MCT-1048)
Refactor examples - test, one_eo_per_frame
- Remove code duplication across test/main.cpp,
test/multiple_executors.cpp and one_eo_per_frame/main.cpp
- Moved common code into common/utils.h, common/utils.cpp
(MCT-1047)
- Remove code duplication across test/main.cpp,
test/multiple_executors.cpp and one_eo_per_frame/main.cpp
- Moved common code into common/utils.h, common/utils.cpp
(MCT-1047)
classification - fixed zero size image clip
(PLSDK-2250)
(PLSDK-2250)
classification - adjust example for API updates
- Enable operation up to 36fps on AM5749 with EVEs at 650MHz
- DisplayHelp update for number of cores
(PLSDK-2250)
- Enable operation up to 36fps on AM5749 with EVEs at 650MHz
- DisplayHelp update for number of cores
(PLSDK-2250)
Added an example to illustrate 1 EO per frame
(MCT-1043)
(MCT-1043)
Documentation - refactoring and updates
Changes:
- Added a release notes section with notes for v1.0 and v1.1
- Reworked the intro section
- Added an overview section, changed the API software picture to show
more detail
- Removed duplicate documentation for tidl::Configuration in the rst
file, moved documentation to doxygen comments in configuration.h
- Moved "building from source" to FAQs
(MCT-1043)
Changes:
- Added a release notes section with notes for v1.0 and v1.1
- Reworked the intro section
- Added an overview section, changed the API software picture to show
more detail
- Removed duplicate documentation for tidl::Configuration in the rst
file, moved documentation to doxygen comments in configuration.h
- Moved "building from source" to FAQs
(MCT-1043)
Update imagenet to take mp4 input
- clean up command line options
- MCT-1015, MCT-1039
- clean up command line options
- MCT-1015, MCT-1039
Report memory usage when device allocation fails
TIDL API creates 2 device side heaps:
1. Parameter heap
2. Network heap
The sizes of these heaps are specified in the Configuration object, via
PARAM_HEAP_SIZE and NETWORK_HEAP_SIZE.
Existing behavior: If the heaps are not large enough, allocation on the
device triggers an assertion failure with no indication of how large the
heaps need to be for successfull allocation.
To improve the usability of the API, provide feedback to the user on the
heap sizes required to satisfy device side allocations when any
allocation fails.
Also added `-Wall -Werror` when building examples and fixed failures.
(MCT-1035)
TIDL API creates 2 device side heaps:
1. Parameter heap
2. Network heap
The sizes of these heaps are specified in the Configuration object, via
PARAM_HEAP_SIZE and NETWORK_HEAP_SIZE.
Existing behavior: If the heaps are not large enough, allocation on the
device triggers an assertion failure with no indication of how large the
heaps need to be for successfull allocation.
To improve the usability of the API, provide feedback to the user on the
heap sizes required to satisfy device side allocations when any
allocation fails.
Also added `-Wall -Werror` when building examples and fixed failures.
(MCT-1035)
ExecutionObjectPipeline for executing layersGroups
- Add top level ExecutionObjectPipeline class to execute multiple
layersGroups.
- An ExecutionObjectPipeline is constructed from multiple
ExecutionObjects, each ExecutionObject executes one layersGroup
in the network, together they execute consecutive layersGroups.
- Same look and feel as ExecutionObject, e.g. ProcessFrameStartAsync,
ProcessFrameWait, GetInputBufferPointer, GetOutputBufferPointer
- MCT-1017, MCT-1029
- Add top level ExecutionObjectPipeline class to execute multiple
layersGroups.
- An ExecutionObjectPipeline is constructed from multiple
ExecutionObjects, each ExecutionObject executes one layersGroup
in the network, together they execute consecutive layersGroups.
- Same look and feel as ExecutionObject, e.g. ProcessFrameStartAsync,
ProcessFrameWait, GetInputBufferPointer, GetOutputBufferPointer
- MCT-1017, MCT-1029
Modified IODeviceArgInfo to enable pipelining EOs
(MCT-1030)
(MCT-1030)
Remove implementation details from ArgInfo
Implementation details such as argument kind and PipeInfo should not be
a part of the user facing ArgInfo class. Also, PipeInfo is relevant only
for input/output arguments.
Moved implementation details out of ArgInfo and created 2 new classes:
DeviceArgInfo and IODeviceArgInfo.
DeviceArgInfo inherits from ArgInfo and adds an
argument kind (buffer, local or scalar). IODeviceArgInfo consists of
DeviceArgInfo and PipeInfo.
(MCT-1030)
Implementation details such as argument kind and PipeInfo should not be
a part of the user facing ArgInfo class. Also, PipeInfo is relevant only
for input/output arguments.
Moved implementation details out of ArgInfo and created 2 new classes:
DeviceArgInfo and IODeviceArgInfo.
DeviceArgInfo inherits from ArgInfo and adds an
argument kind (buffer, local or scalar). IODeviceArgInfo consists of
DeviceArgInfo and PipeInfo.
(MCT-1030)
Remove input, output buffers from process kernel
Input and output OpenCL buffers do not have to be passed into the process
kernel. The host will directly update input and output in the buffers
allocated by the TIDL library via the HostWriteNetInput and
HostReadNetOutput methods.
(MCT-1030)
Input and output OpenCL buffers do not have to be passed into the process
kernel. The host will directly update input and output in the buffers
allocated by the TIDL library via the HostWriteNetInput and
HostReadNetOutput methods.
(MCT-1030)
classification: Update static images, synthetic video clip
(MCT-1031)
Signed-off-by: Djordje Senicic <x0157990@ti.com>
(MCT-1031)
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Support layer group id assignment updates
Provide API support for updating layer -> layer group id assignments
before executing network.
(MCT-1028)
Provide API support for updating layer -> layer group id assignments
before executing network.
(MCT-1028)
Add support for accessing layer output data
* Added API methods to enable tracing and dump layer output buffers to
file
1. ExecutionObject::WriteLayerOutputsToFile
2. ExecutionObject::GetOutputsFromAllLayers
3. ExecutionObject::GetOutputFromLayer
See examples/layer_output/main.cpp, ProcessTrace() for examples of
using these tracing APIs.
* Added a 'enableTrace' field to the configuration file. Set to true
to enable tracing.
* Update configuration file parser to allow comments, blank lines
Note:
Tracing requires ti-opencl, SHA-ID 188cc38627315d3041b80ee86e6ca33087348062
or newer.
(MCT-1023)
* Added API methods to enable tracing and dump layer output buffers to
file
1. ExecutionObject::WriteLayerOutputsToFile
2. ExecutionObject::GetOutputsFromAllLayers
3. ExecutionObject::GetOutputFromLayer
See examples/layer_output/main.cpp, ProcessTrace() for examples of
using these tracing APIs.
* Added a 'enableTrace' field to the configuration file. Set to true
to enable tracing.
* Update configuration file parser to allow comments, blank lines
Note:
Tracing requires ti-opencl, SHA-ID 188cc38627315d3041b80ee86e6ca33087348062
or newer.
(MCT-1023)
Merge tag 'v01.00.00.03' into develop
Hotfix v01.00.00.03 for PSDK 5.0
Hotfix v01.00.00.03 for PSDK 5.0
Merge branch 'hotfix/v01.00.00.03'
Update to version 01.00.00.03
classification example: Updated video clip and list of allowed classes
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Restore version to 01.01.00.00 after merge
Merge tag 'v01.00.00.02' into develop
For PSDK 18Q2 (5.0) release
For PSDK 18Q2 (5.0) release
Merge branch 'hotfix/v01.00.00.02'
Rename test clips
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Signed-off-by: Djordje Senicic <x0157990@ti.com>
classification: Modify readme.md for correct executable name
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Signed-off-by: Djordje Senicic <x0157990@ti.com>
examples: classification example with command line defined labels and class filtering
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Signed-off-by: Djordje Senicic <x0157990@ti.com>
Clarify imagenet example output
- Clarify that softmax layer output are not normalized to be
real probabilities.
- MCT-1010
- Clarify that softmax layer output are not normalized to be
real probabilities.
- MCT-1010
Emit a warning when running on 2 EVEs instead of 4
* By default, the OpenCL runtime is configured with sufficient memory to
offload TIDL networks to 2 devices. On devices with 4 EVEs (e.g.
AM5729), the amount of memory available to the runtime must be
increased. Refer the User's Guide, section "Insufficient OpenCL global
memory" for details
* Documentation
- Add a section on the "test" example
- Include a note on the need to increase the default OpenCL global
memory for 4 devices.
(MCT-1008)
* By default, the OpenCL runtime is configured with sufficient memory to
offload TIDL networks to 2 devices. On devices with 4 EVEs (e.g.
AM5729), the amount of memory available to the runtime must be
increased. Refer the User's Guide, section "Insufficient OpenCL global
memory" for details
* Documentation
- Add a section on the "test" example
- Include a note on the need to increase the default OpenCL global
memory for 4 devices.
(MCT-1008)
Documentation and top-level makefile updates
(MCT-1008)
(MCT-1008)
TIDL-API docu update: time, probability
- Elaborate device and host processing time in examples
- Clarify reported probability in imagenet example
- MCT-1008
- Elaborate device and host processing time in examples
- Clarify reported probability in imagenet example
- MCT-1008
Renamed compute engine to EVE
(MCT-1005)
(MCT-1005)
Update examples Makefile to use /usr/share/ti/tidl
Update Makefile(s) in the examples directory to use tidl-api headers and
libraries from /usr/share/ti/tidl/tidl_api.
(MCT-1005)
Update Makefile(s) in the examples directory to use tidl-api headers and
libraries from /usr/share/ti/tidl/tidl_api.
(MCT-1005)
tidl-viewer: fixes for yocto nativesdk build failures
1. Allow CXX to be overridden - this is required during a yocto
nativesdk build because the -isystem option is suffixed to CXX
2. Switch tidl-viewer to a 64bit x86/Linux binary. Building a 32bit
binary within a 64bit Yocto devkit is complicated.
(MCT-1001)
1. Allow CXX to be overridden - this is required during a yocto
nativesdk build because the -isystem option is suffixed to CXX
2. Switch tidl-viewer to a 64bit x86/Linux binary. Building a 32bit
binary within a 64bit Yocto devkit is complicated.
(MCT-1001)
tidl-viewer: fixes for yocto nativesdk build failures
1. Allow CXX to be overridden - this is required during a yocto
nativesdk build because the -isystem option is suffixed to CXX
2. Switch tidl-viewer to a 64bit x86/Linux binary. Building a 32bit
binary within a 64bit Yocto devkit is complicated.
(MCT-1001)
1. Allow CXX to be overridden - this is required during a yocto
nativesdk build because the -isystem option is suffixed to CXX
2. Switch tidl-viewer to a 64bit x86/Linux binary. Building a 32bit
binary within a 64bit Yocto devkit is complicated.
(MCT-1001)
Updated version to 1.1.0
Merge tag 'v01.00.00' into develop
Merge branch 'release/v01.00.00'
Updated manifest file from SRAS00005051
(MCT-961)
(MCT-961)
Documentation - additions and cleanup
(MCT-990)
(MCT-990)
Add documentation for examples
- MCT-982
- MCT-982
license headers: updated year, added where missing
(MCT-961)
(MCT-961)
Added version to tidl_viewer, build cleanup
(MCT-984)
(MCT-984)
Added manifest from SRAS00005051
(MCT-961)
(MCT-961)
Fixes for Klocwork issues
(MCT-987)
(MCT-987)
Viewer - add layer indices to graph output
(MCT-985)
(MCT-985)
Makefile changes to fix linking errors
- MCT-984
- MCT-984
Rename to TIDL
* Replace references to TINN in the sources and directory structure with
TIDL or TIDL API
* Moved the TIDL network viewer (tidl_viewer) from utils to viewer
(MCT-983)
* Replace references to TINN in the sources and directory structure with
TIDL or TIDL API
* Moved the TIDL network viewer (tidl_viewer) from utils to viewer
(MCT-983)
Documentation - renaming and additional content
(MCT-981)
(MCT-981)
Reduce complexity of ssd_multibox example
- Only support partitioned mode, remove single device mode
- Remove enableInternalInput mode due to no observable performance gain
- Make layersGroupId assignment part of Executor's construction
- MCT-974
- Only support partitioned mode, remove single device mode
- Remove enableInternalInput mode due to no observable performance gain
- Make layersGroupId assignment part of Executor's construction
- MCT-974
Partitioned execution of TI DL network
- Enable pipelined and partitioned execution of TIDL network
by setting the same ArgInfo:
- as the output of ExecutionObject for first layersGroup
- as the input of ExecutionObject for second layersGroup
See ssd_multibox for example.
- Enable internal input mode that intermediate results between
different layersGroup no longer need to be saved in user
application.
- Fixes for correct partitioned execution of TIDL network,
e.g. dataQ needs to be passed between layersGroups
- MCT-969, MCT-974
- Enable pipelined and partitioned execution of TIDL network
by setting the same ArgInfo:
- as the output of ExecutionObject for first layersGroup
- as the input of ExecutionObject for second layersGroup
See ssd_multibox for example.
- Enable internal input mode that intermediate results between
different layersGroup no longer need to be saved in user
application.
- Fixes for correct partitioned execution of TIDL network,
e.g. dataQ needs to be passed between layersGroups
- MCT-969, MCT-974
Compute input/output size based on network
- MCT-974
- MCT-974
Annotate graph with additional properties
* Additional layer specific annotations to nodes
* Generate SVG file if /usr/bin/dot is available
* Refactoring and cleanup
(MCT-975)
* Additional layer specific annotations to nodes
* Generate SVG file if /usr/bin/dot is available
* Refactoring and cleanup
(MCT-975)
Utility to dump TIDL networks to dot graphs
(MCT-973)
(MCT-973)
Fixed color array initialization problem
- Fixed label/color mappings for ssd
- MCT-974
- Fixed label/color mappings for ssd
- MCT-974
Add test images under CC0 license
- https://www.pexels.com/photo-license/
- MCT-974
- https://www.pexels.com/photo-license/
- MCT-974