Preparation for [#1443] saving Netbeans development environment
Preparation for [#1443]
Part of [#1471], update perl libraries used
[#1470] included index for _SIL
[#1469] Add handling of HTK varFloors macro
[#1468] Add arbitrary mixture tying and mean macro sharing
[#1461] modify loop to process mean adaptation so index_mean and nbr_cpy are updated correctly.
[#1455] Add comment on parameter to run continuously.
[#1454] Merge changes from C55 branch revision 143 to add a debug function to enumerate active grammar symbol HMM state scores each frame. This will usually only be used during debugging.
[#1451] Merge changes from C55 branch to expand frames search engine can handle to SHRT_MAX.
[#1455] Add capability to run continuous live-mode testing in TestTIesrSI
[#1455] Add capability to run continuous live-mode testing in TestTIesrSI
[#1450] Clarify documentation.
[#1450] Track beam and time cell usage. Trigger compression when time cell buffer full, or when beam cell buffer is predicted to be full within a number of frames.
[#1449] Added capability in TIesrDT to make phones beginning with _ as special. This changes the decision tree file name for the _ character to "down.olmdtpm".
[#1449] add capability in TIesrDT to handle special HMMs with names beginning with '_' and containing more than one character in the name.
[#1407] add shell script to indicate how to run TestTIesrSD.
[#1271] Merge changes and improvements from C55 branch to trunk.
[#1271] Merge changes and improvements from C55 branch to trunk. Includes feature #1353 for continuous utterance detection and JAC update prior to speech
[#1440] Modify character handling so that hmm indices will never be negative.
[#1437] Add stereo data collection in TIesrFA interface and implement in TIesrFA_ALSA API.
[#1344] add draft document about TIesr parameters. Fix some TIesr documentation.
[#1434] Add Netbeans configurations to build TestTIesrSI for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TIesrSI API for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TestTIesrFA for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TIesrFA_ALSA API for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TIesrEngineSI API for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TIesrEngineCore API for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TestTIesrFlex for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TIesrFlex API for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TestTIesrDict for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TIesrDict API for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TestTIesrDT for ARM using cross-compiler on Windows
[#1434] Add Netbeans configurations to build TIesrDT for ARM using cross-compiler on Windows
[#1429] fixed htk_model_compare bug that did not check correctly if any trailing test models did not align
[#1427] Test specifically for sil or sp phone names
[#1417] Add newline in error message.
[#1417] Add maximum limit to number of allowable phones. This limits the number of words in a small vocabulary model where each word is represented by its own "phone" model. Check the limit and report error if the maximum number of phones is exceeded.
[#1407] Initial commit of the TIesr speaker-dependent set of APIs, and supporting data and documentation
[#1407] For some configurations of TIesr hmm2phone.bin is not needed, so tools should not fail if it does not exist.
9 years ago[#1358] - Prepare documentation additions and release notes for Beta_1.4 release Beta_1.4
[#1358] - Prepare documentation additions and release notes for Beta_1.4 release
[#1354] Add documentation comments to TRAN_DUR_BIAS macro
[#1355] Add default SAMPLE_RATE for windows version of TestTIesrSI. Set check for sample rate in TIesrFA_WM5.cpp to allow other sample rates.
[#1354] Merge r75 changes from cm_mods branch to trunk to implement a penalty for repeated non-silence HMM loop transitions.
[#1350] Set defaults for scaling in the event of an all-zero input vector, or all zero power spectrum.
[#1341] Fix loc_accum normalization to use frame_cnt[0].
[#1348] Merge changes that fix FFT normalization from cm_mods branch to trunk.
[#1347] added relative reference to versioning file in TIesrSIso, TIesrEngineSIso, and TIesrFA_ALSAso Netbeans projects in Resource Files project folder.
[#1345] Update default configuration for TestTIesrDT Netbeans project
10 years ago[#1326] Allow priors for MFCC vectors of any size. User should define constant vector...
[#1326] Allow priors for MFCC vectors of any size. User should define constant vectors for their MFCC configuration.
[#1341] Fixed first two items, sbc_update_SBC call and invvar use in USE_SVA/USE_SBC. loc_accum normalization will be fixed later.
[#1336] allocate same space size for anwer and answer_back
[#1338] Check to ensure inputs to hmm_codes and answers arrays stay within array sizes
[#1323] explicitly check if symbol index is a stop symbol index. Do not assume stop symbol indices are contiguous.
10 years ago[#1302] fixed mfcc_mean update weighting to reflect that mfcc_buf already has mfcc_me...
[#1302] fixed mfcc_mean update weighting to reflect that mfcc_buf already has mfcc_mean subtracted.
[#1325] fixed MATCH_TIME macro input argument.
[#1317] allocate arrays for Sym2PosType structure dynamically from user memory pool.
10 years ago[#1316]: In trunk, merge the changes from r34 in the C55 branch that allow MFCC featu...
[#1316]: In trunk, merge the changes from r34 in the C55 branch that allow MFCC feature vectors to be stored as 16-bit for adaptation.
Part of [#1271]; merge changes to confidence measure headers from C55 branch into trunk to clean up the header partitioning.
[#1304] Add missing dependencies to configurations
[#1303] Fix pmc call so identical offsets are used based on setting of BIT8MEAN
[#1296] Fix output so mean vectors for each HMM are output in state order
[#1294] Change "==" to "=" in Makefile post-build rule command for compatibility.
10 years ago[#1289] enhance documentation for creating dictionaries and add comments for TestTIes...
[#1289] enhance documentation for creating dictionaries and add comments for TestTIesrDict.
Part of [#1270]: Modify TIesrEngine to handle various front-end specifications
Part of [#1270]: In GaussianCluster tool, increase dimension specification to allow up to 32 element feature vector
[#1269] In TestTIesrSI, check sem_wait for interrupt. Reformat code. Add optional mtrace capability and document optional sample rate selections.
[#1268] Delete pathName if read_letter_map fails
[#1267] Free channel_name when initialization fails in TIesrFA_ALSA
10 years ago[#1131] Add capability to bypass use of pronunciation decision trees for small vocabu...
[#1131] Add capability to bypass use of pronunciation decision trees for small vocabulary applications.
[#1186] Memory allocation sizes fixed.
10 years agoPart of [#1147]. Modify TIesrFlex so that it can handles all 8-bit characters accordi...
Part of [#1147]. Modify TIesrFlex so that it can handles all 8-bit characters according to locale.
[#1148] Fix GetPron, so it uppercases word prior to getting default pronunciation.
[#1147] Modifications to enable TIesrDT, dictproc, and TIesrDict to handle non-ASCII characters used as letters to spell words in a dictionary.
[#1133] Modified TIesrDT.c and TIesrDT.h so that byte characters above ASCII could be used.
10 years ago[#1132] Fix htk_ttp_map.pl tool and add c_to_char.pl tool. Allows single byte charact...
[#1132] Fix htk_ttp_map.pl tool and add c_to_char.pl tool. Allows single byte characters above ASCII to be used, for example iso-8859.1. Add hints for creating dictionaries to documentation.
10 years agoPart of [#1112]: Update TIesr project source and documentation files to reflect open... Beta_1.3
Part of [#1112]: Update TIesr project source and documentation files to reflect open source licensing
[#1084] Fix unsigned/signed char error that caused _SIL_* parse fail on ARM. Update testtiesrflex run arguments in netbeans.
[#1077] check sem_wait return. Allows gdb to debug threads
[#1085] Add documentation about no tee models
[#1059] Commit initial trunk line of development.
Initial Repository Skeleton