build_wl18xx: add patch mechanism and bluetooth components
* Add a mechanism allowing to store kernel and driver patches for
known kernels and apply them during the script activation
* Add a patch set adding wilink8 support for the imx6q-sabresd
platform when using the imx-3.10.53 kernel from the 1.1.0_ga release
* Add installation of bluetooth init scripts to the file system
* Add building of the user space agent (uim) for the ti shared transport
layer in the kernel
Signed-off-by: Eyal Reizer <eyalr@ti.com>
- [D] patches/kernel_patches/imx-3.10.53/0004-st_kim-do-not-use-debugfs-functions-if-not-enabled.patch