# \\\// # -(o o)- #========================oOO==(_)==OOo======================= # This file contains the exports needed for automating the # build process of WLAN components. # Place this file in the same directory with wl18xx_build.sh # build scripts. No need to run 'source setup-env', the build # scripts will perfom it internaly. #=========================================================== # User specific environment settings - use full PATH # if DEFAULT toolchain path is set toolchain will be downloaded to ./toolchain. export TOOLCHAIN_PATH=DEFAULT # if DEAFULT path to root filesystem is set ./fs folder will be used. export ROOTFS=DEFAULT #if DEFAULT kernel path is set - kernel will be downloaded (set branch to match kernel version) export KERNEL_PATH=DEFAULT export CROSS_COMPILE=arm-none-linux-gnueabi- export ARCH=arm [ "$TOOLCHAIN_PATH" != "DEFAULT" ] && export PATH=$TOOLCHAIN_PATH:$PATH