wl18xx: update firmware file - Firmware file was updated (8.9.0.0.69), includes bug fixes and improvements. - Added Mesh support (requires supporting driver) More information can be found here: http://www.ti.com/tool/WILINK8-WIFI-NLCP Signed-off-by: Yaniv Machani <yanivma@ti.com>
linux-firmware: Update firmware file for Intel Bluetooth 8260 This patch updates the firmware file for Intel Bluetooth 8260 Also it is known as Intel Snowfield Peak (SfP) Note that there is no change in ibt-11-5.ddc. FW Build: REL0330 BL Ver: 37 0b 12 06 00 02 34 0e 00 FW Ver: 37 0b 12 23 00 1e 12 10 00 Release Version: 19.01 Signed-off-by: Tedd Ho-Jeong An <tedd.an@intel.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
linux-firmware: Update firmware patch for Intel Bluetooth 7265 (C0/D0) This patch updates the firmware patch for Intel Bluetooth 7265 (C0/D0) Also it is known as Intel StP C0 or StP D0 StP C0 Patch Version: 58 StP D0 Patch Version: 37 Release Version: 19.01 Signed-off-by: Tedd Ho-Jeong An <tedd.an@intel.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
linux-firmware: Update firmware patch for Intel Bluetooth 7265 (D1) This patch updates the firmware patch for Intel Bluetooth 7265 (D1) Also, it is known as Intel StP D1 StP D1 FW Patch Version: 20 Release Version: 19.01 Signed-off-by: Tedd Ho-Jeong An <tedd.an@intel.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
radeon: add new SI smc firmware This adds new smc firmware for certain SI hw revisions. Pulled from internal perforce on 20151210 Signed-off-by: Alex Deucher <alexander.deucher@amd.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
radeon: add new CI smc firmware This adds new CI smc firmware for certain Hawaii and Bonaire hw revisions. From internal git commit: 427ac679fea41d6e7ab34128ed45f5623b54b808 Signed-off-by: Alex Deucher <alexander.deucher@amd.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
linux-firmware: update audio firmware for Braswell platform This updates the firmware for BSW platform. This update contains fixes for some randome noise coming during suspend/resume and headset plug events. The firmware version is also added to WHENCE file. The version is v01.0B.02.02. The md5sum of the file is 7344444bff5257718bd9e56d961e899c Signed-off-by: Vinod Koul <vinod.koul@intel.com>
linux-firmware: Update firmware patch for Intel Bluetooth 7260 (B5/B6) This patch updates the firmware patch for Intel Bluetooth 7260 also known as Intel WP2 B5 and WP1 B6. Patch Version: 38 Release Version: 19.01 Signed-off-by: Tedd Ho-Jeong An <tedd.an@intel.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
linux-firmware: Update firmware patch for Intel Bluetooth 7260 (B3/B4) This patch updates the firmware patch for Intel bluetooth 7260 also known as Intel WP2 B3 and WP1 B4. Patch Version: 86 Release Version: 19.01 Signed-off-by: Tedd Ho-Jeong An <tedd.an@intel.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
linux-firmware: intel: Add Broxton audio firmware This adds Broxton audio dsp firmware The version of this firmware release is 9.00.00.430 The md5sum of this firmware binary is a307e8a10045ce78e0744d7479c715a7 Signed-off-by: Vinod Koul <vinod.koul@intel.com>
qed: Add FW 8.10.5.0 The new QED firmware contains several new additions; As for bug-fixes, it fixes a couple of issues: - Wrong classification of packets in 4-port devices. - Anti-spoof interoperability with encapsulated packets. - Tx-switching of encapsulated packets. It also slightly improves Tx performance in several scenarios. >From the driver's feature-set POV, this firmware would allow us to add 2 major enhancements in the near future: - It would allow us produce a register dump from the device, as well as other debug-related information. - It should be sufficient for our iscsi driver, which we [hopefully] plan to push upstream soon. Signed-off-by: Yuval Mintz <Yuval.Mintz@qlogic.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
amdgpu: update firmware internal git commit: 78913cf2b7da3d8b3d7d3e41c59f9776fd1c0f68 Signed-off-by: Alex Deucher <alexander.deucher@amd.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
linux-firmware: update rt2870.bin, rt2800usb driver rt2870.bin from 29 to 0.36 Cc: Shiang Tu <shiang_tu@ralinktech.com> Cc: Hua Shao (邵华) <hua.shao@mediatek.com> Cc: Stanislaw Gruszka <sgruszka@redhat.com> Cc: Kalle Valo <kvalo@codeaurora.org> Cc: linux-wireless@vger.kernel.org Cc: linux-firmware@kernel.org Signed-off-by: Xose Vazquez Perez <xose.vazquez@gmail.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
linux-firmware: update rt2860.bin, rt2800pci driver rt2860.bin: from 34 to 0.40 Cc: Shiang Tu <shiang_tu@ralinktech.com> Cc: Hua Shao (邵华) <hua.shao@mediatek.com> Cc: Stanislaw Gruszka <sgruszka@redhat.com> Cc: Kalle Valo <kvalo@codeaurora.org> Cc: linux-wireless@vger.kernel.org Cc: linux-firmware@kernel.org Signed-off-by: Xose Vazquez Perez <xose.vazquez@gmail.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>
linux-firmware: intel: Update Skylake audio firmware This updates Skylake audio dsp firmware, this version contains fixes for key phrase detection and handling delay for system wakes The version of this firmware release is 8.20.00.927 The md5sum of this firmware binary is 9eb14fe5ccda5d80071f36728f6b2a54 Signed-off-by: Vinod Koul <vinod.koul@intel.com>
ath10k: QCA9377 hw1.0: add firmware and board files QCA9377 is a new chip supported by ath10k. Firmware version is WLAN.TF.1.0-00267-1. Signed-off-by: Kalle Valo <kvalo@qca.qualcomm.com> Signed-off-by: Kyle McMartin <kyle@kernel.org>