mr scripts: dos2unix on some files
[wilink8-wlan/wl18xx-target-scripts.git] / mr / HOW TO USE SCRIPTS.txt
1 ######################################## Texas Instruments - D2I #########################################
2 ###### Before begining to use MR script you must start as STA or AP ( sta_start.sh or ap_start.sh ) ###### 
3 ###### <> -- Mandatory parameter                                                                                                                                        ######
4 ###### [] -- Optional parameter                                                                                                                                         ######
5 ###### Script version : v1.1                                                                                                                                            ######
6 ##########################################################################################################
8 ** All scripts can be loaded to /data/misc/wifi using "Load MR Scripts.ttl" in Tera Term Application.
9         
10 1. sta_add.sh <IP> <New AP Channel> [MAC]
11         Parameters  
12                 1. <IP> - Added STA IP
13                 2. <New AP Channel> - If required channel is different then hostapd.conf channel, AP will be restarted with required channel. 
14                                                           "0" says to skip AP reconfiguration. 
15                                                           Channel enter as number and not as FREQ.
16                 3. [MAC] - Added STA MAC
18         Example
19                 1. "sh sta_add.sh 10.2.46.5 11 08:00:28:13:33:36"
20                         It means new role of STA will load and AP will be restarted if his current channel is diffrent when 11.
21                 2. "sh sta_add.sh 10.2.46.5 0"
22                         It means new role of STA will load and AP will not be restarted.
23                         
24 2. sta_remove.sh (removes wlan0 interface)      
25         Parameters  
26                 None
27                 
28 -----------------------------------------------------------------------------------------------------------
29         
30 3. ap_add.sh <IP> <New AP Channel> [MAC]
31         Parameters  
32                 1. <IP> - Added AP IP
33                 2. <New AP Channel> - Added AP will be load in required channel.
34                                                           Channel enter as number and not as FREQ.
35                 3. [MAC] - Added AP MAC
36         
37         Example
38                 1. "sh ap_add.sh 10.2.46.5 11 08:00:28:13:33:36"
39                         It means new role of AP will load and AP will transmit beacon on required channel.
41 4. ap_remove.sh (removes wlan1 and mon.wlan1 interfaces)
42         Parameters  
43                 None
45 -----------------------------------------------------------------------------------------------------------
47 5. aGO_add.sh <IP> <New aGO Channel> [MAC]
48         Parameters  
49                 1. <IP> - Added aGO IP
50                 2. <New aGO Channel> - Added aGO will be load in required channel.
51                                                           Channel enter as number and not as FREQ.
52                 3. [MAC] - Added aGO MAC
53         
54         Example
55                 1. "sh aGO_add.sh 10.2.46.5 11 08:00:28:13:33:36"
56                         It means new role of aGO will load and aGO will transmit beacon on required channel.
58 6. aGO_remove.sh (removes p2p_wlan0 and mon.p2p_wlan0 interfaces)
59         Parameters  
60                 None
62 -----------------------------------------------------------------------------------------------------------
64 7. p2p_add.sh <IP> [MAC]
65         Parameters  
66                 1. <IP> - Added P2P Device IP
67                 2. [MAC] - Added P2P Device MAC
68         
69         Example
70                 1. "sh p2p_add.sh 10.2.46.5 08:00:28:13:33:36"
71                         It means new role of P2P Device will load.
73 8. p2p_remove.sh (removes p2p_wlan0 interface)
74         Parameters  
75                 None
77                 
80                 
81                 
82