summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 429dea7)
raw | patch | inline | side by side (parent: 429dea7)
author | Yair Shapira <yair.shapira@ti.com> | |
Thu, 15 Nov 2012 10:48:25 +0000 (12:48 +0200) | ||
committer | Yair Shapira <yair.shapira@ti.com> | |
Thu, 15 Nov 2012 10:48:25 +0000 (12:48 +0200) |
MAC Firmware version: 8.5.0.0.27
PHY Firmware version: 8.2.0.0.151
- Bug fix: add the frame to the RX Complete task always at the rx_complete_1273.c
- Handle Mix-Mode state by configure the RX-Streaming to send QoS trigger every 1 second.
- Bug fix: RX-Streaming - in function RxStreaming_TXDescUpdateCallback -
set the frame as a trigger frame for the STA-PSD.
- Bug fix: Device Traffic Monitor - set defult valuses to - no traffic.
- Bug fix: STA-PSD - send trigger on a QoS TID (not always on 0).
- Bug fix: STA-PSD - code bug fix, compare to zero and to to UPSU (=1).
- New Scan-Report event support in R8 FW
Event Functionality:
- Relevant for periodic scan only.
- This event will only be generated (if the proper conditions are met) at the end
of a cycle of the periodic scan. It shall NOT be generated during an ongoing cycle.
- FW will generate a PERIODIC_SCAN_REPORT_EVENT_ID event at the end of a scan cycle,
if the following conditions are met:
o The "Report Threshold" parameter in the scan command was not equal to 0 (zero).
AND
o The number of scan results that were found in this cycle is equal or greater than
the "Report Threshold" parameter in the scan command.
- The host may configure the FW to terminate this scan upon meeting the report conditions.
This is done by setting "Terminate On Report" parameter in the scan command to 1.
- Rx streaming struct modifying fields from unit8 to uint16
Signed-off-by: Yair Shapira <yair.shapira@ti.com>
PHY Firmware version: 8.2.0.0.151
- Bug fix: add the frame to the RX Complete task always at the rx_complete_1273.c
- Handle Mix-Mode state by configure the RX-Streaming to send QoS trigger every 1 second.
- Bug fix: RX-Streaming - in function RxStreaming_TXDescUpdateCallback -
set the frame as a trigger frame for the STA-PSD.
- Bug fix: Device Traffic Monitor - set defult valuses to - no traffic.
- Bug fix: STA-PSD - send trigger on a QoS TID (not always on 0).
- Bug fix: STA-PSD - code bug fix, compare to zero and to to UPSU (=1).
- New Scan-Report event support in R8 FW
Event Functionality:
- Relevant for periodic scan only.
- This event will only be generated (if the proper conditions are met) at the end
of a cycle of the periodic scan. It shall NOT be generated during an ongoing cycle.
- FW will generate a PERIODIC_SCAN_REPORT_EVENT_ID event at the end of a scan cycle,
if the following conditions are met:
o The "Report Threshold" parameter in the scan command was not equal to 0 (zero).
AND
o The number of scan results that were found in this cycle is equal or greater than
the "Report Threshold" parameter in the scan command.
- The host may configure the FW to terminate this scan upon meeting the report conditions.
This is done by setting "Terminate On Report" parameter in the scan command to 1.
- Rx streaming struct modifying fields from unit8 to uint16
Signed-off-by: Yair Shapira <yair.shapira@ti.com>
wl18xx-fw-mc.bin | patch | blob | history |
diff --git a/wl18xx-fw-mc.bin b/wl18xx-fw-mc.bin
index 41f8fe04fb6386257d83dcacda999e683e09afad..29f182b1b15e5429c01297ac15443680ca45178a 100755 (executable)
Binary files a/wl18xx-fw-mc.bin and b/wl18xx-fw-mc.bin differ
Binary files a/wl18xx-fw-mc.bin and b/wl18xx-fw-mc.bin differ