update mc FW version 8.4.0.0.4
MAC Firmware version: 8.4.0.0.4
PHY Firmware version: 8.2.0.0.139
Scheduler fixes:
- Ensure ASU events are considered for canceling a plan and issuing a re-plan
- Increasing the ASU event queue size from 8 to 12.
ASU fixes:
- update the suspend + resume timing
- consider tune duration only if resuming WLAN Role
ACL Fixes:
- adaption to the master slave getters in the SG to read and set the
- real master/slave indication on the ACL link.
Hangover + STA APS fixes:
- set the PS and the hangover timers to generic timers instead of role timers.
- These timers should be independent by the TSF of role.
Presence Adaptor:
- Presence request first request should be initiated at scheduler_role_enable
after calibration
- Remove init of MAX_AMPDU_LEN register in PHY since PHY FW handles it.
SG changes:
- change order of operations when BT is off.
- Removal of STUB role and added protection on access to Role DB for "unreal"
roles
- Change to default state of antenna in case of no BT activities - antenna
will be at WLAN
- Due to this during ELP enter (&PD Enter) the SG changes antenna state to BT
- DHCP: Obsolete patch WL8_BRINGUP_PATCH_24_CHECK_FOR_DATA_PROTECTION
- Roles: A/BG role bitmap replaced MACRO A_BAND_BITMAP with B_G_BAND_BITMAP
- Bug fix:TXL: ACK duration is assumed for each frame, even when not required
(temporary workaround)
- SG: Removed ANTENNA_SWITCH_OVERHEAD_TIME - obsolete
- Bug fix: SG: CTS not TXed on time --- Task priority Template Flow Manager
priority raised to be one before the Tx Ready Queue
- SG: Invoked updateUponBtState() no start/stop role
ELP changes:
- Move of SG functions calls from ELP enter/exit sequence to the ELP
announce mechansim
- Move ELP announce call in Enter ELP to before the prepare to sleep
command to PHY
- Move of ELP announce call in Exit ELP to before interrupt priority
is restored
MAC_PHY API changes
- update to PHY API 12
changes to PLT commands
- New Rate Adaptation module - Oren Shani
- Bug fix: P2P: rapid p2p client connections causes
assert in _SCHED_Ext_OrderTimer
- Bug fix: Add 2 msec to minimum calibration request to cover on ASU
response time.
- Postpone calibration start time delay to 40 msec, to remove A2DP clicks
during WLAN init
- Keep Alive PM register stop activity in stop-role patch
- TX engine suspend tx exchange complete notification
- gTxInprogres clear only if not in burst mode
- Bug fix: TSF Jump - added proper support to removal and updating of time
events during TSF jump.
- Bug fix: RSSI statistics for RTTT
- Bug fix: Change TX Watchdog expiry time to 3 seconds, W/A for BK
traffic system issue in parralel to BE traffic, and also in
order for the watchdog to be bigger then the iperf expiry
packet timeout (~2.05seconds)
- Bug fix: Flush bug W/A - A HW bug was found in verification in regards to
the pending queue handling by HW. A new mechanizm to suspend and
synchronized the flush HW queue is implemented.
- Bug fix: Frames in queue resume was sampled even if no frame is in queue
- Bug fix: rate adaptation 11n or 11g selection issue
- bug in the fallback mechanizm decision when to drop to 11g.
- Bug fix: TX BA Session key of IS-BA-SESSION change from TID to queue-type
in order to avoid asking it about a non-data frame
- Bug fix: StopRole set TX session to INVALID instead of 0 (which can
be a valid session index and then t he frames are not flushed)
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.4.0.0.4
PHY Firmware version: 8.2.0.0.139
Scheduler fixes:
- Ensure ASU events are considered for canceling a plan and issuing a re-plan
- Increasing the ASU event queue size from 8 to 12.
ASU fixes:
- update the suspend + resume timing
- consider tune duration only if resuming WLAN Role
ACL Fixes:
- adaption to the master slave getters in the SG to read and set the
- real master/slave indication on the ACL link.
Hangover + STA APS fixes:
- set the PS and the hangover timers to generic timers instead of role timers.
- These timers should be independent by the TSF of role.
Presence Adaptor:
- Presence request first request should be initiated at scheduler_role_enable
after calibration
- Remove init of MAX_AMPDU_LEN register in PHY since PHY FW handles it.
SG changes:
- change order of operations when BT is off.
- Removal of STUB role and added protection on access to Role DB for "unreal"
roles
- Change to default state of antenna in case of no BT activities - antenna
will be at WLAN
- Due to this during ELP enter (&PD Enter) the SG changes antenna state to BT
- DHCP: Obsolete patch WL8_BRINGUP_PATCH_24_CHECK_FOR_DATA_PROTECTION
- Roles: A/BG role bitmap replaced MACRO A_BAND_BITMAP with B_G_BAND_BITMAP
- Bug fix:TXL: ACK duration is assumed for each frame, even when not required
(temporary workaround)
- SG: Removed ANTENNA_SWITCH_OVERHEAD_TIME - obsolete
- Bug fix: SG: CTS not TXed on time --- Task priority Template Flow Manager
priority raised to be one before the Tx Ready Queue
- SG: Invoked updateUponBtState() no start/stop role
ELP changes:
- Move of SG functions calls from ELP enter/exit sequence to the ELP
announce mechansim
- Move ELP announce call in Enter ELP to before the prepare to sleep
command to PHY
- Move of ELP announce call in Exit ELP to before interrupt priority
is restored
MAC_PHY API changes
- update to PHY API 12
changes to PLT commands
- New Rate Adaptation module - Oren Shani
- Bug fix: P2P: rapid p2p client connections causes
assert in _SCHED_Ext_OrderTimer
- Bug fix: Add 2 msec to minimum calibration request to cover on ASU
response time.
- Postpone calibration start time delay to 40 msec, to remove A2DP clicks
during WLAN init
- Keep Alive PM register stop activity in stop-role patch
- TX engine suspend tx exchange complete notification
- gTxInprogres clear only if not in burst mode
- Bug fix: TSF Jump - added proper support to removal and updating of time
events during TSF jump.
- Bug fix: RSSI statistics for RTTT
- Bug fix: Change TX Watchdog expiry time to 3 seconds, W/A for BK
traffic system issue in parralel to BE traffic, and also in
order for the watchdog to be bigger then the iperf expiry
packet timeout (~2.05seconds)
- Bug fix: Flush bug W/A - A HW bug was found in verification in regards to
the pending queue handling by HW. A new mechanizm to suspend and
synchronized the flush HW queue is implemented.
- Bug fix: Frames in queue resume was sampled even if no frame is in queue
- Bug fix: rate adaptation 11n or 11g selection issue
- bug in the fallback mechanizm decision when to drop to 11g.
- Bug fix: TX BA Session key of IS-BA-SESSION change from TID to queue-type
in order to avoid asking it about a non-data frame
- Bug fix: StopRole set TX session to INVALID instead of 0 (which can
be a valid session index and then t he frames are not flushed)
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version 8.3.0.0.34
MAC Firmware version: 8.3.0.0.34
PHY Firmware version: 8.2.0.0.139
This FW release contains:
- Bug fix: Recovery 0x0 has occurred when moving from WiFi Direct menu,
after disconnect, to WiFi settings and invoke connection.
- Bug fix: let driver ran over other roles templates - assuming we use
single role only. This is done as the driver is not aligned with
the FW implementation of the KLV templates.
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.3.0.0.34
PHY Firmware version: 8.2.0.0.139
This FW release contains:
- Bug fix: Recovery 0x0 has occurred when moving from WiFi Direct menu,
after disconnect, to WiFi settings and invoke connection.
- Bug fix: let driver ran over other roles templates - assuming we use
single role only. This is done as the driver is not aligned with
the FW implementation of the KLV templates.
Signed-off-by: Ido Reis <idor@ti.com>
update firmware version to 8.3.0.0.33
The ol_r8.a3.13_jb moved as well.
- Scan - probe rate fix - change rate swap (introduced in Rev 32) to start with 11Mbps first
- Enable Calibration traces
- Disable BET
- Disable CTS protection
- Handle BAR fix
Signed-off-by: Assaf Azulay <assaf@ti.com>
The ol_r8.a3.13_jb moved as well.
- Scan - probe rate fix - change rate swap (introduced in Rev 32) to start with 11Mbps first
- Enable Calibration traces
- Disable BET
- Disable CTS protection
- Handle BAR fix
Signed-off-by: Assaf Azulay <assaf@ti.com>
update mc FW version 8.3.0.0.32
MAC Firmware version: 8.3.0.0.32
PHY Firmware version: 8.2.0.0.139
The changes in the FW:
Victoria Rev 8.3.0.0.32 -
- Limit aggregation size according to available duration limit & txop limit
- Support CTS protection
- Bug fix: connection takes longer than expected. Due to IOP problem with
CISCO 1250 long probe requests sent in 1Mbps, those probes will be
sent alternately in 11Mbps as well as in 1Mbps
- Bug fix: Auto-ARP and encryption flow problem.
- Fix BA recival after tear down and descriptor release
Avoid caching non-host frames at all
APS fix - notify hangover before setting hangover timer
RPU fix - clear undone bitmask in case of timer expired
Return success on any nesting command to host, driver patch
Rx complete interrupt fix
New Phy version 139
Probe response fixes
- radio generic fix
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.3.0.0.32
PHY Firmware version: 8.2.0.0.139
The changes in the FW:
Victoria Rev 8.3.0.0.32 -
- Limit aggregation size according to available duration limit & txop limit
- Support CTS protection
- Bug fix: connection takes longer than expected. Due to IOP problem with
CISCO 1250 long probe requests sent in 1Mbps, those probes will be
sent alternately in 11Mbps as well as in 1Mbps
- Bug fix: Auto-ARP and encryption flow problem.
- Fix BA recival after tear down and descriptor release
Avoid caching non-host frames at all
APS fix - notify hangover before setting hangover timer
RPU fix - clear undone bitmask in case of timer expired
Return success on any nesting command to host, driver patch
Rx complete interrupt fix
New Phy version 139
Probe response fixes
- radio generic fix
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version 8.3.0.0.31
MAC Firmware version: 8.3.0.0.31
PHY Firmware version: 8.2.0.0.138
The changes in the FW:
Victoria Rev 8.3.0.0.31 -
- Rx double buffer overflow fix
- Bug fix for HW recovery pc: 0x6efc while traffic in 5GHz with Linksys E3000
- Bug fix of HW recovery during TCP Tx in SISO40
- Bug fix of FW crush during TCP Tx with STA Netgear WNDA3100v2
- Tx Limit Integration.
- Tx Limit Bug Fix.
- Tx Limit Disabled.
- RPU Callback bug trace.
- PHY 138 Integration.
- enable BET (fix and enable BET in active mode)
- fix PHY stuck when entering ELP
- add sleep duration in MAC_PHY mailbox (to prevent calibration when exiting ELP)
- stop UART when entering ELP and enable it on exit
Victoria Rev 8.3.0.0.30 -
- Calibration agent BW index fix.
- ELP Uart start & stop remove, and add keep UART_CFG in pwr mgt reg save
- Trigger burst register proper init
- Fix of Keep Alive consecutive retries exceed maximum- no TX Start
- Fix of issue with Cisco 1200 Deauth frame to connected STA that only does background scans
- Fix CTS jitter in FW
- Radio generic - removed delay
- MAC PHY - don't tune if not required
- BT calibration with new handle - change state to running
- Top Init update
- Init update- BGAP delay
- ActivityManger CB stored periodic interval should be uint32 not uint16.
- SG: Merge bug, no consideration for invalid sniff data from BT.
- SG: remove WL8_BRINGUP_PATCH_23_IGNORE_SCB_ACL_COUNTER
- SG: replace some SG GTRACE with GTRACE_NVIC
- SG: add references to TOP_WL_WAKE_UP_REQUEST for ELP
- SG: set correct PWRMGMT activity for BT calibration
- SG: fix a bug in RXTIP regarding SG invocation
- SG: fix a bug in sg_bt_suspend - wrong msi returned after guardtime
- Fix for past transition from PS to Active and Back which caused inconsistent state with AP
- Tx_watchdog - Cleanup of old Tx_Monitor code and added some debug.
- Semantic change in RPU and reduced some traces
- TX_Limit cleanup of debug code.
Signed-off-by: Igal Chernobelsky <igalc@ti.com>
MAC Firmware version: 8.3.0.0.31
PHY Firmware version: 8.2.0.0.138
The changes in the FW:
Victoria Rev 8.3.0.0.31 -
- Rx double buffer overflow fix
- Bug fix for HW recovery pc: 0x6efc while traffic in 5GHz with Linksys E3000
- Bug fix of HW recovery during TCP Tx in SISO40
- Bug fix of FW crush during TCP Tx with STA Netgear WNDA3100v2
- Tx Limit Integration.
- Tx Limit Bug Fix.
- Tx Limit Disabled.
- RPU Callback bug trace.
- PHY 138 Integration.
- enable BET (fix and enable BET in active mode)
- fix PHY stuck when entering ELP
- add sleep duration in MAC_PHY mailbox (to prevent calibration when exiting ELP)
- stop UART when entering ELP and enable it on exit
Victoria Rev 8.3.0.0.30 -
- Calibration agent BW index fix.
- ELP Uart start & stop remove, and add keep UART_CFG in pwr mgt reg save
- Trigger burst register proper init
- Fix of Keep Alive consecutive retries exceed maximum- no TX Start
- Fix of issue with Cisco 1200 Deauth frame to connected STA that only does background scans
- Fix CTS jitter in FW
- Radio generic - removed delay
- MAC PHY - don't tune if not required
- BT calibration with new handle - change state to running
- Top Init update
- Init update- BGAP delay
- ActivityManger CB stored periodic interval should be uint32 not uint16.
- SG: Merge bug, no consideration for invalid sniff data from BT.
- SG: remove WL8_BRINGUP_PATCH_23_IGNORE_SCB_ACL_COUNTER
- SG: replace some SG GTRACE with GTRACE_NVIC
- SG: add references to TOP_WL_WAKE_UP_REQUEST for ELP
- SG: set correct PWRMGMT activity for BT calibration
- SG: fix a bug in RXTIP regarding SG invocation
- SG: fix a bug in sg_bt_suspend - wrong msi returned after guardtime
- Fix for past transition from PS to Active and Back which caused inconsistent state with AP
- Tx_watchdog - Cleanup of old Tx_Monitor code and added some debug.
- Semantic change in RPU and reduced some traces
- TX_Limit cleanup of debug code.
Signed-off-by: Igal Chernobelsky <igalc@ti.com>
update firmware version to 8.3.0.0.29
X TCP TX TCP RX
STA - SISO20 vs Cisco 61.1 59.1 46.1 48.5
STA - SISO40 vs Cisco 116 107 64.2 74.1
AP - SISO20 vs 18xx 60.4 60.8 43.4 45.7
P2P - SISO 20 vs 18xx 58.8 59 42 42.3
5 GHz
TCP TX UDP RX TCP TX TCP RX
STA - SISO40 vs Cisco 115 109 64.7 75.2
AP - SISO40 vs 18xx 105 101 66.2 66.3
P2P - SISO 20 vs 18xx 58.8 56.7 41.4 42.9
This FW release contains the thermal sensor feature,
Which is currently enabled for the HP SISO189x boards only.
Signed-off-by: Ido Reis <idor@ti.com>
X TCP TX TCP RX
STA - SISO20 vs Cisco 61.1 59.1 46.1 48.5
STA - SISO40 vs Cisco 116 107 64.2 74.1
AP - SISO20 vs 18xx 60.4 60.8 43.4 45.7
P2P - SISO 20 vs 18xx 58.8 59 42 42.3
5 GHz
TCP TX UDP RX TCP TX TCP RX
STA - SISO40 vs Cisco 115 109 64.7 75.2
AP - SISO40 vs 18xx 105 101 66.2 66.3
P2P - SISO 20 vs 18xx 58.8 56.7 41.4 42.9
This FW release contains the thermal sensor feature,
Which is currently enabled for the HP SISO189x boards only.
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version 8.3.0.0.26
MAC Firmware version: 8.3.0.0.26
PHY Firmware version: 8.2.0.0.137
- BT suspend fixes
- Clearing block bits fix
- Fixes for channel switch
- Fixes in ASU
- RPU fixes for bt suspend, channel switch, CTS (RPU protection)
- Updates for RPU protection
- Rx_complete: remove double SG interrupt triggering
- Disable MAC FW PFM/PWM Switching
- Force calibrations when working in RTTT mode
- Delivery of PHY FW 137
- TX_WATCHDOG enabled
- Channel Switch
- 20/40 compliance
- DHCP process is performed in active mode due to IOP issues
- RPU fix when timer expires call the SG suspend only if it's not in progres
- Start suspend operation 500 usec before strict timing activity
- Beacon lost detected event or regained bss event is rising after connection
- Add probe rate to scan command
- AP_PSD: for non Qos packet, choose psd_type due to wmm configuration
- Remove uses of get_IE, when the length of IE in beacon is changed
- Scheduler fixes, channel switch support.
- Fast removal of requests (broadcast RX storm), IRQ/SWI trace facility
- Fix Tx Monitor assert due to non-matching structure of pending queues
- Support use of SW GPIOs in serial watch (currently disabled)
- Fix invalid messages in GTRACE
- CTS W/A - CTS is sent directly via NAV protection and not through RPU.
- TX limit module update
- Calibration agent merge to A3 and A2 merge
- Calibration agent to correlate between PHY calibration and MAC scheduler
- Init calibration and regulatory domain update
Signed-off-by: Igal Chernobelsky <igalc@ti.com>
MAC Firmware version: 8.3.0.0.26
PHY Firmware version: 8.2.0.0.137
- BT suspend fixes
- Clearing block bits fix
- Fixes for channel switch
- Fixes in ASU
- RPU fixes for bt suspend, channel switch, CTS (RPU protection)
- Updates for RPU protection
- Rx_complete: remove double SG interrupt triggering
- Disable MAC FW PFM/PWM Switching
- Force calibrations when working in RTTT mode
- Delivery of PHY FW 137
- TX_WATCHDOG enabled
- Channel Switch
- 20/40 compliance
- DHCP process is performed in active mode due to IOP issues
- RPU fix when timer expires call the SG suspend only if it's not in progres
- Start suspend operation 500 usec before strict timing activity
- Beacon lost detected event or regained bss event is rising after connection
- Add probe rate to scan command
- AP_PSD: for non Qos packet, choose psd_type due to wmm configuration
- Remove uses of get_IE, when the length of IE in beacon is changed
- Scheduler fixes, channel switch support.
- Fast removal of requests (broadcast RX storm), IRQ/SWI trace facility
- Fix Tx Monitor assert due to non-matching structure of pending queues
- Support use of SW GPIOs in serial watch (currently disabled)
- Fix invalid messages in GTRACE
- CTS W/A - CTS is sent directly via NAV protection and not through RPU.
- TX limit module update
- Calibration agent merge to A3 and A2 merge
- Calibration agent to correlate between PHY calibration and MAC scheduler
- Init calibration and regulatory domain update
Signed-off-by: Igal Chernobelsky <igalc@ti.com>
update mc FW version 8.3.0.0.22
MAC Firmware version: 8.3.0.0.22
PHY Firmware version: 8.2.999.50.135
- Bug Fix: APUT BAR Attacks Cause TP Drops During Traffic
- TKIP Cisco fragmentation bug
- Pre-TX Disable (+Disable switching PFM/PWM mode)
- Work around for bad decrypted RX broadcast frames going to Host
- reduce ELP WU times
- Bug Fix: TKIP as AP: udp_tx causes assert in IntMemBlockErr()
- disable power save in AP mode scan (Danny)
- add debug for pwrmgt activities
- PHY version 135 => not done, using MR PHY ver 50.135 instead.
- Add workaround for CCA "clock-like"-toggle issue
- Bug Fix: new Rx parser compiler.
- Bug Fix: RSSI and Calibration results for RTTT.
- Bug Fix: BT/ELP changed sequence.
- fix for BA open timeout
- remove workaround for CW increment only after 2nd retry.
- remove AC's priority fix (aifsn-1)
- remove logger mux workaround for 189x.
- generating fw global variable script for driver use
- Bug Fix: Fix TKIP problems
- warning cleanup
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.3.0.0.22
PHY Firmware version: 8.2.999.50.135
- Bug Fix: APUT BAR Attacks Cause TP Drops During Traffic
- TKIP Cisco fragmentation bug
- Pre-TX Disable (+Disable switching PFM/PWM mode)
- Work around for bad decrypted RX broadcast frames going to Host
- reduce ELP WU times
- Bug Fix: TKIP as AP: udp_tx causes assert in IntMemBlockErr()
- disable power save in AP mode scan (Danny)
- add debug for pwrmgt activities
- PHY version 135 => not done, using MR PHY ver 50.135 instead.
- Add workaround for CCA "clock-like"-toggle issue
- Bug Fix: new Rx parser compiler.
- Bug Fix: RSSI and Calibration results for RTTT.
- Bug Fix: BT/ELP changed sequence.
- fix for BA open timeout
- remove workaround for CW increment only after 2nd retry.
- remove AC's priority fix (aifsn-1)
- remove logger mux workaround for 189x.
- generating fw global variable script for driver use
- Bug Fix: Fix TKIP problems
- warning cleanup
Signed-off-by: Ido Reis <idor@ti.com>
update PG2 FW version to 8.2.0.0.107
MAC Firmware version: 8.2.0.0.107
PHY Firmware version: 8.2.999.0.135
ili file updated.
Updates in this version (from FW 102):
- remove dencity
- add ELP WA ;unmask WL8_BRINGUP_PATCH_YIELD_WA
- remove WL8_WA_DISRESPECTABLE_HT_DENSITY; WA to tear down the BA session if
we detect spacing of 8 usec
- add force calibration on radio tune
- increase Max aggergation size to 14
- Remove TCP check sum fro RX and Tx pipline
- update HW Fifo sizes
- Add stop tx stat
- Add retry per rate stat
- fix order of retrey in aggregation
- Add tx monitor on AC trigger Busy
- fix exception on update cashe attributes
- MCS00115464 => new Rx parser compiler.
- MCS00115494 => RSSI and Calibration results for RTTT.
- MCS00115500 => BT/ELP changed sequence.
- fix for BA open timeout
- remove workaround for CW increment only after 2nd retry.
- remove AC's priority fix (aifsn-1)
- remove logger mux workaround for 189x.
- generating fw global variable script for driver use
- MCS00115516 => Fix TKIP problems from version 104
- warning cleanup
- reduce ELP WU times
- MCS00114518 TKIP as AP: udp_tx causes assert in IntMemBlockErr() (Oren S.)
- disable power save in AP mode scan (Danny)
- fixes for PD (still disabled in version)
- add debug for pwrmgt activities
- PHY version 135
- Add workaround for CCA "clock-like"-toggle issue
- TKIP Cisco fragmentation bug
- Pre-TX Disable (+Disable switching PFM/PWM mode)
- Work around for bad decrypted RX broadcast frames going to Host
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.2.0.0.107
PHY Firmware version: 8.2.999.0.135
ili file updated.
Updates in this version (from FW 102):
- remove dencity
- add ELP WA ;unmask WL8_BRINGUP_PATCH_YIELD_WA
- remove WL8_WA_DISRESPECTABLE_HT_DENSITY; WA to tear down the BA session if
we detect spacing of 8 usec
- add force calibration on radio tune
- increase Max aggergation size to 14
- Remove TCP check sum fro RX and Tx pipline
- update HW Fifo sizes
- Add stop tx stat
- Add retry per rate stat
- fix order of retrey in aggregation
- Add tx monitor on AC trigger Busy
- fix exception on update cashe attributes
- MCS00115464 => new Rx parser compiler.
- MCS00115494 => RSSI and Calibration results for RTTT.
- MCS00115500 => BT/ELP changed sequence.
- fix for BA open timeout
- remove workaround for CW increment only after 2nd retry.
- remove AC's priority fix (aifsn-1)
- remove logger mux workaround for 189x.
- generating fw global variable script for driver use
- MCS00115516 => Fix TKIP problems from version 104
- warning cleanup
- reduce ELP WU times
- MCS00114518 TKIP as AP: udp_tx causes assert in IntMemBlockErr() (Oren S.)
- disable power save in AP mode scan (Danny)
- fixes for PD (still disabled in version)
- add debug for pwrmgt activities
- PHY version 135
- Add workaround for CCA "clock-like"-toggle issue
- TKIP Cisco fragmentation bug
- Pre-TX Disable (+Disable switching PFM/PWM mode)
- Work around for bad decrypted RX broadcast frames going to Host
Signed-off-by: Ido Reis <idor@ti.com>
update PG2 FW version to 8.2.0.0.106
MAC Firmware version: 8.2.0.0.106
PHY Firmware version: 8.2.999.0.135
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.2.0.0.106
PHY Firmware version: 8.2.999.0.135
Signed-off-by: Ido Reis <idor@ti.com>
update PG2 FW version to 8.2.0.0.106-candidate
This is a pre-released firmware.
MAC Firmware version: 8.2.0.31.105
PHY Firmware version: 8.2.999.8.134
Signed-off-by: Ido Reis <idor@ti.com>
This is a pre-released firmware.
MAC Firmware version: 8.2.0.31.105
PHY Firmware version: 8.2.999.8.134
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version 8.3.0.0.19
MAC Firmware version: 8.3.0.0.19
PHY Firmware version: 8.2.999.0.133
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.3.0.0.19
PHY Firmware version: 8.2.999.0.133
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version 8.3.0.0.17
MAC Firmware version: 8.3.0.0.17
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.3.0.0.17
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version 8.3.0.0.16
MAC Firmware version: 8.3.0.0.16
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.3.0.0.16
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version 8.3.0.0.15
MAC Firmware version: 8.3.0.0.15
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.3.0.0.15
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version 8.3.0.0.9
MAC Firmware version: 8.3.0.0.9
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.3.0.0.9
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version 8.3.0.0.7
MAC Firmware version: 8.3.0.0.7
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.3.0.0.7
PHY Firmware version: 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
update mc FW version to 8.2.0.2.86
MAC Firmware version: 8.2.0.2.86
PHY Firmware version: 8.2.999.0.126
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.2.0.2.86
PHY Firmware version: 8.2.999.0.126
Signed-off-by: Ido Reis <idor@ti.com>
update PG2 FW version to 8.2.0.0.102
MAC Firmware version: 8.2.0.0.102
PHY Firmware version: 8.2.999.0.131
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.2.0.0.102
PHY Firmware version: 8.2.999.0.131
Signed-off-by: Ido Reis <idor@ti.com>
update Android.mk with mc firmware
added mc firmware 8.3.0.0.4
MAC Firmware Rev 8.3.0.0.4
PHY Firmware Rev 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware Rev 8.3.0.0.4
PHY Firmware Rev 8.4.999.A2.129
Signed-off-by: Ido Reis <idor@ti.com>
update PG2 FW version to 8.2.0.0.100
MAC Firmware version: 8.2.0.0.100
PHY Firmware version: 8.4.999.A2.129
- Bug fix: ASSERT_11N(DB_BA_CONTROL_TID_INFO == tid) need to be removed
an error statistics was added instead to indicate that a false positive
validity on a BA frame (MCS00113209)
- Bug fix: remove function return from TxNotifyTriggeredScanCB when last
transmitted frame is management (MCS00113753)
- Adding assert in "stop logger" host command
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.2.0.0.100
PHY Firmware version: 8.4.999.A2.129
- Bug fix: ASSERT_11N(DB_BA_CONTROL_TID_INFO == tid) need to be removed
an error statistics was added instead to indicate that a false positive
validity on a BA frame (MCS00113209)
- Bug fix: remove function return from TxNotifyTriggeredScanCB when last
transmitted frame is management (MCS00113753)
- Adding assert in "stop logger" host command
Signed-off-by: Ido Reis <idor@ti.com>
update FW to version 8.2.0.0.99
MAC FW 8.2.0.0.98:
- Bug fix - MCS00113220 - correct aifsn value
- integrate PHY FW version 8.4.999.0.129 - fix DC calibration issue
MAC FW 8.2.0.0.99:
- Bug fix MCS00113256: p2p - tx stuck both in GO and client side in 5GHZ
Throughput with this version (Mbps):
2.4 GHz - SISO 20
UDP TX 59.5
UDP RX 59.8
TCP TX 46.6
TCP RX 48.7
2.4 GHz - SISO 40
UDP TX 111
UDP RX 111
TCP TX 72.3
TCP RX 79.5
2.4 GHz - MIMO
UDP TX 103
UDP RX 108
TCP TX 70.9
TCP RX 77.1
5 GHz - SISO 40
UDP TX 103
UDP RX 111
TCP TX 65.1
TCP RX 79.5
5 GHz - SISO 20
UDP TX 60
UDP RX 60.7
TCP TX 43
TCP RX 48.1
Signed-off-by: Assaf Azulay <assaf@ti.com>
MAC FW 8.2.0.0.98:
- Bug fix - MCS00113220 - correct aifsn value
- integrate PHY FW version 8.4.999.0.129 - fix DC calibration issue
MAC FW 8.2.0.0.99:
- Bug fix MCS00113256: p2p - tx stuck both in GO and client side in 5GHZ
Throughput with this version (Mbps):
2.4 GHz - SISO 20
UDP TX 59.5
UDP RX 59.8
TCP TX 46.6
TCP RX 48.7
2.4 GHz - SISO 40
UDP TX 111
UDP RX 111
TCP TX 72.3
TCP RX 79.5
2.4 GHz - MIMO
UDP TX 103
UDP RX 108
TCP TX 70.9
TCP RX 77.1
5 GHz - SISO 40
UDP TX 103
UDP RX 111
TCP TX 65.1
TCP RX 79.5
5 GHz - SISO 20
UDP TX 60
UDP RX 60.7
TCP TX 43
TCP RX 48.1
Signed-off-by: Assaf Azulay <assaf@ti.com>
update PG2 FW version to 8.2.0.0.97
MAC Firmware version: 8.2.0.0.97
PHY Firmware version: 8.2.999.A2.129
- Enable AP Jitter (including time optimization)
- Update PHY FW to 129' to include 11a Radio Fix
- Bug Fix: Scan during Traffic, crash when runing WLAN multiple
scans and Tx traffic
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.2.0.0.97
PHY Firmware version: 8.2.999.A2.129
- Enable AP Jitter (including time optimization)
- Update PHY FW to 129' to include 11a Radio Fix
- Bug Fix: Scan during Traffic, crash when runing WLAN multiple
scans and Tx traffic
Signed-off-by: Ido Reis <idor@ti.com>
update PG2 FW version to 8.2.0.0.96
MAC Firmware version: 8.2.0.0.96
PHY Firmware version: 8.2.999.0.129
- Bug Fix: RSSI measurement per frame is incorrect
- Bug Fix: Fix RTTT PM issue
- Bug Fix: Fix for the WLAN/BT SCO
- Bug Fix: Fix disconnection/tear down
- New pending q implementation
- Bug Fix: PS Poll
- Send Probe Req in 6M
Signed-off-by: Ido Reis <idor@ti.com>
MAC Firmware version: 8.2.0.0.96
PHY Firmware version: 8.2.999.0.129
- Bug Fix: RSSI measurement per frame is incorrect
- Bug Fix: Fix RTTT PM issue
- Bug Fix: Fix for the WLAN/BT SCO
- Bug Fix: Fix disconnection/tear down
- New pending q implementation
- Bug Fix: PS Poll
- Send Probe Req in 6M
Signed-off-by: Ido Reis <idor@ti.com>
update PG2 FW version to 8.2.0.0.94
update PG2 FW version to 8.2.0.0.91
Rev 8.2.0.0.91
- change the number of supported BA sessions to 3
- bug fix: update WLAN_STATUS register according to Connectivity
combo ASD
- bug fix: Auto-ARP does not work properly
(missing post-dma callback, and corrupts encrypted auto-arp frames)
- bug fix: RTS: SUT crash after few packets with RTS generation
Rev 8.2.0.0.90
- Modified rx complete code
- Modified tx aggregation code
Rev 8.2.0.0.89
- Bug Fix: False AES Decrypt failure after reply attack identification.
- Bug Fix: Sending data directly after the CTWindow interval but before
we received a beacon
- Bug Fix: Scheduled Scan: no Prob Req on 5.GHz band
- Bug fix: WiFi TGn: SUT doesn't switch channel after channel switch command
from the AP
- Fix for enndless bar fix (increase the bar counter in tx_interrupt_1273.c)
- Bug Fix: APUT stops transmitting Beacons after initiated recovery
- Bug Fix: P2P: Firmware recovery occur when attempting to connect to a
P2P GO (Both by negotiation or join) as a P2P client
- Bug Fix: FW Panic if SUT trying to connect to AP with different security
- Bug Fix: fixes related to setup and teardown of a BA session (COEX)
- Bug Fix: Protect high scan ID in split scan.
When running immediate scan (Roaming) as split scan
- Bug Fix: (MR scenario) Robustness:Many recoveries (1827) during extSTA
- Bug fix: STA disconnects from AP after 9 failed attempts to enter PS
only 20 msec
- Bug Fix: Send the PEER_REMOVE_COMPLETE_EVENT_ID only after removing
the link context
- Bug fix: roleID is re-set after 'ZeroMem'
- Bug fix: BSS Management, APUT Doesn't send deauthentication frame to STA
in PS mode after configured aging period
- Bug Fix: Bad TSF update in beacon early termination causes beacon Miss
if the absolute difference b/n
- Cross Security roaming issue fix in FreeSecurityContext function
- Added new generic command to enable/disable additional features dynamically
- Bug Fix: SUT(Spec compliancy), Discard multicast/broadcast frames that we
sent ourselves
- Bug Fix: AP ERP Protection, APUT ignores overlapping 11b AP
- Bug Fix: BA Session, An A-MPDU received on a TID not supporting BA session
should send del BA, according to the spec
- Added condition to check that we are not in role device when trying to
delete BA session (rx_complete_task.c)
- Bug Fix: an ASSERT due to an invalid PC address
- Bug Fix: Receiving scan results from other channels for WPL purposes
- Bug Fix: Universal Scan feature, number of passive scan channels for 2.4GHz,
command complete timeout errors (mostly stop role)
- Bug Fix: FmCoexInit function with wrong parameters
- Bug Fix: IOP issue with APs not receiving seq num 0 during EAPOL handshake
- Bug Fix: When connecting to a Hidden SSID AP we keep the host awake
- Bug Fix: If Driver set the EnableRate to Zero, FW use 2.4 low rate (1 Mb/S).
- Bug Fix: Add additional filter decision (dsps_decision) to rx_filter.c
in order to filter out probes/beacons from different channels.
- Bug Fix: After delba caused by expiry of BA session we didn't do tear down
- Bug Fix: the mismatch between the AIFS Register Write as we already made
the fix in teh "define" level
Signed-off-by: Ido Reis <idor@ti.com>
Rev 8.2.0.0.91
- change the number of supported BA sessions to 3
- bug fix: update WLAN_STATUS register according to Connectivity
combo ASD
- bug fix: Auto-ARP does not work properly
(missing post-dma callback, and corrupts encrypted auto-arp frames)
- bug fix: RTS: SUT crash after few packets with RTS generation
Rev 8.2.0.0.90
- Modified rx complete code
- Modified tx aggregation code
Rev 8.2.0.0.89
- Bug Fix: False AES Decrypt failure after reply attack identification.
- Bug Fix: Sending data directly after the CTWindow interval but before
we received a beacon
- Bug Fix: Scheduled Scan: no Prob Req on 5.GHz band
- Bug fix: WiFi TGn: SUT doesn't switch channel after channel switch command
from the AP
- Fix for enndless bar fix (increase the bar counter in tx_interrupt_1273.c)
- Bug Fix: APUT stops transmitting Beacons after initiated recovery
- Bug Fix: P2P: Firmware recovery occur when attempting to connect to a
P2P GO (Both by negotiation or join) as a P2P client
- Bug Fix: FW Panic if SUT trying to connect to AP with different security
- Bug Fix: fixes related to setup and teardown of a BA session (COEX)
- Bug Fix: Protect high scan ID in split scan.
When running immediate scan (Roaming) as split scan
- Bug Fix: (MR scenario) Robustness:Many recoveries (1827) during extSTA
- Bug fix: STA disconnects from AP after 9 failed attempts to enter PS
only 20 msec
- Bug Fix: Send the PEER_REMOVE_COMPLETE_EVENT_ID only after removing
the link context
- Bug fix: roleID is re-set after 'ZeroMem'
- Bug fix: BSS Management, APUT Doesn't send deauthentication frame to STA
in PS mode after configured aging period
- Bug Fix: Bad TSF update in beacon early termination causes beacon Miss
if the absolute difference b/n
- Cross Security roaming issue fix in FreeSecurityContext function
- Added new generic command to enable/disable additional features dynamically
- Bug Fix: SUT(Spec compliancy), Discard multicast/broadcast frames that we
sent ourselves
- Bug Fix: AP ERP Protection, APUT ignores overlapping 11b AP
- Bug Fix: BA Session, An A-MPDU received on a TID not supporting BA session
should send del BA, according to the spec
- Added condition to check that we are not in role device when trying to
delete BA session (rx_complete_task.c)
- Bug Fix: an ASSERT due to an invalid PC address
- Bug Fix: Receiving scan results from other channels for WPL purposes
- Bug Fix: Universal Scan feature, number of passive scan channels for 2.4GHz,
command complete timeout errors (mostly stop role)
- Bug Fix: FmCoexInit function with wrong parameters
- Bug Fix: IOP issue with APs not receiving seq num 0 during EAPOL handshake
- Bug Fix: When connecting to a Hidden SSID AP we keep the host awake
- Bug Fix: If Driver set the EnableRate to Zero, FW use 2.4 low rate (1 Mb/S).
- Bug Fix: Add additional filter decision (dsps_decision) to rx_filter.c
in order to filter out probes/beacons from different channels.
- Bug Fix: After delba caused by expiry of BA session we didn't do tear down
- Bug Fix: the mismatch between the AIFS Register Write as we already made
the fix in teh "define" level
Signed-off-by: Ido Reis <idor@ti.com>
update pg2 fw: 8.2.0.0.88
MAC version 8.2.0.0.88
PHY version 8.2.999.0.128
updates:
* introduced in non-official fw 8.2.0.0.86:
- enable ELP
- disable PD
- enable BET
- add tx monitor
- logger muxing for PG2 HDMB
- close the define:
TNETW18xx_PG2_0_UPDATE_TCXO_LDO_ENABLE_WHEN_EXIT_SLEEP
* introduced in 8.2.0.0.88:
- New HW FIFO sizes
- remove 11b workaround
- TOP init code from Dror that was left "commented"
- open some priority 2 PG 2.0 updates related to power reduction
- PSCON_EN_WAIT_DELAY should be set to 0 instead of 4
- VIO ext_mem_data_9 pad_pull
- AMPDU duration fix
- Beacons are received / missed in pairs (AP Jitter fix)
- Firmware TX stuck / crash when dynamic memory is disabled
- Reduce amount of Dummy frames during TCP traffic
- Registers under Version Control are not written when BT is on
- Tx exchange FW queue operation (push & pop) are not
protected (disable all / enable all)
- BA session teardown bug
- ASSERT WatchPoint (Mem Leak) G41
- Open the PSAT define - now requires driver version
PG2_V1.4 at least.
- RTTT mode memory fix
- Shahar detected a bug for BA fix
- Update MAX_BAR_RETRIES to 200
- merge PHY FW version 8.2.999.0.128
PG1 fw about to become obsolete, default fw is now set to pg2
(file names changes).
Signed-off-by: Ido Reis <idor@ti.com>
MAC version 8.2.0.0.88
PHY version 8.2.999.0.128
updates:
* introduced in non-official fw 8.2.0.0.86:
- enable ELP
- disable PD
- enable BET
- add tx monitor
- logger muxing for PG2 HDMB
- close the define:
TNETW18xx_PG2_0_UPDATE_TCXO_LDO_ENABLE_WHEN_EXIT_SLEEP
* introduced in 8.2.0.0.88:
- New HW FIFO sizes
- remove 11b workaround
- TOP init code from Dror that was left "commented"
- open some priority 2 PG 2.0 updates related to power reduction
- PSCON_EN_WAIT_DELAY should be set to 0 instead of 4
- VIO ext_mem_data_9 pad_pull
- AMPDU duration fix
- Beacons are received / missed in pairs (AP Jitter fix)
- Firmware TX stuck / crash when dynamic memory is disabled
- Reduce amount of Dummy frames during TCP traffic
- Registers under Version Control are not written when BT is on
- Tx exchange FW queue operation (push & pop) are not
protected (disable all / enable all)
- BA session teardown bug
- ASSERT WatchPoint (Mem Leak) G41
- Open the PSAT define - now requires driver version
PG2_V1.4 at least.
- RTTT mode memory fix
- Shahar detected a bug for BA fix
- Update MAX_BAR_RETRIES to 200
- merge PHY FW version 8.2.999.0.128
PG1 fw about to become obsolete, default fw is now set to pg2
(file names changes).
Signed-off-by: Ido Reis <idor@ti.com>
pg2 firmware added 8.2.0.0.85
MAC version: 8.2.0.0.85
PHY version: 8.2.999.0.126
Signed-off-by: Ido Reis <idor@ti.com>
MAC version: 8.2.0.0.85
PHY version: 8.2.999.0.126
Signed-off-by: Ido Reis <idor@ti.com>
update FW version to 8.1.0.1.83
MAC FW: Rev 8.1.0.1.83
PHY FW: Rev 8.1.0.0.116
udp_rx = 106
tcp_rx = 81.3
tcp_tx = 72.2
udp_tx = 106
Linksys 310N3:
The WA works and the FW detects the frame spacing violation immediately, which results in BA session tear down.
No stuck - TP as expected with NO BAs
Dlink 825:
No stuck - TP as expected
Mostly it works with BA while the spacing is valid.
Sometimes, After some time there is a tear down due to our WA, but still we need
to do more tests to verify whether it is related to our frame spacing violation detection mechanism or not .
Signed-off-by: Assaf Azulay <assaf@ti.com>
MAC FW: Rev 8.1.0.1.83
PHY FW: Rev 8.1.0.0.116
udp_rx = 106
tcp_rx = 81.3
tcp_tx = 72.2
udp_tx = 106
Linksys 310N3:
The WA works and the FW detects the frame spacing violation immediately, which results in BA session tear down.
No stuck - TP as expected with NO BAs
Dlink 825:
No stuck - TP as expected
Mostly it works with BA while the spacing is valid.
Sometimes, After some time there is a tear down due to our WA, but still we need
to do more tests to verify whether it is related to our frame spacing violation detection mechanism or not .
Signed-off-by: Assaf Azulay <assaf@ti.com>
update FW version to 8.1.0.0.83
this version contains various bug fixes which were contributed by Lior , Bella and Oren :
1. Fix for the duplicate frame detection .
2. Fix for the infinite BAR sending .
3. WA for the ARP request issue in GO mode (caused indirectly by the multicast filtering configured by the host).
4. Fix for the bad frame hard fault.
5. ignore RX HDR Interrupt when antenna priority is at BT.
6. walkaround for CTS2SELF null frame at tx_start - not ran yesterday --> already merged and will be in the next candidate.
7. addition for patch WL8_PG1_PATCH_1_NO_B_RATES_IN_BW_40 when sending all kind of templates.
8. some compilation warnings and SG specific cleanup.
This version was tested on the Lab Setup with the following TP results:
TX UDP
107 Mbits/sec
RX UDP
106 Mbits/sec
TX TCP
72.3 Mbits/sec
RX TCP
80.5 Mbits/sec
Signed-off-by: Assaf Azulay <assaf@ti.com>
this version contains various bug fixes which were contributed by Lior , Bella and Oren :
1. Fix for the duplicate frame detection .
2. Fix for the infinite BAR sending .
3. WA for the ARP request issue in GO mode (caused indirectly by the multicast filtering configured by the host).
4. Fix for the bad frame hard fault.
5. ignore RX HDR Interrupt when antenna priority is at BT.
6. walkaround for CTS2SELF null frame at tx_start - not ran yesterday --> already merged and will be in the next candidate.
7. addition for patch WL8_PG1_PATCH_1_NO_B_RATES_IN_BW_40 when sending all kind of templates.
8. some compilation warnings and SG specific cleanup.
This version was tested on the Lab Setup with the following TP results:
TX UDP
107 Mbits/sec
RX UDP
106 Mbits/sec
TX TCP
72.3 Mbits/sec
RX TCP
80.5 Mbits/sec
Signed-off-by: Assaf Azulay <assaf@ti.com>
Updated firmware to 8.1.0.0.82
- Cleanup unused statistics field and inserting new counters:
1. Beacon early termination counter.
2. Tx aggregation length vs. Rate.
3. Rx aggregation length.
- Separate between the channel tune command to the Phy and
Calibration command.
- Bug fix: Enabling FCTL_PWR_MGMT bit in aggregated frames.
- Bug fix: fixing txStart workaround, thus timeout will not occur
but exchange status does inserted to queue with FAIL indication.
Signed-off-by: Ido Reis <idor@ti.com>
- Cleanup unused statistics field and inserting new counters:
1. Beacon early termination counter.
2. Tx aggregation length vs. Rate.
3. Rx aggregation length.
- Separate between the channel tune command to the Phy and
Calibration command.
- Bug fix: Enabling FCTL_PWR_MGMT bit in aggregated frames.
- Bug fix: fixing txStart workaround, thus timeout will not occur
but exchange status does inserted to queue with FAIL indication.
Signed-off-by: Ido Reis <idor@ti.com>
Updated firmware to 8.1.0.0.81
- Merge from R5 Soft Gemini
- Enable RX-not-complete interrupt for SG
- Fix TX suspend workaround bug
- Fixes for traffic monitor
- Fix for assert when combining peer enabled rates and rate policy
rates returns null
- Correct FLID classification for broadcast frames (affected exiting
power-save when Beacon + TIM set was received)
- Fix for “MISO mode” blocking 40Mhz TX
- Fixes for TCP (WL8 AP vs. WL8 STA)
- PHY FW 8.1.0.0.116
Signed-off-by: Luciano Coelho <coelho@ti.com>
- Merge from R5 Soft Gemini
- Enable RX-not-complete interrupt for SG
- Fix TX suspend workaround bug
- Fixes for traffic monitor
- Fix for assert when combining peer enabled rates and rate policy
rates returns null
- Correct FLID classification for broadcast frames (affected exiting
power-save when Beacon + TIM set was received)
- Fix for “MISO mode” blocking 40Mhz TX
- Fixes for TCP (WL8 AP vs. WL8 STA)
- PHY FW 8.1.0.0.116
Signed-off-by: Luciano Coelho <coelho@ti.com>
Updated FW to 8.1.0.0.80.
New firmware with stability fixes.
Signed-off-by: Luciano Coelho <coelho@ti.com>
New firmware with stability fixes.
Signed-off-by: Luciano Coelho <coelho@ti.com>
fw updated to 8.1.0.0.79
fw updated to 8.1.20.4.77
Signed-off-by: Ido Reis <idor@ti.com>
Signed-off-by: Ido Reis <idor@ti.com>
fw updated to 8.1.20.3.77
Signed-off-by: Ido Reis <idor@ti.com>
Signed-off-by: Ido Reis <idor@ti.com>
fw updated to 8.1.20.2.77
update fw 8.1.20.1.77
firmware updated
ili file added to Android.mk
Signed-off-by: Ido Reis <idor@ti.com>
firmware updated
ili file added to Android.mk
Signed-off-by: Ido Reis <idor@ti.com>
firmware: updated firmware and added ILI file
Updated the firmware to 8.1.20.1.76 and added its ILI file. This is
still an unofficial version used for integration.
Signed-off-by: Luciano Coelho <coelho@ti.com>
Updated the firmware to 8.1.20.1.76 and added its ILI file. This is
still an unofficial version used for integration.
Signed-off-by: Luciano Coelho <coelho@ti.com>
added Android.mk
firmware: add initial firmware
This is firmware version 8.1.19.1.75, which is an unofficial version
with a merged R5 API. This is based on the firmware used in A1.26.
Signed-off-by: Luciano Coelho <coelho@ti.com>
This is firmware version 8.1.19.1.75, which is an unofficial version
with a merged R5 API. This is based on the firmware used in A1.26.
Signed-off-by: Luciano Coelho <coelho@ti.com>