update FW version to 8.1.0.1.83
MAC FW: Rev 8.1.0.1.83
PHY FW: Rev 8.1.0.0.116
udp_rx = 106
tcp_rx = 81.3
tcp_tx = 72.2
udp_tx = 106
Linksys 310N3:
The WA works and the FW detects the frame spacing violation immediately, which results in BA session tear down.
No stuck - TP as expected with NO BAs
Dlink 825:
No stuck - TP as expected
Mostly it works with BA while the spacing is valid.
Sometimes, After some time there is a tear down due to our WA, but still we need
to do more tests to verify whether it is related to our frame spacing violation detection mechanism or not .
Signed-off-by: Assaf Azulay <assaf@ti.com>
MAC FW: Rev 8.1.0.1.83
PHY FW: Rev 8.1.0.0.116
udp_rx = 106
tcp_rx = 81.3
tcp_tx = 72.2
udp_tx = 106
Linksys 310N3:
The WA works and the FW detects the frame spacing violation immediately, which results in BA session tear down.
No stuck - TP as expected with NO BAs
Dlink 825:
No stuck - TP as expected
Mostly it works with BA while the spacing is valid.
Sometimes, After some time there is a tear down due to our WA, but still we need
to do more tests to verify whether it is related to our frame spacing violation detection mechanism or not .
Signed-off-by: Assaf Azulay <assaf@ti.com>
update FW version to 8.1.0.0.83
this version contains various bug fixes which were contributed by Lior , Bella and Oren :
1. Fix for the duplicate frame detection .
2. Fix for the infinite BAR sending .
3. WA for the ARP request issue in GO mode (caused indirectly by the multicast filtering configured by the host).
4. Fix for the bad frame hard fault.
5. ignore RX HDR Interrupt when antenna priority is at BT.
6. walkaround for CTS2SELF null frame at tx_start - not ran yesterday --> already merged and will be in the next candidate.
7. addition for patch WL8_PG1_PATCH_1_NO_B_RATES_IN_BW_40 when sending all kind of templates.
8. some compilation warnings and SG specific cleanup.
This version was tested on the Lab Setup with the following TP results:
TX UDP
107 Mbits/sec
RX UDP
106 Mbits/sec
TX TCP
72.3 Mbits/sec
RX TCP
80.5 Mbits/sec
Signed-off-by: Assaf Azulay <assaf@ti.com>
this version contains various bug fixes which were contributed by Lior , Bella and Oren :
1. Fix for the duplicate frame detection .
2. Fix for the infinite BAR sending .
3. WA for the ARP request issue in GO mode (caused indirectly by the multicast filtering configured by the host).
4. Fix for the bad frame hard fault.
5. ignore RX HDR Interrupt when antenna priority is at BT.
6. walkaround for CTS2SELF null frame at tx_start - not ran yesterday --> already merged and will be in the next candidate.
7. addition for patch WL8_PG1_PATCH_1_NO_B_RATES_IN_BW_40 when sending all kind of templates.
8. some compilation warnings and SG specific cleanup.
This version was tested on the Lab Setup with the following TP results:
TX UDP
107 Mbits/sec
RX UDP
106 Mbits/sec
TX TCP
72.3 Mbits/sec
RX TCP
80.5 Mbits/sec
Signed-off-by: Assaf Azulay <assaf@ti.com>
Updated firmware to 8.1.0.0.82
- Cleanup unused statistics field and inserting new counters:
1. Beacon early termination counter.
2. Tx aggregation length vs. Rate.
3. Rx aggregation length.
- Separate between the channel tune command to the Phy and
Calibration command.
- Bug fix: Enabling FCTL_PWR_MGMT bit in aggregated frames.
- Bug fix: fixing txStart workaround, thus timeout will not occur
but exchange status does inserted to queue with FAIL indication.
Signed-off-by: Ido Reis <idor@ti.com>
- Cleanup unused statistics field and inserting new counters:
1. Beacon early termination counter.
2. Tx aggregation length vs. Rate.
3. Rx aggregation length.
- Separate between the channel tune command to the Phy and
Calibration command.
- Bug fix: Enabling FCTL_PWR_MGMT bit in aggregated frames.
- Bug fix: fixing txStart workaround, thus timeout will not occur
but exchange status does inserted to queue with FAIL indication.
Signed-off-by: Ido Reis <idor@ti.com>
Updated firmware to 8.1.0.0.81
- Merge from R5 Soft Gemini
- Enable RX-not-complete interrupt for SG
- Fix TX suspend workaround bug
- Fixes for traffic monitor
- Fix for assert when combining peer enabled rates and rate policy
rates returns null
- Correct FLID classification for broadcast frames (affected exiting
power-save when Beacon + TIM set was received)
- Fix for “MISO mode” blocking 40Mhz TX
- Fixes for TCP (WL8 AP vs. WL8 STA)
- PHY FW 8.1.0.0.116
Signed-off-by: Luciano Coelho <coelho@ti.com>
- Merge from R5 Soft Gemini
- Enable RX-not-complete interrupt for SG
- Fix TX suspend workaround bug
- Fixes for traffic monitor
- Fix for assert when combining peer enabled rates and rate policy
rates returns null
- Correct FLID classification for broadcast frames (affected exiting
power-save when Beacon + TIM set was received)
- Fix for “MISO mode” blocking 40Mhz TX
- Fixes for TCP (WL8 AP vs. WL8 STA)
- PHY FW 8.1.0.0.116
Signed-off-by: Luciano Coelho <coelho@ti.com>
Updated FW to 8.1.0.0.80.
New firmware with stability fixes.
Signed-off-by: Luciano Coelho <coelho@ti.com>
New firmware with stability fixes.
Signed-off-by: Luciano Coelho <coelho@ti.com>
fw updated to 8.1.0.0.79
fw updated to 8.1.20.4.77
Signed-off-by: Ido Reis <idor@ti.com>
Signed-off-by: Ido Reis <idor@ti.com>
fw updated to 8.1.20.3.77
Signed-off-by: Ido Reis <idor@ti.com>
Signed-off-by: Ido Reis <idor@ti.com>
fw updated to 8.1.20.2.77
update fw 8.1.20.1.77
firmware updated
ili file added to Android.mk
Signed-off-by: Ido Reis <idor@ti.com>
firmware updated
ili file added to Android.mk
Signed-off-by: Ido Reis <idor@ti.com>
firmware: updated firmware and added ILI file
Updated the firmware to 8.1.20.1.76 and added its ILI file. This is
still an unofficial version used for integration.
Signed-off-by: Luciano Coelho <coelho@ti.com>
Updated the firmware to 8.1.20.1.76 and added its ILI file. This is
still an unofficial version used for integration.
Signed-off-by: Luciano Coelho <coelho@ti.com>
added Android.mk
firmware: add initial firmware
This is firmware version 8.1.19.1.75, which is an unofficial version
with a merged R5 API. This is based on the firmware used in A1.26.
Signed-off-by: Luciano Coelho <coelho@ti.com>
This is firmware version 8.1.19.1.75, which is an unofficial version
with a merged R5 API. This is based on the firmware used in A1.26.
Signed-off-by: Luciano Coelho <coelho@ti.com>