setup-env: update setup-env files master
authorGuy Mishol <guym@ti.com>
Wed, 23 Dec 2015 08:44:27 +0000 (10:44 +0200)
committerGuy Mishol <guym@ti.com>
Wed, 23 Dec 2015 08:44:27 +0000 (10:44 +0200)
update setup-env.sample and setup-env files

Signed-off-by: Guy Mishol <guym@ti.com>
setup-env [changed mode: 0644->0755]
setup-env.sample

old mode 100644 (file)
new mode 100755 (executable)
index 9baa8bf..9ecbebc
--- a/setup-env
+++ b/setup-env
 #
 #===========================================================
 # User specific environment settings
-export CROSS_COMPILE="arm-none-linux-gnueabi-"
-export PATH="/home/shahar/toolchain/arm/bin"
-export ROOTFS=/home/shahar/TI/rootfs
-export WORK_SPACE=/home/shahar/TI/workspace
-export KLIB_BUILD=/home/shahar/arm-kernel/linux-3.4.74/arch/arm/kernel
-export BUILD_VERSION="ol_R5.SP7.01"
+export CROSS_COMPILE=<cross compile>
+export PATH="$PATH:<toolchain path>"
+export ROOTFS=<path to root filesystem>
+export WORK_SPACE=<working directory>
+export KLIB_BUILD=<linux-kernel>
+export BUILD_VERSION=<build version>
 # MACHINE_TYPE - The target machine type. Can have one of the following values: "am1808" , "omap3evm" , "am335x"
 # This is needed to build bluetooth components.
 # This parameter is not relevant for ti814x board.
index 0f1864a9695d770404bf3cf326063911294cd756..9ecbebc36f616f6f127d91a3751fab7bee17c0f6 100644 (file)
 #
 #===========================================================
 # User specific environment settings
-export CROSS_COMPILE="arm-none-linux-gnueabi-"
+export CROSS_COMPILE=<cross compile>
 export PATH="$PATH:<toolchain path>"
 export ROOTFS=<path to root filesystem>
 export WORK_SPACE=<working directory>
 export KLIB_BUILD=<linux-kernel>
-export BUILD_VERSION="r8"
+export BUILD_VERSION=<build version>
 # MACHINE_TYPE - The target machine type. Can have one of the following values: "am1808" , "omap3evm" , "am335x"
 # This is needed to build bluetooth components.
 # This parameter is not relevant for ti814x board.