compat-wireless: activate CONFIG_RT2800{USB,PCI}_RT35XX by default.
[wl12xx/compat-wireless.git] / defconfigs / atheros-debug.mk
1 export
3 ## NOTE
4 ## Make sure to have each variable declaration start
5 ## in the first column, no whitespace allowed.
7 ifeq ($(wildcard $(KLIB_BUILD)/.config),)
8 # These will be ignored by compat autoconf
9  CONFIG_PCI=y
10  CONFIG_USB=y
11  CONFIG_PCMCIA=y
12  CONFIG_SSB=m
13 else
14 include $(KLIB_BUILD)/.config
15 endif
17 # We will warn when you don't have MQ support or NET_SCHED enabled.
18 #
19 # We could consider just quiting if MQ and NET_SCHED is disabled
20 # as I suspect all users of this package want 802.11e (WME) and
21 # 802.11n (HT) support.
22 ifneq ($(wildcard $(KLIB_BUILD)/Makefile),)
23 COMPAT_LATEST_VERSION = 37
24 KERNEL_SUBLEVEL := $(shell $(MAKE) -C $(KLIB_BUILD) kernelversion | sed -n 's/^2\.6\.\([0-9]\+\).*/\1/p')
25 COMPAT_VERSIONS := $(shell I=$(COMPAT_LATEST_VERSION); while [ "$$I" -gt $(KERNEL_SUBLEVEL) ]; do echo $$I; I=$$(($$I - 1)); done)
26 $(foreach ver,$(COMPAT_VERSIONS),$(eval CONFIG_COMPAT_KERNEL_$(ver)=y))
28 ifdef CONFIG_COMPAT_KERNEL_24
29 $(error "ERROR: compat-wireless by default supports kernels >= 2.6.24, try enabling only one driver though")
30 endif #CONFIG_COMPAT_KERNEL_24
32 ifeq ($(CONFIG_CFG80211),y)
33 $(error "ERROR: your kernel has CONFIG_CFG80211=y, you should have it CONFIG_CFG80211=m if you want to use this thing.")
34 endif
37 # 2.6.27 has FTRACE_DYNAMIC borked, so we will complain if
38 # you have it enabled, otherwise you will very likely run into
39 # a kernel panic.
40 ifeq ($(KERNEL_SUBLEVEL),27)
41 ifeq ($(CONFIG_DYNAMIC_FTRACE),y)
42 $(error "ERROR: Your 2.6.27 kernel has CONFIG_DYNAMIC_FTRACE, please upgrade your distribution kernel as newer ones should not have this enabled (and if so report a bug) or remove this warning if you know what you are doing")
43 endif
44 endif
46 # This is because with CONFIG_MAC80211 include/linux/skbuff.h will
47 # enable on 2.6.27 a new attribute:
48 #
49 # skb->do_not_encrypt
50 #
51 # and on 2.6.28 another new attribute:
52 #
53 # skb->requeue
54 #
55 # In kernel 2.6.32 both attributes were removed.
56 #
57 ifeq ($(shell test $(KERNEL_SUBLEVEL) -ge 27 -a $(KERNEL_SUBLEVEL) -le 31 && echo yes),yes)
58 ifeq ($(CONFIG_MAC80211),)
59 $(error "ERROR: Your >=2.6.27 and <= 2.6.31 kernel has CONFIG_MAC80211 disabled, you should have it CONFIG_MAC80211=m if you want to use this thing.")
60 endif
61 endif
63 ifneq ($(KERNELRELEASE),) # This prevents a warning
65 ifeq ($(CONFIG_NET_SCHED),)
66  QOS_REQS_MISSING+=CONFIG_NET_SCHED
67 endif
69 ifneq ($(QOS_REQS_MISSING),) # Complain about our missing dependencies
70 $(warning "WARNING: You are running a kernel >= 2.6.23, you should enable in it $(QOS_REQS_MISSING) for 802.11[ne] support")
71 endif
73 endif # build check
74 endif # kernel Makefile check
76 # These both are needed by compat-wireless || compat-bluetooth so enable them
77  CONFIG_COMPAT_RFKILL=y
79 ifeq ($(CONFIG_MAC80211),y)
80 $(error "ERROR: you have MAC80211 compiled into the kernel, CONFIG_MAC80211=y, as such you cannot replace its mac80211 driver. You need this set to CONFIG_MAC80211=m. If you are using Fedora upgrade your kernel as later version should this set as modular. For further information on Fedora see https://bugzilla.redhat.com/show_bug.cgi?id=470143. If you are using your own kernel recompile it and make mac80211 modular")
81 else
82  CONFIG_COMPAT_WIRELESS=y
83  CONFIG_COMPAT_WIRELESS_MODULES=m
84  CONFIG_COMPAT_VAR_MODULES=m
85 # We could technically separate these but not yet, we only have b44
86 # Note that we don't intend on backporting network drivers that
87 # use Multiqueue as that was a pain to backport to kernels older than
88 # 2.6.27. But -- we could just disable those drivers from kernels
89 # older than 2.6.27
90  CONFIG_COMPAT_NETWORK_MODULES=m
91  CONFIG_COMPAT_NET_USB_MODULES=m
92 endif
94 # The Bluetooth compatibility only builds on kernels >= 2.6.27 for now
95 ifndef CONFIG_COMPAT_KERNEL_27
96 ifeq ($(CONFIG_BT),y)
97 # we'll ignore compiling bluetooth
98 else
99  CONFIG_COMPAT_BLUETOOTH=y
100  CONFIG_COMPAT_BLUETOOTH_MODULES=m
101 endif
102 endif #CONFIG_COMPAT_KERNEL_27
104 ifdef CONFIG_COMPAT_KERNEL_33
105 ifdef CONFIG_FW_LOADER
106  CONFIG_COMPAT_FIRMWARE_CLASS=m
107 endif #CONFIG_FW_LOADER
108 endif #CONFIG_COMPAT_KERNEL_33
111 # Wireless subsystem stuff
112 CONFIG_MAC80211=m
114 CONFIG_MAC80211_DEBUGFS=y
115 CONFIG_MAC80211_NOINLINE=y
116 CONFIG_MAC80211_VERBOSE_DEBUG=y
117 CONFIG_MAC80211_HT_DEBUG=y
118 # CONFIG_MAC80211_TKIP_DEBUG=y
119 # CONFIG_MAC80211_IBSS_DEBUG=y
120 CONFIG_MAC80211_VERBOSE_PS_DEBUG=y
121 # CONFIG_MAC80211_VERBOSE_MPL_DEBUG=y
122 # CONFIG_MAC80211_VERBOSE_MHWMP_DEBUG=y
123 CONFIG_MAC80211_DEBUG_COUNTERS=y
124 # CONFIG_MAC80211_DRIVER_API_TRACER=y
126 # choose between pid and minstrel as default rate control algorithm
127 CONFIG_MAC80211_RC_DEFAULT=minstrel_ht
128 CONFIG_MAC80211_RC_DEFAULT_MINSTREL=y
129 # CONFIG_MAC80211_RC_DEFAULT_PID=y
130 # This is the one used by our compat-wireless net/mac80211/rate.c
131 # in case you have and old kernel which is overriding this to pid.
132 CONFIG_COMPAT_MAC80211_RC_DEFAULT=minstrel_ht
133 CONFIG_MAC80211_RC_PID=y
134 CONFIG_MAC80211_RC_MINSTREL=y
135 CONFIG_MAC80211_RC_MINSTREL_HT=y
136 CONFIG_MAC80211_LEDS=y
138 # enable mesh networking too
139 CONFIG_MAC80211_MESH=y
141 CONFIG_CFG80211=m
142 CONFIG_CFG80211_DEFAULT_PS=y
143 CONFIG_CFG80211_DEBUGFS=y
144 # CONFIG_NL80211_TESTMODE=y
145 CONFIG_CFG80211_DEVELOPER_WARNINGS=y
146 CONFIG_CFG80211_REG_DEBUG=y
147 # See below for wext stuff
149 CONFIG_LIB80211=m
150 CONFIG_LIB80211_CRYPT_WEP=m
151 CONFIG_LIB80211_CRYPT_CCMP=m
152 CONFIG_LIB80211_CRYPT_TKIP=m
153 # CONFIG_LIB80211_DEBUG=y
155 CONFIG_BT=m
156 CONFIG_BT_L2CAP=m
157 CONFIG_BT_SCO=m
158 CONFIG_BT_RFCOMM=m
159 CONFIG_BT_RFCOMM_TTY=y
160 CONFIG_BT_BNEP=m
161 CONFIG_BT_BNEP_MC_FILTER=y
162 CONFIG_BT_BNEP_PROTO_FILTER=y
163 # CONFIG_BT_CMTP depends on ISDN_CAPI
164 ifdef CONFIG_ISDN_CAPI
165 CONFIG_BT_CMTP=m
166 endif #CONFIG_ISDN_CAPI
167 CONFIG_BT_HIDP=m
169 CONFIG_BT_HCIUART=M
170 CONFIG_BT_HCIUART_H4=y
171 CONFIG_BT_HCIUART_BCSP=y
172 CONFIG_BT_HCIUART_ATH3K=y
173 CONFIG_BT_HCIUART_LL=y
175 CONFIG_BT_HCIVHCI=m
176 CONFIG_BT_MRVL=m
178 ifdef CONFIG_PCMCIA
179 CONFIG_BT_HCIDTL1=m
180 CONFIG_BT_HCIBT3C=m
181 CONFIG_BT_HCIBLUECARD=m
182 CONFIG_BT_HCIBTUART=m
183 endif #CONFIG_PCMCIA
186 # We need CONFIG_WIRELESS_EXT for CONFIG_CFG80211_WEXT for every kernel 
187 # version. The new way CONFIG_CFG80211_WEXT is called from the kernel 
188 # does not work with compat-wireless because it calls some callback 
189 # function on struct wiphy. This struct is shipped with compat-wireless 
190 # and changes from kernel version to version. We are using the 
191 # wireless_handlers attribute which will be activated by 
192 # CONFIG_WIRELESS_EXT. 
193 ifdef CONFIG_WIRELESS_EXT
194 CONFIG_CFG80211_WEXT=y
195 else #CONFIG_CFG80211_WEXT
196 $(warning "WARNING: CONFIG_CFG80211_WEXT will be deactivated or not working because kernel was compiled with CONFIG_WIRELESS_EXT=n. Tools using wext interface like iwconfig will not work. To activate it build your kernel e.g. with CONFIG_LIBIPW=m.")
197 endif #CONFIG_WIRELESS_EXT
199 ifneq ($(CONFIG_STAGING),)
200  CONFIG_COMPAT_STAGING=m
201 endif
203 # mac80211 test driver
204 CONFIG_MAC80211_HWSIM=m
206 # PCI Drivers
207 ifdef CONFIG_PCI
209 CONFIG_ATH5K=m
210 CONFIG_ATH5K_DEBUG=y
211 CONFIG_ATH9K_HW=m
212 CONFIG_ATH9K=m
213 # Note: once ath9k_htc is added we'll have to move
214 # CONFIG_ATH9K_COMMON to an area that doesn't depend on PCI
215 # as you could then have ath9k disabled but ath9k_htc enabled.
216 CONFIG_ATH9K_COMMON=m
217 CONFIG_ATH9K_DEBUGFS=y
218 CONFIG_ATH9K_PKTLOG=y
219 # Disable this to get minstrel as default, we leave the ath9k
220 # rate control algorithm as the default for now as that is also
221 # default upstream on the kernel. We will move this to minstrel
222 # as default once we get minstrel properly tested and blessed by
223 # our systems engineering team. CCK rates also need to be used
224 # for long range considerations.
225 CONFIG_ATH9K_RATE_CONTROL=y
228 CONFIG_COMPAT_IWLWIFI=m
229 # CONFIG_IWLWIFI_DEBUG=y
230 # CONFIG_IWLWIFI_DEBUGFS=y
231 # CONFIG_IWLWIFI_DEVICE_TRACING=y
232 CONFIG_IWLAGN=m
233 CONFIG_COMPAT_IWL4965=y
234 CONFIG_IWL5000=y
235 CONFIG_IWL3945=m
238 CONFIG_B43=m
239 CONFIG_B43_HWRNG=y
240 CONFIG_B43_PCI_AUTOSELECT=y
241 ifdef CONFIG_PCMCIA
242 CONFIG_B43_PCMCIA=y
243 endif #CONFIG_PCMCIA
244 CONFIG_B43_LEDS=y
245 CONFIG_B43_PHY_LP=y
246 CONFIG_B43_NPHY=y
247 # CONFIG_B43_FORCE_PIO=y
248 # CONFIG_B43_DEBUG=y
250 CONFIG_B43LEGACY=m
251 CONFIG_B43LEGACY_HWRNG=y
252 CONFIG_B43LEGACY_PCI_AUTOSELECT=y
253 CONFIG_B43LEGACY_LEDS=y
254 # CONFIG_B43LEGACY_DEBUG=y
255 CONFIG_B43LEGACY_DMA=y
256 CONFIG_B43LEGACY_PIO=y
258 ifdef CONFIG_WIRELESS_EXT
259 # The Intel ipws
260 CONFIG_LIBIPW=m
261 # CONFIG_LIBIPW_DEBUG=y
263 CONFIG_IPW2100=m
264 CONFIG_IPW2100_MONITOR=y
265 # CONFIG_IPW2100_DEBUG=y
266 CONFIG_IPW2200=m
267 CONFIG_IPW2200_MONITOR=y
268 CONFIG_IPW2200_RADIOTAP=y
269 CONFIG_IPW2200_PROMISCUOUS=y
270 CONFIG_IPW2200_QOS=y
271 # CONFIG_IPW2200_DEBUG=y
272 # The above enables use a second interface prefixed 'rtap'.
273 #           Example usage:
275 # % modprobe ipw2200 rtap_iface=1
276 # % ifconfig rtap0 up
277 # % tethereal -i rtap0
279 # If you do not specify 'rtap_iface=1' as a module parameter then
280 # the rtap interface will not be created and you will need to turn
281 # it on via sysfs:
283 # % echo 1 > /sys/bus/pci/drivers/ipw2200/*/rtap_iface
284 endif #CONFIG_WIRELESS_EXT
286 ifdef CONFIG_SSB
287 # Sonics Silicon Backplane
288 CONFIG_SSB_SPROM=y
289 # CONFIG_SSB_DEBUG=y
291 CONFIG_SSB_BLOCKIO=y
292 CONFIG_SSB_PCIHOST=y
293 CONFIG_SSB_B43_PCI_BRIDGE=y
294 ifdef CONFIG_PCMCIA
295 CONFIG_SSB_PCMCIAHOST=y
296 endif #CONFIG_PCMCIA
297 # CONFIG_SSB_DEBUG=y
298 CONFIG_SSB_DRIVER_PCICORE=y
299 endif #CONFIG_SSB
301 CONFIG_P54_PCI=m
303 CONFIG_B44=m
304 CONFIG_B44_PCI=y
306 CONFIG_RTL8180=m
308 CONFIG_ADM8211=m
310 CONFIG_RT2X00_LIB_PCI=m
311 CONFIG_RT2400PCI=m
312 CONFIG_RT2500PCI=m
313 ifdef CONFIG_CRC_CCITT
314 CONFIG_RT2800PCI=m
315 CONFIG_RT2800PCI_PCI=y
316 # CONFIG_RT2800PCI_RT30XX=y
317 # CONFIG_RT2800PCI_RT35XX=y
318 # CONFIG_RT2800PCI_SOC=y
319 endif #CONFIG_CRC_CCITT
320 NEED_RT2X00=y
322 # Two rt2x00 drivers require firmware: rt61pci and rt73usb. They depend on
323 # CRC to check the firmware. We check here first for the PCI
324 # driver as we're in the PCI section.
325 ifdef CONFIG_CRC_ITU_T
326 CONFIG_RT61PCI=m
327 NEED_RT2X00_FIRMWARE=y
328 endif #CONFIG_CRC_ITU_T
330 CONFIG_MWL8K=m
332 # Ethernet drivers go here
333 CONFIG_ATL1=m
334 CONFIG_ATL2=m
335 CONFIG_ATL1E=m
336 ifdef CONFIG_COMPAT_KERNEL_27
337 CONFIG_ATL1C=n
338 else #CONFIG_COMPAT_KERNEL_27
339 CONFIG_ATL1C=m
340 endif #CONFIG_COMPAT_KERNEL_27
342 ifdef CONFIG_WIRELESS_EXT
343 CONFIG_HERMES=m
344 CONFIG_HERMES_CACHE_FW_ON_INIT=y
345 ifdef CONFIG_PPC_PMAC
346 CONFIG_APPLE_AIRPORT=m
347 endif #CONFIG_PPC_PMAC
348 CONFIG_PLX_HERMES=m
349 CONFIG_TMD_HERMES=m
350 CONFIG_NORTEL_HERMES=m
351 CONFIG_PCI_HERMES=m
352 ifdef CONFIG_PCMCIA
353 CONFIG_PCMCIA_HERMES=m
354 CONFIG_PCMCIA_SPECTRUM=m
355 endif #CONFIG_PCMCIA
356 endif #CONFIG_WIRELESS_EXT
358 endif #CONFIG_PCI
359 ## end of PCI
361 ifdef CONFIG_PCMCIA
363 ifdef CONFIG_COMPAT_KERNEL_27
364 CONFIG_LIBERTAS=n
365 CONFIG_LIBERTAS_CS=n
366 else #CONFIG_COMPAT_KERNEL_27
367 CONFIG_LIBERTAS_CS=m
368 NEED_LIBERTAS=y
369 endif #CONFIG_COMPAT_KERNEL_27
371 endif #CONFIG_PCMCIA
372 ## end of PCMCIA
374 # This is required for some cards
375 CONFIG_EEPROM_93CX6=m
377 # USB Drivers
378 ifdef CONFIG_USB
379 CONFIG_ZD1211RW=m
380 # CONFIG_ZD1211RW_DEBUG=y
382 # Sorry, rndis_wlan uses cancel_work_sync which is new and can't be done in compat...
384 # Wireless RNDIS USB support (RTL8185 802.11g) A-Link WL54PC
385 # All of these devices are based on Broadcom 4320 chip which
386 # is only wireless RNDIS chip known to date.
387 # Note: this depends on CONFIG_USB_NET_RNDIS_HOST and CONFIG_USB_NET_CDCETHER
388 # it also requires new RNDIS_HOST and CDC_ETHER modules which we add
389 ifdef CONFIG_COMPAT_KERNEL_29
390 CONFIG_USB_COMPAT_USBNET=n
391 CONFIG_USB_NET_COMPAT_RNDIS_HOST=n
392 CONFIG_USB_NET_COMPAT_RNDIS_WLAN=n
393 CONFIG_USB_NET_COMPAT_CDCETHER=n
394 else #CONFIG_COMPAT_KERNEL_29
395 CONFIG_USB_COMPAT_USBNET=m
396 ifdef CONFIG_USB_NET_CDCETHER
397 CONFIG_USB_NET_COMPAT_RNDIS_HOST=m
398 CONFIG_USB_NET_COMPAT_RNDIS_WLAN=m
399 endif #CONFIG_USB_NET_CDCETHER
400 CONFIG_USB_NET_COMPAT_CDCETHER=m
401 endif #CONFIG_COMPAT_KERNEL_29
404 CONFIG_P54_USB=m
405 CONFIG_RTL8187=m
406 CONFIG_RTL8187_LEDS=y
408 CONFIG_AT76C50X_USB=m
410 ifndef CONFIG_COMPAT_KERNEL_28
411 CONFIG_AR9170_USB=m
412 CONFIG_AR9170_LEDS=y
413 endif #CONFIG_COMPAT_KERNEL_28
415 ifndef CONFIG_COMPAT_KERNEL_29
416 CONFIG_CARL9170=m
417 CONFIG_CARL9170_LEDS=y
418 CONFIG_CARL9170_DEBUGFS=y
419 CONFIG_CARL9170_WPC=y
420 endif #CONFIG_COMPAT_KERNEL_29
422 # This activates a threading fix for usb urb.
423 # this is mainline commit: b3e670443b7fb8a2d29831b62b44a039c283e351
424 # This fix will be included in some stable releases.
425 CONFIG_COMPAT_USB_URB_THREAD_FIX=y
427 CONFIG_ATH9K_HTC=m
428 CONFIG_ATH9K_HTC_DEBUGFS=y
430 # RT2500USB does not require firmware
431 CONFIG_RT2500USB=m
432 ifdef CONFIG_CRC_CCITT
433 CONFIG_RT2800USB=m
434 CONFIG_RT2800USB_RT30XX=y
435 CONFIG_RT2800USB_RT35XX=y
436 CONFIG_RT2800USB_UNKNOWN=y
437 endif #CONFIG_CRC_CCITT
438 CONFIG_RT2X00_LIB_USB=m
439 NEED_RT2X00=y
440 # RT73USB requires firmware
441 ifdef CONFIG_CRC_ITU_T
442 CONFIG_RT73USB=m
443 NEED_RT2X00_FIRMWARE=y
444 endif #CONFIG_CRC_ITU_T
446 ifdef CONFIG_COMPAT_KERNEL_27
447 CONFIG_LIBERTAS_THINFIRM_USB=n
448 CONFIG_LIBERTAS_USB=n
449 NEED_LIBERTAS=n
450 else #CONFIG_COMPAT_KERNEL_27
451 CONFIG_LIBERTAS_THINFIRM_USB=m
452 CONFIG_LIBERTAS_USB=m
453 NEED_LIBERTAS=y
454 endif #CONFIG_COMPAT_KERNEL_27
456 CONFIG_ORINOCO_USB=m
458 CONFIG_BT_HCIBTUSB=m
459 CONFIG_BT_HCIBCM203X=m
460 CONFIG_BT_HCIBPA10X=m
461 CONFIG_BT_HCIBFUSB=m
462 CONFIG_BT_ATH3K=m
464 endif #CONFIG_USB end of USB driver list
466 ifdef CONFIG_SPI_MASTER
467 ifndef CONFIG_COMPAT_KERNEL_25
469 ifdef CONFIG_CRC7
470 CONFIG_WL1251_SPI=m
471 CONFIG_WL1271_SPI=m
472 endif #CONFIG_CRC7
473 CONFIG_P54_SPI=m
475 ifdef CONFIG_COMPAT_KERNEL_27
476 CONFIG_LIBERTAS_SPI=n
477 NEED_LIBERTAS=n
478 else #CONFIG_COMPAT_KERNEL_27
479 CONFIG_LIBERTAS_SPI=m
480 NEED_LIBERTAS=y
481 endif #CONFIG_COMPAT_KERNEL_27
483 endif #CONFIG_COMPAT_KERNEL_25
484 endif #CONFIG_SPI_MASTER end of SPI driver list
486 ifdef CONFIG_MMC
488 CONFIG_SSB_SDIOHOST=y
489 CONFIG_B43_SDIO=y
491 ifdef CONFIG_CRC7
492 CONFIG_WL1251_SDIO=m
494 ifndef CONFIG_COMPAT_KERNEL_32
495 ifdef CONFIG_WL12XX_PLATFORM_DATA
496 CONFIG_WL1271_SDIO=m
497 endif #CONFIG_WL12XX_PLATFORM_DATA
498 endif #CONFIG_COMPAT_KERNEL_32
500 endif #CONFIG_CRC7
502 ifdef CONFIG_COMPAT_KERNEL_27
503 CONFIG_LIBERTAS_SDIO=n
504 NEED_LIBERTAS=n
505 else #CONFIG_COMPAT_KERNEL_27
506 CONFIG_LIBERTAS_SDIO=m
507 NEED_LIBERTAS=y
508 endif #CONFIG_COMPAT_KERNEL_27
510 CONFIG_IWM=m
511 # CONFIG_IWM_DEBUG=y
513 CONFIG_BT_HCIBTSDIO=m
514 CONFIG_BT_MRVL_SDIO=m
516 ifneq ($(CONFIG_COMPAT_STAGING),)
517 ifdef CONFIG_WIRELESS_EXT
518 CONFIG_ATH6KL_CFG80211=y
519 CONFIG_ATH6KL_DEBUG=y
520 # CONFIG_ATH6KL_DISABLE_TARGET_DBGLOGS is not set
521 # CONFIG_ATH6KL_ENABLE_COEXISTENCE is not set
522 # CONFIG_ATH6KL_ENABLE_HOST_DEBUG is not set
523 CONFIG_ATH6KL_ENABLE_TARGET_DEBUG_PRINTS=y
524 # CONFIG_ATH6KL_HCI_BRIDGE is not set
525 # CONFIG_ATH6KL_HTC_RAW_INTERFACE is not set
526 # CONFIG_ATH6KL_SKIP_ABI_VERSION_CHECK is not set
527 CONFIG_ATH6KL_VIRTUAL_SCATTER_GATHER=y
528 CONFIG_ATH6K_LEGACY=m
530 CONFIG_BRCM80211=m
531 CONFIG_BRCM80211_PCI=y
533 endif #CONFIG_WIRELESS_EXT
534 endif #CONFIG_MMC
537 endif # end of SDIO driver list
539 # Common rt2x00 requirements
540 ifeq ($(NEED_RT2X00),y)
541 CONFIG_RT2X00=y
542 CONFIG_RT2X00_LIB=m
543 CONFIG_RT2800_LIB=m
544 CONFIG_RT2X00_LIB_HT=y
545 CONFIG_RT2X00_LIB_FIRMWARE=y
546 CONFIG_RT2X00_LIB_CRYPTO=y
547 ifdef CONFIG_COMPAT_KERNEL_25
548 CONFIG_RT2X00_LIB_LEDS=n
549 else #CONFIG_COMPAT_KERNEL_25
550 CONFIG_RT2X00_LIB_LEDS=y
551 endif #CONFIG_COMPAT_KERNEL_25
552 # CONFIG_RT2X00_DEBUG=y
553 # CONFIG_RT2X00_LIB_DEBUGFS
554 endif
556 ifeq ($(NEED_RT2X00_FIRMWARE),y)
557 CONFIG_RT2X00_LIB_FIRMWARE=y
558 endif
560 # p54
561 CONFIG_P54_COMMON=m
562 CONFIG_P54_LEDS=y
564 # Atheros
565 CONFIG_ATH_COMMON=m
566 CONFIG_ATH_DEBUG=y
568 CONFIG_WL12XX=y
569 ifdef CONFIG_CRC7
570 CONFIG_WL1251=m
571 CONFIG_WL1271=m
572 endif #CONFIG_CRC7
574 ifdef CONFIG_COMPAT_KERNEL_27
575 CONFIG_LIBERTAS=n
576 else #CONFIG_COMPAT_KERNEL_27
577 ifeq ($(NEED_LIBERTAS),y)
578 CONFIG_LIBERTAS_THINFIRM=m
579 CONFIG_LIBERTAS=m
580 CONFIG_LIBERTAS_MESH=y
581 # CONFIG_LIBERTAS_DEBUG=y
582 endif
583 endif #CONFIG_COMPAT_KERNEL_27
585 # We need the backported rfkill module on kernel < 2.6.31.
586 # In more recent kernel versions use the in kernel rfkill module.
587 ifdef CONFIG_COMPAT_KERNEL_31
588 CONFIG_RFKILL_BACKPORT=m
589 CONFIG_RFKILL_BACKPORT_LEDS=y
590 CONFIG_RFKILL_BACKPORT_INPUT=y
591 endif #CONFIG_COMPAT_KERNEL_31