compat-wireless: sync atheros-debug.mk with config.mk
[wl12xx/compat-wireless.git] / defconfigs / atheros-debug.mk
1 export
3 ## NOTE
4 ## Make sure to have each variable declaration start
5 ## in the first column, no whitespace allowed.
7 ifeq ($(wildcard $(KLIB_BUILD)/.config),)
8 # These will be ignored by compat autoconf
9  CONFIG_PCI=y
10  CONFIG_USB=y
11  CONFIG_PCMCIA=y
12  CONFIG_SSB=m
13 else
14 include $(KLIB_BUILD)/.config
15 endif
17 ifneq ($(wildcard $(KLIB_BUILD)/Makefile),)
19 COMPAT_LATEST_VERSION = 1
21 KERNEL_VERSION := $(shell $(MAKE) -C $(KLIB_BUILD) kernelversion | sed -n 's/^\([0-9]\)\..*/\1/p')
23 ifneq ($(KERNEL_VERSION),2)
24 KERNEL_SUBLEVEL := $(shell $(MAKE) -C $(KLIB_BUILD) kernelversion | sed -n 's/^3\.\([0-9]\+\).*/\1/p')
25 else
26 COMPAT_26LATEST_VERSION = 39
27 KERNEL_26SUBLEVEL := $(shell $(MAKE) -C $(KLIB_BUILD) kernelversion | sed -n 's/^2\.6\.\([0-9]\+\).*/\1/p')
28 COMPAT_26VERSIONS := $(shell I=$(COMPAT_26LATEST_VERSION); while [ "$$I" -gt $(KERNEL_26SUBLEVEL) ]; do echo $$I; I=$$(($$I - 1)); done)
29 $(foreach ver,$(COMPAT_26VERSIONS),$(eval CONFIG_COMPAT_KERNEL_2_6_$(ver)=y))
30 KERNEL_SUBLEVEL := -1
31 endif
33 COMPAT_VERSIONS := $(shell I=$(COMPAT_LATEST_VERSION); while [ "$$I" -gt $(KERNEL_SUBLEVEL) ]; do echo $$I; I=$$(($$I - 1)); done)
34 $(foreach ver,$(COMPAT_VERSIONS),$(eval CONFIG_COMPAT_KERNEL_3_$(ver)=y))
36 ifdef CONFIG_COMPAT_KERNEL_2_6_24
37 $(error "ERROR: compat-wireless by default supports kernels >= 2.6.24, try enabling only one driver though")
38 endif #CONFIG_COMPAT_KERNEL_2_6_24
40 ifeq ($(CONFIG_CFG80211),y)
41 $(error "ERROR: your kernel has CONFIG_CFG80211=y, you should have it CONFIG_CFG80211=m if you want to use this thing.")
42 endif
45 # 2.6.27 has FTRACE_DYNAMIC borked, so we will complain if
46 # you have it enabled, otherwise you will very likely run into
47 # a kernel panic.
48 ifeq ($(shell test $(KERNEL_VERSION) -eq 2 -a $(KERNEL_SUBLEVEL) -eq 27 && echo yes),yes)
49 ifeq ($(CONFIG_DYNAMIC_FTRACE),y)
50 $(error "ERROR: Your 2.6.27 kernel has CONFIG_DYNAMIC_FTRACE, please upgrade your distribution kernel as newer ones should not have this enabled (and if so report a bug) or remove this warning if you know what you are doing")
51 endif
52 endif
54 # This is because with CONFIG_MAC80211 include/linux/skbuff.h will
55 # enable on 2.6.27 a new attribute:
56 #
57 # skb->do_not_encrypt
58 #
59 # and on 2.6.28 another new attribute:
60 #
61 # skb->requeue
62 #
63 # In kernel 2.6.32 both attributes were removed.
64 #
65 ifeq ($(shell test $(KERNEL_VERSION) -eq 2 -a $(KERNEL_SUBLEVEL) -ge 27 -a $(KERNEL_SUBLEVEL) -le 31 && echo yes),yes)
66 ifeq ($(CONFIG_MAC80211),)
67 $(error "ERROR: Your >=2.6.27 and <= 2.6.31 kernel has CONFIG_MAC80211 disabled, you should have it CONFIG_MAC80211=m if you want to use this thing.")
68 endif
69 endif
71 ifneq ($(KERNELRELEASE),) # This prevents a warning
73 # We will warn when you don't have MQ support or NET_SCHED enabled.
74 #
75 # We could consider just quiting if MQ and NET_SCHED is disabled
76 # as I suspect all users of this package want 802.11e (WME) and
77 # 802.11n (HT) support.
78 ifeq ($(CONFIG_NET_SCHED),)
79  QOS_REQS_MISSING+=CONFIG_NET_SCHED
80 endif
82 ifneq ($(QOS_REQS_MISSING),) # Complain about our missing dependencies
83 $(warning "WARNING: You are running a kernel >= 2.6.23, you should enable in it $(QOS_REQS_MISSING) for 802.11[ne] support")
84 endif
86 endif # build check
87 endif # kernel Makefile check
89 # These both are needed by compat-wireless || compat-bluetooth so enable them
90  CONFIG_COMPAT_RFKILL=y
92 ifeq ($(CONFIG_MAC80211),y)
93 $(error "ERROR: you have MAC80211 compiled into the kernel, CONFIG_MAC80211=y, as such you cannot replace its mac80211 driver. You need this set to CONFIG_MAC80211=m. If you are using Fedora upgrade your kernel as later version should this set as modular. For further information on Fedora see https://bugzilla.redhat.com/show_bug.cgi?id=470143. If you are using your own kernel recompile it and make mac80211 modular")
94 else
95  CONFIG_COMPAT_WIRELESS=y
96  CONFIG_COMPAT_WIRELESS_MODULES=m
97  CONFIG_COMPAT_VAR_MODULES=m
98 # We could technically separate these but not yet, we only have b44
99 # Note that we don't intend on backporting network drivers that
100 # use Multiqueue as that was a pain to backport to kernels older than
101 # 2.6.27. But -- we could just disable those drivers from kernels
102 # older than 2.6.27
103  CONFIG_COMPAT_NETWORK_MODULES=m
104  CONFIG_COMPAT_NET_USB_MODULES=m
105 endif
107 # The Bluetooth compatibility only builds on kernels >= 2.6.27 for now
108 ifndef CONFIG_COMPAT_KERNEL_2_6_27
109 ifeq ($(CONFIG_BT),y)
110 # we'll ignore compiling bluetooth
111 else
112  CONFIG_COMPAT_BLUETOOTH=y
113  CONFIG_COMPAT_BLUETOOTH_MODULES=m
114 endif
115 endif #CONFIG_COMPAT_KERNEL_2_6_27
117 ifdef CONFIG_COMPAT_KERNEL_2_6_33
118 ifdef CONFIG_FW_LOADER
119  CONFIG_COMPAT_FIRMWARE_CLASS=m
120 endif #CONFIG_FW_LOADER
121 endif #CONFIG_COMPAT_KERNEL_2_6_33
123 # Wireless subsystem stuff
124 CONFIG_MAC80211=m
126 CONFIG_MAC80211_DEBUGFS=y
127 CONFIG_MAC80211_NOINLINE=y
128 CONFIG_MAC80211_VERBOSE_DEBUG=y
129 CONFIG_MAC80211_HT_DEBUG=y
130 # CONFIG_MAC80211_TKIP_DEBUG=y
131 # CONFIG_MAC80211_IBSS_DEBUG=y
132 CONFIG_MAC80211_VERBOSE_PS_DEBUG=y
133 # CONFIG_MAC80211_VERBOSE_MPL_DEBUG=y
134 # CONFIG_MAC80211_VERBOSE_MHWMP_DEBUG=y
135 CONFIG_MAC80211_DEBUG_COUNTERS=y
136 # CONFIG_MAC80211_DRIVER_API_TRACER=y
138 # choose between pid and minstrel as default rate control algorithm
139 CONFIG_MAC80211_RC_DEFAULT=minstrel_ht
140 CONFIG_MAC80211_RC_DEFAULT_MINSTREL=y
141 # CONFIG_MAC80211_RC_DEFAULT_PID=y
142 # This is the one used by our compat-wireless net/mac80211/rate.c
143 # in case you have and old kernel which is overriding this to pid.
144 CONFIG_COMPAT_MAC80211_RC_DEFAULT=minstrel_ht
145 CONFIG_MAC80211_RC_PID=y
146 CONFIG_MAC80211_RC_MINSTREL=y
147 CONFIG_MAC80211_RC_MINSTREL_HT=y
148 ifdef CONFIG_LEDS_TRIGGERS
149 CONFIG_MAC80211_LEDS=y
150 endif #CONFIG_LEDS_TRIGGERS
152 # enable mesh networking too
153 CONFIG_MAC80211_MESH=y
155 CONFIG_CFG80211=m
156 CONFIG_CFG80211_DEFAULT_PS=y
157 CONFIG_CFG80211_DEBUGFS=y
158 # CONFIG_NL80211_TESTMODE=y
159 CONFIG_CFG80211_DEVELOPER_WARNINGS=y
160 CONFIG_CFG80211_REG_DEBUG=y
161 # See below for wext stuff
163 CONFIG_LIB80211=m
164 CONFIG_LIB80211_CRYPT_WEP=m
165 CONFIG_LIB80211_CRYPT_CCMP=m
166 CONFIG_LIB80211_CRYPT_TKIP=m
167 # CONFIG_LIB80211_DEBUG=y
169 CONFIG_BT=m
170 CONFIG_COMPAT_BT_L2CAP=y
171 CONFIG_COMPAT_BT_SCO=y
172 CONFIG_BT_RFCOMM=m
173 CONFIG_BT_RFCOMM_TTY=y
174 CONFIG_BT_BNEP=m
175 CONFIG_BT_BNEP_MC_FILTER=y
176 CONFIG_BT_BNEP_PROTO_FILTER=y
177 # CONFIG_BT_CMTP depends on ISDN_CAPI
178 ifdef CONFIG_ISDN_CAPI
179 CONFIG_BT_CMTP=m
180 endif #CONFIG_ISDN_CAPI
181 ifndef CONFIG_COMPAT_KERNEL_2_6_28
182 CONFIG_COMPAT_BT_HIDP=m
183 endif #CONFIG_COMPAT_KERNEL_2_6_28
185 CONFIG_BT_HCIUART=M
186 CONFIG_BT_HCIUART_H4=y
187 CONFIG_BT_HCIUART_BCSP=y
188 CONFIG_BT_HCIUART_ATH3K=y
189 CONFIG_BT_HCIUART_LL=y
191 CONFIG_BT_HCIVHCI=m
192 CONFIG_BT_MRVL=m
194 ifdef CONFIG_PCMCIA
195 CONFIG_BT_HCIDTL1=m
196 CONFIG_BT_HCIBT3C=m
197 CONFIG_BT_HCIBLUECARD=m
198 CONFIG_BT_HCIBTUART=m
199 endif #CONFIG_PCMCIA
202 # We need CONFIG_WIRELESS_EXT for CONFIG_CFG80211_WEXT for every kernel 
203 # version. The new way CONFIG_CFG80211_WEXT is called from the kernel 
204 # does not work with compat-wireless because it calls some callback 
205 # function on struct wiphy. This struct is shipped with compat-wireless 
206 # and changes from kernel version to version. We are using the 
207 # wireless_handlers attribute which will be activated by 
208 # CONFIG_WIRELESS_EXT. 
209 ifdef CONFIG_WIRELESS_EXT
210 CONFIG_CFG80211_WEXT=y
211 else #CONFIG_CFG80211_WEXT
212 $(warning "WARNING: CONFIG_CFG80211_WEXT will be deactivated or not working because kernel was compiled with CONFIG_WIRELESS_EXT=n. Tools using wext interface like iwconfig will not work. To activate it build your kernel e.g. with CONFIG_LIBIPW=m.")
213 endif #CONFIG_WIRELESS_EXT
215 ifdef CONFIG_STAGING
216 CONFIG_COMPAT_STAGING=m
217 endif #CONFIG_STAGING
219 # mac80211 test driver
220 CONFIG_MAC80211_HWSIM=m
222 CONFIG_ATH5K=m
223 CONFIG_ATH5K_DEBUG=y
224 # CONFIG_ATH5K_AHB=y
226 CONFIG_ATH9K=m
227 CONFIG_ATH9K_HW=m
228 CONFIG_ATH9K_COMMON=m
229 CONFIG_ATH9K_DEBUGFS=y
230 # CONFIG_ATH9K_AHB=y
231 CONFIG_ATH9K_PKTLOG=y
233 # Disable this to get minstrel as default, we leave the ath9k
234 # rate control algorithm as the default for now as that is also
235 # default upstream on the kernel. We will move this to minstrel
236 # as default once we get minstrel properly tested and blessed by
237 # our systems engineering team. CCK rates also need to be used
238 # for long range considerations.
239 CONFIG_ATH9K_RATE_CONTROL=y
241 # PCI Drivers
242 ifdef CONFIG_PCI
244 CONFIG_ATH5K_PCI=y
245 CONFIG_ATH9K_PCI=y
247 CONFIG_IWLAGN=m
248 # CONFIG_IWLWIFI_DEBUG=y
249 # CONFIG_IWLWIFI_DEBUGFS=y
250 # CONFIG_IWLWIFI_DEVICE_TRACING=y
251 # CONFIG_IWLWIFI_DEBUG_EXPERIMENTAL_UCODE=y
252 CONFIG_IWL_P2P=y
254 CONFIG_IWLWIFI_LEGACY=m
255 CONFIG_COMPAT_IWL4965=m
256 CONFIG_IWL3945=m
257 # CONFIG_IWLWIFI_LEGACY_DEBUG=y
258 # CONFIG_IWLWIFI_LEGACY_DEBUGFS=y
259 # CONFIG_IWLWIFI_LEGACY_DEVICE_TRACING=y
262 CONFIG_B43=m
263 CONFIG_B43_HWRNG=y
264 CONFIG_B43_PCI_AUTOSELECT=y
265 ifdef CONFIG_PCMCIA
266 CONFIG_B43_PCMCIA=y
267 endif #CONFIG_PCMCIA
268 ifdef CONFIG_MAC80211_LEDS
269 CONFIG_B43_LEDS=y
270 endif #CONFIG_MAC80211_LEDS
271 CONFIG_B43_PHY_LP=y
272 CONFIG_B43_PHY_N=y
273 # CONFIG_B43_FORCE_PIO=y
274 # CONFIG_B43_DEBUG=y
276 CONFIG_B43LEGACY=m
277 CONFIG_B43LEGACY_HWRNG=y
278 CONFIG_B43LEGACY_PCI_AUTOSELECT=y
279 ifdef CONFIG_MAC80211_LEDS
280 CONFIG_B43LEGACY_LEDS=y
281 endif #CONFIG_MAC80211_LEDS
282 # CONFIG_B43LEGACY_DEBUG=y
283 CONFIG_B43LEGACY_DMA=y
284 CONFIG_B43LEGACY_PIO=y
286 ifdef CONFIG_WIRELESS_EXT
287 # The Intel ipws
288 CONFIG_LIBIPW=m
289 # CONFIG_LIBIPW_DEBUG=y
291 CONFIG_IPW2100=m
292 CONFIG_IPW2100_MONITOR=y
293 # CONFIG_IPW2100_DEBUG=y
294 CONFIG_IPW2200=m
295 CONFIG_IPW2200_MONITOR=y
296 CONFIG_IPW2200_RADIOTAP=y
297 CONFIG_IPW2200_PROMISCUOUS=y
298 CONFIG_IPW2200_QOS=y
299 # CONFIG_IPW2200_DEBUG=y
300 # The above enables use a second interface prefixed 'rtap'.
301 #           Example usage:
303 # % modprobe ipw2200 rtap_iface=1
304 # % ifconfig rtap0 up
305 # % tethereal -i rtap0
307 # If you do not specify 'rtap_iface=1' as a module parameter then
308 # the rtap interface will not be created and you will need to turn
309 # it on via sysfs:
311 # % echo 1 > /sys/bus/pci/drivers/ipw2200/*/rtap_iface
312 endif #CONFIG_WIRELESS_EXT
314 ifdef CONFIG_SSB
315 # Sonics Silicon Backplane
316 CONFIG_SSB_SPROM=y
318 CONFIG_SSB_BLOCKIO=y
319 CONFIG_SSB_PCIHOST=y
320 CONFIG_SSB_B43_PCI_BRIDGE=y
321 ifdef CONFIG_PCMCIA
322 CONFIG_SSB_PCMCIAHOST=y
323 endif #CONFIG_PCMCIA
324 # CONFIG_SSB_DEBUG=y
325 CONFIG_SSB_DRIVER_PCICORE=y
326 endif #CONFIG_SSB
328 CONFIG_P54_PCI=m
330 CONFIG_B44=m
331 CONFIG_B44_PCI=y
333 CONFIG_RTL8180=m
335 CONFIG_ADM8211=m
337 CONFIG_RT2X00_LIB_PCI=m
338 CONFIG_RT2400PCI=m
339 CONFIG_RT2500PCI=m
340 ifdef CONFIG_CRC_CCITT
341 CONFIG_RT2800PCI=m
342 CONFIG_RT2800PCI_RT33XX=y
343 CONFIG_RT2800PCI_RT35XX=y
344 # CONFIG_RT2800PCI_RT53XX=y
345 endif #CONFIG_CRC_CCITT
346 NEED_RT2X00=y
348 # Two rt2x00 drivers require firmware: rt61pci and rt73usb. They depend on
349 # CRC to check the firmware. We check here first for the PCI
350 # driver as we're in the PCI section.
351 ifdef CONFIG_CRC_ITU_T
352 CONFIG_RT61PCI=m
353 endif #CONFIG_CRC_ITU_T
355 CONFIG_MWL8K=m
357 # Ethernet drivers go here
358 CONFIG_ATL1=m
359 CONFIG_ATL2=m
360 CONFIG_ATL1E=m
361 ifdef CONFIG_COMPAT_KERNEL_2_6_27
362 CONFIG_ATL1C=n
363 else #CONFIG_COMPAT_KERNEL_2_6_27
364 CONFIG_ATL1C=m
365 endif #CONFIG_COMPAT_KERNEL_2_6_27
367 ifdef CONFIG_WIRELESS_EXT
368 CONFIG_HERMES=m
369 CONFIG_HERMES_CACHE_FW_ON_INIT=y
370 ifdef CONFIG_PPC_PMAC
371 CONFIG_APPLE_AIRPORT=m
372 endif #CONFIG_PPC_PMAC
373 CONFIG_PLX_HERMES=m
374 CONFIG_TMD_HERMES=m
375 CONFIG_NORTEL_HERMES=m
376 CONFIG_PCI_HERMES=m
377 ifdef CONFIG_PCMCIA
378 CONFIG_PCMCIA_HERMES=m
379 CONFIG_PCMCIA_SPECTRUM=m
380 endif #CONFIG_PCMCIA
381 endif #CONFIG_WIRELESS_EXT
383 CONFIG_RTL8192CE=m
384 CONFIG_RTL8192SE=m
386 ifdef CONFIG_COMPAT_STAGING
387 CONFIG_BRCMSMAC=m
388 endif #CONFIG_COMPAT_STAGING
390 endif #CONFIG_PCI
391 ## end of PCI
393 ifdef CONFIG_PCMCIA
395 ifdef CONFIG_COMPAT_KERNEL_2_6_27
396 CONFIG_LIBERTAS=n
397 CONFIG_LIBERTAS_CS=n
398 else #CONFIG_COMPAT_KERNEL_2_6_27
399 CONFIG_LIBERTAS_CS=m
400 NEED_LIBERTAS=y
401 endif #CONFIG_COMPAT_KERNEL_2_6_27
403 endif #CONFIG_PCMCIA
404 ## end of PCMCIA
406 # This is required for some cards
407 CONFIG_EEPROM_93CX6=m
409 # USB Drivers
410 ifdef CONFIG_USB
411 ifndef CONFIG_COMPAT_KERNEL_2_6_29
412 CONFIG_COMPAT_ZD1211RW=m
413 # CONFIG_ZD1211RW_DEBUG=y
414 endif #CONFIG_COMPAT_KERNEL_2_6_29
416 # Sorry, rndis_wlan uses cancel_work_sync which is new and can't be done in compat...
418 # Wireless RNDIS USB support (RTL8185 802.11g) A-Link WL54PC
419 # All of these devices are based on Broadcom 4320 chip which
420 # is only wireless RNDIS chip known to date.
421 # Note: this depends on CONFIG_USB_NET_RNDIS_HOST and CONFIG_USB_NET_CDCETHER
422 # it also requires new RNDIS_HOST and CDC_ETHER modules which we add
423 ifdef CONFIG_COMPAT_KERNEL_2_6_29
424 CONFIG_USB_COMPAT_USBNET=n
425 CONFIG_USB_NET_COMPAT_RNDIS_HOST=n
426 CONFIG_USB_NET_COMPAT_RNDIS_WLAN=n
427 CONFIG_USB_NET_COMPAT_CDCETHER=n
428 else #CONFIG_COMPAT_KERNEL_2_6_29
429 CONFIG_USB_COMPAT_USBNET=m
430 ifdef CONFIG_USB_NET_CDCETHER
431 CONFIG_USB_NET_COMPAT_RNDIS_HOST=m
432 CONFIG_USB_NET_COMPAT_RNDIS_WLAN=m
433 endif #CONFIG_USB_NET_CDCETHER
434 ifdef CONFIG_USB_NET_CDCETHER_MODULE
435 CONFIG_USB_NET_COMPAT_RNDIS_HOST=m
436 CONFIG_USB_NET_COMPAT_RNDIS_WLAN=m
437 endif #CONFIG_USB_NET_CDCETHER
438 CONFIG_USB_NET_COMPAT_CDCETHER=m
439 endif #CONFIG_COMPAT_KERNEL_2_6_29
442 CONFIG_P54_USB=m
443 CONFIG_RTL8187=m
444 ifdef CONFIG_MAC80211_LEDS
445 CONFIG_RTL8187_LEDS=y
446 endif #CONFIG_MAC80211_LEDS
448 CONFIG_AT76C50X_USB=m
450 ifndef CONFIG_COMPAT_KERNEL_2_6_29
451 CONFIG_CARL9170=m
452 ifdef CONFIG_MAC80211_LEDS
453 CONFIG_CARL9170_LEDS=y
454 endif #CONFIG_MAC80211_LEDS
455 CONFIG_CARL9170_DEBUGFS=y
456 CONFIG_CARL9170_WPC=y
457 endif #CONFIG_COMPAT_KERNEL_2_6_29
459 # This activates a threading fix for usb urb.
460 # this is mainline commit: b3e670443b7fb8a2d29831b62b44a039c283e351
461 # This fix will be included in some stable releases.
462 CONFIG_COMPAT_USB_URB_THREAD_FIX=y
464 CONFIG_ATH9K_HTC=m
465 CONFIG_ATH9K_HTC_DEBUGFS=y
467 # RT2500USB does not require firmware
468 CONFIG_RT2500USB=m
469 ifdef CONFIG_CRC_CCITT
470 CONFIG_RT2800USB=m
471 CONFIG_RT2800USB_RT33XX=y
472 CONFIG_RT2800USB_RT35XX=y
473 # CONFIG_RT2800USB_RT53XX=y
474 CONFIG_RT2800USB_UNKNOWN=y
475 endif #CONFIG_CRC_CCITT
476 CONFIG_RT2X00_LIB_USB=m
477 NEED_RT2X00=y
478 # RT73USB requires firmware
479 ifdef CONFIG_CRC_ITU_T
480 CONFIG_RT73USB=m
481 endif #CONFIG_CRC_ITU_T
483 ifdef CONFIG_COMPAT_KERNEL_2_6_27
484 CONFIG_LIBERTAS_THINFIRM_USB=n
485 CONFIG_LIBERTAS_USB=n
486 NEED_LIBERTAS=n
487 else #CONFIG_COMPAT_KERNEL_2_6_27
488 CONFIG_LIBERTAS_THINFIRM_USB=m
489 CONFIG_LIBERTAS_USB=m
490 NEED_LIBERTAS=y
491 endif #CONFIG_COMPAT_KERNEL_2_6_27
493 CONFIG_ORINOCO_USB=m
495 CONFIG_BT_HCIBTUSB=m
496 CONFIG_BT_HCIBCM203X=m
497 CONFIG_BT_HCIBPA10X=m
498 CONFIG_BT_HCIBFUSB=m
499 CONFIG_BT_ATH3K=m
501 CONFIG_RTL8192CU=m
503 endif #CONFIG_USB end of USB driver list
505 ifdef CONFIG_SPI_MASTER
506 ifndef CONFIG_COMPAT_KERNEL_2_6_25
508 ifdef CONFIG_CRC7
509 CONFIG_WL1251_SPI=m
510 CONFIG_WL12XX_SPI=m
511 endif #CONFIG_CRC7
512 CONFIG_P54_SPI=m
514 ifdef CONFIG_COMPAT_KERNEL_2_6_27
515 CONFIG_LIBERTAS_SPI=n
516 NEED_LIBERTAS=n
517 else #CONFIG_COMPAT_KERNEL_2_6_27
518 CONFIG_LIBERTAS_SPI=m
519 NEED_LIBERTAS=y
520 endif #CONFIG_COMPAT_KERNEL_2_6_27
522 endif #CONFIG_COMPAT_KERNEL_2_6_25
523 endif #CONFIG_SPI_MASTER end of SPI driver list
525 ifdef CONFIG_MMC
527 CONFIG_SSB_SDIOHOST=y
528 CONFIG_B43_SDIO=y
530 ifdef CONFIG_CRC7
531 ifdef CONFIG_WL12XX_PLATFORM_DATA
532 CONFIG_COMPAT_WL1251_SDIO=m
533 endif #CONFIG_WL12XX_PLATFORM_DATA
535 ifndef CONFIG_COMPAT_KERNEL_2_6_32
536 ifdef CONFIG_WL12XX_PLATFORM_DATA
537 CONFIG_COMPAT_WL12XX_SDIO=m
538 endif #CONFIG_WL12XX_PLATFORM_DATA
539 endif #CONFIG_COMPAT_KERNEL_2_6_32
541 endif #CONFIG_CRC7
543 CONFIG_MWIFIEX_SDIO=m
545 ifdef CONFIG_COMPAT_KERNEL_2_6_27
546 CONFIG_LIBERTAS_SDIO=n
547 NEED_LIBERTAS=n
548 else #CONFIG_COMPAT_KERNEL_2_6_27
549 CONFIG_LIBERTAS_SDIO=m
550 NEED_LIBERTAS=y
551 endif #CONFIG_COMPAT_KERNEL_2_6_27
553 CONFIG_IWM=m
554 # CONFIG_IWM_DEBUG=y
556 CONFIG_BT_HCIBTSDIO=m
557 CONFIG_BT_MRVL_SDIO=m
559 ifdef CONFIG_COMPAT_STAGING
560 ifdef CONFIG_WIRELESS_EXT
561 # CONFIG_ATH6KL_DISABLE_TARGET_DBGLOGS is not set
562 # CONFIG_ATH6KL_ENABLE_COEXISTENCE is not set
563 # CONFIG_ATH6KL_ENABLE_HOST_DEBUG is not set
564 CONFIG_ATH6KL_ENABLE_TARGET_DEBUG_PRINTS=y
565 # CONFIG_ATH6KL_HCI_BRIDGE is not set
566 # CONFIG_ATH6KL_HTC_RAW_INTERFACE is not set
567 # CONFIG_ATH6KL_SKIP_ABI_VERSION_CHECK is not set
568 CONFIG_ATH6KL_VIRTUAL_SCATTER_GATHER=y
569 CONFIG_ATH6K_LEGACY=m
571 CONFIG_BRCMFMAC=m
573 endif #CONFIG_WIRELESS_EXT
574 endif #CONFIG_COMPAT_STAGING
577 endif #CONFIG_MMC
579 CONFIG_RTLWIFI=m
580 CONFIG_RTL8192C_COMMON=m
582 # Common rt2x00 requirements
583 ifeq ($(NEED_RT2X00),y)
584 CONFIG_RT2X00=y
585 CONFIG_RT2X00_LIB=m
586 CONFIG_RT2800_LIB=m
587 CONFIG_RT2X00_LIB_FIRMWARE=y
588 CONFIG_RT2X00_LIB_CRYPTO=y
589 # CONFIG_RT2X00_LIB_SOC=y
590 ifdef CONFIG_COMPAT_KERNEL_2_6_25
591 CONFIG_RT2X00_LIB_LEDS=n
592 else #CONFIG_COMPAT_KERNEL_2_6_25
593 ifdef CONFIG_LEDS_CLASS
594 CONFIG_RT2X00_LIB_LEDS=y
595 endif #CONFIG_LEDS_CLASS
596 endif #CONFIG_COMPAT_KERNEL_2_6_25
597 # CONFIG_RT2X00_DEBUG=y
598 # CONFIG_RT2X00_LIB_DEBUGFS
599 endif
601 # p54
602 CONFIG_P54_COMMON=m
603 ifdef CONFIG_MAC80211_LEDS
604 CONFIG_P54_LEDS=y
605 endif #CONFIG_MAC80211_LEDS
607 # Atheros
608 CONFIG_ATH_COMMON=m
609 CONFIG_ATH_DEBUG=y
611 ifdef CONFIG_COMPAT_STAGING
612 CONFIG_BRCMUTIL=m
613 # CONFIG_BRCMDBG=y
614 endif #CONFIG_COMPAT_STAGING
616 ifdef CONFIG_CRC7
617 CONFIG_WL1251=m
618 CONFIG_WL12XX=m
619 CONFIG_WL12XX_HT=y
620 endif #CONFIG_CRC7
622 CONFIG_MWIFIEX=m
624 ifdef CONFIG_COMPAT_KERNEL_2_6_27
625 CONFIG_LIBERTAS=n
626 else #CONFIG_COMPAT_KERNEL_2_6_27
627 ifeq ($(NEED_LIBERTAS),y)
628 CONFIG_LIBERTAS_THINFIRM=m
629 CONFIG_LIBERTAS=m
630 CONFIG_LIBERTAS_MESH=y
631 # CONFIG_LIBERTAS_DEBUG=y
632 endif
633 endif #CONFIG_COMPAT_KERNEL_2_6_27
635 # We need the backported rfkill module on kernel < 2.6.31.
636 # In more recent kernel versions use the in kernel rfkill module.
637 ifdef CONFIG_COMPAT_KERNEL_2_6_31
638 CONFIG_RFKILL_BACKPORT=m
639 ifdef CONFIG_LEDS_TRIGGERS
640 CONFIG_RFKILL_BACKPORT_LEDS=y
641 endif #CONFIG_LEDS_TRIGGERS
642 CONFIG_RFKILL_BACKPORT_INPUT=y
643 endif #CONFIG_COMPAT_KERNEL_2_6_31