diff --git a/linux-next-pending/0011-ath9k-remove-VEOL-support-for-ad-hoc.patch b/linux-next-pending/0011-ath9k-remove-VEOL-support-for-ad-hoc.patch
+++ /dev/null
@@ -1,120 +0,0 @@
-From 6b0d6c3dd1cbc5508420115cc9401c3bccaa8f60 Mon Sep 17 00:00:00 2001
-From: Felix Fietkau <nbd@openwrt.org>
-Date: Thu, 13 May 2010 20:37:25 +0200
-Subject: [PATCH 11/20] ath9k: remove VEOL support for ad-hoc
-
-With VEOL, Beacon transmission in ad-hoc does not currently work.
-I believe for larger ad-hoc networks, VEOL is too unreliable, as
-it can get beacon transmissions stuck during synchronization.
-Use SWBA based beacon trasmission similar to AP mode instead.
-
-Signed-off-by: Felix Fietkau <nbd@openwrt.org>
----
- drivers/net/wireless/ath/ath9k/beacon.c | 63 +++++--------------------------
- 1 files changed, 10 insertions(+), 53 deletions(-)
-
-diff --git a/drivers/net/wireless/ath/ath9k/beacon.c b/drivers/net/wireless/ath/ath9k/beacon.c
-index 77face7..f43d85a 100644
---- a/drivers/net/wireless/ath/ath9k/beacon.c
-+++ b/drivers/net/wireless/ath/ath9k/beacon.c
-@@ -76,22 +76,13 @@ static void ath_beacon_setup(struct ath_softc *sc, struct ath_vif *avp,
- ds = bf->bf_desc;
- flags = ATH9K_TXDESC_NOACK;
-
-- if (((sc->sc_ah->opmode == NL80211_IFTYPE_ADHOC) ||
-- (sc->sc_ah->opmode == NL80211_IFTYPE_MESH_POINT)) &&
-- (ah->caps.hw_caps & ATH9K_HW_CAP_VEOL)) {
-- ds->ds_link = bf->bf_daddr; /* self-linked */
-- flags |= ATH9K_TXDESC_VEOL;
-- /* Let hardware handle antenna switching. */
-- antenna = 0;
-- } else {
-- ds->ds_link = 0;
-- /*
-- * Switch antenna every beacon.
-- * Should only switch every beacon period, not for every SWBA
-- * XXX assumes two antennae
-- */
-- antenna = ((sc->beacon.ast_be_xmit / sc->nbcnvifs) & 1 ? 2 : 1);
-- }
-+ ds->ds_link = 0;
-+ /*
-+ * Switch antenna every beacon.
-+ * Should only switch every beacon period, not for every SWBA
-+ * XXX assumes two antennae
-+ */
-+ antenna = ((sc->beacon.ast_be_xmit / sc->nbcnvifs) & 1 ? 2 : 1);
-
- sband = &sc->sbands[common->hw->conf.channel->band];
- rate = sband->bitrates[rateidx].hw_value;
-@@ -215,36 +206,6 @@ static struct ath_buf *ath_beacon_generate(struct ieee80211_hw *hw,
- return bf;
- }
-
--/*
-- * Startup beacon transmission for adhoc mode when they are sent entirely
-- * by the hardware using the self-linked descriptor + veol trick.
--*/
--static void ath_beacon_start_adhoc(struct ath_softc *sc,
-- struct ieee80211_vif *vif)
--{
-- struct ath_hw *ah = sc->sc_ah;
-- struct ath_common *common = ath9k_hw_common(ah);
-- struct ath_buf *bf;
-- struct ath_vif *avp;
-- struct sk_buff *skb;
--
-- avp = (void *)vif->drv_priv;
--
-- if (avp->av_bcbuf == NULL)
-- return;
--
-- bf = avp->av_bcbuf;
-- skb = bf->bf_mpdu;
--
-- ath_beacon_setup(sc, avp, bf, 0);
--
-- /* NB: caller is known to have already stopped tx dma */
-- ath9k_hw_puttxbuf(ah, sc->beacon.beaconq, bf->bf_daddr);
-- ath9k_hw_txstart(ah, sc->beacon.beaconq);
-- ath_print(common, ATH_DBG_BEACON, "TXDP%u = %llx (%p)\n",
-- sc->beacon.beaconq, ito64(bf->bf_daddr), bf->bf_desc);
--}
--
- int ath_beacon_alloc(struct ath_wiphy *aphy, struct ieee80211_vif *vif)
- {
- struct ath_softc *sc = aphy->sc;
-@@ -265,7 +226,8 @@ int ath_beacon_alloc(struct ath_wiphy *aphy, struct ieee80211_vif *vif)
- list_del(&avp->av_bcbuf->list);
-
- if (sc->sc_ah->opmode == NL80211_IFTYPE_AP ||
-- !(sc->sc_ah->caps.hw_caps & ATH9K_HW_CAP_VEOL)) {
-+ sc->sc_ah->opmode == NL80211_IFTYPE_ADHOC ||
-+ sc->sc_ah->opmode == NL80211_IFTYPE_MESH_POINT) {
- int slot;
- /*
- * Assign the vif to a beacon xmit slot. As
-@@ -715,8 +677,7 @@ static void ath_beacon_config_adhoc(struct ath_softc *sc,
- * self-linked tx descriptor and let the hardware deal with things.
- */
- intval |= ATH9K_BEACON_ENA;
-- if (!(ah->caps.hw_caps & ATH9K_HW_CAP_VEOL))
-- ah->imask |= ATH9K_INT_SWBA;
-+ ah->imask |= ATH9K_INT_SWBA;
-
- ath_beaconq_config(sc);
-
-@@ -726,10 +687,6 @@ static void ath_beacon_config_adhoc(struct ath_softc *sc,
- ath9k_beacon_init(sc, nexttbtt, intval);
- sc->beacon.bmisscnt = 0;
- ath9k_hw_set_interrupts(ah, ah->imask);
--
-- /* FIXME: Handle properly when vif is NULL */
-- if (vif && ah->caps.hw_caps & ATH9K_HW_CAP_VEOL)
-- ath_beacon_start_adhoc(sc, vif);
- }
-
- void ath_beacon_config(struct ath_softc *sc, struct ieee80211_vif *vif)
---
-1.6.3.3
-