11 years agoctrl_iface: allow forcing go_intent during p2p_connect (ANDROID) R5.xx_Build-10 R5.xx_Build-11 R5.xx_Build-12 R5.xx_Build-13 R5.xx_Build-14 R5.xx_Build-15 R5.xx_Build-16 R5.xx_Build-17 R5.xx_Build-19 R5.xx_Build-57 R5.xx_Build-58 R5.xx_Build-6 R5.xx_Build-7 R5.xx_Build-8 R5.xx_Build-9 R8.xx_Build-10 R8.xx_Build-2 R8.xx_Build-3 R8.xx_Build-4 R8.xx_Build-5 R8.xx_Build-6 R8.xx_Build-7 R8.xx_Build-8 R8.xx_Build-9 ol_r8.a3.14 ol_r8.a4.01
ctrl_iface: allow forcing go_intent during p2p_connect (ANDROID)
Allow the p2p_connect command to ignore android p2p concurrency
considerations.
Use the command line argument "no_p2p_conc" to p2p_connect in order to
be able to set the go_intent.
For instance:
wpa_cli p2p_connect 00:11:22:33:44:55 pbc no_p2p_conc go_intent=3
Signed-off-by: Arik Nemtsov <arik@wizery.com>
Allow the p2p_connect command to ignore android p2p concurrency
considerations.
Use the command line argument "no_p2p_conc" to p2p_connect in order to
be able to set the go_intent.
For instance:
wpa_cli p2p_connect 00:11:22:33:44:55 pbc no_p2p_conc go_intent=3
Signed-off-by: Arik Nemtsov <arik@wizery.com>
Add P2P IEs to probe requests only when in P2P (UPSTREAM)
The current code caused P2P and consquently WPS IEs to be added
to any probe as the check was for non null global->p2p.
global->p2p gets set whenever P2P is initialized globally
and that occurs on the first interface init.
Fix this by indicating wps is in use only when in active P2P
discovery or connection establishement.
(i.e. not P2P_IDLE - either doing search, neg or provisioning)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
The current code caused P2P and consquently WPS IEs to be added
to any probe as the check was for non null global->p2p.
global->p2p gets set whenever P2P is initialized globally
and that occurs on the first interface init.
Fix this by indicating wps is in use only when in active P2P
discovery or connection establishement.
(i.e. not P2P_IDLE - either doing search, neg or provisioning)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
WPS: fix nonce comparisons (UPSTREAM)
Multiple memcmps of nonces were actually comparing
only the first byte instead of all 16 bytes.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Multiple memcmps of nonces were actually comparing
only the first byte instead of all 16 bytes.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Fix adding extra ies in sched scan (UPSTREAM)
Refactoring done in
commit 46ee04 IEEE 802.11u: Allow Interworking and HESSID to be configured
broke adding extra ies in sched scan.
Fix it and remove unused params arg in wpa_supplicant_extra_ies.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Refactoring done in
commit 46ee04 IEEE 802.11u: Allow Interworking and HESSID to be configured
broke adding extra ies in sched scan.
Fix it and remove unused params arg in wpa_supplicant_extra_ies.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
P2P: Increase GO Negotiation timeouts
p2p_set_timeout() calls in GO Neg Req/Resp TX callbacks used timeout of
100 ms which is the value given in the P2P specification for GO
Negotiation, but this was actually shorter than the
wait-for-offchannel-TX value (200 ms) used for the driver call. In
addition, it looks like some devices (e.g., Galaxy Nexus with JB image)
can take longer time to reply to GO Negotiation Response (somewhere
between 200 and 250 ms has been observed).
Increase the wait-for-GO-Neg-Resp timeout from 100 ms to 200 ms if GO
Negotiation Request frame was acknowledged (this matches with the
offchannel wait timeout that used previously). The no-ack case is left
at 100 ms since we use GO Negotiation Request frame also to discover
whether the peer is on its Listen channel.
Increase the wait-for-GO-Neg-Conf timeout from 100 ms to 250 ms (and
increase the offchannel wait timeout to matching 250 ms) as a workaround
for devices that take over 200 ms to reply to GO Negotiation Response.
Signed-hostap: Jouni Malinen <j@w1.fi>
p2p_set_timeout() calls in GO Neg Req/Resp TX callbacks used timeout of
100 ms which is the value given in the P2P specification for GO
Negotiation, but this was actually shorter than the
wait-for-offchannel-TX value (200 ms) used for the driver call. In
addition, it looks like some devices (e.g., Galaxy Nexus with JB image)
can take longer time to reply to GO Negotiation Response (somewhere
between 200 and 250 ms has been observed).
Increase the wait-for-GO-Neg-Resp timeout from 100 ms to 200 ms if GO
Negotiation Request frame was acknowledged (this matches with the
offchannel wait timeout that used previously). The no-ack case is left
at 100 ms since we use GO Negotiation Request frame also to discover
whether the peer is on its Listen channel.
Increase the wait-for-GO-Neg-Conf timeout from 100 ms to 250 ms (and
increase the offchannel wait timeout to matching 250 ms) as a workaround
for devices that take over 200 ms to reply to GO Negotiation Response.
Signed-hostap: Jouni Malinen <j@w1.fi>
Fix wpa_s crash and kickstart sched scan (INTERNAL-SQ)
data may be NULL and should be checked before dereferencing it.
This can happen when scan times out for example.
Another bug fixed is that sched scan wouldn't be kick started
from anywhere. Previously it was started following a normal scan
which didn't find any results. Fix it by start it if it's not running.
(These issues were introduced by commit
a523a28 wpa_s: don't reschedule the sched scan on each scan complete event
and the fix should be squashed into it)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Signed-off-by: Victor Goldenshtein <victorg@ti.com>
data may be NULL and should be checked before dereferencing it.
This can happen when scan times out for example.
Another bug fixed is that sched scan wouldn't be kick started
from anywhere. Previously it was started following a normal scan
which didn't find any results. Fix it by start it if it's not running.
(These issues were introduced by commit
a523a28 wpa_s: don't reschedule the sched scan on each scan complete event
and the fix should be squashed into it)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Signed-off-by: Victor Goldenshtein <victorg@ti.com>
SME: Fix handle Netgear APs WEP shared quirks (UPSTREAM-SQ)
If the network entry is created with both WPA_AUTH_ALG_OPEN and
WPA_AUTH_ALG_SHARED set in wpa_s->current_ssid->auth_alg, the
existing logic will end up picking WPA_AUTH_ALG_LEAP instead of
shared when open authentication fails.
Fix this by using a bitwise-and to check for WPA_AUTH_ALG_OPEN instead.
(Should be squashed into commit
2e35a02 SME: Handle Netgear APs WEP shared quirks)
Signed-Off-By: William List <wlist@ti.com>
Signed-Off-By: Eyal Shapira <eyal@wizery.com>
If the network entry is created with both WPA_AUTH_ALG_OPEN and
WPA_AUTH_ALG_SHARED set in wpa_s->current_ssid->auth_alg, the
existing logic will end up picking WPA_AUTH_ALG_LEAP instead of
shared when open authentication fails.
Fix this by using a bitwise-and to check for WPA_AUTH_ALG_OPEN instead.
(Should be squashed into commit
2e35a02 SME: Handle Netgear APs WEP shared quirks)
Signed-Off-By: William List <wlist@ti.com>
Signed-Off-By: Eyal Shapira <eyal@wizery.com>
WPS: Update dev.config_methods in wps_update_config
dev.config_methods was not updated when wps_update_config was called.
This could lead to mismatching config methods between Probe Request and
M1 packets. Add missing part for it.
dev.config_methods was not updated when wps_update_config was called.
This could lead to mismatching config methods between Probe Request and
M1 packets. Add missing part for it.
Fix a couple memory leaks
Found using valgrind.
Signed-hostap: Paul Stewart <pstew@chromium.org>
Found using valgrind.
Signed-hostap: Paul Stewart <pstew@chromium.org>
android: wpa_s template: set p2p_go_max_inactivity (ANDROID)
Set p2p_go_max_inactivity to 30 secs (instead of the default
of 300 secs) to avoid creating a user of experience of a
WiFi Direct connection which doesn't disconnect. This may
happen if the P2P GO interface misses a deauth/disassoc frame
and keeps on thinking the client is connected. Limit this
time to 30 secs which creates a better user experience.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Set p2p_go_max_inactivity to 30 secs (instead of the default
of 300 secs) to avoid creating a user of experience of a
WiFi Direct connection which doesn't disconnect. This may
happen if the P2P GO interface misses a deauth/disassoc frame
and keeps on thinking the client is connected. Limit this
time to 30 secs which creates a better user experience.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Add p2p_go_max_inactivity config option (UPSTREAM)
This enables setting a different max inactivity timeout for P2P GO.
This timeout is used to detect inactive clients. In some scenarios
it may be useful to have control over this and set a shorter timeout
than the default 300s. For example when running STA and P2P GO interfaces
concurrently, the STA interface may perform scans which may cause the
GO to miss a disassoc / deauth frames from a client and keep assuming
that the client is connected until the inactivity detection kicks in.
300 secs is a bit too long for such scenarios and creates a bad user
experience.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
This enables setting a different max inactivity timeout for P2P GO.
This timeout is used to detect inactive clients. In some scenarios
it may be useful to have control over this and set a shorter timeout
than the default 300s. For example when running STA and P2P GO interfaces
concurrently, the STA interface may perform scans which may cause the
GO to miss a disassoc / deauth frames from a client and keep assuming
that the client is connected until the inactivity detection kicks in.
300 secs is a bit too long for such scenarios and creates a bad user
experience.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
11 years agoandroid: wpa_s template: use group interface and set conc mode ol_R5.SP2.04 ol_r8.a3.11_jb
android: wpa_s template: use group interface and set conc mode
Make sure we operate the same way as BRCM, with a separate group
interface, by incorporating a driver param.
Also set a default p2p_conc_mode (set to 2), to fit WL6/7 cards. Note
this will have to be changed to p2p_conc_mode=1 for WL8 cards.
Signed-off-by: Arik Nemtsov <arik@wizery.com>
Make sure we operate the same way as BRCM, with a separate group
interface, by incorporating a driver param.
Also set a default p2p_conc_mode (set to 2), to fit WL6/7 cards. Note
this will have to be changed to p2p_conc_mode=1 for WL8 cards.
Signed-off-by: Arik Nemtsov <arik@wizery.com>
wpa_s: support p2p concurrency modes when connecting P2P
Prevent P2P connection when STA concurrency requirements do not allow
it. The behavior is determined according to the p2p_conc_mode
config file parameter.
We force go_intent=15 if only GO is allowed and abort the connection
if join is attempted with go_intent=15.
Also manipulate go_intent in our favor (go_intent=14) to minimize the
chances of a concurrency conflict in p2p_conc_mode=2. This supersedes a
similar previous patch by Eyal S.
Signed-off-by: Arik Nemtsov <arik@wizery.com>
Prevent P2P connection when STA concurrency requirements do not allow
it. The behavior is determined according to the p2p_conc_mode
config file parameter.
We force go_intent=15 if only GO is allowed and abort the connection
if join is attempted with go_intent=15.
Also manipulate go_intent in our favor (go_intent=14) to minimize the
chances of a concurrency conflict in p2p_conc_mode=2. This supersedes a
similar previous patch by Eyal S.
Signed-off-by: Arik Nemtsov <arik@wizery.com>
wpa_s: support different p2p concurrency modes when connecting STA
support p2p concurrency modes using the p2p_conc_mode=0/1/2 config
file parameter. Meaning is as follows:
0 - support STA + P2P CL/GO on the same channel (BRCM default)
1 - support only one connection at a time (WL8)
2 - support STA + P2P GO on same channel, but not P2P CL (WL6/7)
When connecting STA, disallow the connection or disconnect existing
p2p connection, according to existing concurrency preference.
Signed-off-by: Arik Nemtsov <arik@wizery.com>
support p2p concurrency modes using the p2p_conc_mode=0/1/2 config
file parameter. Meaning is as follows:
0 - support STA + P2P CL/GO on the same channel (BRCM default)
1 - support only one connection at a time (WL8)
2 - support STA + P2P GO on same channel, but not P2P CL (WL6/7)
When connecting STA, disallow the connection or disconnect existing
p2p connection, according to existing concurrency preference.
Signed-off-by: Arik Nemtsov <arik@wizery.com>
nl80211: avoid using another interface for P2P GO (INTERNAL)
Relevant for wl6/7 only, we need to figure out the wl8 MR case.
We now declare iface combinations in wlcore due to cfg80211
enforcement of that. Since we declare support for concurrent
STA and P2P_GO, wpa_s would like to use another interface for
GO. However, since we don't really support P2P_GO so well in MR
but we do want to enable it in MR, prevent wpa_s from using P2P
concurrent mode.
This should be removed once we support P2P_GO properly in MR.
[Arik - should be changed to a configuration parameter to wpa_s, and the
current default should be preserved]
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Relevant for wl6/7 only, we need to figure out the wl8 MR case.
We now declare iface combinations in wlcore due to cfg80211
enforcement of that. Since we declare support for concurrent
STA and P2P_GO, wpa_s would like to use another interface for
GO. However, since we don't really support P2P_GO so well in MR
but we do want to enable it in MR, prevent wpa_s from using P2P
concurrent mode.
This should be removed once we support P2P_GO properly in MR.
[Arik - should be changed to a configuration parameter to wpa_s, and the
current default should be preserved]
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Initialize P2P on p2p0 and not wlan0 (JB)
P2P is being initialized using a global struct
which points to the first initialized interface wpa_s
struct. That's causing P2P commands sent on the control
socket matching p2p0 to generate scan and ROC on the
wrong interface (wlan0) as well as events like PEER_DEVICE_FOUND
are sent on the wrong control socket to the Android framework.
This caused the framework to ignore these and prevent
displaying the P2P peer in the UI.
Solve it by an ugly hack for now to enable P2P only when the
interface p2p0 is being initialized.
This probably should be fixed upstream as well by marking
somehow on which interface you can do p2p or enable p2p per
interface.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
P2P is being initialized using a global struct
which points to the first initialized interface wpa_s
struct. That's causing P2P commands sent on the control
socket matching p2p0 to generate scan and ROC on the
wrong interface (wlan0) as well as events like PEER_DEVICE_FOUND
are sent on the wrong control socket to the Android framework.
This caused the framework to ignore these and prevent
displaying the P2P peer in the UI.
Solve it by an ugly hack for now to enable P2P only when the
interface p2p0 is being initialized.
This probably should be fixed upstream as well by marking
somehow on which interface you can do p2p or enable p2p per
interface.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Increase P2P_MAX_CLIENT_IDLE to 20 secs (BRCM)
This is from Jithu Jance submission to hostap ML:
Consider the disconnect event generated due to EAP-FAILURE(after WPS handshake)
during the P2P connection.
In this disconnect context, the group idle timer will be set to 10 and assoc retry starts.
If the connection doesn't go through in the first attempt the group will be removed.
This is because the authentication timeout happens at 10secs and the assoc will be retried only after that.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
This is from Jithu Jance submission to hostap ML:
Consider the disconnect event generated due to EAP-FAILURE(after WPS handshake)
during the P2P connection.
In this disconnect context, the group idle timer will be set to 10 and assoc retry starts.
If the connection doesn't go through in the first attempt the group will be removed.
This is because the authentication timeout happens at 10secs and the assoc will be retried only after that.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Handle new interface parameter in ctrl commands (BRCM)
Some commands sent to wpa_s by the framework in JB include
a new interface parameter. Handle it and dispatch the the
command on the correct interface.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Some commands sent to wpa_s by the framework in JB include
a new interface parameter. Handle it and dispatch the the
command on the correct interface.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Fix a crash in WPS PBC overlap (BRCM)
Supposedly fixed a crash which occurs during actual PBC overlap
according to BRCM commit log.
(Not quite sure what's the exact cause of the crash here. However
this looks like a non BRCM specific change so take it).
p2p_dev_addr can be NULL in some of the calls. Might cause a problem ?)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Supposedly fixed a crash which occurs during actual PBC overlap
according to BRCM commit log.
(Not quite sure what's the exact cause of the crash here. However
this looks like a non BRCM specific change so take it).
p2p_dev_addr can be NULL in some of the calls. Might cause a problem ?)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
P2P: Avoid peer expiration while connection in progress (BRCM)
(This seems to be a bug fix squashed in one of the BRCM patches.
Could be that the probability of this occuring once the expiration
time was reduced to 30s is higher)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
(This seems to be a bug fix squashed in one of the BRCM patches.
Could be that the probability of this occuring once the expiration
time was reduced to 30s is higher)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
P2P: Improve scan results handling (BRCM)
Avoid reporting scan results to the application in case a P2P search
is in progress as there will be many events but the scan is only
done on channels 1,6,11. This may cause APs on other channels to "disappear"
from the scan results.
Also avoid updating P2P interfaces with STA interfaces scan results
in order to avoid having results which are not on the social channels.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Avoid reporting scan results to the application in case a P2P search
is in progress as there will be many events but the scan is only
done on channels 1,6,11. This may cause APs on other channels to "disappear"
from the scan results.
Also avoid updating P2P interfaces with STA interfaces scan results
in order to avoid having results which are not on the social channels.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
P2P: Start blocked p2p find even if scan was on another interface (BRCM)
p2p find can now defer starting the p2p scan due to an ongoing
scan on a different interface. Relying on p2p_cb_on_scan_complete
which is a per interface flag is wrong here and we won't resume
the p2p find in case the scan wasn't on the same interface (which is
the case in Android JB).
Fix this by relying on the global p2p state instead.
(This description is based on analysis of the code as the original
BRCM commit doesn't contain any useful information)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
p2p find can now defer starting the p2p scan due to an ongoing
scan on a different interface. Relying on p2p_cb_on_scan_complete
which is a per interface flag is wrong here and we won't resume
the p2p find in case the scan wasn't on the same interface (which is
the case in Android JB).
Fix this by relying on the global p2p state instead.
(This description is based on analysis of the code as the original
BRCM commit doesn't contain any useful information)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
P2P: Defer p2p scan if scanning on other interfaces (BRCM)
The current defer p2p scan until scan complete works
only when the scanning is done on the same interface.
However in Android case there are scans in progress on the STA
interface so these would fail the p2p_scan and consequently
the p2p find.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
The current defer p2p scan until scan complete works
only when the scanning is done on the same interface.
However in Android case there are scans in progress on the STA
interface so these would fail the p2p_scan and consequently
the p2p find.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
P2P: Decrease peer expiry time (BRCM)
Changed from 5 min to 30 secs probably in order
to avoid stale peers appearing in the Android UI.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Changed from 5 min to 30 secs probably in order
to avoid stale peers appearing in the Android UI.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
nl80211: add parameter to force multi channel concurrency (BRCM)
Add a parameter which can be set from wpa_s commandline
or conf file to force real multi channel.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Add a parameter which can be set from wpa_s commandline
or conf file to force real multi channel.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
nl80211: fix extending shared_freq detection to AP/GO (BRCM)
Commit d3bd0f "nl80211: Extend shared_freq to handle AP/GO mode interfaces"
still discards AP/GO interfaces so effectively shared_freq
won't work on AP/GO interaces like intended.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Commit d3bd0f "nl80211: Extend shared_freq to handle AP/GO mode interfaces"
still discards AP/GO interfaces so effectively shared_freq
won't work on AP/GO interaces like intended.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
P2P: fix freq conflict resolution in case of P2P and STA
The conflict resolution code doesn't run in case wpa_s SME is used
so moved it up wpa_supplicant_associate.
wpas_p2p_handle_frequency_conflicts assumes use of a different interface
created for p2p group (p2p_group_interface != 0) but that's not
necessarily the case with all drivers. Switch to detect if an iface
is used for P2P_GO by looking at current_ssid->mode.
[Arik - fix the separate interface case, was broken by the original
patch]
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Signed-off-by: Arik Nemtsov <arik@wizery.com>
The conflict resolution code doesn't run in case wpa_s SME is used
so moved it up wpa_supplicant_associate.
wpas_p2p_handle_frequency_conflicts assumes use of a different interface
created for p2p group (p2p_group_interface != 0) but that's not
necessarily the case with all drivers. Switch to detect if an iface
is used for P2P_GO by looking at current_ssid->mode.
[Arik - fix the separate interface case, was broken by the original
patch]
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Signed-off-by: Arik Nemtsov <arik@wizery.com>
P2P: Resolve frequency conflicts between STA and P2P (BRCM)
Upon association check whether there's a a frequency
conflict given that no support for multi channel. In case
there's a freq conflict with an existing P2P_GO or P2P_CLI
decide how to resolve it (which one to disable or disconnect)
according to the priority configuration.
Effectively on Android JB, STA is always prioritized over P2P
so in case of a conflict P2P will be disconnected so that STA
can associate on a different channel.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Upon association check whether there's a a frequency
conflict given that no support for multi channel. In case
there's a freq conflict with an existing P2P_GO or P2P_CLI
decide how to resolve it (which one to disable or disconnect)
according to the priority configuration.
Effectively on Android JB, STA is always prioritized over P2P
so in case of a conflict P2P will be disconnected so that STA
can associate on a different channel.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Prep work to configure a prioritized interface (BRCM)
Add a new configurable property which points to the interface
name that should prioritized in case of resolving connection
conflicts.
(This appears to be prep work which doesn't get used however
we include it to better align with JB)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Add a new configurable property which points to the interface
name that should prioritized in case of resolving connection
conflicts.
(This appears to be prep work which doesn't get used however
we include it to better align with JB)
Signed-off-by: Eyal Shapira <eyal@wizery.com>
nl80211: Use native cfg80211 sta events (BRCM)
[Eyal - Keep specific BRCM specific stuff under
ANDROID_BRCM_P2P_PATCH and not ANDROID_P2P which
TI solution compiles with]
Change-Id: I0f6222839ac87241f1bfbbb1fdc6469bf6359652
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Signed-off-by: Eyal Shapira <eyal@wizery.com>
[Eyal - Keep specific BRCM specific stuff under
ANDROID_BRCM_P2P_PATCH and not ANDROID_P2P which
TI solution compiles with]
Change-Id: I0f6222839ac87241f1bfbbb1fdc6469bf6359652
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Fix p2p service discovery
- Fix listen timing to improve SD reliability
- Fix SD packet scheduling
Signed-off-by: Eyal Shapira <eyal@wizery.com>
- Fix listen timing to improve SD reliability
- Fix SD packet scheduling
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Fix null pointer access for SSID printing.
Fix SSID printing in events
Add SSID in supplicant change event
Allow immediate scan request even if another scan was scheduled later
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android.mk: Define ANDROID_P2P
Changes within #ifdef ANDROID_P2P are BRCM additions
which are non BRCM specific and there should be included.
That's in contrast of ANDROID_BRCM_P2P_PATCH which mark
parts that are BRCM implementation specific (like device_ap_sme)
and therefore would be compiled in only when compiling with BRCM
driver.
Change-Id: I031f0908055756b6e85b64c5151c18b8a73b9841
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Changes within #ifdef ANDROID_P2P are BRCM additions
which are non BRCM specific and there should be included.
That's in contrast of ANDROID_BRCM_P2P_PATCH which mark
parts that are BRCM implementation specific (like device_ap_sme)
and therefore would be compiled in only when compiling with BRCM
driver.
Change-Id: I031f0908055756b6e85b64c5151c18b8a73b9841
Signed-off-by: Eyal Shapira <eyal@wizery.com>
wpa_supplicant: Fix compilation without BOARD_WPA_SUPPLICANT_DRIVER
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Use keystore ENGINE for private key operations
The new keystore ENGINE is usable to perform private key operations when
we can't get the actual private key data. This is the case when hardware
crypto is enabled: the private key never leaves the hardware.
Subsequently, we need to be able to talk to OpenSSL ENGINEs that aren't
PKCS#11 or OpenSC. This just changes a few #define variables to allow us
to talk to our keystore engine without having one of those enabled and
without using a PIN.
The new keystore ENGINE is usable to perform private key operations when
we can't get the actual private key data. This is the case when hardware
crypto is enabled: the private key never leaves the hardware.
Subsequently, we need to be able to talk to OpenSSL ENGINEs that aren't
PKCS#11 or OpenSC. This just changes a few #define variables to allow us
to talk to our keystore engine without having one of those enabled and
without using a PIN.
Restore OpenSSL ENGINE support
We now use an OpenSSL ENGINE to support keystore functionality.
We now use an OpenSSL ENGINE to support keystore functionality.
Add network connection event for status
We need both supplicant state and network connection state
for proper sync up with framework
We need both supplicant state and network connection state
for proper sync up with framework
Add state message sent after 'status' command
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Moving keystore to system/security
keystore used to be in frameworks/base/cmds/keystore, but this include
needs to be changed to support the move to system/security
keystore used to be in frameworks/base/cmds/keystore, but this include
needs to be changed to support the move to system/security
wpa_supplicant: delay scans only for android builds (INTERNAL)
commit e48cd17 ("android: Delay scan after startup to
prevent race with framework (INTERNAL)") is fixing some
bug wrt. android framework, but introduce pretty annoying
delay when working with native linux.
Surround the new functionality with ifdefs in order
to apply it only for android build.
Signed-off-by: Eliad Peller <eliad@wizery.com>
commit e48cd17 ("android: Delay scan after startup to
prevent race with framework (INTERNAL)") is fixing some
bug wrt. android framework, but introduce pretty annoying
delay when working with native linux.
Surround the new functionality with ifdefs in order
to apply it only for android build.
Signed-off-by: Eliad Peller <eliad@wizery.com>
android: Delay scan after startup to prevent race with framework (INTERNAL)
On Android, the immediate scan may cause the following race:
1. Framework starts wpa_s
2. wpa_s loads and initates a scan
3. A matching AP is found and successfully connected to
4. wpa_s reports CTRL-EVENT-CONNECTED but the framework
WiFi state machine didn't progress yet to the correct state
so this event is unexpected.
5. As a result the DHCP state machine isn't triggered.
The end result is successful assoc with the AP but no DHCP request
being sent. Avoid this by delaying the initial scan by scan_interval.
This doesn't delay getting scan results or connectibg to a rememebered AP
as the Android framework initiates a scan through the control interface
anyways after detecting that the supplicant started.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
On Android, the immediate scan may cause the following race:
1. Framework starts wpa_s
2. wpa_s loads and initates a scan
3. A matching AP is found and successfully connected to
4. wpa_s reports CTRL-EVENT-CONNECTED but the framework
WiFi state machine didn't progress yet to the correct state
so this event is unexpected.
5. As a result the DHCP state machine isn't triggered.
The end result is successful assoc with the AP but no DHCP request
being sent. Avoid this by delaying the initial scan by scan_interval.
This doesn't delay getting scan results or connectibg to a rememebered AP
as the Android framework initiates a scan through the control interface
anyways after detecting that the supplicant started.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Use normal scan on first scan after init
Avoid using sched scan as the initial scan after wpa_s
init. This prevents a scenario on Android in which
the Android framework scan is preempted by a saved scan_ssid AP
being connected to due to immediate sched scan.
This delays receiving scan results.
Avoid using sched scan as the initial scan after wpa_s
init. This prevents a scenario on Android in which
the Android framework scan is preempted by a saved scan_ssid AP
being connected to due to immediate sched scan.
This delays receiving scan results.
wpa_supplicant: reduce wps2 IE in conf template (INTERNAL)
wpa_supplicant: VERSION_STR_POSTFIX is now defined to 'git describe'
print ctrl_iface commands
the android wpa_supplicant currently doesn't implement
wpa_hexdump_ascii, so add a simple print for the control
interface commands
Signed-off-by: Eliad Peller <eliad@wizery.com>
the android wpa_supplicant currently doesn't implement
wpa_hexdump_ascii, so add a simple print for the control
interface commands
Signed-off-by: Eliad Peller <eliad@wizery.com>
Use exact interface as socket parameter for init
For p2p, there are virtual interfaces (like p2p-wlan0-X) created and
that results in binding to the common init socket right now.
Instead, have the init bind fail for p2p interfaces and create seperate
sockets specified by the ctrl_interface path in config file
Bug: 5002384
Change-Id: Ia155df079a0bcca1871b6bcab2ef7111f0cba6c1
For p2p, there are virtual interfaces (like p2p-wlan0-X) created and
that results in binding to the common init socket right now.
Instead, have the init bind fail for p2p interfaces and create seperate
sockets specified by the ctrl_interface path in config file
Bug: 5002384
Change-Id: Ia155df079a0bcca1871b6bcab2ef7111f0cba6c1
Android: wpa_s: changes to default build config
Enable roaming and bgscan
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Signed-off-by: Ido Reis <idor@ti.com>
Enable roaming and bgscan
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Signed-off-by: Ido Reis <idor@ti.com>
Android: hostapd: enable N rates in build config
Signed-off-by: Ido Reis <idor@ti.com>
Signed-off-by: Ido Reis <idor@ti.com>
config: enable NL80211
Just enable it in both hostapd and wpa_s.
Signed-off-by: Luciano Coelho <coelho@ti.com>
Just enable it in both hostapd and wpa_s.
Signed-off-by: Luciano Coelho <coelho@ti.com>
nl80211_driver: add private commands to use dropbcast
Add DRIVER DROPBCAST {GET,ENABLE,DISABLE} commands to show the current
setting, enable and disable the feature of dropping all broadcast
packets while in suspend mode.
Signed-off-by: Luciano Coelho <coelho@ti.com>
Add DRIVER DROPBCAST {GET,ENABLE,DISABLE} commands to show the current
setting, enable and disable the feature of dropping all broadcast
packets while in suspend mode.
Signed-off-by: Luciano Coelho <coelho@ti.com>
nl80211: Implement some private cmds
Implement the LINKSPEED and RSSI/RSSI-APPROX private commands.
Upstream implementation sends the HANGED state event on
private command failure. Unimplemented commands were
sent to the driver as-is, causing the HANGED event to be sent
and cause a recovery. Private command handling was modified so
that only implemented commands are sent to the driver and
the sending of the HANGED event was removed.
[Arik - The "linkspeed" driver command incorrectly reported the
rate in kbps. Fix this]
Signed-off-by: Arik Nemtsov <arik@wizery.com>
Signed-off-by: Yotam Rubin <yotam@wizery.com>
Implement the LINKSPEED and RSSI/RSSI-APPROX private commands.
Upstream implementation sends the HANGED state event on
private command failure. Unimplemented commands were
sent to the driver as-is, causing the HANGED event to be sent
and cause a recovery. Private command handling was modified so
that only implemented commands are sent to the driver and
the sending of the HANGED event was removed.
[Arik - The "linkspeed" driver command incorrectly reported the
rate in kbps. Fix this]
Signed-off-by: Arik Nemtsov <arik@wizery.com>
Signed-off-by: Yotam Rubin <yotam@wizery.com>
nl80211: add support for drop rx filters
Enable configuring rx filters which will be
dropped even if matching another rx filter. This
can be used for generating exception filters.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Enable configuring rx filters which will be
dropped even if matching another rx filter. This
can be used for generating exception filters.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
driver_nl80211: Enable only unicast RXFILTER by default
In GB the framework always enabled RXFILTER for unicast
and bcast. This seems to be missing in ICS so enable
unicast by default as this is always required.
Signed-off-by: Pontus Fuchs <pontus.fuchs@gmail.com>
Signed-off-by: Eyal Shapira <eyal@wizery.com>
In GB the framework always enabled RXFILTER for unicast
and bcast. This seems to be missing in ICS so enable
unicast by default as this is always required.
Signed-off-by: Pontus Fuchs <pontus.fuchs@gmail.com>
Signed-off-by: Eyal Shapira <eyal@wizery.com>
driver_nl80211: Add and align rx filters IDs
Add more patterns (SSDP, ARP, DHCP) and align IDs to a common
vendor Android framework implementation.
Note that ARP pattern shouldn't be used as our FW
responds to ARPs by default without waking up the host.
It is added only for ID alignments purposes.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Add more patterns (SSDP, ARP, DHCP) and align IDs to a common
vendor Android framework implementation.
Note that ARP pattern shouldn't be used as our FW
responds to ARPs by default without waking up the host.
It is added only for ID alignments purposes.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
driver_nl80211: rx filters - add support for longer patterns
- Add support for long patterns (longer than 8 bytes)
- Separate Rx filters static configuration from code
- Add DHCP and ARP Rx filters
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Signed-off-by: Assaf Azulay <assaf@ti.com>
- Add support for long patterns (longer than 8 bytes)
- Separate Rx filters static configuration from code
- Add DHCP and ARP Rx filters
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Signed-off-by: Assaf Azulay <assaf@ti.com>
driver_nl80211: Add support for DRIVER RXFILTER command
Add support for this Android specific feature using WoWLAN packet
pattern triggers.
Signed-off-by: Pontus Fuchs <pontus.fuchs@tactel.se>
Add support for this Android specific feature using WoWLAN packet
pattern triggers.
Signed-off-by: Pontus Fuchs <pontus.fuchs@tactel.se>
hostapd: add support for android created sockets (/dev/socket/)
Add the same support that wpa_supplicant has with sockets created
by the Android system using the init.rc services options
Just as the supplicant, if the ctrl_iface is a name and not a path
(i.e. doesn't start with '/') the hostapd will assume that this is
an Android created socket named wpa_$(ctrl_iface) which is opened
in /dev/socket/
hostapd_cli sockets will be created in /data/misc/wifi/sockets
The hardcoded configuration is set in the Android.mk of hostapd
just like it is with the supplicant.
In addition, the hostapd_cli needs an Android property by the name
ap.interface to hold the ctrl_iface name to connect to the hostapd's
socket.
Add the same support that wpa_supplicant has with sockets created
by the Android system using the init.rc services options
Just as the supplicant, if the ctrl_iface is a name and not a path
(i.e. doesn't start with '/') the hostapd will assume that this is
an Android created socket named wpa_$(ctrl_iface) which is opened
in /dev/socket/
hostapd_cli sockets will be created in /data/misc/wifi/sockets
The hardcoded configuration is set in the Android.mk of hostapd
just like it is with the supplicant.
In addition, the hostapd_cli needs an Android property by the name
ap.interface to hold the ctrl_iface name to connect to the hostapd's
socket.
wpa_s: make SETBAND take immediate effect
Make SETBAND disconnect from the current AP if it's not
in the correct band. Also expire APs which aren't in the correct
band so scan results will immediately reflect the band change.
[Eyal - ammended commit description]
Signed-off-by: Panduranga Mallireddy <panduranga_mallireddy@ti.com>
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Make SETBAND disconnect from the current AP if it's not
in the correct band. Also expire APs which aren't in the correct
band so scan results will immediately reflect the band change.
[Eyal - ammended commit description]
Signed-off-by: Panduranga Mallireddy <panduranga_mallireddy@ti.com>
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Android: Implement SETBAND for scan requests
This provides partial SETBAND driver command implementation by
converting the request into a filter for which channels are scanned
by wpa_supplicant.
This provides partial SETBAND driver command implementation by
converting the request into a filter for which channels are scanned
by wpa_supplicant.
nl80211: Add get_noa() support for WFD certification (BRCM)
BUG: b/5367351
Change-Id: I14ed79e10ade205c5dd4cdc0d2e888ed1279d1bb
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
BUG: b/5367351
Change-Id: I14ed79e10ade205c5dd4cdc0d2e888ed1279d1bb
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
nl80211: Special send_mlme rules (BRCM)
Fix WFD and WPS certification problem for GO (BRCM)
Change-Id: I5bbac818aad7c0a14fddb3beb88a6a2d87c07ea0
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Fix WFD and WPS certification problem for GO (BRCM)
Change-Id: I5bbac818aad7c0a14fddb3beb88a6a2d87c07ea0
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
nl80211: Add MLME events (BRCM)
Fix WFD and WPS certification problem for GO (BRCM)
Change-Id: I5bbac818aad7c0a14fddb3beb88a6a2d87c07ea0
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Fix WFD and WPS certification problem for GO (BRCM)
Change-Id: I5bbac818aad7c0a14fddb3beb88a6a2d87c07ea0
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
nl80211: Add set_noa, set_p2p_powersave, set_ap_wps_ie
Fix WFD and WPS certification problem for GO (BRCM)
Change-Id: I5bbac818aad7c0a14fddb3beb88a6a2d87c07ea0
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Fix WFD and WPS certification problem for GO (BRCM)
Change-Id: I5bbac818aad7c0a14fddb3beb88a6a2d87c07ea0
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Broadcom: nl80211: Register assoc/disassoc/deauth frames with Probe Request
TODO: This is not the correct place for registering these frames. Would
need to first figure out whether these are still needed and if so, for
what.
Change-Id: Iafec4bedbd33836d0a64e7ea054d8a46ef8ec204
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
TODO: This is not the correct place for registering these frames. Would
need to first figure out whether these are still needed and if so, for
what.
Change-Id: Iafec4bedbd33836d0a64e7ea054d8a46ef8ec204
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Add P2P support for BRCM CFG80211 driver (nl80211)
Change-Id: Iafec4bedbd33836d0a64e7ea054d8a46ef8ec204
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Change-Id: Iafec4bedbd33836d0a64e7ea054d8a46ef8ec204
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: Add private commands support for nl80211
Change-Id: If189933aaf6e629fe8ede0f4e0d0b527f3b47f2e
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Change-Id: If189933aaf6e629fe8ede0f4e0d0b527f3b47f2e
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: nl80211: Add driver_cmd POWERMODE and GETPOWER
nl80211: Add private function support
Change-Id: Iba9b2ac21f5c7760900c57826b7048ee58928338
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Change-Id: Iba9b2ac21f5c7760900c57826b7048ee58928338
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: Do not use separate private lib
The separate private library mechanism used in Android ICS is not
very robust when wpa_supplicant/hostapd version changes since the
external code is accessing some internal data structures directly.
Avoid this type of issues by integrating the private library to be
part of wpa_supplicant/hostapd build.
The separate private library mechanism used in Android ICS is not
very robust when wpa_supplicant/hostapd version changes since the
external code is accessing some internal data structures directly.
Avoid this type of issues by integrating the private library to be
part of wpa_supplicant/hostapd build.
Set buffer length the same as in wpa_supplicant_ctrl_iface_process()
Bug: 5236589
Change-Id: Iae8405aa17d5cc6bbffcff3a37d81df74143aabe
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Bug: 5236589
Change-Id: Iae8405aa17d5cc6bbffcff3a37d81df74143aabe
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Fix reporting hidden APs during scan
Change-Id: I2f3274c6f89ac0100331f4987c40e23f36577817
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Change-Id: I2f3274c6f89ac0100331f4987c40e23f36577817
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Add P2P support for BRCM CFG80211 driver (P2P invite running-GO check)
Change-Id: Iafec4bedbd33836d0a64e7ea054d8a46ef8ec204
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Change-Id: Iafec4bedbd33836d0a64e7ea054d8a46ef8ec204
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: Define ANDROID_BRCM_P2P_PATCH for Broadcom specific builds
This is combination of part from
Dmitry Shmidt <dimitrysh@google.com>
Thu, 21 Jul 2011 15:19:46 -0700
Change-Id: Iafec4bedbd33836d0a64e7ea054d8a46ef8ec204
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
and
Jean-Baptiste Queru <jbq@google.com>
Tue, 15 Nov 2011 18:41:36 -0800
Enable broadcom-specific patch with proper flag
Change-Id: I5a0f5a2d65963deff3cd62b5e7ec090619c75a2c
This is combination of part from
Dmitry Shmidt <dimitrysh@google.com>
Thu, 21 Jul 2011 15:19:46 -0700
Change-Id: Iafec4bedbd33836d0a64e7ea054d8a46ef8ec204
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
and
Jean-Baptiste Queru <jbq@google.com>
Tue, 15 Nov 2011 18:41:36 -0800
Enable broadcom-specific patch with proper flag
Change-Id: I5a0f5a2d65963deff3cd62b5e7ec090619c75a2c
Add WPA_UNICODE_SSID support
Change-Id: I1f938b97169d4468ee5b05316826ee509a10d9ad
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Change-Id: I1f938b97169d4468ee5b05316826ee509a10d9ad
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: wext: Add signal_poll command support (wext)
Change-Id: I0ccd9e39928c3e51f1350d2ab34e47ea3191ed0b
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Change-Id: I0ccd9e39928c3e51f1350d2ab34e47ea3191ed0b
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: wext: Suppress additional DISASSOCIATE events
Change-Id: Id65428908bca59e71a3ab479b63d992eff96e433
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Change-Id: Id65428908bca59e71a3ab479b63d992eff96e433
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: wext: Add driver_cmd CSCAN
Android: wext: Add combo_scan()
Android: wext: Add driver_cmd
Android: Convert driver_cmd BGSCAN-START/STOP to proper driver_ops
Instead of driver specific specific command, use a cleaner design
for handling the Android BGSCAN-START/STOP commands.
Instead of driver specific specific command, use a cleaner design
for handling the Android BGSCAN-START/STOP commands.
Add extended 'driver' command
Change-Id: Ib589f44f471c1198973ee0a0695b90097fcc9b33
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Change-Id: Ib589f44f471c1198973ee0a0695b90097fcc9b33
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Set ap_scan to default in case of disassociation
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Fix scan notification in case of canceling scan
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: Add src directory symlinks
These are from Android wpa_supplicant_8.git initial 0.8.X commit
8d520ff1dc2da35cdca849e982051b86468016d8.
Change-Id: I26aec5afbbd4f4a1f5fd900912545b6f5050de64
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
These are from Android wpa_supplicant_8.git initial 0.8.X commit
8d520ff1dc2da35cdca849e982051b86468016d8.
Change-Id: I26aec5afbbd4f4a1f5fd900912545b6f5050de64
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: Add MODULE_LICENSE_BSD_LIKE
These are from Android wpa_supplicant_8.git initial 0.8.X commit
8d520ff1dc2da35cdca849e982051b86468016d8.
Change-Id: I26aec5afbbd4f4a1f5fd900912545b6f5050de64
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
These are from Android wpa_supplicant_8.git initial 0.8.X commit
8d520ff1dc2da35cdca849e982051b86468016d8.
Change-Id: I26aec5afbbd4f4a1f5fd900912545b6f5050de64
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Android: Add top level makefiles
These are from Android wpa_supplicant_8.git initial 0.8.X commit
8d520ff1dc2da35cdca849e982051b86468016d8.
Change-Id: I26aec5afbbd4f4a1f5fd900912545b6f5050de64
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
These are from Android wpa_supplicant_8.git initial 0.8.X commit
8d520ff1dc2da35cdca849e982051b86468016d8.
Change-Id: I26aec5afbbd4f4a1f5fd900912545b6f5050de64
Signed-off-by: Dmitry Shmidt <dimitrysh@google.com>
Revert "P2P: Assume GO Negotiation failed if GO Neg Conf wait times out"
Galaxy Nexus takes time to send the GO Neg Confirm (~200ms) and this
commit caused the GO Neg to fail because of this.
This reverts commit 579a80982ad07619373876c09cdd60e2afcba5b5.
Galaxy Nexus takes time to send the GO Neg Confirm (~200ms) and this
commit caused the GO Neg to fail because of this.
This reverts commit 579a80982ad07619373876c09cdd60e2afcba5b5.
add set/cancel_priority to ap mode as well
ROC when the ap gets the first auth request, and CROC
after authorization (or after connection fails).
Signed-off-by: Eliad Peller <eliad@wizery.com>
ROC when the ap gets the first auth request, and CROC
after authorization (or after connection fails).
Signed-off-by: Eliad Peller <eliad@wizery.com>
add set/cancel_priority calls
implement set_priority/cancel_priority functions,
and call them in the appropriate places in the
STA connection flow.
Signed-off-by: Eliad Peller <eliad@wizery.com>
implement set_priority/cancel_priority functions,
and call them in the appropriate places in the
STA connection flow.
Signed-off-by: Eliad Peller <eliad@wizery.com>
Disconnect if we can't roam following beacon loss
The driver reports the 1st beacon loss event but doesn't
disconnect until further consecutive beacon loss events are
received. That's being done in order to give the supplicant time
to roam seamlessly (i.e. without reporting DISCONNECTED to upper
layers). However, in case we can't find any roaming candidates
it's better to disconnect as soon as possible so any supplicant
client will be able to switch quickly to another communication
channel (e.g. mobile 3G). This change initiates up to two immediate
specific SSID scans on all channels following a beacon loss in order
to locate a roaming candidate. Two scans are performed in case
a roaming candidate was preivously blacklisted. That way, it'll be
explored if there's no other option.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
The driver reports the 1st beacon loss event but doesn't
disconnect until further consecutive beacon loss events are
received. That's being done in order to give the supplicant time
to roam seamlessly (i.e. without reporting DISCONNECTED to upper
layers). However, in case we can't find any roaming candidates
it's better to disconnect as soon as possible so any supplicant
client will be able to switch quickly to another communication
channel (e.g. mobile 3G). This change initiates up to two immediate
specific SSID scans on all channels following a beacon loss in order
to locate a roaming candidate. Two scans are performed in case
a roaming candidate was preivously blacklisted. That way, it'll be
explored if there's no other option.
Signed-off-by: Eyal Shapira <eyal@wizery.com>
Prevent roaming to a different ESS while connected
While connected to a certain ESS prevent roaming to a different
ESS AP even if its signal is better. This prevents an undesired
switch between networks in this example scenario:
2 network profiles configured Net1 and Net2. We're already associated
to an AP on the ESS Net1 and while walking with the device we get close
to an AP from ESS Net2. Before this change a decision to switch to
Net2 was made.
While connected to a certain ESS prevent roaming to a different
ESS AP even if its signal is better. This prevents an undesired
switch between networks in this example scenario:
2 network profiles configured Net1 and Net2. We're already associated
to an AP on the ESS Net1 and while walking with the device we get close
to an AP from ESS Net2. Before this change a decision to switch to
Net2 was made.
Ignore a deauth from a different BSS than the current one
This fixes an issue with roaming where the previous
BSS would send a DEAUTH during the roaming and this
would caused the supplicant to disconnect.
This fixes an issue with roaming where the previous
BSS would send a DEAUTH during the roaming and this
would caused the supplicant to disconnect.
Roam back to the origin AP when assoc/auth times out
When roaming, avoid going to DISCONNECTED in case assoc or auth
times out with the new AP. Instead attempt to reconnect
back to old AP.
When roaming, avoid going to DISCONNECTED in case assoc or auth
times out with the new AP. Instead attempt to reconnect
back to old AP.
initiate roaming on beacon_loss
Add wpa_s->roaming to indicate (forced) roaming request.
set it on beacon_loss event.
(no need to disconnect if there is no available ap, as
the driver will send disassoc after some time)
Signed-off-by: Eliad Peller <eliad@wizery.com>
Add wpa_s->roaming to indicate (forced) roaming request.
set it on beacon_loss event.
(no need to disconnect if there is no available ap, as
the driver will send disassoc after some time)
Signed-off-by: Eliad Peller <eliad@wizery.com>
wpa_s: don't reschedule the sched scan on each scan complete event
wpa_supplicant doesn't distinguish between NL80211_CMD_SCHED_SCAN_RESULTS
and NL80211_CMD_NEW_SCAN_RESULTS, this causing unnecessary rescheduling
of the sched scan on each scan complete event.
Reschedule the sched scan (stop + start) only if the scan results are from
the sched scan.
Signed-off-by: Victor Goldenshtein <victorg@ti.com>
wpa_supplicant doesn't distinguish between NL80211_CMD_SCHED_SCAN_RESULTS
and NL80211_CMD_NEW_SCAN_RESULTS, this causing unnecessary rescheduling
of the sched scan on each scan complete event.
Reschedule the sched scan (stop + start) only if the scan results are from
the sched scan.
Signed-off-by: Victor Goldenshtein <victorg@ti.com>
Initiate a periodic normal scan in addition to sched scan
Some applications (e.g. detecting open network around
in Android) require periodic broadcast scan results.
The periodic broadcast scan was replaced by sched scan
completely. Re-enable these scan alongside sched scans.
Some applications (e.g. detecting open network around
in Android) require periodic broadcast scan results.
The periodic broadcast scan was replaced by sched scan
completely. Re-enable these scan alongside sched scans.
P2P: Ignore PBC overlap in P2P provisioning
PBC overlap can be ignored as the P2P client knows
that it should connect to the P2P GO so no point of failing
the WPS session in case of overlap because some other
AP had WPS PBC on at the same time.
PBC overlap can be ignored as the P2P client knows
that it should connect to the P2P GO so no point of failing
the WPS session in case of overlap because some other
AP had WPS PBC on at the same time.