set execute permissions (again!)
[zumo-cc3200/zumo-cc3200.git] / etc / rbload.bat
1 @echo off
2 setlocal
4 set binpath=%~dp0\..\build
6 if "%1"=="" (
7     echo usage: %~nx0 binary [[com_port_id] [energia_install_dir]]
8     exit /b 1
9 )
11 set bin=%1
12 if not exist %1 (
13     if exist %binpath%\%1 (
14         set bin=%binpath%\%1
15     ) else (
16         echo error: can't find the binary file "%1"
17         exit /b 1
18     )
19 )
21 set comid=%2
22 if "%2"=="" (
23     set comid=9
24 )
26 if "%3"=="" (
27     set eidir=C:\ti
28 ) else (
29     set eidir=%3
30 )
32 for /f "usebackq delims=" %%f in (`dir /b /o:n %eidir%\energia-*`) do (
33     REM cc3200prog must also be run from it's home directory (!)
34     echo chdir %eidir%\%%f\hardware\tools\lm4f\bin
35     chdir %eidir%\%%f\hardware\tools\lm4f\bin
37     echo cc3200prog %comid% %bin%
38     cc3200prog %comid% %bin% || exit /b 1
39     echo Upload succeeded.
40     echo Push the reset button on the ZumoCC3200 to start the sketch.
41     exit /b 0
42 )
44 echo error: energia is not installed in %eidir%
45 exit /b 1