46e1c2019fde3b5d150a8f13eb6645f20c2caa32
[zumo-cc3200/zumo-cc3200.git] / src / Energia / libraries / ZumoCC3200 / examples / MasterSlave / apLoop.ino
1 /*
2  *  ======== apLoop ========
3  *  This sketch waits on either a button press or a 
4  *
5  *  The name and password of the network and the port number of the server
6  *  (always at IP address 192.168.1.1) can be changed below.
7  */
9 #include <WiFi.h>
10 #include <Pushbutton.h>
11 #include <ti/sysbios/knl/Task.h>
13 #include <string.h>
15 /* name of the network and its password */
16 char ssid[] = "zumo_group";
17 char wifipw[] = "password";
19 /* zumo command port */
20 #define CMD_PORT 8080
22 /* IMU data port */
23 #define DATA_PORT 6000
25 /* Create a Pushbutton object for pin 12 (the Zumo user pushbutton pin) */
26 Pushbutton button(ZUMO_BUTTON);
28 IPAddress broadcastIP(192,168,1,255);
31 static bool waiting = true;
33 /* 1 is master, 0 is slave, -1 is unassigned */
34 int rank = -1;
36 static void sendIMUPacket(WiFiUDP Udp, IPAddress ip, int localPort);
38 //WiFiUDP UdpRX; /* UDP connection for receiving */ 
39 //WiFiUDP UdpTX; /* UDP connection for transmitting */
41 WiFiUDP Udp;
43 /*
44  *  ======== apSetup ========
45  */
46 void apSetup()
47 {
48     Serial.begin(9600);
50     /* set priority of this task to be lower than other tasks */
51     //Task_setPri(Task_self(), 1);
52     
53     // attempt to connect to group network:
54     Serial.print("Attempting to connect to Network named: ");
55     Serial.println(ssid); 
56     WiFi.begin(ssid, wifipw);
57     
58     while (waiting) {
59  
60       /* if group network is found */
61       if(WiFi.status() == WL_CONNECTED){
62          Serial.println("Connected to the group network");
63          Serial.println("Waiting for an ip address");
64   
65          while (WiFi.localIP() == INADDR_NONE) {
66            // print dots while we wait for an ip addresss
67            Serial.print(".");
68            delay(300);
69          }
70          
71          Serial.println("\nIP Address obtained");
72          printWifiStatus();
73          
74          /* this zumo is a slave */
75          rank = 0;
76          
77          waiting = false;
78       }
79       /* if zumo button is pressed */
80       else if(button.getSingleDebouncedRelease()){
81          Serial.println("Button press detected");
82          /* startup a new network and get the first IP address: 192.168.1.1 */
83          Serial.print("Starting a new network: "); Serial.println(ssid);
84          WiFi.beginNetwork((char *)ssid, (char *)wifipw);
85          while (WiFi.localIP() == INADDR_NONE) {
86             Serial.print(".");
87             delay(300);
88          }
89          
90          /* this zumo is the master */
91          rank = 1;
92          
93          waiting = false;
94       }
95       else{
96          WiFi.begin(ssid, wifipw);
97          Serial.print(".");
98          delay(300);
99       }
100     }
101     
102     Udp.begin(CMD_PORT);                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                              
105 /*
106  *  ======== apLoop ========
107  */
108  
109 void apLoop()
111   int packetSize = 0;
112   
113   switch(rank){
114       case -1: /* unassigned case: should theoretically never happen */
115         Serial.println("rank was not assigned, please exit the program and try again");
116         break;
117         
118       case 0: /* slave case: listen for motor commands from group network */
119         // if there's data available, read a packet
120         packetSize = Udp.parsePacket();
121         if (packetSize){
122            static char buffer[64] = {0}; 
123           
124            Serial.print("Received packet from ");
125            IPAddress remoteIp = Udp.remoteIP();
126            Serial.print(remoteIp);
127            Serial.print(", port ");
128            Serial.println(Udp.remotePort());
129         
130            /* if packet is from master */
131            if(Udp.remotePort() == CMD_PORT){
132              // read the packet into packetBufffer
133              int len = Udp.read(buffer, 64);
134              
135              if (len > 0) buffer[len] = 0;
136              Serial.print("Contents: ");
137              Serial.println(buffer);
138              
139              motorWASD = buffer[0];  
140            }  
141            
142         }      
143         break;
144         
145       case 1: /* master case: listen for motor commands from processing, and multicast them over the group network */
146         // if there's data available, read a packet
147         packetSize = Udp.parsePacket();
148         if (packetSize){
149            static char buffer[64] = {0}; 
150           
151            Serial.print("Received packet from ");
152            IPAddress remoteIp = Udp.remoteIP();
153            Serial.print(remoteIp);
154            Serial.print(", port ");
155            Serial.println(Udp.remotePort());
156            
157            /* if packet is from processing */
158            if(Udp.remotePort() == DATA_PORT){
159              // read the packet into packetBufffer
160              int len = Udp.read(buffer, 64);
161              
162              if (len > 0) buffer[len] = 0;
163              Serial.print("Contents: ");
164              Serial.println(buffer);
165              
166              motorWASD = buffer[0];  
167              
168              /* broadcast the command */
169              Udp.beginPacket(broadcastIP, CMD_PORT);
170              Udp.write(motorWASD);
171              Udp.endPacket();
172            }
173         }
174         /* broadcast the command */
175         Udp.beginPacket(broadcastIP, CMD_PORT);
176         Udp.write("hello slaves");
177         Udp.endPacket();
178         break;
179   }
182 /*
183  *  ======== doWASD ========
184  */
185 static void sendIMUPacket(WiFiUDP Udp, IPAddress ip, int localPort)
187     static char report[80];
189     /* send current IMU data */
190     System_snprintf(report, sizeof(report),
191         "A: %6d %6d %6d G: %6d %6d %6d M: %6d %6d %6d",
192         imuCompass.a.x, imuCompass.a.y, imuCompass.a.z,
193         imuGyro.g.x,    imuGyro.g.y,    imuGyro.g.z, 
194         imuCompass.m.x, imuCompass.m.y, imuCompass.m.z);
195     
196     Udp.beginPacket(ip, localPort);
197     Udp.write(report);
198     Udp.endPacket();
201 void printWifiStatus() {
202   // print the SSID of the network you're attached to:
203   Serial.print("SSID: ");
204   Serial.println(WiFi.SSID());
206   // print your WiFi IP address:
207   IPAddress ip = WiFi.localIP();
208   Serial.print("IP Address: ");
209   Serial.println(ip);
211   // print the received signal strength:
212   long rssi = WiFi.RSSI();
213   Serial.print("signal strength (RSSI):");
214   Serial.print(rssi);
215   Serial.println(" dBm");