#ifndef LSM303_h #define LSM303_h #include // for byte data type class LSM303 { public: template struct vector { T x, y, z; }; enum deviceType { device_DLH, device_DLM, device_DLHC, device_D, device_auto }; enum sa0State { sa0_low, sa0_high, sa0_auto }; // register addresses enum regAddr { TEMP_OUT_L = 0x05, // D TEMP_OUT_H = 0x06, // D STATUS_M = 0x07, // D INT_CTRL_M = 0x12, // D INT_SRC_M = 0x13, // D INT_THS_L_M = 0x14, // D INT_THS_H_M = 0x15, // D OFFSET_X_L_M = 0x16, // D OFFSET_X_H_M = 0x17, // D OFFSET_Y_L_M = 0x18, // D OFFSET_Y_H_M = 0x19, // D OFFSET_Z_L_M = 0x1A, // D OFFSET_Z_H_M = 0x1B, // D REFERENCE_X = 0x1C, // D REFERENCE_Y = 0x1D, // D REFERENCE_Z = 0x1E, // D CTRL0 = 0x1F, // D CTRL1 = 0x20, // D CTRL_REG1_A = 0x20, // DLH, DLM, DLHC CTRL2 = 0x21, // D CTRL_REG2_A = 0x21, // DLH, DLM, DLHC CTRL3 = 0x22, // D CTRL_REG3_A = 0x22, // DLH, DLM, DLHC CTRL4 = 0x23, // D CTRL_REG4_A = 0x23, // DLH, DLM, DLHC CTRL5 = 0x24, // D CTRL_REG5_A = 0x24, // DLH, DLM, DLHC CTRL6 = 0x25, // D CTRL_REG6_A = 0x25, // DLHC HP_FILTER_RESET_A = 0x25, // DLH, DLM CTRL7 = 0x26, // D REFERENCE_A = 0x26, // DLH, DLM, DLHC STATUS_A = 0x27, // D STATUS_REG_A = 0x27, // DLH, DLM, DLHC OUT_X_L_A = 0x28, OUT_X_H_A = 0x29, OUT_Y_L_A = 0x2A, OUT_Y_H_A = 0x2B, OUT_Z_L_A = 0x2C, OUT_Z_H_A = 0x2D, FIFO_CTRL = 0x2E, // D FIFO_CTRL_REG_A = 0x2E, // DLHC FIFO_SRC = 0x2F, // D FIFO_SRC_REG_A = 0x2F, // DLHC IG_CFG1 = 0x30, // D INT1_CFG_A = 0x30, // DLH, DLM, DLHC IG_SRC1 = 0x31, // D INT1_SRC_A = 0x31, // DLH, DLM, DLHC IG_THS1 = 0x32, // D INT1_THS_A = 0x32, // DLH, DLM, DLHC IG_DUR1 = 0x33, // D INT1_DURATION_A = 0x33, // DLH, DLM, DLHC IG_CFG2 = 0x34, // D INT2_CFG_A = 0x34, // DLH, DLM, DLHC IG_SRC2 = 0x35, // D INT2_SRC_A = 0x35, // DLH, DLM, DLHC IG_THS2 = 0x36, // D INT2_THS_A = 0x36, // DLH, DLM, DLHC IG_DUR2 = 0x37, // D INT2_DURATION_A = 0x37, // DLH, DLM, DLHC CLICK_CFG = 0x38, // D CLICK_CFG_A = 0x38, // DLHC CLICK_SRC = 0x39, // D CLICK_SRC_A = 0x39, // DLHC CLICK_THS = 0x3A, // D CLICK_THS_A = 0x3A, // DLHC TIME_LIMIT = 0x3B, // D TIME_LIMIT_A = 0x3B, // DLHC TIME_LATENCY = 0x3C, // D TIME_LATENCY_A = 0x3C, // DLHC TIME_WINDOW = 0x3D, // D TIME_WINDOW_A = 0x3D, // DLHC Act_THS = 0x3E, // D Act_DUR = 0x3F, // D CRA_REG_M = 0x00, // DLH, DLM, DLHC CRB_REG_M = 0x01, // DLH, DLM, DLHC MR_REG_M = 0x02, // DLH, DLM, DLHC SR_REG_M = 0x09, // DLH, DLM, DLHC IRA_REG_M = 0x0A, // DLH, DLM, DLHC IRB_REG_M = 0x0B, // DLH, DLM, DLHC IRC_REG_M = 0x0C, // DLH, DLM, DLHC WHO_AM_I = 0x0F, // D WHO_AM_I_M = 0x0F, // DLM TEMP_OUT_H_M = 0x31, // DLHC TEMP_OUT_L_M = 0x32, // DLHC // dummy addresses for registers in different locations on different // devices; the library translates these based on device type value // with sign flipped is used as index into translated_regs array OUT_X_H_M = -1, OUT_X_L_M = -2, OUT_Y_H_M = -3, OUT_Y_L_M = -4, OUT_Z_H_M = -5, OUT_Z_L_M = -6, // update dummy_reg_count if registers are added here! // device-specific register addresses DLH_OUT_X_H_M = 0x03, DLH_OUT_X_L_M = 0x04, DLH_OUT_Y_H_M = 0x05, DLH_OUT_Y_L_M = 0x06, DLH_OUT_Z_H_M = 0x07, DLH_OUT_Z_L_M = 0x08, DLM_OUT_X_H_M = 0x03, DLM_OUT_X_L_M = 0x04, DLM_OUT_Z_H_M = 0x05, DLM_OUT_Z_L_M = 0x06, DLM_OUT_Y_H_M = 0x07, DLM_OUT_Y_L_M = 0x08, DLHC_OUT_X_H_M = 0x03, DLHC_OUT_X_L_M = 0x04, DLHC_OUT_Z_H_M = 0x05, DLHC_OUT_Z_L_M = 0x06, DLHC_OUT_Y_H_M = 0x07, DLHC_OUT_Y_L_M = 0x08, D_OUT_X_L_M = 0x08, D_OUT_X_H_M = 0x09, D_OUT_Y_L_M = 0x0A, D_OUT_Y_H_M = 0x0B, D_OUT_Z_L_M = 0x0C, D_OUT_Z_H_M = 0x0D }; vector a; // accelerometer readings vector m; // magnetometer readings vector m_max; // maximum magnetometer values, used for calibration vector m_min; // minimum magnetometer values, used for calibration /* * ======== last_status ======== */ byte last_status; // status of last I2C transmission /* * ======== LSM303 ======== */ LSM303(void); /* * ======== init ======== */ bool init(deviceType device = device_auto, sa0State sa0 = sa0_auto); /* * ======== getDeviceType ======== */ deviceType getDeviceType(void) { return _device; } /* * ======== enableDefault ======== */ void enableDefault(void); /* * ======== writeAccReg ======== */ void writeAccReg(byte reg, byte value); /* * ======== readAccReg ======== */ byte readAccReg(byte reg); /* * ======== writeMagReg ======== */ void writeMagReg(byte reg, byte value); /* * ======== readMagReg ======== */ byte readMagReg(int reg); /* * ======== writeReg ======== */ void writeReg(byte reg, byte value); /* * ======== readReg ======== */ byte readReg(int reg); /* * ======== readAcc ======== */ void readAcc(void); /* * ======== readMag ======== */ void readMag(void); /* * ======== read ======== */ void read(void); /* * ======== setTimeout ======== */ void setTimeout(unsigned int timeout); /* * ======== getTimeout ======== */ unsigned int getTimeout(void); /* * ======== timeoutOccurred ======== */ bool timeoutOccurred(void); /* * ======== heading ======== */ float heading(void); template float heading(vector from); /* * ======== vector_cross ======== */ template static void vector_cross( const vector *a, const vector *b, vector *out); /* * ======== vector_dot ======== */ template static float vector_dot(const vector *a, const vector *b); /* * ======== vector_normalize ======== */ static void vector_normalize(vector *a); private: deviceType _device; // chip type (D, DLHC, DLM, or DLH) byte acc_address; byte mag_address; static const int dummy_reg_count = 6; regAddr translated_regs[dummy_reg_count + 1]; // index 0 not used unsigned int io_timeout; bool did_timeout; }; /* * ======== heading ======== * Returns the angular difference in the horizontal plane between the * "from" vector and north, in degrees. * * Description of heading algorithm: * Shift and scale the magnetic reading based on calibration data to find * the North vector. Use the acceleration readings to determine the Up * vector (gravity is measured as an upward acceleration). The cross * product of North and Up vectors is East. The vectors East and North * form a basis for the horizontal plane. The From vector is projected * into the horizontal plane and the angle between the projected vector * and horizontal north is returned. */ template float LSM303::heading(vector from) { vector temp_m = {m.x, m.y, m.z}; /* subtract offset (average of min and max) from magnetometer readings */ temp_m.x -= ((int32_t)m_min.x + m_max.x) / 2; temp_m.y -= ((int32_t)m_min.y + m_max.y) / 2; temp_m.z -= ((int32_t)m_min.z + m_max.z) / 2; /* compute E and N */ vector E; vector N; vector_cross(&temp_m, &a, &E); vector_normalize(&E); vector_cross(&a, &E, &N); vector_normalize(&N); /* compute heading */ float heading = atan2(vector_dot(&E, &from), vector_dot(&N, &from)) * 180 / M_PI; if (heading < 0) { heading += 360; } return heading; } /* * ======== vector_cross ======== * To = Ta x Tb */ template void LSM303::vector_cross( const vector *a, const vector *b, vector *out) { out->x = (a->y * b->z) - (a->z * b->y); out->y = (a->z * b->x) - (a->x * b->z); out->z = (a->x * b->y) - (a->y * b->x); } /* * ======== vector_dot ======== * Returns Ta * Tb */ template float LSM303::vector_dot(const vector *a, const vector *b) { return (a->x * b->x) + (a->y * b->y) + (a->z * b->z); } #endif